#include #include #include const int Resetz = 15; const int ADC_RDY = 4; #define HRM_ADD 0x58 #define adc_step_size 0.0000057220458984 #define MAX 500 #define TEN_MIN 1000000 #define counting 500 double adc_ ; double arr_0x2A[MAX], arr_0x2B[MAX], arr_0x2C[MAX], arr_0x2D[MAX], arr_0x2E[MAX], arr_0x2F[MAX], arr_R_40[MAX]; void setup() { Wire.begin(); Serial.begin(115200); pinMode(Resetz, OUTPUT); pinMode(ADC_RDY, INPUT); pinMode(Resetz, OUTPUT); pinMode(ADC_RDY, INPUT); HRM_power_on(); //Powering on the AFE and trigger also Reset_all_Reg__to_zero();// setting all reg to zero HRM_power_down(); //Powering down delay(1000); HRM_power_on(); //Powering on the AFE and trigger also AFE_Reg_Init(); //Enabling Register Write set_ALL_reg(); //Writting to all registers HRM_power_down(); //Powering down delay(1000); } void loop() { // put your main code here, to run repeatedly: HRM_power_on(); //Powering on the AFE and trigger also AFE_Reg_Init(); //Enabling Register Write set_ALL_reg(); //Writting to all registers delay(100); AFE_Enable_Read (); // Read Enable // Serial.println("ADC_RDY input>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>"); // int adc = digitalRead(ADC_RDY); // Serial.println(adc); // if (adc > 0) { // Serial.println("ADC_RDY input available"); // } // Serial.println("ADC_RDY input>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>"); int count = 0; while (count <= counting) { //Serial.print("0x2A :"); adc_ = AFE_Reg_Read(0x2A); adc_ *= adc_step_size; adc_ *= 0.1; //Serial.print(adc_, HEX); arr_0x2A[count] = adc_; //Stoaring values in array delay(10); //Serial.print("0x2B :"); adc_ = AFE_Reg_Read(0x2B); adc_ *= adc_step_size; adc_ *= 0.1; //Serial.print(adc_, HEX); arr_0x2B[count] = adc_; //Stoaring values in array delay(10); // Serial.print("0x2C :"); adc_ = AFE_Reg_Read(0x2C); adc_ *= adc_step_size; adc_ *= 0.1; // Serial.print(adc_, HEX); arr_0x2C[count] = adc_; //Stoaring values in array delay(10); // Serial.print("0x2D :"); adc_ = AFE_Reg_Read(0x2D); adc_ *= adc_step_size; adc_ *= 0.1; // Serial.print(adc_, HEX); arr_0x2D[count] = adc_; //Stoaring values in array delay(10); // Serial.print("0x2E :"); adc_ = AFE_Reg_Read(0x2E); adc_ *= adc_step_size; adc_ *= 0.1; // Serial.print(adc_, HEX); arr_0x2E[count] = adc_; //Stoaring values in array delay(10); // Serial.print("0x2F :"); adc_ = AFE_Reg_Read(0x2F); adc_ *= adc_step_size; adc_ *= 0.1; // Serial.print(adc_, HEX); arr_0x2F[count] = adc_; //Stoaring values in array delay(10); // Serial.print("0x40 :"); adc_ = AFE_Reg_Read(0x40); adc_ *= adc_step_size; adc_ *= 0.1; // Serial.print(adc_, HEX); arr_R_40[count] = adc_; //Stoaring values in array Serial.println("\n"); count++; delay(10); } //AFE_Reg_Read(47); // AFE_Disable_Read (); HRM_power_down(); //Powering down Serial.println("#############\n"); for (int k = 0; k <= counting; k++) { Serial.print("arr_0x2A ::"); Serial.println(arr_0x2A[k], DEC); Serial.print("arr_0x2B ::"); Serial.println(arr_0x2B[k], DEC); Serial.print("arr_0x2C ::"); Serial.println(arr_0x2C[k], DEC); Serial.print("arr_0x2D ::"); Serial.println(arr_0x2D[k], DEC); Serial.print("arr_0x2E ::"); Serial.println(arr_0x2E[k], DEC); Serial.print("arr_0x2F ::"); Serial.println(arr_0x2F[k], DEC); Serial.print("arr_R_40 ::"); Serial.println(arr_R_40[k], DEC); //delay(10); } Serial.println(" "); delay(TEN_MIN); } /**************************************** HRM powering on *****************************************/ void HRM_power_on() { Serial.println("HRM_power_on"); delay(1000); digitalWrite(Resetz, HIGH);//AFE init delay(10); digitalWrite(Resetz, LOW); delayMicroseconds(35);//25us to 50 us. digitalWrite(Resetz, HIGH);// Reset internal registers by setting RESETZ = LOW for 25 - 50 us delay(10); } /**************************************************************** Power Down by setting the RESETZ pin to LOW for more than 200 us ****************************************************************/ void HRM_power_down() { Serial.println("\nHRM_power_down"); delay(100); digitalWrite(Resetz, LOW); delayMicroseconds(200); } /******************************************** Reegister Write mode *********************************************/ void AFE_Reg_Init() { Serial.println("Setting up INIT registers"); delay(1000); Wire.beginTransmission(HRM_ADD); AFE_Reg_Write(0x00, 0x000000); } /**********************************************************************************************************/ /* AFE4404_Enable_Read */ /**********************************************************************************************************/ void AFE_Enable_Read () //Prohibit writing to registers { //Serial.println("AFE_Reg_read"); //delay(10); byte configData[3]; configData[0] = 0x00; configData[1] = 0x00; configData[2] = 0x01; i2c_write(0x00, configData); } /**********************************************************************************************************/ /* AFE4404_Disable_Read */ /**********************************************************************************************************/ void AFE_Disable_Read () //Permitt writing to registers { // Serial.println("AFE_Reg_disable read"); delay(10); byte configData[3]; configData[0] = 0x00; configData[1] = 0x00; configData[2] = 0x00; i2c_write ( 0x00, configData); } /******************************************** Reegister Writting *********************************************/ void AFE_Reg_Write(int reg_address, unsigned long data1) { byte configData[3]; configData[0] = (byte)(data1 >> 16); configData[1] = (byte)(((data1 & 0x00FFFF) >> 8)); configData[2] = (byte)(((data1 & 0x0000FF))); i2c_write(reg_address, configData); } char i2c_write(int reg_address, byte configData[]) { /*24 bit data writtern on register in MSB first pattern */ int trans_end = 0; Wire.beginTransmission(HRM_ADD); // Serial.println(reg_address); Wire.write(reg_address); // Serial.print(configData[0]); Wire.write(configData[0]); //MSB // Serial.print(configData[1]); Wire.write(configData[1]); // Serial.print(configData[2]); Wire.write(configData[2]);//LSB Wire.endTransmission(); delay(10); // Serial.println(" "); return (trans_end); } /*********************************************************************************************************/ /* AFE4404_Reg_Read */ /*********************************************************************************************************/ signed long AFE_Reg_Read(int reg_address) { byte configData[3]; signed long retVal; i2c_read (reg_address, configData); retVal = configData[0]; retVal = (retVal << 8) | configData[1]; retVal = (retVal << 8) | configData[2]; //Serial.println("#########HEX_value##########"); Serial.print(reg_address); Serial.print("::"); Serial.println(retVal); //Serial.println("#########HEX_value##########"); //delay(20); if (reg_address >= 0x2A && reg_address <= 0x40) { if (retVal & 0x00200000) // check if the ADC value is positive or negative { retVal &= 0x003FFFFF; // convert it to a 22 bit value Serial.print(reg_address); Serial.print("::22 bit Conversion cos -ve:: "); Serial.println(retVal); return (retVal ^ 0xFFC00000); } } // Serial.println("#########retVal ^ 0xFFC00000##########"); // Serial.print(reg_address); Serial.print("::"); Serial.println(retVal); // Serial.println("#########Conversion_value##########"); //delay(10); return retVal; } char i2c_read(int reg_address, byte *read_Data) { int trans_end = 0; int byteCount = 3; Wire.beginTransmission(HRM_ADD); Wire.write(reg_address); Wire.endTransmission(); Wire.requestFrom(HRM_ADD, 3); // delay(10); while (Wire.available() && (byteCount != 0)) { *read_Data++ = Wire.read(); byteCount--; } return (trans_end); } /********************************************************* Setting up All write registers **********************************************************/ void set_ALL_reg() { //Waveform AFE_Reg_Write (01, 0x000064);//1h AFE_Reg_Write (02, 0x00018E);//2h AFE_Reg_Write (03, 0x000320);//3h AFE_Reg_Write (04, 0x0004AE);//4h AFE_Reg_Write (05, 0x0001F4);//5h AFE_Reg_Write (06, 0x00031E);//6h AFE_Reg_Write (07, 0x000384);//7h AFE_Reg_Write (0x08, 0x0004AE);//8h AFE_Reg_Write (0x09, 0x000000);//9h AFE_Reg_Write (10, 0x00018E);//Ah AFE_Reg_Write (11, 0x000514);//Bh AFE_Reg_Write (12, 0x00063E);//Ch AFE_Reg_Write (13, 0x0015E8);//Dh AFE_Reg_Write (14, 0x0017B3);//Eh AFE_Reg_Write (15, 0x0017BD);//Fh AFE_Reg_Write (16, 0x001988);//10h AFE_Reg_Write (17, 0x001992);//11h AFE_Reg_Write (18, 0x001B5E);//12h AFE_Reg_Write (19, 0x001B68);//13h AFE_Reg_Write (20, 0x001D33);//14h AFE_Reg_Write (21, 0x0015E0);//15h AFE_Reg_Write (22, 0x0015E6);//16h AFE_Reg_Write (23, 0x0017B5);//17h AFE_Reg_Write (24, 0x0017BB);//18h AFE_Reg_Write (25, 0x00198A);//19h AFE_Reg_Write (26, 0x001990);//1Ah AFE_Reg_Write (27, 0x001B60);//1Bh AFE_Reg_Write (28, 0x001B66);//1Ch AFE_Reg_Write (29, 0x009C3F);//1Dh //################################## configuiration reg AFE_Reg_Write (30, 0x000103);//1E //0000//160 milisec//103 10101/02 AFE_Reg_Write (32, 0x008000);//20h//8006 AFE_Reg_Write (33, 0x000000);//21h AFE_Reg_Write (34, 0x005142);//22h Led A28A//4104 //104//5140 AFE_Reg_Write (35, 0x000200);//23h AFE_Reg_Write (41, 0x000200);//29h //################################## AFE_Reg_Write (49, 0x000000);//31h AFE_Reg_Write (50, 0x001DFB);//32h AFE_Reg_Write (51, 0x00991F);//33h AFE_Reg_Write (52, 0x000000);//34h AFE_Reg_Write (53, 0x000000);//35h AFE_Reg_Write (54, 0x000000);//36h// Two LED mode 36 AFE_Reg_Write (55, 0x000000);//37h AFE_Reg_Write (57, 0x000000);//39h AFE_Reg_Write (58, 0x000000);//3Ah //24 decimation mode on AFE_Reg_Write (61, 0x000024);//3Dh } void Reset_all_Reg__to_zero() { int k; Serial.println("Restting All registers"); for (k = 0; k <= 61; k++) AFE_Reg_Write (k, 0x000000); delay(1000); }