#!/bin/sh # timer_run.sh # # This script configures Timer4 to be run # on the VP1 Board. After configured, # the timer runs indefinitely at a fixed # freq and duty cycle, fed from the # internal CLK_M_OSC clock # echo "Configuring Timer 4...\n" # Enable Timer4's clock in CM_PER # This allows us to access it's control regs devmem2 0x44e00088 w 0x2 # Set the Pinmux for Timer4 (0x2 because its mode 2 of this pin) # Using the pin mux linux driver from the SDK #echo 0x22 > /sys/kernel/debug/omap_mux/xdma_event_intr0 # Timer configurations.. Stop Timer. # Auto-Reload # Compare Mode Enabled # Trigger set on overflow # Toggle Mode devmem2 0x48044038 w 0x1842 # Write to the CM_DPLL registers to select the clk source # Selected the clk source for the Timer4 # This should be &= (default 0x12) (writing a 0x2 for 32kHz) #0x1 = SEL2 : Select CLK_M_OSC clock devmem2 0x44e00510 w 0x1 # Initial count value devmem2 0x4804403C w 0xFFFFAFFF # Set the re-load value devmem2 0x48044040 w 0xFFFFDFFF # Setting a duty cycle devmem2 0x4804404C w 0xFFFFAFFF # Force the Timer to Smart-Idle devmem2 0x48044010 w 0x8 # Start Timer devmem2 0x48044038 w 0x1843 # Verify that the timer is running, # by polling the count register a # few times. We should we up counting. for i in {1..10} do echo "Timer Value $i" devmem2 0x4804403C done # End echo "Timer is Running!" echo "" echo "See TP31 on the EVM" echo "" # Delay added to allow time for the first timer # overflow to occur, before any consecutive memory # accesses are made. (Just for standby testing). sleep 1 # Disable MODULEMODE of CM_PER_TIMER4_CLKCTRL register # Only if this value is 0, are we able to wake-up from standby?? devmem2 0x44e00088 w 0x0 #END