U-Boot 2017.01 ALC (Aug 12 2021 - 17:23:13 -0400) CPU : AM335X-GP rev 2.1 Model: TI AM335x ALC DRAM: 256 MiB MMC: OMAP SD/MMC: 0 MMC Device 1 not found *** Warning - No MMC card found, using default environment Device tree fdtfile: am335x-alc_ngzn.dtb not set. Validating first E-fuse MAC Press and hold recovery switch to enter Recovery Mode Recovery Switch Set to OFF Net: Enable RMII mode on Ethernet PHY cpsw, usb_ether Hit any key to stop autoboot: 0 cpsw Waiting for PHY auto negotiation to complete.. done link up on port 0, speed 100, full duplex BOOTP broadcast 1 DHCP client bound to address 169.254.1.6 (61 ms) link up on port 0, speed 100, full duplex Using cpsw device TFTP from server 169.254.1.3; our IP address is 169.254.1.6 Filename 'debrick.scr'. Load address: 0x80000000 Loading: # 1.1 MiB/s done Bytes transferred = 2224 (8b0 hex) ## Executing script at 80000000 ===== U-Boot Settings ===== ===== Linux Kernel ===== bootfile=zImage-main.bin ===== Device Tree ===== Enter the target fdtfile (am335x-alc_router.dtb or press enter): fdtfile=am335x-alc_ngzn.dtb edit: fdtfile=am335x-alc_ngzn.dtb ===== NFSroot Path ===== rootpath=/home/user/ng5_mfg/Release-2-0/b5/main/nfsroot ===== NFSvar Path ===== Enter the target NFSvar path: varpath=/home/user/ng5_mfg/Release-2-0/b5/main/nfsvar edit: varpath=/home/user/ng5_mfg/Release-2-0/b5/main/nfsvar ===== Save new definitions ===== ipaddr=169.254.1.6 serverip=169.254.1.3 ===== Setting SLC ===== MMC Device 1 not found no mmc device at slot 1 mmc_reinit: Startup init mmc_reinit: Complete init eMMC Capacity: 3.6 GiB ===== Done ===== net_args=setenv bootargs VARPATH=${varpath} console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=:::::eth0:dhcp loginShell=allow Booting from network ... link up on port 0, speed 100, full duplex Using cpsw device TFTP from server 169.254.1.3; our IP address is 169.254.1.6 Filename 'zImage-main.bin'. Load address: 0x80200000 Loading: ################################################################# ################################################################# ################################################################# ################################################################# ################################################################# ############################################### 3.7 MiB/s done Bytes transferred = 5455776 (533fa0 hex) link up on port 0, speed 100, full duplex Using cpsw device TFTP from server 169.254.1.3; our IP address is 169.254.1.6 Filename 'am335x-alc_ngzn.dtb'. Load address: 0x88000000 Loading: ####### 3.5 MiB/s done Bytes transferred = 96588 (1794c hex) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8df1b000, end 8df3594b ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.10.131-alc-g999 (oe-user@oe-host) (arm-poky-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 PREEMPT Wed Sep 7 07:01:55 UTC 2022 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x ALC [ 0.000000] Memory policy: Data cache writeback [ 0.000000] cma: Reserved 24 MiB at 0x8e000000 [ 0.000000] Zone ranges: [ 0.000000] Normal [mem 0x0000000080000000-0x000000008fdfffff] [ 0.000000] HighMem empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000008fdfffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000008fdfffff] [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (neon) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64516 [ 0.000000] Kernel command line: VARPATH=/home/user/ng5_mfg/Release-2-0/b5/main/nfsvar console=ttyO0,115200n8 root=/dev/nfs nfsroot=169.254.1.3:/home/user/ng5_mfg/Release-2-0/b5/main/nfsroot,nolock,udp,rsize=8192,wsize=8192,timeo=1,retrans=1 rw ip=:::::eth0:dhcp loginShell=allow [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes, linear) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 219816K/260096K available (8192K kernel code, 516K rwdata, 2520K rodata, 1024K init, 254K bss, 15704K reserved, 24576K cma-reserved, 0K highmem) [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] TI gptimer clocksource: always-on /ocp/interconnect@44c00000/segment@200000/target-module@31000 [ 0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000044] clocksource: dmtimer: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000549] TI gptimer clockevent: 24000000 Hz at /ocp/interconnect@48000000/segment@0/target-module@40000 [ 0.002846] Console: colour dummy device 80x30 [ 0.002939] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032) [ 0.060588] pid_max: default: 32768 minimum: 301 [ 0.060777] LSM: Security Framework initializing [ 0.060894] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.060921] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.061983] CPU: Testing write buffer coherency: ok [ 0.062083] CPU0: Spectre v2: using BPIALL workaround [ 0.063437] Setting up static identity map for 0x80100000 - 0x80100078 [ 0.063676] rcu: Hierarchical SRCU implementation. [ 0.064438] devtmpfs: initialized [ 0.082704] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.083410] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.083450] futex hash table entries: 256 (order: -1, 3072 bytes, linear) [ 0.085331] pinctrl core: initialized pinctrl subsystem [ 0.087455] NET: Registered protocol family 16 [ 0.093842] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.115687] l3-aon-clkctrl:0000:0: failed to disable [ 0.119081] thermal_sys: Registered thermal governor 'fair_share' [ 0.119100] thermal_sys: Registered thermal governor 'step_wise' [ 0.119121] thermal_sys: Registered thermal governor 'user_space' [ 2.139363] No ATAGs? [ 2.139409] hw-breakpoint: debug architecture 0x4 unsupported. [ 2.231574] Kprobes globally optimized [ 2.262630] SCSI subsystem initialized [ 2.265332] usbcore: registered new interface driver usbfs [ 2.265550] usbcore: registered new interface driver hub [ 2.265751] usbcore: registered new device driver usb [ 2.267477] pps_core: LinuxPPS API ver. 1 registered [ 2.267503] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 2.268033] PTP clock support registered [ 2.279075] clocksource: Switched to clocksource dmtimer [ 2.279392] VFS: Disk quotas dquot_6.6.0 [ 2.279513] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 2.323958] NET: Registered protocol family 2 [ 2.324297] IP idents hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 2.325634] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear) [ 2.325702] TCP established hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 2.325746] TCP bind hash table entries: 2048 (order: 1, 8192 bytes, linear) [ 2.325787] TCP: Hash tables configured (established 2048 bind 2048) [ 2.325932] UDP hash table entries: 256 (order: 0, 4096 bytes, linear) [ 2.325966] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear) [ 2.326188] NET: Registered protocol family 1 [ 2.326992] RPC: Registered named UNIX socket transport module. [ 2.327018] RPC: Registered udp transport module. [ 2.327031] RPC: Registered tcp transport module. [ 2.327043] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 2.330616] NetWinder Floating Point Emulator V0.97 (double precision) [ 2.331566] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 2.335504] Initialise system trusted keyrings [ 2.338555] workingset: timestamp_bits=30 max_order=16 bucket_order=0 [ 2.340632] NFS: Registering the id_resolver key type [ 2.340721] Key type id_resolver registered [ 2.340736] Key type id_legacy registered [ 2.492729] NET: Registered protocol family 38 [ 2.492771] Key type asymmetric registered [ 2.492787] Asymmetric key parser 'x509' registered [ 2.492827] io scheduler mq-deadline registered [ 2.492844] io scheduler kyber registered [ 2.741684] ti-sysc 44e07000.target-module: dts flag should be at module level for ti,no-reset-on-init [ 3.011048] ti-sysc: probe of 44e31000.target-module failed with error -16 [ 3.130153] ti-sysc: probe of 48040000.target-module failed with error -16 [ 3.292186] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 3.627009] debugfs: Directory '49000000.dma' with parent 'dmaengine' already present! [ 3.627067] edma 49000000.dma: TI EDMA DMA engine driver [ 3.708442] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 3.756275] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 3.761431] omap_uart 44e09000.serial: no wakeirq for uart0 [ 3.765033] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 20, base_baud = 3000000) is a OMAP UART0 [ 4.418149] printk: console [ttyO0] enabled [ 4.427769] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 4.434551] random: crng init done [ 4.467293] brd: module loaded [ 4.490187] loop: module loaded [ 4.537804] vcan: Virtual CAN interface driver [ 4.545474] slcan: serial line CAN interface driver [ 4.551037] slcan: 10 dynamic interface channels. [ 4.555963] CAN device driver interface [ 4.573414] mdio_bus 4a101000.mdio: mii_bus 4a101000.mdio couldn't get reset GPIO [ 4.583987] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 4.591662] cpsw 4a100000.ethernet: ALE Table size 1024 [ 4.597257] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 4.605036] cpsw 4a100000.ethernet: Detected MACID = 38:0b:3c:95:ed:04 [ 4.615584] usbcore: registered new interface driver asix [ 4.624677] usbcore: registered new interface driver ax88179_178a [ 4.631723] usbcore: registered new interface driver cdc_ether [ 4.638442] usbcore: registered new interface driver smsc95xx [ 4.644810] usbcore: registered new interface driver net1080 [ 4.651487] usbcore: registered new interface driver rndis_host [ 4.658275] usbcore: registered new interface driver cdc_subset [ 4.664755] usbcore: registered new interface driver zaurus [ 4.671161] usbcore: registered new interface driver cdc_ncm [ 4.680570] am335x-phy-driver 47401300.usb-phy: supply vcc not found, using dummy regulator [ 4.690617] am335x-phy-driver 47401300.usb-phy: dummy supplies not allowed for exclusive requests [ 4.710980] am335x-phy-driver 47401b00.usb-phy: supply vcc not found, using dummy regulator [ 4.721275] am335x-phy-driver 47401b00.usb-phy: dummy supplies not allowed for exclusive requests [ 4.740792] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver [ 4.747626] ehci-omap: OMAP-EHCI Host Controller driver [ 4.755556] usbcore: registered new interface driver cdc_wdm [ 4.762436] usbcore: registered new interface driver usb-storage [ 4.769916] usbcore: registered new interface driver usbserial_generic [ 4.777318] usbserial: USB Serial support registered for generic [ 4.783985] usbcore: registered new interface driver ftdi_sio [ 4.790642] usbserial: USB Serial support registered for FTDI USB Serial Device [ 4.806190] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 4.812773] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1 [ 4.821232] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 [ 4.830073] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.837617] usb usb1: Product: MUSB HDRC host driver [ 4.842875] usb usb1: Manufacturer: Linux 5.10.131-alc-g999 musb-hcd [ 4.849571] usb usb1: SerialNumber: musb-hdrc.0 [ 4.855470] hub 1-0:1.0: USB hub found [ 4.860157] hub 1-0:1.0: 1 port detected [ 4.878903] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 4.885761] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2 [ 4.894349] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 [ 4.903186] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 4.910794] usb usb2: Product: MUSB HDRC host driver [ 4.915979] usb usb2: Manufacturer: Linux 5.10.131-alc-g999 musb-hcd [ 4.922658] usb usb2: SerialNumber: musb-hdrc.1 [ 4.928546] hub 2-0:1.0: USB hub found [ 4.933226] hub 2-0:1.0: 1 port detected [ 4.952740] i2c /dev entries driver [ 4.962689] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 4.977625] ledtrig-cpu: registered to indicate activity on CPUs [ 4.988287] usbcore: registered new interface driver usbhid [ 4.996477] usbhid: USB HID core driver [ 5.002580] Initializing XFRM netlink socket [ 5.007210] NET: Registered protocol family 10 [ 5.014218] Segment Routing with IPv6 [ 5.018216] NET: Registered protocol family 17 [ 5.023071] NET: Registered protocol family 15 [ 5.027713] can: controller area network core [ 5.032445] NET: Registered protocol family 29 [ 5.037091] can: raw protocol [ 5.040308] can: broadcast manager protocol [ 5.044692] can: netlink gateway - max_hops=1 [ 5.049549] Key type dns_resolver registered [ 5.055153] oprofile: using arm/armv7 [ 5.060213] ThumbEE CPU extension supported. [ 5.064695] omap_voltage_late_init: Voltage driver support not added [ 5.072143] registered taskstats version 1 [ 5.076436] Loading compiled-in X.509 certificates [ 5.099289] OMAP GPIO hardware version 0.1 [ 5.143121] vrtc: supplied by vcc_5v0_pmic [ 5.151584] vio: supplied by vcc_5v0_pmic [ 5.158192] vdd_mpu: supplied by vcc_5v0_pmic [ 5.165136] vdd_core: supplied by vcc_5v0_pmic [ 5.173599] vdig1: supplied by vcc_5v0_pmic [ 5.179844] vdig2: supplied by vcc_5v0_pmic [ 5.186024] vpll: supplied by vcc_5v0_pmic [ 5.192165] vdac: supplied by vcc_5v0_pmic [ 5.198197] vaux1: supplied by vcc_5v0_pmic [ 5.204546] vaux2: supplied by vcc_5v0_pmic [ 5.210836] vaux33: supplied by vcc_5v0_pmic [ 5.217242] vmmc: supplied by vcc_5v0_pmic [ 5.223844] vbb: supplied by vcc_5v0_pmic [ 5.234830] rtc-pcf8523 0-0068: registered as rtc0 [ 5.240945] rtc-pcf8523 0-0068: setting system clock to 2022-09-08T12:38:17 UTC (1662640697) [ 5.251087] at24 0-0051: supply vcc not found, using dummy regulator [ 5.260103] at24 0-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 5.269524] pca953x 0-0022: supply vcc not found, using dummy regulator [ 5.277832] pca953x 0-0022: using AI [ 5.284048] at24 0-0050: supply vcc not found, using dummy regulator [ 5.292995] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 5.301223] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 5.311489] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz [ 5.334351] omap_reset_deassert: timedout waiting for gfx:0 [ 5.340445] ti-sysc: probe of 5600fe00.target-module failed with error -110 [ 5.409123] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 5.420968] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver TI DP83825S [ 5.430410] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver TI DP83825S [ 5.452013] cpsw 4a100000.ethernet: initializing cpsw version 1.12 (0) [ 5.470175] TI DP83825S 4a101000.mdio:00: attached PHY driver [TI DP83825S] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL) [ 5.484249] net eth0: could not add device link to 4a101000.mdio:01 err -17 [ 5.499663] TI DP83825S 4a101000.mdio:01: attached PHY driver [TI DP83825S] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL) [ 7.610304] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off [ 7.619140] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ 7.649285] Sending DHCP requests ., OK [ 7.693178] IP-Config: Got DHCP answer from 169.254.1.3, my address is 169.254.1.6 [ 7.701120] IP-Config: Complete: [ 7.704497] device=eth0, hwaddr=38:0b:3c:95:ed:04, ipaddr=169.254.1.6, mask=255.255.255.0, gw=169.254.1.2 [ 7.714954] host=169.254.1.6, domain=, nis-domain=(none) [ 7.720971] bootserver=169.254.1.3, rootserver=169.254.1.3, rootpath= [ 7.720980] nameserver0=169.254.1.3 [ 7.732885] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 7.746680] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ 7.753940] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2 [ 7.764414] cfg80211: failed to load regulatory.db [ 103.529246] VFS: Unable to mount root fs via NFS. [ 103.534286] devtmpfs: mounted [ 103.539434] Freeing unused kernel memory: 1024K [ 103.544852] Run /sbin/init as init process [ 103.549509] Run /etc/init as init process [ 103.553886] Run /bin/init as init process [ 103.558235] Run /bin/sh as init process [ 103.562526] Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance. [ 103.577329] ---[ end Kernel panic - not syncing: No working init found. Try passing init= option to kernel. See Linux Documentation/admin-guide/init.rst for guidance. ]---