[ 6.019188] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit [ 6.019213] tps6594: probe of 0-0048 failed with error -121 [ 6.032390] tps6594 0-004c: error -EREMOTEIO: Failed to set PMIC state [ 6.038934] tps6594: probe of 0-004c failed with error -121 [ 6.046141] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, g) [ 6.056370] ti-udma 31150000.dma-controller: Channels: 50 (tchan: 25, rchan: 25, g) [ 6.068110] spi-nor spi0.0: unrecognized JEDEC id bytes: 80 00 00 00 00 00 [ 6.075434] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode [ 6.106351] mmc0: Command Queue Engine enabled [ 6.110816] mmc0: new HS400 MMC card at address 0001 [ 6.116126] mmcblk0: mmc0:0001 G1M15L 29.6 GiB [ 6.120619] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 6.121565] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB [ 6.128666] mdio_bus 46000f00.mdio: MDIO device at address 0 is missing. [ 6.133827] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB [ 6.139886] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0 [ 6.145343] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (239:0) [ 6.157600] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 6.170991] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 6.177182] pps pps0: new PPS source ptp1 [ 6.181347] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000,1 [ 6.198330] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 6.209445] debugfs: Directory 'pd:49' with parent 'pm_genpd' already present! [ 6.217922] debugfs: Directory 'pd:35' with parent 'pm_genpd' already present! [ 6.225606] clk: Disabling unused clocks [ 6.241792] ALSA device list: [ 6.244764] No soundcards found. [ 6.248309] ========================wsc before: [ 6.252857] ========================wsc after:/dev/mmcblk1p2 [ 6.258865] /dev/root: Can't open blockdev [ 6.262977] VFS: Cannot open root device "/dev/mmcblk1p2" or unknown-block(0,0): e6 [ 6.271145] Please append a correct "root=" boot option; here are the available pa: [ 6.279492] b300 31080448 mmcblk0 [ 6.279496] driver: mmcblk [ 6.286284] b320 32256 mmcblk0boot0 [ 6.286287] (driver?) [ 6.293072] b340 32256 mmcblk0boot1 [ 6.293075] (driver?) [ 6.299856] List of all bdev filesystems: [ 6.303856] ext3 [ 6.303858] ext4 [ 6.305777] ext2 [ 6.307692] squashfs [ 6.309611] vfat [ 6.311873] [ 6.315273] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-bl) [ 6.323521] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 6.6.32-g6de6e418c80e-dirty #2 [ 6.331162] Hardware name: Texas Instruments J7200 EVM (DT) [ 6.336719] Call trace: [ 6.339156] dump_backtrace+0x90/0xe8 [ 6.342819] show_stack+0x18/0x24 [ 6.346124] dump_stack_lvl+0x48/0x60 [ 6.349776] dump_stack+0x18/0x24 [ 6.353079] panic+0x324/0x380 [ 6.356126] mount_root_generic+0x268/0x338 [ 6.360300] mount_root+0x170/0x334 [ 6.363777] prepare_namespace+0xa8/0x2c4 [ 6.367776] kernel_init_freeable+0x248/0x288 [ 6.372121] kernel_init+0x24/0x1dc [ 6.375602] ret_from_fork+0x10/0x20 [ 6.379166] SMP: stopping secondary CPUs [ 6.383078] Kernel Offset: 0x80000 from 0xffff800080000000 [ 6.388549] PHYS_OFFSET: 0x80000000 [ 6.392026] CPU features: 0x0,80000200,28020000,1000420b [ 6.397325] Memory Limit: none [ 6.400370] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on u-