U-Boot SPL 2011.09 (Apr 08 2012 - 18:29:14) Texas Instruments Revision detection unimplemented OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2011.09 (Apr 08 2012 - 18:25:03) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled Found a daughter card connected NAND: HW ECC Hamming Code selected 256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - bad CRC, using default environment Net: cpsw Hit any key to stop autoboot: 0 SD/MMC found on device 0 reading uEnv.txt ** Unable to read "uEnv.txt" from mmc 0:1 ** reading uImage 3061672 bytes read ## Booting kernel from Legacy Image at 80007fc0 ... Image Name: Arago/3.2/am335x-evm Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3061608 Bytes = 2.9 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK XIP Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (jenkins@sdit-build01) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Mon Apr 9 10:19:16 CDT 2012 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 253468k/253468k available, 8676k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc0575000 (5556 kB) [ 0.000000] .init : 0xc0575000 - 0xc05b2000 ( 244 kB) [ 0.000000] .data : 0xc05b2000 - 0xc060fb18 ( 375 kB) [ 0.000000] .bss : 0xc060fb3c - 0xc063c7e4 ( 180 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.058929] pid_max: default: 32768 minimum: 301 [ 0.059051] Security Framework initialized [ 0.059173] Mount-cache hash table entries: 512 [ 0.059539] CPU: Testing write buffer coherency: ok [ 0.079528] omap_hwmod: gfx: failed to hardreset [ 0.095794] omap_hwmod: pruss: failed to hardreset [ 0.096923] print_constraints: dummy: [ 0.097290] NET: Registered protocol family 16 [ 0.099426] OMAP GPIO hardware version 0.1 [ 0.102020] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.104248] omap_i2c.1: alias fck already exists [ 0.105163] omap2_mcspi.1: alias fck already exists [ 0.105377] omap2_mcspi.2: alias fck already exists [ 0.105621] edma.0: alias fck already exists [ 0.105651] edma.0: alias fck already exists [ 0.105682] edma.0: alias fck already exists [ 0.130340] bio: create slab at 0 [ 0.132507] SCSI subsystem initialized [ 0.134124] usbcore: registered new interface driver usbfs [ 0.134460] usbcore: registered new interface driver hub [ 0.134643] usbcore: registered new device driver usb [ 0.134796] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.135101] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.148986] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.150848] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.153228] print_constraints: VRTC: [ 0.154693] print_constraints: VIO: at 1800 mV [ 0.157012] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.159332] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.160308] print_constraints: VDD3: 5000 mV [ 0.161712] print_constraints: VDIG1: at 1800 mV [ 0.163146] print_constraints: VDIG2: at 1800 mV [ 0.164550] print_constraints: VPLL: at 1800 mV [ 0.165985] print_constraints: VDAC: at 1800 mV [ 0.167388] print_constraints: VAUX1: at 1800 mV [ 0.168853] print_constraints: VAUX2: at 3300 mV [ 0.170288] print_constraints: VAUX33: at 3300 mV [ 0.171722] print_constraints: VMMC: at 3300 mV [ 0.172210] tps65910 1-002d: No interrupt support, no core IRQ [ 0.173126] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.174285] Switching to clocksource gp timer [ 0.189849] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.190032] musb-hdrc musb-hdrc.0: dma type: pio [ 0.190887] musb-hdrc musb-hdrc.0: USB OTG mode controller at d081c000 using PIO, IRQ 18 [ 0.191070] musb-hdrc musb-hdrc.1: dma type: pio [ 0.191467] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.191528] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.191680] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.191680] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.191680] usb usb1: Product: MUSB HDRC host driver [ 0.191711] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.191711] usb usb1: SerialNumber: musb-hdrc.1 [ 0.192504] hub 1-0:1.0: USB hub found [ 0.192535] hub 1-0:1.0: 1 port detected [ 0.193084] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using PIO, IRQ 19 [ 0.193481] NET: Registered protocol family 2 [ 0.193695] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.194000] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.194152] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.194244] TCP: Hash tables configured (established 8192 bind 8192) [ 0.194274] TCP reno registered [ 0.194366] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.194396] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.194580] NET: Registered protocol family 1 [ 0.194854] RPC: Registered named UNIX socket transport module. [ 0.194854] RPC: Registered udp transport module. [ 0.194885] RPC: Registered tcp transport module. [ 0.194885] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.195129] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.207275] VFS: Disk quotas dquot_6.5.2 [ 0.207336] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.207885] msgmni has been set to 495 [ 0.208648] io scheduler noop registered [ 0.208679] io scheduler deadline registered [ 0.208740] io scheduler cfq registered (default) [ 0.212524] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.817657] console [ttyO0] enabled [ 0.821929] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.829772] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.837585] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.845367] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.853118] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.870269] brd: module loaded [ 0.878356] loop: module loaded [ 0.881835] i2c-core: driver [tsl2550] using legacy suspend method [ 0.888305] i2c-core: driver [tsl2550] using legacy resume method [ 0.894744] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.908660] Detected a daughter card on AM335x EVM.. [ 0.913635] Unknown CPLD version found, falling back to 1.0A [ 0.919769] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.934967] Board name: A33515BB [ 0.938323] Board version: 1.4A [ 0.941589] SKU: SKU#01 [ 0.944671] The board is general purpose EVM in profile 0 [ 0.950317] Found invalid GP EVM revision, falling back to Rev1.1A [ 0.957061] da8xx_lcdc.0: alias fck already exists [ 0.962890] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel [ 0.986572] Console: switching to colour frame buffer device 100x30 [ 1.001983] TSC connected to beta GP EVM [ 1.007507] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 1.012512] Registering NAND on CS0 [ 1.016937] omap_i2c.2: alias fck already exists [ 1.034881] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 1.041534] tsl2550 2-0039: standard operating mode [ 1.047363] tsl2550 2-0039: support ver. 1.2 enabled [ 1.053009] davinci-mcasp.1: alias fck already exists [ 1.058898] omap_hsmmc.0: alias fck already exists [ 1.064300] omap_hsmmc.2: alias fck already exists [ 1.069580] usb 1-1: new low-speed USB device number 2 using musb-hdrc [ 1.076629] Configure Bluetooth Enable pin... [ 1.082519] _regulator_get: 2-0018 supply Vdd not found, using dummy regulator [ 1.090179] _regulator_get: 2-0018 supply Vdd_IO not found, using dummy regulator [ 1.118591] lis3lv02d: 8 bits 3DLH sensor found [ 1.205291] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0 [ 1.216461] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.223815] omap2-nand driver initializing [ 1.228485] ONFI flash detected [ 1.231903] ONFI param page 0 valid [ 1.235565] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP) [ 1.244018] usb 1-1: New USB device found, idVendor=04b3, idProduct=310b [ 1.251037] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0 [ 1.259124] Creating 8 MTD partitions on "omap2-nand.0": [ 1.264678] 0x000000000000-0x000000020000 : "SPL" [ 1.272155] 0x000000020000-0x000000040000 : "SPL.backup1" [ 1.279113] 0x000000040000-0x000000060000 : "SPL.backup2" [ 1.286010] 0x000000060000-0x000000080000 : "SPL.backup3" [ 1.292907] 0x000000080000-0x000000260000 : "U-Boot" [ 1.300140] 0x000000260000-0x000000280000 : "U-Boot Env" [ 1.306976] 0x000000280000-0x000000780000 : "Kernel" [ 1.315582] 0x000000780000-0x000010000000 : "File System" [ 1.425781] OneNAND driver initializing [ 1.431213] CAN device driver interface [ 1.435241] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.484924] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.491363] davinci_mdio davinci_mdio.0: detected phy mask fffffffe [ 1.498596] davinci_mdio.0: probed [ 1.502136] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.509857] usbcore: registered new interface driver zd1201 [ 1.515869] usbcore: registered new interface driver cdc_ether [ 1.522125] usbcore: registered new interface driver cdc_eem [ 1.528198] usbcore: registered new interface driver dm9601 [ 1.534057] cdc_ncm: 04-Aug-2011 [ 1.537597] usbcore: registered new interface driver cdc_ncm [ 1.543487] Initializing USB Mass Storage driver... [ 1.548858] usbcore: registered new interface driver usb-storage [ 1.555114] USB Mass Storage support registered. [ 1.560394] mousedev: PS/2 mouse device common for all mice [ 1.567169] input: matrix-keypad as /devices/platform/matrix-keypad/input/input1 [ 1.576354] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input2 [ 1.584808] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.591705] i2c /dev entries driver [ 1.596008] Linux video capture interface: v2.00 [ 1.601165] usbcore: registered new interface driver uvcvideo [ 1.607208] USB Video Class driver (1.1.1) [ 1.612365] lm75 2-0048: hwmon0: sensor 'tmp275' [ 1.620056] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.628631] cpuidle: using governor ladder [ 1.633422] cpuidle: using governor menu [ 1.646850] input: HID 04b3:310b as /devices/platform/omap/musb-ti81xx/musb-hdrc.1/usb1/1-1/1-1:1.0/input/input3 [ 1.658325] generic-usb 0003:04B3:310B.0001: input: USB HID v1.00 Mouse [HID 04b3:310b] on usb-musb-hdrc.1-1/input0 [ 1.669464] usbcore: registered new interface driver usbhid [ 1.675292] usbhid: USB HID core driver [ 1.679962] usbcore: registered new interface driver snd-usb-audio [ 1.691589] _regulator_get: 2-001b supply IOVDD not found, using dummy regulator [ 1.699432] _regulator_get: 2-001b supply DVDD not found, using dummy regulator [ 1.707122] _regulator_get: 2-001b supply AVDD not found, using dummy regulator [ 1.714782] _regulator_get: 2-001b supply DRVDD not found, using dummy regulator [ 1.725433] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok [ 1.734283] ALSA device list: [ 1.737426] #0: AM335X EVM [ 1.740447] oprofile: hardware counters not available [ 1.745697] oprofile: using timer interrupt. [ 1.750183] nf_conntrack version 0.5.0 (3960 buckets, 15840 max) [ 1.756988] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.762634] TCP cubic registered [ 1.766021] NET: Registered protocol family 17 [ 1.770690] can: controller area network core (rev 20090105 abi 8) [ 1.777252] NET: Registered protocol family 29 [ 1.781890] can: raw protocol (rev 20090105) [ 1.786346] can: broadcast manager protocol (rev 20090105 t) [ 1.792297] Registering the dns_resolver key type [ 1.797302] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.805297] ThumbEE CPU extension supported. [ 1.809814] mux: Failed to setup hwmod io irq -22 [ 1.815399] Power Management for AM33XX family [ 1.820220] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.826904] Copied the M3 firmware to UMEM [ 1.831207] omap_hwmod: wkup_m3: wkup_m3: hwmod data error: OMAP4 does not support st_shift [ 1.847381] clock: disabling unused clocks to save power [ 1.855072] Detected MACID=d4:94:a1:8d:81:16 [ 1.861602] input: gpio-keys as /devices/platform/gpio-keys/input/input4 [ 1.869323] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 1.878570] Waiting for root device /dev/mmcblk0p2... [ 1.907928] mmc0: new high speed SDHC card at address 1234 [ 1.914306] mmcblk0: mmc0:1234 SA04G 3.63 GiB [ 1.921295] mmcblk0: p1 p2 p3 [ 2.039947] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 2.060791] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 2.067871] mmc1: new SDIO card at address 0001 [ 8.433746] kjournald starting. Commit interval 5 seconds [ 9.132232] EXT3-fs (mmcblk0p2): using internal journal [ 9.137695] EXT3-fs (mmcblk0p2): recovery complete [ 9.146423] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 9.153656] VFS: Mounted root (ext3 filesystem) on device 179:2. [ 9.160339] Freeing init memory: 244K INIT: version 2.86 booting Please wait: booting... Starting udev [ 9.723114] udevd (714): /proc/714/oom_adj is deprecated, please use /proc/714/oom_score_adj instead. [ 11.027282] Disabling lock debugging due to kernel taint [ 11.045837] cfg80211: Calling CRDA to update world regulatory domain [ 14.639862] cfg80211: World regulatory domain updated: [ 14.645263] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) [ 14.654022] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 14.662292] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 14.670562] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 14.678833] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 14.687103] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 16.141418] wl1271: loaded [ 16.290618] kjournald starting. Commit interval 5 seconds [ 16.956970] EXT3-fs (mmcblk0p3): using internal journal [ 16.962432] EXT3-fs (mmcblk0p3): recovery complete [ 16.967437] EXT3-fs (mmcblk0p3): mounted filesystem with ordered data mode [ 17.020294] alignment: ignoring faults is unsafe on this CPU. Defaulting to fixup mode. Remounting root file system... Caching udev devnodes ALSA: Restoring mixer settings... Configuring network interfaces... [ 20.824981] [ 20.825012] CPSW phy found : id is : 0x4dd074 [ 20.831939] PHY 0:01 not found eth0 no wireless extensions. udhcpc (v1.13.2) started Sending discover... Sending discover... Sending discover... No lease, forking to background done. Setting up IP spoofing protection: rp_filter. Fri Aug 16 02:10:00 UTC 2013 INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Hardware abstraction layer hald Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR Starting Lighttpd Web Server: lighttpd. 2013-08-16 02:10:02: (log.c.166) server started / Starting Matrix GUI application. [ 33.681610] gadget: Mass Storage Function, version: 2009/09/11 [ 33.687896] gadget: Number of LUNs=2 [ 33.691711] lun0: LUN: removable file: /dev/mmcblk0p1 [ 33.697113] lun1: LUN: removable file: /dev/mmcblk0p3 [ 33.702514] gadget: Mass Storage Gadget, version: 2009/09/11 [ 33.708526] gadget: userspace failed to provide iSerialNumber [ 33.714630] gadget: g_mass_storage ready [ 33.718841] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 33.724395] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 33.732269] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 33.739349] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 33.746917] usb usb2: Product: MUSB HDRC host driver [ 33.752075] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 33.757629] usb usb2: SerialNumber: musb-hdrc.0 [ 33.762969] hub 2-0:1.0: USB hub found [ 33.766937] hub 2-0:1.0: 1 port detected *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2011.09 am335x-evm ttyO0 am335x-evm login: root root@am335x-evm:~#