user@computer:~$ cd ti-processor-sdk-linux-am335x-evm-06.03.00.106 user@computer:~/ti-processor-sdk-linux-am335x-evm-06.03.00.106$ ls bin board-support docs example-applications filesystem linux-devkit linux-devkit.sh Makefile Rules.make setup.sh tslib user@computer:~/ti-processor-sdk-linux-am335x-evm-06.03.00.106$ source linux-devkit/environment-setup [linux-devkit]:~/ti-processor-sdk-linux-am335x-evm-06.03.00.106> cd tslib/ [linux-devkit]:~/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib> ./autogen.sh libtoolize: putting auxiliary files in '.'. libtoolize: copying file './ltmain.sh' libtoolize: putting macros in AC_CONFIG_MACRO_DIRS, 'm4/internal'. libtoolize: copying file 'm4/internal/libtool.m4' libtoolize: copying file 'm4/internal/ltoptions.m4' libtoolize: copying file 'm4/internal/ltsugar.m4' libtoolize: copying file 'm4/internal/ltversion.m4' libtoolize: copying file 'm4/internal/lt~obsolete.m4' configure.ac:58: installing './compile' configure.ac:7: installing './missing' plugins/Makefile.am: installing './depcomp' [linux-devkit]:~/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib> ./configure $CONFIGURE_FLAGS configure: loading site script /home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/site-config-armv7at2hf-neon-linux-gnueabi checking for a BSD-compatible install... /usr/bin/install -c checking whether build environment is sane... yes checking for arm-linux-gnueabi-strip... arm-linux-gnueabihf-strip checking for a thread-safe mkdir -p... /bin/mkdir -p checking for gawk... gawk checking whether make sets $(MAKE)... yes checking whether make supports nested variables... yes checking whether make supports nested variables... (cached) yes checking build system type... x86_64-pc-linux-gnu checking host system type... arm-unknown-linux-gnueabi checking for arm-linux-gnueabi-gcc... arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi checking whether the C compiler works... yes checking for C compiler default output file name... a.out checking for suffix of executables... checking whether we are cross compiling... yes checking for suffix of object files... o checking whether we are using the GNU C compiler... yes checking whether arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi accepts -g... yes checking for arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi option to accept ISO C89... none needed checking whether arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi understands -c and -o together... yes checking whether make supports the include directive... yes (GNU style) checking dependency style of arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi... none checking how to run the C preprocessor... arm-linux-gnueabihf-gcc -E --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi checking whether the C compiler supports -fvisibility=hidden... yes checking whether to use -fvisibility=hidden... yes checking whether ln -s works... yes checking whether make sets $(MAKE)... (cached) yes checking how to print strings... printf checking for a sed that does not truncate output... (cached) sed checking for grep that handles long lines and -e... /bin/grep checking for egrep... /bin/grep -E checking for fgrep... /bin/grep -F checking for ld used by arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi... arm-linux-gnueabihf-ld --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi checking if the linker (arm-linux-gnueabihf-ld --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi) is GNU ld... yes checking for BSD- or MS-compatible name lister (nm)... arm-linux-gnueabihf-nm checking the name lister (arm-linux-gnueabihf-nm) interface... BSD nm checking the maximum length of command line arguments... 1572864 checking how to convert x86_64-pc-linux-gnu file names to arm-unknown-linux-gnueabi format... func_convert_file_noop checking how to convert x86_64-pc-linux-gnu file names to toolchain format... func_convert_file_noop checking for arm-linux-gnueabihf-ld --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi option to reload object files... -r checking for arm-linux-gnueabi-objdump... arm-linux-gnueabihf-objdump checking how to recognize dependent libraries... pass_all checking for arm-linux-gnueabi-dlltool... no checking for dlltool... no checking how to associate runtime and link libraries... printf %s\n checking for arm-linux-gnueabi-ar... arm-linux-gnueabihf-ar checking for archiver @FILE support... @ checking for arm-linux-gnueabi-strip... (cached) arm-linux-gnueabihf-strip checking for arm-linux-gnueabi-ranlib... arm-linux-gnueabihf-ranlib checking command to parse arm-linux-gnueabihf-nm output from arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi object... ok checking for sysroot... /home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi checking for a working dd... /bin/dd checking how to truncate binary pipes... /bin/dd bs=4096 count=1 checking for arm-linux-gnueabi-mt... no checking for mt... mt configure: WARNING: using cross tools not prefixed with host triplet checking if mt is a manifest tool... no checking for ANSI C header files... yes checking for sys/types.h... yes checking for sys/stat.h... yes checking for stdlib.h... yes checking for string.h... yes checking for memory.h... yes checking for strings.h... yes checking for inttypes.h... yes checking for stdint.h... yes checking for unistd.h... yes checking for dlfcn.h... yes checking for objdir... .libs checking if arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi supports -fno-rtti -fno-exceptions... no checking for arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi option to produce PIC... -fPIC -DPIC checking if arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi PIC flag -fPIC -DPIC works... yes checking if arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi static flag -static works... yes checking if arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi supports -c -o file.o... yes checking if arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi supports -c -o file.o... (cached) yes checking whether the arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi linker (arm-linux-gnueabihf-ld --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi) supports shared libraries... yes checking whether -lc should be explicitly linked in... no checking dynamic linker characteristics... GNU/Linux ld.so checking how to hardcode library paths into programs... immediate checking for shl_load... no checking for shl_load in -ldld... no checking for dlopen... no checking for dlopen in -ldl... yes checking whether a program can dlopen itself... cross checking whether stripping libraries is possible... yes checking if libtool supports shared libraries... yes checking whether to build shared libraries... yes checking whether to build static libraries... no checking for dlopen in -ldl... (cached) yes checking for size_t... yes checking for working alloca.h... yes checking for alloca... yes checking for ANSI C header files... (cached) yes checking fcntl.h usability... yes checking fcntl.h presence... yes checking for fcntl.h... yes checking limits.h usability... yes checking limits.h presence... yes checking for limits.h... yes checking for stdlib.h... (cached) yes checking for string.h... (cached) yes checking sys/ioctl.h usability... yes checking sys/ioctl.h presence... yes checking for sys/ioctl.h... yes checking sys/time.h usability... yes checking sys/time.h presence... yes checking for sys/time.h... yes checking for unistd.h... (cached) yes checking for stdint.h... (cached) yes checking for sys/types.h... (cached) yes checking errno.h usability... yes checking errno.h presence... yes checking for errno.h... yes checking dirent.h usability... yes checking dirent.h presence... yes checking for dirent.h... yes checking linux/spi/cy8mrln.h usability... no checking linux/spi/cy8mrln.h presence... no checking for linux/spi/cy8mrln.h... no checking for an ANSI C-conforming const... yes checking for inline... inline checking for size_t... (cached) yes checking for uint16_t... yes checking for uint8_t... yes checking whether time.h and sys/time.h may both be included... yes checking whether arm-linux-gnueabihf-gcc --sysroot=/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/armv7at2hf-neon-linux-gnueabi needs -traditional... no checking for stdlib.h... (cached) yes checking for unistd.h... (cached) yes checking for sys/param.h... yes checking for getpagesize... (cached) yes checking for working mmap... (cached) yes checking sys/select.h usability... yes checking sys/select.h presence... yes checking for sys/select.h... yes checking sys/socket.h usability... yes checking sys/socket.h presence... yes checking for sys/socket.h... yes checking types of arguments for select... int,fd_set *,struct timeval * checking return type of signal handlers... void checking whether lstat correctly handles trailing slash... (cached) yes checking whether stat accepts an empty string... (cached) no checking for vprintf... yes checking for _doprnt... no checking for gettimeofday... yes checking for memmove... yes checking for memset... yes checking for munmap... yes checking for select... yes checking for strcasecmp... yes checking for strchr... yes checking for strdup... yes checking for strtoul... yes checking for strtol... yes checking for strsep... yes checking for arm-linux-gnueabi-pkg-config... no checking for pkg-config... /home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/linux-devkit/sysroots/x86_64-arago-linux/usr/bin//pkg-config checking pkg-config is at least version 0.9.0... yes checking whether debounce module is requested... yes checking whether dejitter module is requested... yes checking whether evthres module is requested... yes checking whether iir module is requested... yes checking whether linear module is requested... yes checking whether median module is requested... yes checking whether pthres module is requested... yes checking whether skip module is requested... yes checking whether lowpass module is requested... yes checking whether invert module is requested... yes checking whether variance module is requested... yes checking whether input module is requested... yes checking whether touchkit module is requested... yes checking whether waveshare module is requested... yes checking whether input-evdev module is requested... no checking whether tatung module is requested... no checking whether ucb1x00 module is requested... no checking whether mk712 module is requested... no checking whether h3600 module is requested... no checking whether dmc module is requested... no checking whether linear-h2200 module is requested... no checking whether corgi module is requested... no checking whether collie module is requested... no checking whether arctic2 module is requested... no checking whether dmc_dus3000 module is requested... no checking whether cy8mrln-palmpre module is requested... no checking whether galax module is requested... no checking whether one-wire-ts-input module is requested... no checking where to place modules... ${libdir}/ts checking whether to enable debugging... no checking whether to enable tools... yes configure: creating ./config.status config.status: creating Makefile config.status: creating etc/Makefile config.status: creating plugins/Makefile config.status: creating src/Makefile config.status: creating tests/Makefile config.status: creating tools/Makefile config.status: creating doc/Makefile config.status: creating tslib.pc config.status: creating config.h config.status: config.h is unchanged config.status: executing depfiles commands config.status: executing libtool commands [linux-devkit]:~/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib> make make all-recursive make[1]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib' Making all in etc make[2]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/etc' make[2]: Nothing to be done for 'all'. make[2]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/etc' Making all in src make[2]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/src' make[2]: Nothing to be done for 'all'. make[2]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/src' Making all in plugins make[2]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/plugins' make[2]: Nothing to be done for 'all'. make[2]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/plugins' Making all in tests make[2]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/tests' make[2]: Nothing to be done for 'all'. make[2]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/tests' Making all in tools make[2]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/tools' make[2]: Nothing to be done for 'all'. make[2]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/tools' Making all in doc make[2]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/doc' make[2]: Nothing to be done for 'all'. make[2]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib/doc' make[2]: Entering directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib' make[2]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib' make[1]: Leaving directory '/home/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib' [linux-devkit]:~/ti-processor-sdk-linux-am335x-evm-06.03.00.106/tslib>