=> printenv bootpart bootpart=1:2 => setenv mmcdev 0 => setenv bootpart 0 => boot switch to partitions #0, OK mmc0(part 0) is current device SD/MMC found on device 0 Failed to load 'boot.scr' Can't set block device ## Error: "main_cpsw0_qsgmii_phyinit" not defined Failed to load '/boot/Image' Failed to load '/boot/dtb/ti/k3-am62a7-sk.dtb' libfdt fdt_check_header(): FDT_ERR_BADMAGIC No FDT memory address configured. Please configure the FDT address via "fdt addr
" command. Aborting! Bad Linux ARM64 Image magic! switch to partitions #0, OK mmc0(part 0) is current device Scanning mmc 0:1... No EFI system partition No EFI system partition Failed to persist EFI variables Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed BootOrder not defined EFI boot manager: Cannot load any image MMC: no card present starting USB... No working controllers found USB is stopped. Please issue 'usb start' first. starting USB... No working controllers found Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed "Synchronous Abort" handler, esr 0x86000004 elr: 3030302ff0c23840 lr : 3030302ff0c23840 (reloc) elr: 3030303030303840 lr : 3030303030303840 x0 : 00000000ffffffed x1 : 0000000000000000 x2 : 0000000000000008 x3 : 00000000bdebb910 x4 : 00000000bffc5e10 x5 : 00000000bffc5eb0 x6 : 00000000bffc5e20 x7 : 00000000bdebc6a0 x8 : 00000000bde94270 x9 : 0000000000000008 x10: 00000000ffffffd8 x11: 000000000000000a x12: 0000000000003f54 x13: 0000000000000000 x14: 00000000bde94270 x15: 0000000000000002 x16: 00000000bff41260 x17: 0000000000000000 x18: 00000000bde9fdb0 x19: 0000314074726f70 x20: 00000000bffec000 x21: 00000000bffee000 x22: 0000000000000004 x23: 00000000bffec000 x24: 0000000000000000 x25: 00000000bffee000 x26: 00000000bffec000 x27: 0000000000000000 x28: 00000000bdeb5980 x29: 74656e7265687465 Code: "Synchronous Abort" handler, esr 0x96000004 elr: 0000000080802b08 lr : 0000000080802ae8 (reloc) elr: 00000000bfee2b08 lr : 00000000bfee2ae8 x0 : 00000000bffa7cf0 x1 : 0000000000000000 x2 : 0000000000000020 x3 : 0000000002800000 x4 : 0000000002800000 x5 : 00000000bde92f33 x6 : 0000000000000035 x7 : 00000000bde933c0 x8 : 0000000000000001 x9 : 0000000000000008 x10: 00000000ffffffe8 x11: 0000000000000010 x12: 000000000001869f x13: 0000000000000000 x14: 00000000bde94270 x15: 0000000000000021 x16: 00000000bff41260 x17: 0000000000000000 x18: 00000000bde9fdb0 x19: 3030303030303830 x20: 00000000bffb1822 x21: 00000000fffffffc x22: 00000000bffb3357 x23: 00000000bffa7cf0 x24: 0000000000000000 x25: 00000000bffee000 x26: 00000000bffec000 x27: 0000000000000000 x28: 00000000bdeb5980 x29: 00000000bde933c0 Code: d1004273 910d5ed6 aa0003f7 12800075 (b9400261) Resetting CPU ... resetting ... U-Boot SPL 2023.04-g756ba776d4 (Sep 20 2023 - 12:01:11 +0800) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') am62a_init: board_init_f done SPL initial stack usage: 17032 bytes am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Trying to boot from MMC1 am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 00:42:57, Jan 13 2023 U-Boot SPL 2023.04-g756ba776d4 (Sep 20 2023 - 12:00:33 +0800) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') am62a_init: board_init_f done am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Trying to boot from MMC1 am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Authentication passed am62a_init: spl_boot_device: devstat = 0x4b bootmedia = 0x9 bootindex = 0 Authentication passed U-Boot 2023.04-g756ba776d4 (Sep 20 2023 - 12:00:33 +0800) SoC: AM62AX SR1.0 HS-FS Model: Texas Instruments AM62A7 SK DRAM: 1 GiB Core: 57 devices, 27 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000port@1: phy_connect() failed No ethernet found. Hit any key to stop autoboot: 0 MMC: no card present SD/MMC found on device 1 MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1 Can't set block device MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1 Can't set block device MMC: no card present ** Bad device specification mmc 1 ** ## Error: "main_cpsw0_qsgmii_phyinit" not defined MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1:2 Can't set block device MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1:2 Can't set block device libfdt fdt_check_header(): FDT_ERR_BADMAGIC No FDT memory address configured. Please configure the FDT address via "fdt addr
" command. Aborting! Bad Linux ARM64 Image magic! switch to partitions #0, OK mmc0(part 0) is current device Scanning mmc 0:1... MMC: no card present No EFI system partition No EFI system partition Failed to persist EFI variables Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed BootOrder not defined EFI boot manager: Cannot load any image MMC: no card present starting USB... No working controllers found USB is stopped. Please issue 'usb start' first. starting USB... No working controllers found Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed Could not get PHY for ethernet@8000000port@1: addr 0 am65_cpsw_nuss_port ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000ethernet@8000000port@1: phy_connect() failed "Synchronous Abort" handler, esr 0x86000004 elr: 3030302ff0c23840 lr : 3030302ff0c23840 (reloc) elr: 3030303030303840 lr : 3030303030303840 x0 : 00000000ffffffed x1 : 0000000000000000 x2 : 0000000000000002 x3 : 00000000bdeb44f0 x4 : 00000000bffc5e10 x5 : 00000000bdeb4510 x6 : 0000000000000021 x7 : 00000000bdeb8ed0 x8 : 00000000bde94270 x9 : 0000000000000008 x10: 00000000ffffffd8 x11: 000000000000000a x12: 0000000000003f54 x13: 0000000000000000 x14: 00000000bde94270 x15: 0000000000000002 x16: 00000000bff41260 x17: 0000000000000000 x18: 00000000bde9fdb0 x19: 0000314074726f70 x20: 00000000bffec000 x21: 00000000bffee000 x22: 0000000000000004 x23: 00000000bffec000 x24: 0000000000000000 x25: 00000000bffee000 x26: 00000000bffec000 x27: 0000000000000000 x28: 00000000bdeb4590 x29: 74656e7265687465 Code: "Synchronous Abort" handler, esr 0x96000004 elr: 0000000080802b08 lr : 0000000080802ae8 (reloc) elr: 00000000bfee2b08 lr : 00000000bfee2ae8 x0 : 00000000bffa7cf0 x1 : 0000000000000000 x2 : 0000000000000020 x3 : 0000000002800000 x4 : 0000000002800000 x5 : 00000000bde93113 x6 : 0000000000000035 x7 : 00000000bde935a0 x8 : 0000000000000001 x9 : 0000000000000008 x10: 00000000ffffffe8 x11: 0000000000000010 x12: 000000000001869f x13: 0000000000000000 x14: 00000000bde94270 x15: 0000000000000021 x16: 00000000bff41260 x17: 0000000000000000 x18: 00000000bde9fdb0 x19: 3030303030303830 x20: 00000000bffb1822 x21: 00000000fffffffc x22: 00000000bffb3357 x23: 00000000bffa7cf0 x24: 0000000000000000 x25: 00000000bffee000 x26: 00000000bffec000 x27: 0000000000000000 x28: 00000000bdeb4590 x29: 00000000bde935a0 Code: d1004273 910d5ed6 aa0003f7 12800075 (b9400261) Resetting CPU ... resetting ...