# # This file defines the modules included in $(MAKECONFIG) config # # Modules are split into, # - Use-cases specified in uc_cfg.mk # - Other system config/feature, specified in this file # # Any specific overrides are also specified in this file # Example, for TDA3x SoC EVE2/3/4 are not present and hence force marked as , i.e disabled # # # Additional config options # # # CPUs to included in build # # IPU1 (core 0 & 1 are) not supported when IPU_PRIMARY_CORE=ipu2 PROC_IPU1_0_INCLUDE=yes PROC_IPU1_1_INCLUDE=ys PROC_IPU2_INCLUDE=yes PROC_A15_0_INCLUDE=yes PROC_DSP1_INCLUDE=yes PROC_DSP2_INCLUDE=yes PROC_EVE1_INCLUDE=yes PROC_EVE2_INCLUDE=yes PROC_EVE3_INCLUDE=yes PROC_EVE4_INCLUDE=yes VSDK_BOARD_TYPE=TDA2XX_EVM # Supported values: DDR_MEM_1024M DDR_MEM=DDR_MEM_1024M # Supported values: ipu1_0 ipu1_1 ipu2 a15_0 none NDK_PROC_TO_USE=a15_0 # # Used to control building of algorithm source. # By default algorithm source not included in Vision SDK # BUILD_ALGORITHMS=no # # Applies profile to all cores # # Supported profiles: release debug #PROFILE=debug PROFILE ?= release PROFILE_ipu1_0 ?= $(PROFILE) PROFILE_ipu1_1 ?= $(PROFILE) PROFILE_ipu2 ?= $(PROFILE) PROFILE_c66xdsp_1 ?= $(PROFILE) PROFILE_c66xdsp_2 ?= $(PROFILE) PROFILE_arp32_1 ?= $(PROFILE) PROFILE_arp32_2 ?= $(PROFILE) PROFILE_arp32_3 ?= $(PROFILE) PROFILE_arp32_4 ?= $(PROFILE) PROFILE_a15_0 ?= $(PROFILE) # # For TDA2xx & TDA2Ex - vision SDK can run on either IPU1 or IPU2 subsystem # For TDA3xx - We have only IPU1 and hence IPU1 is the only option # Select IPU primary core from the available IPU1 & IPU2 subsytems # # Supported values: ipu1_0 ipu2 IPU_PRIMARY_CORE=ipu2 IPU_SECONDARY_CORE=ipu1_0 # # Set A15_TARGET_OS # A15 can run Linux or Bios # # A15_TARGET_OS support # Platform BIOS Linux # # TDA2XX_EVM yes yes # TDA3XX_EVM yes no # TDA2EX_EVM yes yes # # Supported values: Bios Linux A15_TARGET_OS=Linux # Both IVAHD_INCLUDE & IPUMM_INCLUDE should not be set to "yes" # Only one should be enabled to avoid IVA-HD resource conflict IPUMM_INCLUDE=no IVAHD_INCLUDE=yes VPE_INCLUDE=yes DSS_INCLUDE=yes AVB_INCLUDE=no # # Enable below macro to enable DCAN integration into Vision SDK. # DCAN_INCLUDE=no CPU_IDLE_ENABLED=yes # # Enable below macro to view the bandwidth used by different IPs in the device # as a graphical plot on the display screen. # DATA_VIS_INCLUDE=no # # Enable below macro to enable OPENVX into Vision SDK # OPENVX_INCLUDE=no CIO_REDIRECT=yes HS_DEVICE=no #Enable/Disable early use-cases (yes/no) EARLY_USECASE_ENABLE=no #OPENVX doesn't work with early-boot late-attach. Disable if EARLY_USECASE=yes ifeq ($(EARLY_USECASE_ENABLE),yes) OPENVX_INCLUDE=no endif DEFAULT_UBOOT_CONFIG := dra7xx_evm_vision_config DEFAULT_KERNEL_CONFIG := ti_sdk_dra7x_release_defconfig # For TDA2x DEFAULT_DTB := dra7-evm-infoadas.dtb dra7-evm-infoadas-lcd-lg.dtb CMEM_INCLUDE=yes include $($(MAKEAPPNAME)_PATH)/configs/$(MAKECONFIG)/uc_cfg.mk