U-Boot 2015.07 (Jan 08 2016 - 18:45:34 -0500) CPU : DRA752 ES1.1 Board: UNKNOWN(BeagleBoard X15?) I2C: ready DRAM: 2 GiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 reading uboot.env ** Unable to read "uboot.env" from mmc0:1 ** Using default environment SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst Invalid EEPROM data(@0x4031e028). Default to X15 SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: not set. Validating first E-fuse MAC Phy 1 not found cpsw Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt 574 bytes read in 3 ms (186.5 KiB/s) Loaded env from uEnv.txt Importing environment from mmc0 ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 3394944 bytes read in 189 ms (17.1 MiB/s) 92206 bytes read in 27 ms (3.3 MiB/s) Booting from mmc0 ... Kernel image @ 0x82000000 [ 0x000000 - 0x33cd80 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffe6000, end 8ffff82d ... OK Starting kernel ...