[ 164.733235] Unable to handle kernel paging request at virtual address 000000040021ae1b [ 164.733262] Mem abort info: [ 164.733264] ESR = 0x0000000096000045 [ 164.733268] EC = 0x25: DABT (current EL), IL = 32 bits [ 164.733275] SET = 0, FnV = 0 [ 164.733277] EA = 0, S1PTW = 0 [ 164.733280] FSC = 0x05: level 1 translation fault [ 164.733284] Data abort info: [ 164.733286] ISV = 0, ISS = 0x00000045, ISS2 = 0x00000000 [ 164.733289] CM = 0, WnR = 1, TnD = 0, TagAccess = 0 [ 164.733293] GCS = 0, Overlay = 0, DirtyBit = 0, Xs = 0 [ 164.733299] user pgtable: 4k pages, 48-bit VAs, pgdp=00000000851cd000 [ 164.733304] [000000040021ae1b] pgd=0800000087590003, p4d=0800000087590003, pud=0000000000000000 [ 164.733320] Internal error: Oops: 0000000096000045 [#1] PREEMPT_RT SMP [ 164.733326] Modules linked in: [ 164.733336] CPU: 1 UID: 0 PID: 77 Comm: irq/206-8000000 Not tainted 6.12.0-rc5 #2 [ 164.733345] Hardware name: Texas Instruments K3 AM625 SoC (DT) [ 164.733350] pstate: 00000005 (nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 164.733358] pc : __build_skb_around+0x58/0xd8 [ 164.733379] lr : build_skb+0x4c/0xa8 [ 164.733388] sp : ffff00000179fa50 [ 164.733391] x29: ffff00000179fa50 x28: ffff00007b4d4700 x27: ffff0000038a56c8 [ 164.733401] x26: ffff000003516080 x25: 0000000000000040 x24: ffff0000038e1000 [ 164.733410] x23: 0000000000000000 x22: 0000000000000000 x21: 000000040021a673 [ 164.733419] x20: 00000000000009e8 x19: ffff0000019b0100 x18: 000000265a15ef6b [ 164.733428] x17: 0000000000000000 x16: 0000000000000000 x15: ffff00007f5b0540 [ 164.733437] x14: 00b4fbe3d79fd785 x13: 0000000000000000 x12: 00000179d77682a0 [ 164.733446] x11: ffff80008130a000 x10: ffff800080aa37a0 x9 : 0000000000000000 [ 164.733455] x8 : ffff0000019b01b8 x7 : 0000000000000000 x6 : 000000000000003f [ 164.733464] x5 : 0000000000000040 x4 : 0000000000000000 x3 : 00000000ffffffff [ 164.733472] x2 : 0000000000000001 x1 : 0000000000000001 x0 : 000000040021ae1b [ 164.733481] Call trace: [ 164.733485] __build_skb_around+0x58/0xd8 [ 164.733493] build_skb+0x4c/0xa8 [ 164.733502] am65_cpsw_nuss_rx_poll+0x1ec/0x938 [ 164.733518] __napi_poll.constprop.0+0x34/0x174 [ 164.733529] net_rx_action+0x140/0x268 [ 164.733537] handle_softirqs.isra.0+0xdc/0x1d0 [ 164.733548] __local_bh_enable_ip+0x90/0xe0 [ 164.733555] irq_forced_thread_fn+0x94/0xa8 [ 164.733566] irq_thread+0x1cc/0x280 [ 164.733575] kthread+0x10c/0x110 [ 164.733586] ret_from_fork+0x10/0x20 [ 164.733598] Code: b900d274 b900d661 b9401042 79011262 (a9007c1f) [ 164.733605] ---[ end trace 0000000000000000 ]--- [ 164.733611] Kernel panic - not syncing: Oops: Fatal exception in interrupt [ 164.733616] SMP: stopping secondary CPUs [ 164.733625] Kernel Offset: disabled [ 164.733628] CPU features: 0x00,00000080,00000000,4200400b [ 164.733634] Memory Limit: none [ 164.988917] ---[ end Kernel panic - not syncing: Oops: Fatal exception in interrupt ]---