Welcome to minicom 2.4 OPTIONS: I18n Compiled on Jan 25 2010, 06:49:09. Port /dev/ttyS0 Press CTRL-A Z for help on special keys CCCCCCCC U-Boot SPL 2011.09 (Jul 26 2012 - 17:18:20) Texas Instruments Revision detection unimplemented Found a daughter card connected OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2011.09 (Jul 26 2012 - 17:13:38) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled Found a daughter card connected NAND: HW ECC Hamming Code selected 256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - bad CRC, using default environment Net: cpsw Hit any key to stop autoboot: 1 CTRL-A Z for help |115200 8N1 | NOR | Minicom 2.4 | VT102 | Offline 0 SD/MMC found on device 0 reading uEnv.txt ** Unable to read "uEnv.txt" from mmc 0:1 ** reading uImage 3163784 bytes read ## Booting kernel from Legacy Image at 80007fc0 ... Image Name: Linux-3.2.0 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3163720 Bytes = 3 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK XIP Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (root@cts-desktop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Fri Jan 25 15:04:31 IST 2013 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 253256k/253256k available, 8888k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc059d000 (5716 kB) [ 0.000000] .init : 0xc059d000 - 0xc05db000 ( 248 kB) [ 0.000000] .data : 0xc05dc000 - 0xc0644198 ( 417 kB) [ 0.000000] .bss : 0xc06441bc - 0xc0671024 ( 180 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.058929] pid_max: default: 32768 minimum: 301 [ 0.059051] Security Framework initialized [ 0.059143] Mount-cache hash table entries: 512 [ 0.059539] CPU: Testing write buffer coherency: ok [ 0.079498] omap_hwmod: pruss: failed to hardreset [ 0.080627] print_constraints: dummy: [ 0.080963] NET: Registered protocol family 16 [ 0.083099] OMAP GPIO hardware version 0.1 [ 0.085693] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.087921] omap_i2c.1: alias fck already exists [ 0.088806] omap2_mcspi.1: alias fck already exists [ 0.089080] omap2_mcspi.2: alias fck already exists [ 0.089843] edma.0: alias fck already exists [ 0.089874] edma.0: alias fck already exists [ 0.089904] edma.0: alias fck already exists [ 0.090270] d_can.1: alias fck already exists [ 0.116943] bio: create slab at 0 [ 0.119232] SCSI subsystem initialized [ 0.120849] usbcore: registered new interface driver usbfs [ 0.121154] usbcore: registered new interface driver hub [ 0.121337] usbcore: registered new device driver usb [ 0.121490] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.121795] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.139007] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.140899] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.143280] print_constraints: VRTC: [ 0.144744] print_constraints: VIO: at 1800 mV [ 0.147033] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.149322] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.150329] print_constraints: VDD3: 5000 mV [ 0.151733] print_constraints: VDIG1: at 1800 mV [ 0.153167] print_constraints: VDIG2: at 1800 mV [ 0.154571] print_constraints: VPLL: at 1800 mV [ 0.156005] print_constraints: VDAC: at 1800 mV [ 0.157440] print_constraints: VAUX1: at 1800 mV [ 0.158843] print_constraints: VAUX2: at 3300 mV [ 0.160308] print_constraints: VAUX33: at 3300 mV [ 0.161712] print_constraints: VMMC: at 3300 mV [ 0.162231] tps65910 1-002d: No interrupt support, no core IRQ [ 0.163482] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.164611] Switching to clocksource gp timer [ 0.180053] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.180236] musb-hdrc musb-hdrc.0: dma type: pio [ 0.180541] MUSB0 controller's USBSS revision = 4ea20800 [ 0.181121] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using PIO, IRQ 18 [ 0.181274] musb-hdrc musb-hdrc.1: dma type: pio [ 0.181579] MUSB1 controller's USBSS revision = 4ea20800 [ 0.181671] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.181762] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.181884] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.181915] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.181915] usb usb1: Product: MUSB HDRC host driver [ 0.181945] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.181945] usb usb1: SerialNumber: musb-hdrc.1 [ 0.182708] hub 1-0:1.0: USB hub found [ 0.182739] hub 1-0:1.0: 1 port detected [ 0.183288] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19 [ 0.183715] NET: Registered protocol family 2 [ 0.183898] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.184204] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.184356] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.184448] TCP: Hash tables configured (established 8192 bind 8192) [ 0.184478] TCP reno registered [ 0.184478] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.184509] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.184753] NET: Registered protocol family 1 [ 0.185028] RPC: Registered named UNIX socket transport module. [ 0.185058] RPC: Registered udp transport module. [ 0.185058] RPC: Registered tcp transport module. [ 0.185058] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.185333] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.197418] VFS: Disk quotas dquot_6.5.2 [ 0.197509] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.198028] msgmni has been set to 494 [ 0.201232] alg: No test for stdrng (krng) [ 0.201904] io scheduler noop registered [ 0.201934] io scheduler deadline registered [ 0.201995] io scheduler cfq registered (default) [ 0.205749] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.825256] console [ttyO0] enabled [ 0.829498] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.837310] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.845123] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.852905] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.860687] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.877868] brd: module loaded [ 0.885955] loop: module loaded [ 0.889434] i2c-core: driver [tsl2550] using legacy suspend method [ 0.895904] i2c-core: driver [tsl2550] using legacy resume method [ 0.902313] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.916229] Detected a daughter card on AM335x EVM.. [ 0.921234] CPLD version: CPLD1.0F [ 0.924987] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.940155] Board name: A33515BB [ 0.943542] Board version: 1.4A [ 0.946807] SKU: SKU#01 [ 0.949890] The board is general purpose EVM in profile 0 [ 0.956024] da8xx_lcdc.0: alias fck already exists [ 0.961669] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel [ 0.985351] Console: switching to colour frame buffer device 100x30 [ 1.002136] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 1.007202] Registering NAND on CS0 [ 1.011535] omap_i2c.2: alias fck already exists [ 1.035278] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 1.041778] tsl2550 2-0039: standard operating mode [ 1.047576] tsl2550 2-0039: support ver. 1.2 enabled [ 1.053436] davinci-mcasp.1: alias fck already exists [ 1.059051] usb 1-1: new low-speed USB device number 2 using musb-hdrc [ 1.066284] omap_hsmmc.0: alias fck already exists [ 1.071807] omap_hsmmc.2: alias fck already exists [ 1.077301] Configure Bluetooth Enable pin... [ 1.083312] registered am33xx_sr device [ 1.087585] _regulator_get: 2-0018 supply Vdd not found, using dummy regulator [ 1.095184] _regulator_get: 2-0018 supply Vdd_IO not found, using dummy regulator [ 1.123626] lis3lv02d: 8 bits 3DLH sensor found [ 1.207733] usb 1-1: New USB device found, idVendor=04b3, idProduct=310b [ 1.214721] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0 [ 1.223144] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0 [ 1.234436] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.241790] omap2-nand driver initializing [ 1.246398] ONFI flash detected [ 1.249816] ONFI param page 0 valid [ 1.253448] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP) [ 1.262054] Creating 8 MTD partitions on "omap2-nand.0": [ 1.267608] 0x000000000000-0x000000020000 : "SPL" [ 1.273925] 0x000000020000-0x000000040000 : "SPL.backup1" [ 1.280883] 0x000000040000-0x000000060000 : "SPL.backup2" [ 1.287780] 0x000000060000-0x000000080000 : "SPL.backup3" [ 1.294677] 0x000000080000-0x000000260000 : "U-Boot" [ 1.301910] 0x000000260000-0x000000280000 : "U-Boot Env" [ 1.308746] 0x000000280000-0x000000780000 : "Kernel" [ 1.317291] 0x000000780000-0x000010000000 : "File System" [ 1.427551] OneNAND driver initializing [ 1.432952] CAN device driver interface [ 1.437011] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.443450] d_can d_can.1: device registered (irq=55, irq_obj=56) [ 1.495269] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.501708] davinci_mdio davinci_mdio.0: detected phy mask fffffffe [ 1.509155] davinci_mdio.0: probed [ 1.512695] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.520416] usbcore: registered new interface driver zd1201 [ 1.526458] usbcore: registered new interface driver cdc_ether [ 1.532714] usbcore: registered new interface driver cdc_eem [ 1.538787] usbcore: registered new interface driver dm9601 [ 1.544647] cdc_ncm: 04-Aug-2011 [ 1.548187] usbcore: registered new interface driver cdc_ncm [ 1.554107] Initializing USB Mass Storage driver... [ 1.559448] usbcore: registered new interface driver usb-storage [ 1.565704] USB Mass Storage support registered. [ 1.570983] mousedev: PS/2 mouse device common for all mice [ 1.577819] input: matrix-keypad as /devices/platform/matrix-keypad/input/input1 [ 1.586944] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input2 [ 1.595458] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.602294] i2c /dev entries driver [ 1.606597] Linux video capture interface: v2.00 [ 1.611755] usbcore: registered new interface driver uvcvideo [ 1.617767] USB Video Class driver (1.1.1) [ 1.622924] lm75 2-0048: hwmon0: sensor 'tmp275' [ 1.630615] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.639221] cpuidle: using governor ladder [ 1.643981] cpuidle: using governor menu [ 1.651855] omap4_aes_mod_init: loading AM33X AES driver [ 1.657562] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02 [ 1.664093] omap4_aes_probe: probe() done [ 1.668792] omap4_sham_mod_init: loading AM33X SHA/MD5 driver [ 1.674926] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03 [ 1.689575] omap4_sham_probe: probe() done [ 1.703186] input: HID 04b3:310b as /devices/platform/omap/musb-ti81xx/musb-hdrc.1/usb1/1-1/1-1:1.0/input/input3 [ 1.714385] generic-usb 0003:04B3:310B.0001: input: USB HID v1.00 Mouse [HID 04b3:310b] on usb-musb-hdrc.1-1/input0 [ 1.725555] usbcore: registered new interface driver usbhid [ 1.731353] usbhid: USB HID core driver [ 1.736053] usbcore: registered new interface driver snd-usb-audio [ 1.744445] _regulator_get: 2-001b supply IOVDD not found, using dummy regulator [ 1.752319] _regulator_get: 2-001b supply DVDD not found, using dummy regulator [ 1.759979] _regulator_get: 2-001b supply AVDD not found, using dummy regulator [ 1.767669] _regulator_get: 2-001b supply DRVDD not found, using dummy regulator [ 1.778320] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok [ 1.786163] ALSA device list: [ 1.789276] #0: AM335X EVM [ 1.792266] oprofile: hardware counters not available [ 1.797576] oprofile: using timer interrupt. [ 1.802032] nf_conntrack version 0.5.0 (3957 buckets, 15828 max) [ 1.808837] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.814514] TCP cubic registered [ 1.817901] NET: Registered protocol family 17 [ 1.822540] can: controller area network core (rev 20090105 abi 8) [ 1.829101] NET: Registered protocol family 29 [ 1.833770] can: raw protocol (rev 20090105) [ 1.838226] can: broadcast manager protocol (rev 20090105 t) [ 1.844146] Registering the dns_resolver key type [ 1.849151] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.857147] ThumbEE CPU extension supported. [ 1.861663] mux: Failed to setup hwmod io irq -22 [ 1.867218] Power Management for AM33XX family [ 1.872100] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.878784] Copied the M3 firmware to UMEM [ 1.883270] smartreflex smartreflex: am33xx_sr_probe: Zero NValue read from EFUSE [ 1.891113] smartreflex: probe of smartreflex failed with error -22 [ 1.898162] sr_init: platform driver register failed [ 1.908538] clock: disabling unused clocks to save power [ 1.927551] Detected MACID=d4:94:a1:8d:81:16 [ 1.932800] mmc0: new high speed SDHC card at address aaaa [ 1.939178] cpsw: Detected MACID = d4:94:a1:8d:81:17 [ 1.945404] mmcblk0: mmc0:aaaa SU08G 7.40 GiB [ 1.952239] input: gpio-keys as /devices/platform/gpio-keys/input/input4 [ 1.959533] mmcblk0: p1 p2 [ 1.963623] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:01 UTC (946684801) [ 2.080322] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 2.101440] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 2.108673] mmc1: new SDIO card at address 0001 [ 4.544616] kjournald starting. Commit interval 5 seconds [ 4.552490] EXT3-fs (mmcblk0p2): using internal journal [ 4.557983] EXT3-fs (mmcblk0p2): recovery complete [ 4.650512] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 4.657775] VFS: Mounted root (ext3 filesystem) on device 179:2. [ 4.664398] Freeing init memory: 248K INIT: version 2.86 booting Please wait: booting... Starting udev [ 5.622009] Disabling lock debugging due to kernel taint [ 6.618255] cfg80211: Calling CRDA to update world regulatory domain [ 7.010986] cfg80211: World regulatory domain updated: [ 7.016448] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) [ 7.025177] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.033447] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 7.041717] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 7.049987] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.058258] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 7.368530] wl12xx: driver version: ol_R5.00.17 [ 7.373260] wl12xx: compilation time: Thu May 17 05:25:00 2012 [ 7.755584] wl12xx: loaded [ 7.850555] alignment: ignoring faults is unsafe on this CPU. Defaulting to fixup mode. Remounting root file system... Caching udev devnodes ALSA: Restoring mixer settings... Configuring network interfaces... [ 10.025817] net eth0: CPSW phy found : id is : 0x4dd074 eth0 no wireless extensions. udhcpc (v1.13.2) started Sending discover... Sending discover... Sending discover... No lease, forking to background done. Setting up IP spoofing protection: rp_filter. Fri Jul 27 12:26:00 UTC 2012 INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Hardware abstraction layer hald Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR Starting Lighttpd Web Server: lighttpd. 2012-07-27 12:26:02: (log.c.166) server started / Starting Matrix GUI application. [ 23.136322] gadget: Mass Storage Function, version: 2009/09/11 [ 23.142608] gadget: Number of LUNs=1 [ 23.146453] lun0: LUN: removable file: /dev/mmcblk0p1 [ 23.151855] gadget: Mass Storage Gadget, version: 2009/09/11 [ 23.157867] gadget: userspace failed to provide iSerialNumber [ 23.163970] gadget: g_mass_storage ready [ 23.168182] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 23.173767] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 23.181610] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 23.188690] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 23.196228] usb usb2: Product: MUSB HDRC host driver [ 23.201416] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 23.206939] usb usb2: SerialNumber: musb-hdrc.0 [ 23.212219] hub 2-0:1.0: USB hub found [ 23.216156] hub 2-0:1.0: 1 port detected *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2011.09 am335x-evm ttyO0 am335x-evm login: root root@am335x-evm:~#