U-Boot SPL 2020.01-dirty (Dec 10 2021 - 17:44:26 -0600) Trying to boot from NAND U-Boot 2020.01-dirty (Dec 10 2021 - 17:44:26 -0600) CPU : AM335X-GP rev 2.0 Model: TI AM335x EVM DRAM: 512 MiB WDT: Started with servicing (60s timeout) NAND: 256 MiB MMC: OMAP SD/MMC: 0 Loading Environment from FAT... not set. Validating first E-fuse MAC Net: eth0: ethernet@4a100000 Warning: usb_ether MAC addresses don't match: Address in ROM is de:ad:be:ef:00:01 Address in environment is c8:a0:30:7d:1a:92 , eth1: usb_ether Hit any key to stop autoboot: 2 0 => run nandboot Booting from nand ... NAND read: device 0 offset 0x80000, size 0x40000 262144 bytes read: OK NAND read: device 0 offset 0x200000, size 0x800000 8388608 bytes read: OK ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffec000, end 8ffff20f ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.4.106-g023faefa70 (oe-user@oe-host) (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 PREEMPT Mon Sep 6 22:18:18 UTC 2021 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x EVM [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x9c800000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.0 (sgx neon) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129666 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1 [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 453820K/523264K available (9216K kernel code, 295K rwdata, 3092K rodata, 1024K init, 254K bss, 20292K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] random: get_random_bytes called from start_kernel+0x2b4/0x470 with crng_init=0 [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000022] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000049] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000063] OMAP clocksource: timer1 at 24000000 Hz [ 0.000448] timer_probe: no matching timers found [ 0.000697] Console: colour dummy device 80x30 [ 0.000744] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000753] This ensures that you still see kernel messages. Please [ 0.000760] update your kernel commandline. [ 0.000823] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032) [ 0.118648] pid_max: default: 32768 minimum: 301 [ 0.118955] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.118975] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear) [ 0.120193] CPU: Testing write buffer coherency: ok [ 0.120284] CPU0: Spectre v2: using BPIALL workaround [ 0.121408] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.121613] rcu: Hierarchical SRCU implementation. [ 0.121731] EFI services will not be available. [ 0.122245] devtmpfs: initialized [ 0.138543] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.139194] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.139227] futex hash table entries: 256 (order: -1, 3072 bytes, linear) [ 0.144339] pinctrl core: initialized pinctrl subsystem [ 0.145403] DMI not present or invalid. [ 0.146016] NET: Registered protocol family 16 [ 0.149376] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.180053] l3-aon-clkctrl:0000:0: failed to disable [ 0.182752] cpuidle: using governor ladder [ 0.182799] cpuidle: using governor menu [ 0.207982] No ATAGs? [ 0.207997] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.231314] debugfs: Directory '49000000.edma' with parent 'dmaengine' already present! [ 0.231362] edma 49000000.edma: TI EDMA DMA engine driver [ 0.233764] v1_8d: supplied by vbat [ 0.234236] v3_3d: supplied by vbat [ 0.235635] iommu: Default domain type: Translated [ 0.239254] SCSI subsystem initialized [ 0.239975] mc: Linux media interface: v0.10 [ 0.240029] videodev: Linux video capture interface: v2.00 [ 0.240169] pps_core: LinuxPPS API ver. 1 registered [ 0.240179] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.240209] PTP clock support registered [ 0.240255] EDAC MC: Ver: 3.0.0 [ 0.241913] Advanced Linux Sound Architecture Driver Initialized. [ 0.243569] clocksource: Switched to clocksource timer1 [ 0.254894] thermal_sys: Registered thermal governor 'fair_share' [ 0.254906] thermal_sys: Registered thermal governor 'bang_bang' [ 0.254928] thermal_sys: Registered thermal governor 'step_wise' [ 0.254938] thermal_sys: Registered thermal governor 'user_space' [ 0.254946] thermal_sys: Registered thermal governor 'power_allocator' [ 0.255726] NET: Registered protocol family 2 [ 0.256780] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear) [ 0.256823] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear) [ 0.256886] TCP bind hash table entries: 4096 (order: 2, 16384 bytes, linear) [ 0.256947] TCP: Hash tables configured (established 4096 bind 4096) [ 0.257093] UDP hash table entries: 256 (order: 0, 4096 bytes, linear) [ 0.257120] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear) [ 0.257326] NET: Registered protocol family 1 [ 0.258111] RPC: Registered named UNIX socket transport module. [ 0.258131] RPC: Registered udp transport module. [ 0.258139] RPC: Registered tcp transport module. [ 0.258147] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.258168] PCI: CLS 0 bytes, default 64 [ 0.259461] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.261236] Initialise system trusted keyrings [ 0.261675] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 0.268986] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.270061] NFS: Registering the id_resolver key type [ 0.270115] Key type id_resolver registered [ 0.270125] Key type id_legacy registered [ 0.270192] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.271167] Key type asymmetric registered [ 0.271185] Asymmetric key parser 'x509' registered [ 0.271255] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244) [ 0.271269] io scheduler mq-deadline registered [ 0.271279] io scheduler kyber registered [ 0.278750] OMAP GPIO hardware version 0.1 [ 0.312999] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.344600] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 0.350779] pwm-backlight backlight: backlight supply power not found, using dummy regulator [ 0.420862] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.427252] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 1.056759] printk: console [ttyS0] enabled [ 1.062950] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 37, base_baud = 3000000) is a 8250 [ 1.075885] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 1.083830] random: fast init done [ 1.087575] random: crng init done [ 1.094160] OF: graph: no port node found in /ocp/interconnect@48000000/segment@300000/target-module@e000/lcdc@0 [ 1.105448] OF: graph: no port node found in /ocp/interconnect@48000000/segment@300000/target-module@e000/lcdc@0 [ 1.116280] OF: graph: no port node found in /ocp/interconnect@48000000/segment@300000/target-module@e000/lcdc@0 [ 1.126572] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 1.133215] [drm] No driver support for vblank timestamp query. [ 1.140019] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on minor 0 [ 1.195319] Console: switching to colour frame buffer device 100x30 [ 1.217704] tilcdc 4830e000.lcdc: fb0: tilcdcdrmfb frame buffer device [ 1.246286] brd: module loaded [ 1.259616] loop: module loaded [ 1.270977] libphy: Fixed MDIO Bus: probed [ 1.333604] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.341334] libphy: 4a101000.mdio: probed [ 1.347356] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Atheros 8031 ethernet [ 1.357027] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.363418] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.368910] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 1.376260] cpsw 4a100000.ethernet: Detected MACID = c8:a0:30:7d:1a:90 [ 1.385591] i2c /dev entries driver [ 1.393060] cpuidle: enable-method property 'ti,am3352' found operations [ 1.401002] sdhci: Secure Digital Host Controller Interface driver [ 1.407349] sdhci: Copyright(c) Pierre Ossman [ 1.413846] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22) [ 1.422625] omap_hsmmc 48060000.mmc: Got CD GPIO [ 1.435742] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.443340] ledtrig-cpu: registered to indicate activity on CPUs [ 1.455845] davinci-mcasp 4803c000.mcasp: IRQ common not found [ 1.464318] NET: Registered protocol family 10 [ 1.470402] Segment Routing with IPv6 [ 1.474387] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.481317] NET: Registered protocol family 17 [ 1.486435] Key type dns_resolver registered [ 1.490941] omap_voltage_late_init: Voltage driver support not added [ 1.498292] Loading compiled-in X.509 certificates [ 1.521034] omap-gpmc 50000000.gpmc: GPMC revision 6.0 [ 1.526460] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000 [ 1.535214] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xda [ 1.541609] nand: Micron MT29F2G08ABAEAWP [ 1.545742] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 [ 1.553591] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme [ 1.559122] 10 fixed-partitions partitions found on MTD device omap2-nand.0 [ 1.566183] Creating 10 MTD partitions on "omap2-nand.0": [ 1.571620] 0x000000000000-0x000000020000 : "NAND.SPL" [ 1.579234] 0x000000020000-0x000000040000 : "NAND.SPL.backup1" [ 1.587061] 0x000000040000-0x000000060000 : "NAND.SPL.backup2" [ 1.594836] 0x000000060000-0x000000080000 : "NAND.SPL.backup3" [ 1.602456] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os" [ 1.610379] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot" [ 1.618085] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env" [ 1.625751] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1" [ 1.634064] 0x000000200000-0x000000a00000 : "NAND.kernel" [ 1.645109] 0x000000a00000-0x000010000000 : "NAND.file-system" [ 1.793868] tps65910 0-002d: No interrupt support, no core IRQ [ 1.805110] vrtc: supplied by vbat [ 1.810163] vio: supplied by vbat [ 1.815437] vdd_mpu: supplied by vbat [ 1.821011] vdd_core: supplied by vbat [ 1.827656] vdig1: supplied by vbat [ 1.832597] vdig2: supplied by vbat [ 1.837601] vpll: supplied by vbat [ 1.842452] vdac: supplied by vbat [ 1.847343] vaux1: supplied by vbat [ 1.852307] vaux2: supplied by vbat [ 1.857296] vaux33: supplied by vbat [ 1.862332] vmmc: supplied by vbat [ 1.867167] vbb: supplied by vbat [ 1.871292] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.879847] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz [ 1.891864] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22) [ 1.900865] omap_hsmmc 48060000.mmc: Got CD GPIO [ 2.050083] ubi0: attaching mtd9 [ 2.059116] omap_hsmmc 47810000.mmc: card claims to support voltages below defined range [ 2.081196] mmc1: new SDIO card at address 0001 [ 3.226949] ubi0: scanning is finished [ 3.250045] ubi0: attached mtd9 (name "NAND.file-system", size 246 MiB) [ 3.256829] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes [ 3.264100] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512 [ 3.271043] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096 [ 3.278082] ubi0: good PEBs: 1968, bad PEBs: 0, corrupted PEBs: 0 [ 3.284243] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128 [ 3.291506] ubi0: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 1759344572 [ 3.300694] ubi0: available PEBs: 0, total reserved PEBs: 1968, PEBs reserved for bad PEB handling: 40 [ 3.310087] ubi0: background thread "ubi_bgt0d" started, PID 57 [ 3.317268] input: volume_keys0 as /devices/platform/volume_keys0/input/input0 [ 3.325452] hctosys: unable to open rtc device (rtc0) [ 3.331422] ALSA device list: [ 3.334606] No soundcards found. [ 3.340102] UBIFS (ubi0:0): Mounting in unauthenticated mode [ 3.353667] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 58 [ 3.430861] UBIFS (ubi0:0): recovery needed [ 3.586528] UBIFS (ubi0:0): recovery completed [ 3.591398] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs" [ 3.598882] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 3.609202] UBIFS (ubi0:0): FS size: 242778112 bytes (231 MiB, 1912 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs) [ 3.620069] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB) [ 3.626042] UBIFS (ubi0:0): media format: w4/r0 (latest is w5/r0), UUID AF09DAE9-2295-491F-89F1-DD785CFE4A34, small LPT model [ 3.638606] VFS: Mounted root (ubifs filesystem) on device 0:17. [ 3.646166] devtmpfs: mounted [ 3.651023] Freeing unused kernel memory: 1024K [ 3.656260] Run /sbin/init as init process INIT: version 2.88 booting hwclock: can't open '/dev/misc/rtc': No such file or directory Mon Apr 20 03:50:24 UTC 2020 hwclock: can't open '/dev/misc/rtc': No such file or directory INIT: Entering runlevel: 5 Configuring network interfaces... [ 5.169549] cpsw 4a100000.ethernet: initializing cpsw version 1.12 (0) [ 5.179936] Atheros 8031 ethernet 4a101000.mdio:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL) udhcpc: started, v1.29.3 udhcpc: sending discover udhcpc: sending discover udhcpc: sending discover udhcpc: no lease, forking to background ifconfig: SIOCGIFFLAGS: No such device ifconfig: SIOCSIFADDR: No such device done. hwclock: can't open '/dev/misc/rtc': No such file or directory Starting syslogd/klogd: done _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm /dev/ttyS0 Arago 2019.11 am335x-evm /dev/ttyS0 am335x-evm login: root root@am335x-evm:~#