# # This file defines the modules included in $(MAKECONFIG) config # # Modules are split into, # - Use-cases specified in uc_cfg.mk # - Other system config/feature, specified in this file # # Any specific overrides are also specified in this file # Example, for TDA3x SoC EVE2/3/4 are not present and hence force marked as , i.e disabled # # # Additional config options # # # CPUs to included in build # PROC_IPU1_0_INCLUDE=yes PROC_IPU1_1_INCLUDE=yes PROC_DSP1_INCLUDE=yes PROC_DSP2_INCLUDE=no PROC_EVE1_INCLUDE=yes VSDK_BOARD_TYPE=TDA3XX_EVM #Enable SMP on IPU1 IPU1_SMP_BIOS=no # Supported values: DDR_MEM_512M DDR_MEM_128M DDR_MEM=DDR_MEM_512M # Supported values: ipu1_0 ipu1_1 none NDK_PROC_TO_USE=none #Used to control TFDTP stack (supported only when NDK_PROC_TO_USE = ipu1_1) NSP_TFDTP_INCLUDE=yes # Supported values: ipu1_0 none FATFS_PROC_TO_USE=ipu1_0 # # Used to control building of algorithm source. # By default algorithm source not included in Vision SDK # BUILD_ALGORITHMS=no # # Applies profile to all cores # # Supported profiles: release debug #PROFILE=debug PROFILE ?= release PROFILE_ipu1_0 ?= $(PROFILE) PROFILE_ipu1_1 ?= $(PROFILE) PROFILE_c66xdsp_1 ?= $(PROFILE) PROFILE_c66xdsp_2 ?= $(PROFILE) PROFILE_arp32_1 ?= $(PROFILE) DSS_INCLUDE=yes CAL_INCLUDE=yes ISS_INCLUDE=yes ISS_ENABLE_DEBUG_TAPS=no WDR_LDC_INCLUDE=yes RTI_INCLUDE=no # # EMIF ECC and Freedom from Interference (FFI) are clubbed together as they # involve consolidated memory map changes # ECC_FFI_INCLUDE=yes is not supported for DDR_MEM_128M # If ECC_FFI_INCLUDE is set to no - memory map will match older versions. # Firewall configuration and DSP XMC configuration is enabled/disabled using this # flag # Vision SDK does not enable EMIF ECC but expects SBL to enable it. # Vision SDK sets up ECC error handlers irrespective of value of ECC_FFI_INCLUDE. # ECC_FFI_INCLUDE=no # # DCC is integrated in a way that requires ESM. # Both modules are, therefore, clubbed together # These are present only in TDA3XX # Setting this to "no" only disables usage of these modules # Source files are always enabled in build for TDA3XX # DCC_ESM_INCLUDE=no # # Enable below macro to enable DCAN integration into Vision SDK. # DCAN_INCLUDE=yes # # Enable below macro to enable OPENVX into Vision SDK # OPENVX_INCLUDE=no CIO_REDIRECT=yes # Fast boot usecase is currently supported only for tda3x FAST_BOOT_INCLUDE=no # Fast Boot for 3D Surround View on TDA3XX SRV_FAST_BOOT_INCLUDE=no ifeq ($(SRV_FAST_BOOT_INCLUDE), yes) PROC_EVE1_INCLUDE=no PROC_IPU1_1_INCLUDE=no endif CPU_IDLE_ENABLED=yes # # Enable below macro to view the bandwidth used by different IPs in the device # as a graphical plot on the display screen. # DATA_VIS_INCLUDE=no HS_DEVICE=no ifeq ($(DDR_MEM), DDR_MEM_128M) PROC_DSP2_INCLUDE=no PROC_EVE1_INCLUDE=no ECC_FFI_INCLUDE=no endif ifeq ($(FAST_BOOT_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(SRV_FAST_BOOT_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(ECC_FFI_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(RTI_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(HS_DEVICE), yes) OPENVX_INCLUDE=no endif ifeq ($(IPU1_SMP_BIOS), yes) #OPENVX is not tested with SMP OPENVX_INCLUDE=no endif # #Flag for task profiling # ENABLE_TASK_PROFILE_UTIL=yes include $($(MAKEAPPNAME)_PATH)/configs/$(MAKECONFIG)/uc_cfg.mk # # This file defines the modules included in $(MAKECONFIG) config # # Modules are split into, # - Use-cases specified in uc_cfg.mk # - Other system config/feature, specified in this file # # Any specific overrides are also specified in this file # Example, for TDA3x SoC EVE2/3/4 are not present and hence force marked as , i.e disabled # # # Additional config options # # # CPUs to included in build # PROC_IPU1_0_INCLUDE=yes PROC_IPU1_1_INCLUDE=no PROC_DSP1_INCLUDE=yes PROC_DSP2_INCLUDE=no PROC_EVE1_INCLUDE=yes VSDK_BOARD_TYPE=TDA3XX_EVM #Enable SMP on IPU1 IPU1_SMP_BIOS=no # Supported values: DDR_MEM_512M DDR_MEM_128M DDR_MEM=DDR_MEM_512M # Supported values: ipu1_0 ipu1_1 none NDK_PROC_TO_USE=ipu1_1 #Used to control TFDTP stack (supported only when NDK_PROC_TO_USE = ipu1_1) NSP_TFDTP_INCLUDE=yes # Supported values: ipu1_0 none FATFS_PROC_TO_USE=ipu1_0 # # Used to control building of algorithm source. # By default algorithm source not included in Vision SDK # BUILD_ALGORITHMS=no # # Applies profile to all cores # # Supported profiles: release debug #PROFILE=debug PROFILE ?= release PROFILE_ipu1_0 ?= $(PROFILE) PROFILE_ipu1_1 ?= $(PROFILE) PROFILE_c66xdsp_1 ?= $(PROFILE) PROFILE_c66xdsp_2 ?= $(PROFILE) PROFILE_arp32_1 ?= $(PROFILE) DSS_INCLUDE=yes CAL_INCLUDE=yes ISS_INCLUDE=yes ISS_ENABLE_DEBUG_TAPS=no WDR_LDC_INCLUDE=yes RTI_INCLUDE=no # # EMIF ECC and Freedom from Interference (FFI) are clubbed together as they # involve consolidated memory map changes # ECC_FFI_INCLUDE=yes is not supported for DDR_MEM_128M # If ECC_FFI_INCLUDE is set to no - memory map will match older versions. # Firewall configuration and DSP XMC configuration is enabled/disabled using this # flag # Vision SDK does not enable EMIF ECC but expects SBL to enable it. # Vision SDK sets up ECC error handlers irrespective of value of ECC_FFI_INCLUDE. # ECC_FFI_INCLUDE=no # # DCC is integrated in a way that requires ESM. # Both modules are, therefore, clubbed together # These are present only in TDA3XX # Setting this to "no" only disables usage of these modules # Source files are always enabled in build for TDA3XX # DCC_ESM_INCLUDE=no # # Enable below macro to enable DCAN integration into Vision SDK. # DCAN_INCLUDE=yes # # Enable below macro to enable OPENVX into Vision SDK # OPENVX_INCLUDE=no CIO_REDIRECT=yes # Fast boot usecase is currently supported only for tda3x FAST_BOOT_INCLUDE=no # Fast Boot for 3D Surround View on TDA3XX SRV_FAST_BOOT_INCLUDE=no ifeq ($(SRV_FAST_BOOT_INCLUDE), yes) PROC_EVE1_INCLUDE=no PROC_IPU1_1_INCLUDE=no endif CPU_IDLE_ENABLED=yes # # Enable below macro to view the bandwidth used by different IPs in the device # as a graphical plot on the display screen. # DATA_VIS_INCLUDE=no HS_DEVICE=no ifeq ($(DDR_MEM), DDR_MEM_128M) PROC_DSP2_INCLUDE=no PROC_EVE1_INCLUDE=no ECC_FFI_INCLUDE=no endif ifeq ($(FAST_BOOT_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(SRV_FAST_BOOT_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(ECC_FFI_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(RTI_INCLUDE), yes) OPENVX_INCLUDE=no endif ifeq ($(HS_DEVICE), yes) OPENVX_INCLUDE=no endif ifeq ($(IPU1_SMP_BIOS), yes) #OPENVX is not tested with SMP OPENVX_INCLUDE=no endif # #Flag for task profiling # ENABLE_TASK_PROFILE_UTIL=yes include $($(MAKEAPPNAME)_PATH)/configs/$(MAKECONFIG)/uc_cfg.mk