U-Boot SPL 2013.01.01-dirty (Feb 20 2013 - 11:43:00) OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2013.01.01-dirty (Feb 20 2013 - 11:43:00) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled NAND: No NAND device found!!! 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 *** Warning - readenv() failed, using default environment musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 Net: cpsw, usb_ether Hit any key to stop autoboot: 1 [08][08][08] 0 mmc0 is current device SD/MMC found on device 0 reading uEnv.txt 630 bytes read in 3 ms (205.1 KiB/s) Loaded environment from uEnv.txt Importing environment from mmc ... reading zImage 2727672 bytes read in 311 ms (8.4 MiB/s) Booting from mmc ... Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Initializing cgroup subsys cpuset [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Linux version 3.2.33-psp26.1 (daniele@ubuntu) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #1 Wed Feb 20 12:26:33 CET 2013 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait fixrtc [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] allocated 1048576 bytes of page_cgroup [ 0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 251024k/251024k available, 11120k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc06d4000 (6960 kB) [ 0.000000] .init : 0xc06d4000 - 0xc0713000 ( 252 kB) [ 0.000000] .data : 0xc0714000 - 0xc075dbe0 ( 295 kB) [ 0.000000] .bss : 0xc075dc04 - 0xc079fa1c ( 264 kB) [ 0.000000] NR_IRQS:410 nr_irqs:410 410 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000183] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320) [ 0.048339] pid_max: default: 32768 minimum: 301 [ 0.048492] Security Framework initialized [ 0.048553] AppArmor: AppArmor initialized [ 0.048614] Mount-cache hash table entries: 512 [ 0.049072] Initializing cgroup subsys cpuacct [ 0.049102] Initializing cgroup subsys memory [ 0.049163] Initializing cgroup subsys devices [ 0.049163] Initializing cgroup subsys freezer [ 0.049194] Initializing cgroup subsys blkio [ 0.049224] Initializing cgroup subsys perf_event [ 0.049316] CPU: Testing write buffer coherency: ok [ 0.050384] devtmpfs: initialized [ 0.071014] omap_hwmod: gfx: failed to hardreset [ 0.087738] omap_hwmod: pruss: failed to hardreset [ 0.088623] print_constraints: dummy: [ 0.088897] NET: Registered protocol family 16 [ 0.090179] OMAP GPIO hardware version 0.1 [ 0.091461] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.092956] omap_i2c.1: alias fck already exists [ 0.093414] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.093627] omap2_mcspi.1: alias fck already exists [ 0.093750] omap2_mcspi.2: alias fck already exists [ 0.093841] omap_init_sham: platform not supported [ 0.093872] omap_init_aes: platform not supported [ 0.093963] edma.0: alias fck already exists [ 0.093994] edma.0: alias fck already exists [ 0.093994] edma.0: alias fck already exists [ 0.094085] cape: pcm register [ 0.104034] bio: create slab at 0 [ 0.105621] SCSI subsystem initialized [ 0.106628] usbcore: registered new interface driver usbfs [ 0.106781] usbcore: registered new interface driver hub [ 0.106994] usbcore: registered new device driver usb [ 0.107330] registerd cppi-dma Intr @ IRQ 17 [ 0.107330] Cppi41 Init Done Qmgr-base(d083a000) dma-base(d0838000) [ 0.107360] Cppi41 Init Done [ 0.107391] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.107543] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.108123] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.109497] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.111724] print_constraints: VRTC: [ 0.113128] print_constraints: VIO: at 1500 mV [ 0.115386] print_constraints: VDD1: 600 <--> 1500 mV at 1200 mV normal [ 0.117645] print_constraints: VDD2: 600 <--> 1500 mV at 1100 mV normal [ 0.118591] print_constraints: VDD3: 5000 mV [ 0.119934] print_constraints: VDIG1: at 1800 mV [ 0.121307] print_constraints: VDIG2: at 1800 mV [ 0.122680] print_constraints: VPLL: at 1800 mV [ 0.124053] print_constraints: VDAC: at 1800 mV [ 0.125396] print_constraints: VAUX1: at 1800 mV [ 0.126770] print_constraints: VAUX2: at 3300 mV [ 0.128143] print_constraints: VAUX33: at 3300 mV [ 0.129516] print_constraints: VMMC: at 3300 mV [ 0.129852] tps65910 1-002d: No interrupt support, no core IRQ [ 0.130493] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.131164] NetLabel: Initializing [ 0.131164] NetLabel: domain hash size = 128 [ 0.131195] NetLabel: protocols = UNLABELED CIPSOv4 [ 0.131256] NetLabel: unlabeled traffic allowed by default [ 0.131317] Switching to clocksource gp timer [ 0.131561] AppArmor: AppArmor Filesystem Enabled [ 0.144012] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.144226] musb-hdrc musb-hdrc.0: dma type: dma-cppi41 [ 0.144409] MUSB0 controller's USBSS revision = 4ea20800 [ 0.145263] musb-hdrc musb-hdrc.0: USB OTG mode controller at d081c000 using DMA, IRQ 18 [ 0.145599] musb-hdrc musb-hdrc.1: dma type: dma-cppi41 [ 0.145782] MUSB1 controller's USBSS revision = 4ea20800 [ 0.146240] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.146362] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.146514] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.146514] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.146545] usb usb1: Product: MUSB HDRC host driver [ 0.146575] usb usb1: Manufacturer: Linux 3.2.33-psp26.1 musb-hcd [ 0.146575] usb usb1: SerialNumber: musb-hdrc.1 [ 0.147369] hub 1-0:1.0: USB hub found [ 0.147399] hub 1-0:1.0: 1 port detected [ 0.147949] musb-hdrc musb-hdrc.1: USB Host mode controller at d081e800 using DMA, IRQ 19 [ 0.148468] NET: Registered protocol family 2 [ 0.148834] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.149810] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.150024] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.150146] TCP: Hash tables configured (established 8192 bind 8192) [ 0.150177] TCP reno registered [ 0.150177] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.150207] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.150604] NET: Registered protocol family 1 [ 0.151031] RPC: Registered named UNIX socket transport module. [ 0.151062] RPC: Registered udp transport module. [ 0.151062] RPC: Registered tcp transport module. [ 0.151092] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.153442] audit: initializing netlink socket (disabled) [ 0.153503] type=2000 audit(0.150:1): initialized [ 0.354064] VFS: Disk quotas dquot_6.5.2 [ 0.354187] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.356018] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.356079] fuse init (API version 7.17) [ 0.356842] Btrfs loaded [ 0.356872] msgmni has been set to 490 [ 0.358245] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252) [ 0.358398] io scheduler noop registered [ 0.358398] io scheduler deadline registered [ 0.358489] io scheduler cfq registered (default) [ 0.359802] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.361145] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 1.135833] console [ttyO0] enabled [ 1.140197] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 1.148101] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 1.155944] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 1.163818] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 1.171600] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 1.187957] brd: module loaded [ 1.195587] loop: module loaded [ 1.199005] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.261962] No daughter card found [ 1.265594] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.280914] Board config.name: A335X_SK1.2B30124P190929SKU#00FFFFFFFFFFFFFFFFFFFFFFFFFF [ 1.289367] Board name: A335X_SK [ 1.292785] Board version: 1.2B [ 1.296112] SKU: SKU#00 [ 1.298675] The board is a AM335x Low Cost EVM. [ 1.304412] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 1.309478] Registering NAND on CS0 [ 1.314910] CAN device driver interface [ 1.318969] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.371978] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.378509] davinci_mdio davinci_mdio.0: detected phy mask fffffffc [ 1.386810] davinci_mdio.0: probed [ 1.390411] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.397888] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown [ 1.405426] PPP generic driver version 2.4.2 [ 1.410247] PPP BSD Compression module registered [ 1.415252] PPP Deflate Compression module registered [ 1.420684] usbcore: registered new interface driver zd1201 [ 1.426696] usbcore: registered new interface driver cdc_ether [ 1.432952] usbcore: registered new interface driver rndis_host [ 1.439239] cdc_ncm: 04-Aug-2011 [ 1.442749] usbcore: registered new interface driver cdc_ncm [ 1.448883] usbcore: registered new interface driver cdc_acm [ 1.454895] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters [ 1.463439] usbcore: registered new interface driver cdc_wdm [ 1.469421] Initializing USB Mass Storage driver... [ 1.474700] usbcore: registered new interface driver usb-storage [ 1.481048] USB Mass Storage support registered. [ 1.486053] usbcore: registered new interface driver libusual [ 1.492340] usbcore: registered new interface driver usbserial [ 1.498535] USB Serial support registered for generic [ 1.503967] usbcore: registered new interface driver usbserial_generic [ 1.510864] usbserial: USB Serial Driver core [ 1.515594] gadget: using random self ethernet address [ 1.521118] gadget: using random host ethernet address [ 1.527770] usb0: MAC 6e:c6:19:6a:95:0b [ 1.531829] usb0: HOST MAC 3e:ac:16:c8:12:26 [ 1.536437] gadget: Ethernet Gadget, version: Memorial Day 2008 [ 1.542816] gadget: g_ether ready [ 1.546417] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 1.552124] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 1.560058] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 1.567260] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 1.574890] usb usb2: Product: MUSB HDRC host driver [ 1.580139] usb usb2: Manufacturer: Linux 3.2.33-psp26.1 musb-hcd [ 1.586578] usb usb2: SerialNumber: musb-hdrc.0 [ 1.592224] hub 2-0:1.0: USB hub found [ 1.596160] hub 2-0:1.0: 1 port detected [ 1.601318] mousedev: PS/2 mouse device common for all mice [ 1.608337] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.615112] omap_rtc: already running [ 1.619049] i2c /dev entries driver [ 1.623016] Linux media interface: v0.10 [ 1.627319] lirc_dev: IR Remote Control driver registered, major 249 [ 1.634124] Linux video capture interface: v2.00 [ 1.639312] Driver for 1-wire Dallas network protocol. [ 1.645812] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.656768] cpuidle: using governor ladder [ 1.661224] cpuidle: using governor menu [ 1.666076] usbcore: registered new interface driver usbhid [ 1.671905] usbhid: USB HID core driver [ 1.676849] usbcore: registered new interface driver snd-usb-6fire [ 1.683898] ALSA device list: [ 1.686981] No soundcards found. [ 1.691772] TCP cubic registered [ 1.695404] NET: Registered protocol family 10 [ 1.703521] NET: Registered protocol family 17 [ 1.708374] can: controller area network core (rev 20090105 abi 8) [ 1.714996] NET: Registered protocol family 29 [ 1.719635] can: raw protocol (rev 20090105) [ 1.724151] Registering the dns_resolver key type [ 1.729125] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.737152] ThumbEE CPU extension supported. [ 1.741668] mux: Failed to setup hwmod io irq -22 [ 1.747344] Power Management for AM33XX family [ 1.756774] registered taskstats version 1 [ 1.761383] Detected MACID=d4:94:a1:87:dd:3b [ 1.768798] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:02:27 UTC (946684947) [ 1.778381] Waiting for root device /dev/mmcblk0p2... [ 6.072631] Unable to handle kernel paging request at virtual address ffff8d17 [ 6.080169] pgd = c0004000 [ 6.082977] [ffff8d17] *pgd=8fffe821, *pte=00000000, *ppte=00000000 [ 6.089538] Internal error: Oops: 801 [#1] [ 6.093811] Modules linked in: [ 6.097015] CPU: 0 Not tainted (3.2.33-psp26.1 #1) [ 6.102386] PC is at get_next_timer_interrupt+0x4/0x23c [ 6.107849] LR is at tick_nohz_stop_sched_tick+0x324/0x35c [ 6.113586] pc : [] lr : [] psr: 60000093 [ 6.113586] sp : c0715f38 ip : c0715f38 fp : c0715f94 [ 6.125549] r10: 00000000 r9 : c071c700 r8 : ffff8d2f [ 6.131011] r7 : c0738b68 r6 : c0781f58 r5 : c07820c0 r4 : 00000162 [ 6.137817] r3 : c07378f0 r2 : 69ccd980 r1 : 00002e6a r0 : ffff8d2f [ 6.144653] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel [ 6.152374] Control: 10c5387d Table: 80004019 DAC: 00000015 [ 6.158355] Process swapper (pid: 0, stack limit = 0xc07142f0) [ 6.164459] Stack: (0xc0715f38 to 0xc0716000) [ 6.169006] 5f20: 00000000 c001eda8 [ 6.177520] 5f40: 20000013 00000001 69ccd980 40000013 69cd6ce3 00000001 c8300000 00002e6a [ 6.186065] 5f60: 69cd6ce3 00000001 c071a5bc c0714000 c075dd04 c071a5c8 c071a5bc 80004059 [ 6.194610] 5f80: 413fc082 00000000 c0715fb4 c0715f98 c000e0e4 c005eb68 00000000 c07161a4 [ 6.203155] 5fa0: c0705e0c c09a0900 c0715fc4 c0715fb8 c04f55a4 c000e0c4 c0715ff4 c0715fc8 [ 6.211700] 5fc0: c06d4798 c04f5550 c06d41a8 00000000 00000000 c0705e0c 00000000 10c53c7d [ 6.220245] 5fe0: c0716084 c0705e08 00000000 c0715ff8 80008040 c06d4504 00000000 00000000 [ 6.228759] Backtrace: [ 6.231323] [] (tick_nohz_stop_sched_tick+0x0/0x35c) from [] (cpu_idle+0x2c/0x9c) [ 6.240966] [] (cpu_idle+0x0/0x9c) from [] (rest_init+0x60/0x78) [ 6.249053] r6:c09a0900 r5:c0705e0c r4:c07161a4 r3:00000000 [ 6.254974] [] (rest_init+0x0/0x78) from [] (start_kernel+0x2a0/0x2f8) [ 6.263610] [] (start_kernel+0x0/0x2f8) from [<80008040>] (0x80008040) [ 6.271331] r6:c0705e08 r5:c0716084 r4:10c53c7d [ 6.276184] Code: b912cce9 f88a6501 16526530 1f42a6bd (0808a694) [ 6.282592] ---[ end trace 87eb690f9cbaa350 ]--- [ 6.287414] Kernel panic - not syncing: Attempted to kill the idle task! [ 6.294403] Backtrace: [ 6.296997] [] (dump_backtrace+0x0/0x110) from [] (dump_stack+0x18/0x1c) [ 6.305816] r6:00000001 r5:0000000b r4:c075fee8 r3:c07378d0 [ 6.311737] [] (dump_stack+0x0/0x1c) from [] (panic+0x5c/0x190) [ 6.319763] [] (panic+0x0/0x190) from [] (do_exit+0xa8/0x624) [ 6.327606] r3:c0714000 r2:00000000 r1:00000000 r0:c06412d5 [ 6.333526] r7:c004403e [ 6.336181] [] (do_exit+0x0/0x624) from [] (die+0x2c8/0x304) [ 6.343902] r7:c004403e [ 6.346557] [] (die+0x0/0x304) from [] (__do_kernel_fault.part.3+0x5c/0x7c) [ 6.355682] [] (__do_kernel_fault.part.3+0x0/0x7c) from [] (do_bad_area+0x7c/0x88) [ 6.365386] r7:c073b708 r3:c0715ef0 [ 6.369140] [] (do_bad_area+0x0/0x88) from [] (do_alignment+0x56c/0x6e8) [ 6.377960] r7:c0715ef0 r6:ffff8d17 r5:00000000 r4:0808a694 [ 6.383911] [] (do_alignment+0x0/0x6e8) from [] (do_DataAbort+0x3c/0xa0) [ 6.392730] [] (do_DataAbort+0x0/0xa0) from [] (__dabt_svc+0x38/0x60) [ 6.401275] Exception stack(0xc0715ef0 to 0xc0715f38) [ 6.406555] 5ee0: ffff8d2f 00002e6a 69ccd980 c07378f0 [ 6.415130] 5f00: 00000162 c07820c0 c0781f58 c0738b68 ffff8d2f c071c700 00000000 c0715f94 [ 6.423675] 5f20: c0715f38 c0715f38 c005ee80 c004403c 60000093 ffffffff [ 6.430572] r7:c0715f24 r6:ffffffff r5:60000093 r4:c004403c [ 6.436523] [] (tick_nohz_stop_sched_tick+0x0/0x35c) from [] (cpu_idle+0x2c/0x9c) [ 6.446197] [] (cpu_idle+0x0/0x9c) from [] (rest_init+0x60/0x78) [ 6.454284] r6:c09a0900 r5:c0705e0c r4:c07161a4 r3:00000000 [ 6.460205] [] (rest_init+0x0/0x78) from [] (start_kernel+0x2a0/0x2f8) [ 6.468872] [] (start_kernel+0x0/0x2f8) from [<80008040>] (0x80008040) [ 6.476593] r6:c0705e08 r5:c0716084 r4:10c53c7d