U-Boot SPL 2016.05 (Oct 23 2019 - 18:08:17) DRA752-GP ES2.0 Trying to boot from MMC2_2 reading single-stage-boot.dtb spl_load_image_fat_os: error reading image single-stage-boot.dtb, err - -1 reading u-boot.img reading u-boot.img U-Boot 2016.05 (Oct 23 2019 - 18:08:17 +0800) CPU : DRA752-GP ES2.0 Board: D3 TDA2x I2C: ready DRAM: i2c_read (addr phase): pads on bus probably not configured (status=0x10) 2 GiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 i2c_write: pads on bus probably not configured (status=0x10) tps65903x: could not set LDO1 voltage. i2c_write: pads on bus probably not configured (status=0x10) tps65903x: could not set LDO1 voltage. Card did not respond to voltage select! ** Bad device mmc 0 ** Using default environment i2c_write: pads on bus probably not configured (status=0x10) i2c_write: pads on bus probably not configured (status=0x10) tps65903x: could not turn CLK32KGAUDIO on: err = 2 i2c_read (addr phase): pads on bus probably not configured (status=0x10) Unable to read Board-ID i2c_read (addr phase): pads on bus probably not configured (status=0x10) i2c_read (addr phase): pads on bus probably not configured (status=0x10) Unable to read Baseboard-ID i2c_probe: pads on bus probably not configured (status=0x10) Unable to read Expansion-ID SCSI: 0 device not found ERROR: scsi device not found at drivers/block/disk-uclass.c:43/scsi_init() Net: not set. Validating first E-fuse MAC i2c_read (addr phase): pads on bus probably not configured (status=0x10) i2c_read (addr phase): pads on bus probably not configured (status=0x10) Could not get PHY for cpsw: addr 2 cpsw Hit any key to stop autoboot: 0 i2c_write: pads on bus probably not configured (status=0x10) tps65903x: could not set LDO1 voltage. Card did not respond to voltage select! i2c_write: pads on bus probably not configured (status=0x10) tps65903x: could not set LDO1 voltage. Card did not respond to voltage select! i2c_write: pads on bus probably not configured (status=0x10) tps65903x: could not set LDO1 voltage. Card did not respond to voltage select! Tuning failed, dropping HS200 mode. dropping DDR52 mode. switch to partitions #0, OK mmc1(part 0) is current device Tuning failed, dropping HS200 mode. dropping DDR52 mode. mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value Booting from eMMC ... Wrong Image Format for bootm command ERROR: can't get kernel image! => mmc list OMAP SD/MMC: 0 OMAP SD/MMC: 1 (eMMC) => mmc dev 1 Tuning failed, dropping HS200 mode. dropping DDR52 mode. switch to partitions #0, OK mmc1(part 0) is current device => mmc part Partition Map for MMC device 1 -- Partition Type: DOS Part Start Sector Num Sectors UUID Type 1 63 144522 00000000-01 0c Boot 2 144585 7405965 00000000-02 83 =>