Welcome to minicom 2.7.1 OPTIONS: I18n Compiled on Aug 13 2017, 15:25:34. Port /dev/ttyUSB0, 15:28:27 Press CTRL-A Z for help on special keys � U-Boot SPL 2019.01-g66126341c8 (Oct 24 2019 - 03:52:25 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.8.0-v2019.08 (Terrific Llama') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Remoteproc 2 started successfully ** File not found /lib/firmware/j7-mcu-r5f0_0-fw ** Starting ATF on ARM64 core... NOTICE: BL31: v2.1(release):ti2019.02-rc4 NOTICE: BL31: Built : 03:52:00, Oct 24 2019 I/TC: I/TC: OP-TEE version: ti2019.02-89-ge5a8779-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Thu Oct 24 03:52:22 UTC 2019 aarch64 I/TC: Initialized U-Boot SPL 2019.01-g66126341c8 (Oct 24 2019 - 03:52:45 +0000) Detected: J7X-BASE-CPB rev E2 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 ti_sci_power_domain_on: get_device(91) failed (-19) U-Boot 2019.01-g66126341c8 (Oct 24 2019 - 03:52:45 +0000) SoC: J721E PG 1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM1-SOM rev E2 DRAM: 4 GiB Flash: 0 Bytes MMC: ti_sci_power_domain_on: get_device(91) failed (-19) sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E2 Detected: J7X-VSC8514-ETH rev E2 Net: eth0: ethernet@046000000 Hit any key to stop autobo 0 =>env default -f -a ## Resetting to default environment =>saveenv Saving Environment to MMC... Writing to redundant MMC(0)... OK =>reset resetting ...� U-Boot SPL 2019.01-g66126341c8 (Oct 24 2019 - 03:52:25 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.8.0-v2019.08 (Terrific Llama') Trying to boot from MMC2 Loading Environment from MMC... *** Warning - No MMC card found, using default environment Remoteproc 2 started successfully ** File not found /lib/firmware/j7-mcu-r5f0_0-fw ** Starting ATF on ARM64 core... NOTICE: BL31: v2.1(release):ti2019.02-rc4 NOTICE: BL31: Built : 03:52:00, Oct 24 2019 I/TC: I/TC: OP-TEE version: ti2019.02-89-ge5a8779-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Thu Oct 24 03:52:22 UTC 2019 aarch64 I/TC: Initialized U-Boot SPL 2019.01-g66126341c8 (Oct 24 2019 - 03:52:45 +0000) Detected: J7X-BASE-CPB rev E2 Detected: J7X-VSC8514-ETH rev E2 Trying to boot from MMC2 ti_sci_power_domain_on: get_device(91) failed (-19) U-Boot 2019.01-g66126341c8 (Oct 24 2019 - 03:52:45 +0000) SoC: J721E PG 1.0 Model: Texas Instruments K3 J721E SoC Board: J721EX-PM1-SOM rev E2 DRAM: 4 GiB Flash: 0 Bytes MMC: ti_sci_power_domain_on: get_device(91) failed (-19) sdhci@4f80000: 0, sdhci@4fb0000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Detected: J7X-BASE-CPB rev E2 Detected: J7X-VSC8514-ETH rev E2 Net: Warning: ethernet@046000000 using MAC address from ROM eth0: ethernet@046000000 Hit any key to stop autobo 0 =>setenv serverip 192.168.1.100 =>setenv nfs_root /home/aneesh/ti-processor-sdk-linux-automotive-j7-evm-06_01_00_05/targetNFS =>setenv name_kern Image-j7-evm.bin =>setenv bootcmd 'run findfdt; run envboot; run setup_${kern_boot}; run init_${rootfs_boot}; run get_kern_${kern_boot}; run get_fdt_${kern_boot}; run get_overlay_${kern_boot}; run run_kern' =>setenv init_net 'run args_all args_net; setenv autoload no; dhcp' =>setenv args_net 'setenv bootargs ${optargs} rootfstype=nfs root=/dev/nfs rw nfsroot=${serverip}:${nfs_root},${nfs_options} ip=dhcp' =>setenv get_kern_net 'tftp ${loadaddr} ${name_kern}' =>setenv get_fdt_net 'tftp ${fdtaddr} ${name_fdt}' =>setenv get_overlay_net 'fdt address ${fdtaddr};fdt resize 0x100000;for overlay in ${overlay_files};do;tftp ${overlayaddr} ${overlay};fdt apply ${overlayaddr}; done' =>setenv nfs_options 'nolock,v3,tcp,rsize=4096,wsize=4096' =>setenv setup_mmc '' =>setenv setup_net 'setenv autoload no; dhcp' =>setenv kern_boot net =>setenv rootfs_boot net =>saveenv Saving Environment to MMC... Writing to MMC(0)... OK =>boot switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 ** Unable to read file boot.scr ** 15 bytes read in 1 ms (14.6 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... am65_cpsw_start end error am65_cpsw_start end error am65_cpsw_start end error am65_cpsw_start end error libfdt fdt_check_header(): FDT_ERR_BADMAGIC No FDT memory address configured. Please configure the FDT address via "fdt addr
" command. Aborting! Bad Linux ARM64 Image magic! => nfs link up on port 1, speed 1000, full duplex *** ERROR: `ipaddr' not set => link up on port 1, speed 1000, full duplex *** ERROR: `ipaddr' not set => link up on port 1, speed 1000, full duplex *** ERROR: `ipaddr' not set => dhcp link up on port 1, speed 1000, full duplex BOOTP broadcast 1 BOOTP broadcast 2 BOOTP broadcast 3 BOOTP broadcast 4 BOOTP broadcast 5 BOOTP broadcast 6 BOOTP broadcast 7 BOOTP broadcast 8 BOOTP broadcast 9 BOOTP broadcast 10 BOOTP broadcast 11 BOOTP broadcast 12 BOOTP broadcast 13 BOOTP broadcast 14 BOOTP broadcast 15 BOOTP broadcast 16