#include "ezdsp5535.h" #include #include #include "ezdsp5535_led.h" #include "registers.h" #include "interrupts.h" Uint16 led = FALSE; void GPIO_IntrTest(void); interrupt void INT_GPIO(void); void gpio_output_pin_toggle(void); void main(void) { EZDSP5535_LED_init( ); EZDSP5535_XF_toggle(); /*CALL THE FUNCTION!!!!!*/ GPIO_IntrTest(); gpio_output_pin_toggle(); printf("test....\n"); while(1) {} }//ENDMAIN /*THE FUNCTION FOR BLINKING THE LED*/ void gpio_output_pin_toggle(void) { if (led) { EZDSP5535_LED_off(1); led=~led; } else { EZDSP5535_LED_on(1); led=~led; } //printf("TOGGLE PIN!\n"); } /*THE FUNCTION FOR SETTING THE INTERRUPT REGISTERS*/ void GPIO_IntrTest(void) { IODIR1|=(0<