7-sdk m335x-evm:/media/sdb1# arm-arago-linux-gnueabi-readelf -l hellogl_es2_05-07 Elf file type is EXEC (Executable file) Entry point 0xc6d0 There are 8 program headers, starting at offset 52 Program Headers: Type Offset VirtAddr PhysAddr FileSiz MemSiz Flg Align EXIDX 0x00dbbc 0x00015bbc 0x00015bbc 0x00368 0x00368 R 0x4 PHDR 0x000034 0x00008034 0x00008034 0x00100 0x00100 R E 0x4 INTERP 0x000134 0x00008134 0x00008134 0x00013 0x00013 R 0x1 [Requesting program interpreter: /lib/ld-linux.so.3] LOAD 0x000000 0x00008000 0x00008000 0x0df24 0x0df24 R E 0x8000 LOAD 0x00e000 0x0001e000 0x0001e000 0x004c8 0x0057c RW 0x8000 DYNAMIC 0x00e010 0x0001e010 0x0001e010 0x00150 0x00150 RW 0x4 NOTE 0x000148 0x00008148 0x00008148 0x00020 0x00020 R 0x4 GNU_STACK 0x000000 0x00000000 0x00000000 0x00000 0x00000 RW 0x4 Section to Segment mapping: Segment Sections... 00 .ARM.exidx 01 02 .interp 03 .interp .note.ABI-tag .hash .dynsym .dynstr .gnu.version .gnu.version_r .rel.dyn .rel.plt .init .plt .text .fini .rodata .ARM.extab .ARM.exidx 04 .init_array .fini_array .jcr .dynamic .got .data .bss 05 .dynamic 06 .note.ABI-tag 07 root@am335x-evm:/media/sdb1#