U-Boot SPL 2019.01 (Jul 20 2021 - 14:43:32 +0530) Trying to boot from MMC1 U-Boot 2019.01 (Jul 20 2021 - 14:43:32 +0530) CPU : AM335X-GP rev 2.1 Model: TI AM335x EVM DRAM: 1 GiB NAND: 0 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Loading Environment from FAT... *** Warning - bad CRC, using default environment not set. Validating first E-fuse MAC Net: eth0: ethernet@4a100000 Hit any key to stop autoboot: 2 1 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Unable to read file boot.scr ** ** Unable to read file uEnv.txt ** switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 4297216 bytes read in 362 ms (11.3 MiB/s) 37407 bytes read in 4 ms (8.9 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff3000, end 8ffff21e ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.94-gbe5389fd85 (madhu@madhu-VirtualBox) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #17 PREEMPT Tue Jul 20 14:58:04 IST 2021 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x EVM [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0xbd000000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon) [ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x434 with crng_init=0 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 260416 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=6e31ec68-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Memory: 975336K/1048576K available (9216K kernel code, 315K rwdata, 2760K rodata, 1024K init, 252K bss, 24088K reserved, 49152K cma-reserved, 212992K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB) [ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0x(ptrval) - 0x(ptrval) (10208 kB) [ 0.000000] .init : 0x(ptrval) - 0x(ptrval) (1024 kB) [ 0.000000] .data : 0x(ptrval) - 0x(ptrval) ( 316 kB) [ 0.000000] .bss : 0x(ptrval) - 0x(ptrval) ( 253 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000022] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000053] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000068] OMAP clocksource: timer1 at 24000000 Hz [ 0.000301] timer_probe: no matching timers found [ 0.000535] Console: colour dummy device 80x30 [ 0.000571] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000581] This ensures that you still see kernel messages. Please [ 0.000590] update your kernel commandline. [ 0.000661] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032) [ 0.118820] pid_max: default: 32768 minimum: 301 [ 0.119100] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.119125] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.120185] CPU: Testing write buffer coherency: ok [ 0.120266] CPU0: Spectre v2: using BPIALL workaround [ 0.121387] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.121597] rcu: Hierarchical SRCU implementation. [ 0.122064] EFI services will not be available. [ 0.124050] devtmpfs: initialized [ 0.134924] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.135417] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.135452] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.140187] pinctrl core: initialized pinctrl subsystem [ 0.141135] DMI not present or invalid. [ 0.141703] NET: Registered protocol family 16 [ 0.144686] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.174107] l4_wkup_cm:clk:0010:0: failed to disable [ 0.241958] cpuidle: using governor ladder [ 0.242013] cpuidle: using governor menu [ 0.249087] OMAP GPIO hardware version 0.1 [ 0.264881] No ATAGs? [ 0.264897] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.285184] edma 49000000.edma: TI EDMA DMA engine driver [ 0.291581] SCSI subsystem initialized [ 0.292284] media: Linux media interface: v0.10 [ 0.292348] videodev: Linux video capture interface: v2.00 [ 0.292472] pps_core: LinuxPPS API ver. 1 registered [ 0.292484] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.292516] PTP clock support registered [ 0.292565] EDAC MC: Ver: 3.0.0 [ 0.293987] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.294823] Advanced Linux Sound Architecture Driver Initialized. [ 0.296372] clocksource: Switched to clocksource timer1 [ 0.308362] NET: Registered protocol family 2 [ 0.309457] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes) [ 0.309505] TCP established hash table entries: 8192 (order: 3, 32768 bytes) [ 0.309618] TCP bind hash table entries: 8192 (order: 3, 32768 bytes) [ 0.309728] TCP: Hash tables configured (established 8192 bind 8192) [ 0.309893] UDP hash table entries: 512 (order: 1, 8192 bytes) [ 0.309934] UDP-Lite hash table entries: 512 (order: 1, 8192 bytes) [ 0.310145] NET: Registered protocol family 1 [ 0.310901] RPC: Registered named UNIX socket transport module. [ 0.310923] RPC: Registered udp transport module. [ 0.310933] RPC: Registered tcp transport module. [ 0.310942] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.312178] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.313992] Initialise system trusted keyrings [ 0.314400] workingset: timestamp_bits=14 max_order=18 bucket_order=4 [ 0.321301] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.322301] NFS: Registering the id_resolver key type [ 0.322356] Key type id_resolver registered [ 0.322368] Key type id_legacy registered [ 0.322426] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.325543] Key type asymmetric registered [ 0.325568] Asymmetric key parser 'x509' registered [ 0.325661] bounce: pool size: 64 pages [ 0.325746] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.325763] io scheduler noop registered [ 0.325774] io scheduler deadline registered [ 0.326099] io scheduler cfq registered (default) [ 0.326116] io scheduler mq-deadline registered [ 0.326127] io scheduler kyber registered [ 0.329041] pinctrl-single 44e10800.pinmux: 142 pins, size 568 [ 0.334034] pwm-backlight backlight: backlight supply power not found, using dummy regulator [ 0.334160] pwm-backlight backlight: Linked as a consumer to regulator.0 [ 0.403808] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.409379] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 1.047730] console [ttyS0] enabled [ 1.052760] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250 [ 1.063024] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 32, base_baud = 3000000) is a 8250 [ 1.074669] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 1.081147] random: fast init done [ 1.084828] random: crng init done [ 1.091000] OF: graph: no port node found in /ocp/lcdc@4830e000 [ 1.098023] OF: graph: no port node found in /ocp/lcdc@4830e000 [ 1.104597] OF: graph: no port node found in /ocp/lcdc@4830e000 [ 1.110664] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 1.117336] [drm] No driver support for vblank timestamp query. [ 1.127215] Console: switching to colour frame buffer device 40x30 [ 1.135035] tilcdc 4830e000.lcdc: fb0: DRM emulated frame buffer device [ 1.142483] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on minor 0 [ 1.166573] brd: module loaded [ 1.178954] loop: module loaded [ 1.186703] libphy: Fixed MDIO Bus: probed [ 1.266476] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.274188] libphy: 4a101000.mdio: probed [ 1.280751] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver TI DP83867 [ 1.289208] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver TI DP83867 [ 1.298730] cpsw 4a100000.ethernet: Detected MACID = 40:2e:71:cd:50:03 [ 1.305462] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.312042] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.317405] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 1.325713] cpsw 4a100000.ethernet: cpsw: Detected MACID = 40:2e:71:cd:50:05 [ 1.334780] i2c /dev entries driver [ 1.341322] cpuidle: enable-method property 'ti,am3352' found operations [ 1.348771] sdhci: Secure Digital Host Controller Interface driver [ 1.354989] sdhci: Copyright(c) Pierre Ossman [ 1.360180] [ 1.360180] [ 1.360180] hey mad inside omap_hsmmc_probe [ 1.368746] omap_hsmmc 48060000.mmc: Linked as a consumer to regulator.6 [ 1.399508] [ 1.399508] [ 1.399508] hey mad inside omap_hsmmc_probe [ 1.408073] omap_hsmmc 481d8000.mmc: Linked as a consumer to regulator.6 [ 1.439715] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.447056] ledtrig-cpu: registered to indicate activity on CPUs [ 1.463949] NET: Registered protocol family 10 [ 1.470832] Segment Routing with IPv6 [ 1.474763] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.481900] NET: Registered protocol family 17 [ 1.487062] Key type dns_resolver registered [ 1.491766] omap_voltage_late_init: Voltage driver support not added [ 1.498330] mmc0: host does not support reading read-only switch, assuming write-enable [ 1.507736] Loading compiled-in X.509 certificates [ 1.517704] mmc0: new high speed SDHC card at address aaaa [ 1.527951] mmc1: new high speed MMC card at address 0001 [ 1.537356] mmcblk0: mmc0:aaaa SC16G 14.8 GiB [ 1.545102] mmcblk1: mmc1:0001 Q2J55L 7.09 GiB [ 1.551351] mmcblk1boot0: mmc1:0001 Q2J55L partition 1 16.0 MiB [ 1.557606] mmcblk0: p1 p2 [ 1.561489] mmcblk1boot1: mmc1:0001 Q2J55L partition 2 16.0 MiB [ 1.568978] mmcblk1rpmb: mmc1:0001 Q2J55L partition 3 4.00 MiB, chardev (244:0) [ 1.578389] mmcblk1: p1 p2 [ 1.582168] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.592791] max9860 2-0010: Linked as a consumer to regulator.3 [ 1.628225] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 400 kHz [ 1.635431] max9860 2-0010: Linked as a consumer to regulator.4 [ 1.643104] asoc-simple-card sound@0: max9860-hifi <-> 4803c000.mcasp mapping ok [ 1.650647] asoc-simple-card sound@0: ASoC: no DMI vendor name! [ 1.660631] asoc-simple-card sound: pcm5102a-hifi <-> 48038000.mcasp mapping ok [ 1.668112] asoc-simple-card sound: ASoC: no source widget found for OUT [ 1.674854] asoc-simple-card sound: ASoC: Failed to add route OUT -> direct -> Headphone Jack [ 1.683458] asoc-simple-card sound: ASoC: no DMI vendor name! [ 1.691618] hctosys: unable to open rtc device (rtc0) [ 1.697624] ALSA device list: [ 1.700624] #0: MAX9860 [ 1.703255] #1: DSP [ 1.818221] EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended [ 1.833296] EXT4-fs (mmcblk0p2): Errors on filesystem, clearing orphan list. [ 1.833296] [ 1.841952] EXT4-fs (mmcblk0p2): recovery complete [ 1.850142] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 1.858413] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 1.876247] devtmpfs: mounted [ 1.881248] Freeing unused kernel memory: 1024K [ 1.886557] Run /sbin/init as init process [ 2.181234] systemd[1]: System time before build time, advancing clock. [ 2.231964] systemd[1]: Configuration file /etc/systemd/system.conf is marked executable. Please remove executable permission bits. Proceeding anyway. [ 2.245750] systemd[1]: Configuration file /etc/systemd/system.conf is marked world-writable. Please remove world writability permission bits. Proceeding anyway. [ 2.269600] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 2.292085] systemd[1]: Detected architecture arm. Welcome to Arago 2019.11! [ 2.350188] systemd[1]: Set hostname to . [ 2.733044] systemd[1]: Configuration file /lib/systemd/system/local-fs.target is marked executable. Please remove executable permission bits. Proceeding anyway. [ 2.748053] systemd[1]: Configuration file /lib/systemd/system/local-fs.target is marked world-writable. Please remove world writability permission bits. Proceeding anyway. [ 2.778815] systemd[1]: Configuration file /lib/systemd/system/swap.target is marked executable. Please remove executable permission bits. Proceeding anyway. [ 2.793175] systemd[1]: Configuration file /lib/systemd/system/swap.target is marked world-writable. Please remove world writability permission bits. Proceeding anyway. [ 2.813012] systemd[1]: Configuration file /lib/systemd/system/umount.target is marked executable. Please remove executable permission bits. Proceeding anyway. [ 2.827549] systemd[1]: Configuration file /lib/systemd/system/umount.target is marked world-writable. Please remove world writability permission bits. Proceeding anyway. [ 2.847254] systemd[1]: Configuration file /lib/systemd/system/systemd-journald.socket is marked executable. Please remove executable permission bits. Proceeding anyway. [ OK ] Listening on Process Core Dump Socket. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ OK ] Created slice system-serial\x2dgetty.slice. [ OK ] Listening on udev Kernel Socket. [ OK ] Reached target Remote File Systems. [ OK ] Listening on Journal Socket. Mounting Kernel Debug File System... [ OK ] Started Forward Password Requests to Wall Directory Watch. [ OK ] Listening on udev Control Socket. Starting udev Coldplug all Devices... [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Listening on initctl Compatibility Named Pipe. Starting Load Kernel Modules... [ OK ] Reached target Paths. [ OK ] Reached target Swap. Mounting Temporary Directory (/tmp)... [ 4.086623] cryptodev: loading out-of-tree module taints kernel. [ OK ] Listening on Network Service Netlink Socket. Starting Remount Root and Kernel File Systems... [ 4.143923] cryptodev: driver 1.9 loaded. [ OK ] Created slice User and Session Slice. [ OK ] Reached target Slices. [ OK ] Listening on Journal Socket (/dev/log). Starting Journal Service... [ 4.262616] usbcore: registered new interface driver usbfs Mounting POSIX Message Queue File System... [ OK ] Created slice system-getty.slice. [ 4.341164] usbcore: registered new interface driver hub [ 4.364482] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) [ 4.383013] usbcore: registered new device driver usb Starting Psplash Boot Screen... [ 4.462104] systemd-journald[81]: Configuration file /etc/systemd/journald.conf is marked executable. Please remove executable permission bits. Proceeding anyway. [ OK ] Mounted Kernel Debug File System. [ 4.529856] usbcore: registered new interface driver ftdi_sio [ 4.535803] usbserial: USB Serial support registered for FTDI USB Serial Device [ 4.544030] systemd-journald[81]: Configuration file /etc/systemd/journald.conf is marked world-writable. Please remove world writability permission bits. Proceeding anyway. [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Started Load Kernel Modules. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Started Psplash Boot Screen. Starting Create Static Device Nodes in /dev... Starting Apply Kernel Variables... Mounting Kernel Configuration File System... [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Started Journal Service. [ OK ] Started Apply Kernel Variables. Starting Flush Journal to Persistent Storage... Starting udev Kernel Device Manager... [ OK ] Reached target Local File Systems (Pre). [ OK ] Reached target Containers. Mounting /var/volatile... Mounting /media/ram... [ OK ] Mounted /var/volatile. [ OK ] Mounted /media/ram. [ 5.753690] systemd-journald[81]: Received request to flush runtime journal from PID 1 Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. [ OK ] Started udev Kernel Device Manager. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Load/Save Random Seed. Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. Starting Update UTMP about System Boot/Shutdown... Starting Network Time Synchronization... Starting Network Service... [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Service. Starting Network Name Resolution... Starting Wait for Network to be Configured... [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Synchronized. [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. [ 8.949962] input: matrix_keypad0 as /devices/platform/matrix_keypad0/input/input0 [ 9.157055] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 9.337556] omap_rtc 44e3e000.rtc: registered as rtc0 [ OK ] Found device /dev/ttyS0. [ OK ] Started udev Coldplug all Devices. [ 10.686297] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 10.759408] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 10.896628] omap-aes 53500000.aes: will run requests pump with realtime priority [ OK ] Created slice system-systemd\x2dbacklight.slice. Starting Load/Save Screen Backlight…ightness of backlight:backlight... [ 11.108421] remoteproc remoteproc0: wkup_m3 is available [ 11.141985] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.sgx on minor 1 [ OK ] Started Load/Save Screen Backlight Brightness of backlight:backlight. [ OK ] Reached target System Initialization. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Listening on RPCbind Server Activation Socket. [ 11.967699] remoteproc remoteproc0: powering up wkup_m3 [ 12.092921] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 242888 [ 12.109470] net eth0: initializing cpsw version 1.12 (0) [ OK ] Listening on dropbear.socket. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ 12.264986] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192 [ OK ] Reached target Sockets. [ 12.322907] TI DP83867 4a101000.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL) [ OK ] Reached target Basic System. [ 12.372473] PM: Cannot get wkup_m3_ipc handle [ 12.420640] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 12.551214] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready Starting Print notice about GPLv3 packages... [ OK ] Started Periodic Command Scheduler. Starting rc.pvr.service... [ 12.958878] net eth1: initializing cpsw version 1.12 (0) [ 13.128194] TI DP83867 4a101000.mdio:01: attached PHY driver [TI DP83867] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL) Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started Job spooling tools. [ 13.377564] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready [ 13.386976] snd_soc_simple_card_utils: exports duplicate symbol asoc_simple_card_canonicalize_cpu (owned by kernel) Starting Lightning Fast Webserver With Light System Requirements... [ 13.607400] snd_soc_simple_card_utils: exports duplicate symbol asoc_simple_card_canonicalize_cpu (owned by kernel) Starting Simple Network Management Protocol (SNMP) Daemon.... [ 13.874300] snd_soc_simple_card_utils: exports duplicate symbol asoc_simple_card_canonicalize_cpu (owned by kernel) [ 13.905591] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ] [ OK ] Started Redis In-Memory Data Store. Starting Permit User Sessions... [ 14.142583] snd_soc_simple_card_utils: exports duplicate symbol asoc_simple_card_canonicalize_cpu (owned by kernel) [ OK ] Started Daily rotation of log files. [ OK ] Reached target Timers. Starting Enable and configure wl18xx bluetooth stack... [ OK ] Started D-Bus System Message Bus. [ 15.058938] BUG: FP instruction issued in kernel mode with FP unit disabled [ 15.065991] Internal error: Oops - undefined instruction: 0 [#1] PREEMPT ARM [ 15.073075] Modules linked in: pm33xx wkup_m3_ipc wkup_m3_rproc remoteproc pvrsrvkm(O) omap_aes_driver crypto_engine omap_sham omap_crypto ti_emif_sram pruss_soc_bus rtc_omap omap_wdt matrix_keypad matrix_keymap sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common cryptodev(O) [ 15.099511] CPU: 0 PID: 361 Comm: basename Tainted: G O 4.19.94-gbe5389fd85 #17 [ 15.108162] Hardware name: Generic AM33XX (Flattened Device Tree) [ 15.114312] PC is at load_elf_binary+0x884/0x14c8 [ 15.119040] LR is at padzero+0x60/0x78 [ 15.122807] pc : [] lr : [] psr: a0060013 [ 15.129103] sp : edf8fe68 ip : 00000003 fp : edf8ff04 [ 15.134351] r10: edf8fe68 r9 : 0009d6a9 r8 : 0009d6a9 [ 15.139600] r7 : 00000000 r6 : edfbfa00 r5 : c0e03048 r4 : edfc1500 [ 15.146157] r3 : 00000001 r2 : 00000000 r1 : 00000957 r0 : 00000000 [ 15.152719] Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none [ 15.159887] Control: 10c5387d Table: ad178019 DAC: 00000051 [ 15.165667] Process basename (pid: 361, stack limit = 0x95656f57) [ 15.171788] Stack: (0xedf8fe68 to 0xedf90000) [ 15.176173] fe60: 00101802 00000000 00000000 edf8fe68 ffffe000 0009cf08 [ 15.184395] fe80: 0008cdbc 00010000 00010000 0009d6a9 edee4140 edfc1534 00000000 0008cdbc [ 15.192617] fea0: 0009cf08 0009dca4 eddd9c00 edfc1500 edf5e840 eda1ce00 00000034 00000000 [ 15.200840] fec0: c024358c c014e18c ee4eea50 00000004 00000000 bf9b4762 edfbfa00 c0e1babc [ 15.209061] fee0: edfbfa00 ffffe000 c0e1b618 c0bd8df4 00000002 fffffff8 edf8ff34 edf8ff08 [ 15.217284] ff00: c023e4b4 c02920e0 00000000 c0e03048 ee8bd000 edfbfa00 00000169 00000000 [ 15.225505] ff20: 00000000 00000001 edf8ff84 edf8ff38 c023ee04 c023e41c ffffe000 00000000 [ 15.233725] ff40: edf543b8 edd40e40 edf54380 000d0f98 00000000 bf9b4762 0000000b 000d79b0 [ 15.241947] ff60: 000d0f98 000d3f30 0000000b c0101204 edf8e000 0000000b edf8ffa4 edf8ff88 [ 15.250169] ff80: c023f334 c023e958 00000000 00000000 000d3f08 000c4084 00000000 edf8ffa8 [ 15.258392] ffa0: c0101000 c023f304 000d3f08 000c4084 000d3f30 000d79b0 000d0f98 000c2ae4 [ 15.266614] ffc0: 000d3f08 000c4084 000d3f30 0000000b 000d79b0 000d0f98 00000000 000c4098 [ 15.274835] ffe0: b6e61990 bee67064 000373a5 b6e6199c 60060010 000d3f30 00000000 00000000 [ 15.283046] Backtrace: [ 15.285522] [] (load_elf_binary) from [] (search_binary_handler.part.2+0xa4/0x240) [ 15.294878] r10:fffffff8 r9:00000002 r8:c0bd8df4 r7:c0e1b618 r6:ffffe000 r5:edfbfa00 [ 15.302742] r4:c0e1babc [ 15.305294] [] (search_binary_handler.part.2) from [] (__do_execve_file+0x4b8/0x754) [ 15.314823] r10:00000001 r9:00000000 r8:00000000 r7:00000169 r6:edfbfa00 r5:ee8bd000 [ 15.322689] r4:c0e03048 r3:00000000 [ 15.326287] [] (__do_execve_file) from [] (sys_execve+0x3c/0x44) [ 15.334072] r10:0000000b r9:edf8e000 r8:c0101204 r7:0000000b r6:000d3f30 r5:000d0f98 [ 15.341936] r4:000d79b0 [ 15.344490] [] (sys_execve) from [] (ret_fast_syscall+0x0/0x54) [ 15.352181] Exception stack(0xedf8ffa8 to 0xedf8fff0) [ 15.357261] ffa0: 000d3f08 000c4084 000d3f30 000d79b0 000d0f98 000c2ae4 [ 15.365482] ffc0: 000d3f08 000c4084 000d3f30 0000000b 000d79b0 000d0f98 00000000 000c4098 [ 15.373700] ffe0: b6e61990 bee67064 000373a5 b6e6199c [ 15.378775] r5:000c4084 r4:000d3f08 [ 15.382375] Code: e3530000 0a0000ae e1d434b4 e2433002 (f3530001) [ 15.388504] ---[ end trace a2f72798f99d10b1 ]--- [ 15.393360] note: basename[361] exited with preempt_count 1 Starting Reboot and dump vmcore via kexec... Starting Login Service... Starting RPC Bind Service... [ 16.307053] gpio gpiochip3: Persistence not supported for GPIO 21 [ OK ] Started rc.pvr.service. [ OK ] Started Lightning Fast Webserver With Light System Requirements. [ OK ] Started Permit User Sessions. [ OK ] Started Reboot and dump vmcore via kexec. [ OK ] Started RPC Bind Service. [ OK ] Started Enable and configure wl18xx bluetooth stack. [ OK ] Started Simple Network Management Protocol (SNMP) Daemon.. [ OK ] Found device /dev/ttyS3. [ 27.356231] Ploader does not support rtc-only! [ 27.888754] rroc remoteproc1: 4a334000.pru is available [ 27.894749] pru-rproc 4a334000.pru: PRU rproc node pru@4a334000 probed successfully [ 28.014842] remoteproc remoteproc2: 4a338000.pru is available [ 28.045813] pru-rproc 4a338000.pru: PRU rproc node pru@4a338000 probed successfully [ 31.846591] vsabling [ 31.849441] lis3_reg: disabling [ 31.852599] v3v3: disabling [ 31.855406] vdig1: disabling *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash-dev bash bc binutils cifs-utils cpio cpp-symlinks cpp dosfstools elfutils findutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext glmark2 gstreamer1.0-libav gzip hidapi libbfd libcairo-perf-utils libdw1 libelf1 libgdbm-compat4 libgdbm-dev libgdbm6 libgettextlib libgettextsrc libgmp10 libidn2-0 libmavconn libmpc3 libmpfr6 libreadline-dev libreadline7 libunistring2 m4-dev m4 make mavlink mavros-extras mavros-msgs mavros nettle pdm-anomaly-detection socketcan-interface swig-dev swig which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ OK ] Started Print notice about GPLv3 packages. [ *** ] (4 of 5) A start job is running for…mDNS/DNS-SD Stack (34s / 1min 39s)[ *** ] (4 of 5) A start job is running for…mDNS/DNS-SD Stack (34s / 1min 39s)[*** ] (5 of 5) A start job is running for… to be Configured (35s / no limit)[ OK ] Found device /dev/mmcblk0p1. Starting Start USB gadget... [ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. Starting Save/Restore Sound Card State... [ OK ] Created slice system-systemd\x2dfsck.slice. Starting File System Check on /dev/mmcblk1p2... [ 39.696734] udc-core: couldn't find an available UDC - added [g_multi] to list of pending drivers Starting File System Check on /dev/mmcblk0p1... Starting File System Check on /dev/mmcblk1p1... [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS0. [ OK ] Started Serial Getty on ttyS3. Starting weston.service... [ 40.417640] mmc1: cache flush error -110 [ 40.421654] print_req_error: I/O error, dev mmcblk1, sector 0 [ OK ] Started Save/Restore Sound Card State. [ OK ] Started File System Check on /dev/mmcblk0p1. [ OK ] Started File System Check on /dev/mmcblk1p1. [ OK ] Started File System Check on /dev/mmcblk1p2. Mounting /run/media/mmcblk1p2... Mounting /run/media/mmcblk1p1... Mounting /run/media/mmcblk0p1... [ OK hed target Sound Card. [ 41.463634] E(mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [FAILED] Failed to start Start USB gadget. See 'systemctl status gadget-init.service' for details. [ OK ] Started weston.service. [ OK ] Mounted /run/media/mmcblk1p2. [ OK nted /run/media/mmcblk1p1. [ OK ] Mounted /run/media/mmcblk0p1. Startinix GUI... Startinlnetd.service... Starting Matrix GUI... [ OK arted Login Service. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ted Matrix GUI. [ 42.272747] gpio gpiochip2: Persistence not supported for GPIO 1 [ OK ] Started telnetd.service. Starting busybox-udhcpd.service... Starting thttpd.service... [ OK ted Matrix GUI. [ OK ted busybox-udhcpd.service. [ OK ] Started thttpd.service. [][][][] [][][][] [][] [][] [] [][] [][] [][] [] [][] [][] [][*][*] []*[][] [][] [][] [] [][] [][] [][] [] [][] [][] [][][][] [][][][] [*[][][][] ## ## ## ## ##### ### ### ## ## ## ## ## # ## ## ## ##### ## ## #### ## ## ## ## ## ## ## BEL-MVR login: root (automatic login) [ 45.760560] BUG: FP instruction issued in kernel mode with FP unit disabled [ 45.767609] Internal error: Oops - undefined instruction: 0 [#2] PREEMPT ARM [ 45.774693] Modules linked in: g_multi usb_f_mass_storage usb_f_rndis u_ether libcomposite udc_core pru_rproc irq_pruss_intc pruss pm33xx wkup_m3_ipc wkup_m3_rproc remoteproc pvrsrvkm(O) omap_aes_driver crypto_engine omap_sham omap_crypto ti_emif_sram pruss_soc_bus rtc_omap omap_wdt matrix_keypad matrix_keymap sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common cryptodev(O) [ 45.809875] CPU: 0 PID: 1011 Comm: systemd Tainted: G D O 4.19.94-gbe5389fd85 #17 [ 45.818525] Hardware name: Generic AM33XX (Flattened Device Tree) [ 45.824674] PC is at load_elf_binary+0x884/0x14c8 [ 45.829401] LR is at padzero+0x60/0x78 [ 45.833169] pc : [] lr : [] psr: a0030013 [ 45.839464] sp : ed167e68 ip : 00000000 fp : ed167f04 [ 45.844712] r10: ed167e68 r9 : 000ef27c r8 : 005bd27c [ 45.849961] r7 : 00000000 r6 : ed257100 r5 : c0e03048 r4 : ed1f8f00 [ 45.856518] r3 : 00000001 r2 : 00000000 r1 : 00000d84 r0 : 00000000 [ 45.863078] Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none [ 45.870246] Control: 10c5387d Table: ad200019 DAC: 00000051 [ 45.876026] Process systemd (pid: 1011, stack limit = 0x3d391909) [ 45.882147] Stack: (0xed167e68 to 0xed168000) [ 45.886531] 7e60: 00101802 00000000 00000000 ed167e68 ffffe000 0059c2b0 [ 45.894754] 7e80: 0058c0f4 004ce000 004ce000 005bd27c ed269b00 ed1f8f34 004ce000 000be0f4 [ 45.902978] 7ea0: 000ce2b0 000ef324 ed2619c0 ed1f8f00 ed223600 ed9f6000 00000034 00000000 [ 45.911199] 7ec0: c024358c c014e18c ee191410 00000004 00000000 b6cda846 ed257100 c0e1babc [ 45.919421] 7ee0: ed257100 ffffe000 c0e1b618 c0bd8df4 00000002 fffffff8 ed167f34 ed167f08 [ 45.927642] 7f00: c023e4b4 c02920e0 00000000 c0e03048 edbb9000 ed257100 000003f3 00000000 [ 45.935864] 7f20: 00000000 00000001 ed167f84 ed167f38 c023ee04 c023e41c ffffe000 00000000 [ 45.944086] 7f40: edb4e038 ed21a960 edb4e000 0072a348 00000000 b6cda846 0000000b 00604b70 [ 45.952308] 7f60: 0072a348 0069dcb0 0000000b c0101204 ed166000 0000000b ed167fa4 ed167f88 [ 45.960530] 7f80: c023f334 c023e958 00000000 00000000 00604b70 00000000 00000000 ed167fa8 [ 45.968752] 7fa0: c0101000 c023f304 00604b70 00000000 006e79d0 00604b70 0072a348 00679eb0 [ 45.976973] 7fc0: 00604b70 00000000 0069dcb0 0000000b 00000001 bee3e878 00726a98 ffffffff [ 45.985194] 7fe0: 005ea920 bee3e6b4 0052a98b b6c1699c 60030010 006e79d0 00000000 00000000 [ 45.993405] Backtrace: [ 45.995881] [] (load_elf_binary) from [] (search_binary_handler.part.2+0xa4/0x240) [ 46.005237] r10:fffffff8 r9:00000002 r8:c0bd8df4 r7:c0e1b618 r6:ffffe000 r5:ed257100 [ 46.013103] r4:c0e1babc [ 46.015655] [] (search_binary_handler.part.2) from [] (__do_execve_file+0x4b8/0x754) [ 46.025185] r10:00000001 r9:00000000 r8:00000000 r7:000003f3 r6:ed257100 r5:edbb9000 [ 46.033050] r4:c0e03048 r3:00000000 [ 46.036650] [] (__do_execve_file) from [] (sys_execve+0x3c/0x44) [ 46.044434] r10:0000000b r9:ed166000 r8:c0101204 r7:0000000b r6:0069dcb0 r5:0072a348 [ 46.052298] r4:00604b70 [ 46.054853] [] (sys_execve) from [] (ret_fast_syscall+0x0/0x54) [ 46.062544] Exception stack(0xed167fa8 to 0xed167ff0) [ 46.067625] 7fa0: 00604b70 00000000 006e79d0 00604b70 0072a348 00679eb0 [ 46.075846] 7fc0: 00604b70 00000000 0069dcb0 0000000b 00000001 bee3e878 00726a98 ffffffff [ 46.084064] 7fe0: 005ea920 bee3e6b4 0052a98b b6c1699c [ 46.089138] r5:00000000 r4:00604b70 [ 46.092737] Code: e3530000 0a0000ae e1d434b4 e2433002 (f3530001) [ 46.098867] ---[ end trace a2f72798f99d10b2 ]--- [ 46.103796] note: systemd[1011] exited with preempt_count 1 root@BEL-MVR:~# [ 49.965665] gpio gpiochip0: Persistence not supported for GPIO 19 [ 49.978866] gpio gpiochip0: Persistence not supported for GPIO 6 [ 50.005256] gpio gpiochip0: Persistence not supported for GPIO 20 [ 50.022769] gpio gpiochip3: Persistence not supported for GPIO 18 [ 50.044963] gpio gpiochip1: Persistence not supported for GPIO 28 [ 50.068525] gpio gpiochip1: Persistence not supported for GPIO 29 [ 50.098280] gpio gpiochip2: Persistence not supported for GPIO 0 [ 59.653883] BUG: FP instruction issued in kernel mode with FP unit disabled [ 59.660933] Internal error: Oops - undefined instruction: 0 [#3] PREEMPT ARM [ 59.668016] Modules linked in: g_multi usb_f_mass_storage usb_f_rndis u_ether libcomposite udc_core pru_rproc irq_pruss_intc pruss pm33xx wkup_m3_ipc wkup_m3_rproc remoteproc pvrsrvkm(O) omap_aes_driver crypto_engine omap_sham omap_crypto ti_emif_sram pruss_soc_bus rtc_omap omap_wdt matrix_keypad matrix_keymap sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common cryptodev(O) [ 59.703195] CPU: 0 PID: 0 Comm: swapper Tainted: G D O 4.19.94-gbe5389fd85 #17 [ 59.711583] Hardware name: Generic AM33XX (Flattened Device Tree) [ 59.717731] PC is at amx3_idle_enter+0xc/0x48 [ 59.722114] LR is at arm_cpuidle_suspend+0x1c/0x20 [ 59.726926] pc : [] lr : [] psr: 60060093 [ 59.733221] sp : c0e01e98 ip : c0e01ea8 fp : c0e01ea4 [ 59.738470] r10: e3a59bbc r9 : 000000a0 r8 : eed8e000 [ 59.743718] r7 : eee480a0 r6 : 0000000d r5 : eed8e000 r4 : 00000001 [ 59.750276] r3 : c011f13c r2 : fc1edce2 r1 : 00000000 r0 : 00000001 [ 59.756837] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment none [ 59.764092] Control: 10c5387d Table: adfd0019 DAC: 00000051 [ 59.769870] Process swapper (pid: 0, stack limit = 0xf1943372) [ 59.775730] Stack: (0xc0e01e98 to 0xc0e02000) [ 59.780110] 1e80: c0e01eb4 c0e01ea8 [ 59.788332] 1ea0: c010d0b4 c011f148 c0e01ecc c0e01eb8 c070fc40 c010d0a4 ffffe000 eed8e000 [ 59.796555] 1ec0: c0e01f0c c0e01ed0 c070d664 c070fc00 000007a0 00000000 00000001 00000000 [ 59.804777] 1ee0: 0026a659 ffffe000 eed8e000 c0e030b4 eee48000 c0e3f1b8 c0e03048 c0e030c8 [ 59.813000] 1f00: c0e01f1c c0e01f10 c070d930 c070d5fc c0e01f2c c0e01f20 c015494c c070d920 [ 59.821222] 1f20: c0e01f74 c0e01f30 c0154cf0 c0154930 c015501c 00000001 c0bce3c8 c0e4d8a8 [ 59.829444] 1f40: 00000051 fc1edce2 c0e01f6c c0e0e2e0 00000002 c0e03048 ffffffff c0e03040 [ 59.837666] 1f60: c0e4eec0 c0d3da30 c0e01f84 c0e01f78 c015501c c0154b14 c0e01f9c c0e01f88 [ 59.845889] 1f80: c092b084 c0155014 c0e4ef18 c0e4eec0 c0e01ff4 c0e01fa0 c0d00dbc c092afe0 [ 59.854111] 1fa0: ffffffff ffffffff 00000000 c0d005dc 00000000 efffc740 00000000 c0d3da30 [ 59.862334] 1fc0: fc1acfbc 00000000 00000000 c0d00330 00000051 10c03c7d 00000e05 8fff3000 [ 59.870555] 1fe0: 413fc082 10c53c7d 00000000 c0e01ff8 00000000 c0d009bc 00000000 00000000 [ 59.878767] Backtrace: [ 59.881239] [] (amx3_idle_enter) from [] (arm_cpuidle_suspend+0x1c/0x20) [ 59.889731] [] (arm_cpuidle_suspend) from [] (arm_enter_idle_state+0x4c/0x64) [ 59.898651] [] (arm_enter_idle_state) from [] (cpuidle_enter_state+0x74/0x300) [ 59.907651] r5:eed8e000 r4:ffffe000 [ 59.911248] [] (cpuidle_enter_state) from [] (cpuidle_enter+0x1c/0x20) [ 59.919556] r10:c0e030c8 r9:c0e03048 r8:c0e3f1b8 r7:eee48000 r6:c0e030b4 r5:eed8e000 [ 59.927420] r4:ffffe000 [ 59.929981] [] (cpuidle_enter) from [] (call_cpuidle+0x28/0x40) [ 59.937680] [] (call_cpuidle) from [] (do_idle+0x1e8/0x234) [ 59.945030] [] (do_idle) from [] (cpu_startup_entry+0x14/0x18) [ 59.952641] r10:c0d3da30 r9:c0e4eec0 r8:c0e03040 r7:ffffffff r6:c0e03048 r5:00000002 [ 59.960505] r4:c0e0e2e0 [ 59.963061] [] (cpu_startup_entry) from [] (rest_init+0xb0/0xb4) [ 59.970857] [] (rest_init) from [] (start_kernel+0x40c/0x434) [ 59.978374] r5:c0e4eec0 r4:c0e4ef18 [ 59.981972] [] (start_kernel) from [<00000000>] ( (null)) [ 59.988363] Code: e89da800 e1a0c00d e92dd800 e24cb004 (f30f3484) [ 59.994498] ---[ end trace a2f72798f99d10b3 ]--- [ 59.999141] Kernel panic - not syncing: Attempted to kill the idle task! [ 60.005880] ---[ end Kernel panic - not syncing: Attempted to kill the idle task! ]--- [ 305.360385] EXT4-fs (mmcblk0p2): error count since last fsck: 1 [ 305.366391] EXT4-fs (mmcblk0p2): initial error at time 1587262234: ext4_lookup:1590: inode 262647 [ 305.375321] EXT4-fs (mmcblk0p2): last error at time 1587262234: ext4_lookup:1590: inode 262647