# This uEnv.txt file can contain additional environment settings that you # want to set in U-Boot at boot time. This can be simple variables such # as the serverip or custom variables. The format of this file is: # variable=value # NOTE: This file will be evaluated after the bootcmd is run and the # bootcmd must be set to load this file if it exists (this is the # default on all newer U-Boot images. This also means that some # variables such as bootdelay cannot be changed by this file since # it is not evaluated until the bootcmd is run. psdk_setup_file=.psdk_setup check_psdk_setup=load mmc 1:1 ${loadaddr} ${psdk_setup_file} # Reset to the default environment do_psdk_setup=env default -f -a; saveenv # If not done previously, then reset to the default environment and indicate this by writing a file # Also update the Linux hostname based on board_name uenvcmd=if run check_psdk_setup; then echo "Already setup."; else run do_psdk_setup; mw.b ${loadaddr} 0 1; fatwrite mmc 1:1 ${loadaddr} .psdk_setup 1; reset; fi; if test "$board_name" = "j721e-sk"; then ; setenv args_all $args_all systemd.hostname=tda4vm-sk ; fi; if test ${boot_fit} -eq 1; then setenv name_overlays $name_overlays_fit; fi; # Setting the right U-Boot environment variables dorprocboot=1 # name_overlays=ti/k3-j721e-edgeai-apps.dtbo # Name overlays when booting from fit image name_overlays_fit=conf-ti_k3-j721e-edgeai-apps.dtbo