U-Boot SPL 2018.01-00444-g96cdbefd5c-dirty (Jan 31 2019 - 16:06:34) Trying to boot from NAND U-Boot 2018.01-00444-g96cdbefd5c-dirty (Feb 06 2019 - 13:25:29 +0530) CPU : AM335X-GP rev 2.1 Model: TI AM335x EVM DRAM: 512 MiB NAND: 256 MiB MMC: OMAP SD/MMC: 0 Net: Could not get PHY for cpsw: addr 0 cpsw, usb_ether Hit any key to stop autoboot: 0 Booting from nand ... NAND read: device 0 offset 0x80000, size 0x40000 262144 bytes read: OK NAND read: device 0 offset 0x200000, size 0x800000 8388608 bytes read: OK ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff3000, end 8ffff6be ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.67-gd315a9bb00 (astra@astra-OptiPlex-3020) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #11 PREEMPT Sat Feb 2 17:32:16 IST 29 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM3359 ICE-V2 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x9d000000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1 [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 456912K/524288K available (8192K kernel code, 318K rwdata, 2476K rodata, 1024K init, 275K bss, 18224K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB) [ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB) [ 0.000000] .data : 0xc0d00000 - 0xc0d4fb08 ( 319 kB) [ 0.000000] .bss : 0xc0d4fb08 - 0xc0d948a4 ( 276 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 25000000 Hz [ 0.000014] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 85899345900ns [ 0.000035] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 76450417870 ns [ 0.000047] OMAP clocksource: timer1 at 25000000 Hz [ 0.000244] timer_probe: no matching timers found [ 0.000465] Console: colour dummy device 80x30 [ 0.000494] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000502] This ensures that you still see kernel messages. Please [ 0.000508] update your kernel commandline. [ 0.000538] Calibrating delay loop... 795.44 BogoMIPS (lpj=3977216) [ 0.089042] pid_max: default: 32768 minimum: 301 [ 0.089245] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.089262] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.090088] CPU: Testing write buffer coherency: ok [ 0.090867] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.091034] Hierarchical SRCU implementation. [ 0.091395] EFI services will not be available. [ 0.092836] devtmpfs: initialized [ 0.101470] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0 [ 0.101983] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.102302] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.102326] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.106358] pinctrl core: initialized pinctrl subsystem [ 0.107146] DMI not present or invalid. [ 0.107578] NET: Registered protocol family 16 [ 0.110029] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.124818] omap_hwmod: debugss: _wait_target_disable failed [ 0.177769] cpuidle: using governor ladder [ 0.177807] cpuidle: using governor menu [ 0.182094] GPIO line 7 (FET_SWITCH_CTRL) hogged as output/high [ 0.182542] OMAP GPIO hardware version 0.1 [ 0.190617] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_s0, deferring probe [ 0.192762] No ATAGs? [ 0.192779] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.206299] edma 49000000.edma: TI EDMA DMA engine driver [ 0.210212] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/i2c0_pins_default, deferring probe [ 0.211154] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz [ 0.211389] media: Linux media interface: v0.10 [ 0.211445] Linux video capture interface: v2.00 [ 0.211566] pps_core: LinuxPPS API ver. 1 registered [ 0.211576] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.211601] PTP clock support registered [ 0.211636] EDAC MC: Ver: 3.0.0 [ 0.212015] dmi: Firmware registration failed. [ 0.212463] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.212813] Advanced Linux Sound Architecture Driver Initialized. [ 0.214061] clocksource: Switched to clocksource timer1 [ 0.222693] NET: Registered protocol family 2 [ 0.223464] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.223520] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.223566] TCP: Hash tables configured (established 4096 bind 4096) [ 0.223669] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.223689] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.223854] NET: Registered protocol family 1 [ 0.224409] RPC: Registered named UNIX socket transport module. [ 0.224426] RPC: Registered udp transport module. [ 0.224433] RPC: Registered tcp transport module. [ 0.224440] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.225363] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 0.225497] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.227039] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 0.231525] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.232382] NFS: Registering the id_resolver key type [ 0.232431] Key type id_resolver registered [ 0.232440] Key type id_legacy registered [ 0.232492] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.234825] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.234849] io scheduler noop registered [ 0.234858] io scheduler deadline registered [ 0.235089] io scheduler cfq registered (default) [ 0.235100] io scheduler mq-deadline registered [ 0.235108] io scheduler kyber registered [ 0.236474] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.288837] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled [ 0.292061] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 0.935396] console [ttyS0] enabled [ 0.940772] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 0.959323] brd: module loaded [ 0.969287] loop: module loaded [ 0.975749] m25p80 spi0.0: found s25fl064k, expected w25q64 [ 0.981376] m25p80 spi0.0: s25fl064k (8192 Kbytes) [ 0.986379] 4 ofpart partitions found on MTD device spi0.0 [ 0.991891] Creating 4 MTD partitions on "spi0.0": [ 0.996740] 0x000000000000-0x000000080000 : "u-boot-spl" [ 1.003120] 0x000000080000-0x000000180000 : "u-boot" [ 1.008996] 0x000000180000-0x0000001a0000 : "u-boot-env" [ 1.015160] 0x0000001a0000-0x000000800000 : "misc" [ 1.021704] libphy: Fixed MDIO Bus: probed [ 1.094154] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.101862] libphy: 4a101000.mdio: probed [ 1.107237] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver TI DP83867 [ 1.116549] cpsw 4a100000.ethernet: Missing dual_emac_res_vlan in DT. [ 1.123033] cpsw 4a100000.ethernet: Using 1 as Reserved VLAN for 0 slave [ 1.129897] cpsw 4a100000.ethernet: No slave[1] phy_id, phy-handle, or fixed-link property [ 1.138289] cpsw 4a100000.ethernet: Missing dual_emac_res_vlan in DT. [ 1.144801] cpsw 4a100000.ethernet: Using 2 as Reserved VLAN for 1 slave [ 1.151535] cpsw 4a100000.ethernet: Detected MACID = c4:f3:12:e7:2a:4a [ 1.158249] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.164668] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.169957] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 1.178007] cpsw 4a100000.ethernet: cpsw: Detected MACID = c4:f3:12:e7:2a:4c [ 1.186454] i2c /dev entries driver [ 1.190673] IR NEC protocol handler initialized [ 1.195311] IR RC5(x/sz) protocol handler initialized [ 1.200386] IR RC6 protocol handler initialized [ 1.205088] IR JVC protocol handler initialized [ 1.209639] IR Sony protocol handler initialized [ 1.214295] IR SANYO protocol handler initialized [ 1.219017] IR Sharp protocol handler initialized [ 1.223739] IR MCE Keyboard/mouse protocol handler initialized [ 1.229647] IR XMP protocol handler initialized [ 1.236278] cpuidle: enable-method property 'ti,am3352' found operations [ 1.243399] sdhci: Secure Digital Host Controller Interface driver [ 1.249696] sdhci: Copyright(c) Pierre Ossman [ 1.254471] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.260738] ledtrig-cpu: registered to indicate activity on CPUs [ 1.270227] NET: Registered protocol family 10 [ 1.276391] Segment Routing with IPv6 [ 1.280160] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.287010] NET: Registered protocol family 17 [ 1.291755] Key type dns_resolver registered [ 1.296413] omap_voltage_late_init: Voltage driver support not added [ 1.308456] omap-gpmc 50000000.gpmc: GPMC revision 6.0 [ 1.313648] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000 [ 1.321652] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xca [ 1.328200] nand: Micron MT29F2G16ABAEAWP [ 1.332232] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 [ 1.339971] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme [ 1.345492] 10 ofpart partitions found on MTD device omap2-nand.0 [ 1.351610] Creating 10 MTD partitions on "omap2-nand.0": [ 1.357071] 0x000000000000-0x000000020000 : "NAND.SPL" [ 1.363396] 0x000000020000-0x000000040000 : "NAND.SPL.backup1" [ 1.370218] 0x000000040000-0x000000060000 : "NAND.SPL.backup2" [ 1.376987] 0x000000060000-0x000000080000 : "NAND.SPL.backup3" [ 1.383702] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os" [ 1.390712] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot" [ 1.397469] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env" [ 1.404147] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1" [ 1.411475] 0x000000200000-0x000000a00000 : "NAND.kernel" [ 1.421284] 0x000000a00000-0x000010000000 : "NAND.file-system" [ 1.564477] tps65910 0-002d: No interrupt support, no core IRQ [ 1.573954] vrtc: supplied by vbat [ 1.581738] vio: supplied by vbat [ 1.586716] vdd1: supplied by vbat [ 1.592015] vdd2: supplied by vbat [ 1.597429] random: fast init done [ 1.602478] vdig1: supplied by vbat [ 1.607373] vdig2: supplied by vbat [ 1.612218] vpll: supplied by vbat [ 1.617090] vdac: supplied by vbat [ 1.621908] vaux1: supplied by vbat [ 1.626801] vaux2: supplied by vbat [ 1.631645] vaux33: supplied by vbat [ 1.636699] vmmc: supplied by vbat [ 1.641537] vbb: supplied by vbat [ 1.646730] pca953x 0-0041: 0-0041 supply vcc not found, using dummy regulator [ 1.655637] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.661609] ubi0: attaching mtd13 [ 2.467627] ubi0: scanning is finished [ 2.484000] ubi0: attached mtd13 (name "NAND.file-system", size 246 MiB) [ 2.491050] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes [ 2.497988] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512 [ 2.504735] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096 [ 2.511726] ubi0: good PEBs: 1968, bad PEBs: 0, corrupted PEBs: 0 [ 2.517885] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128 [ 2.525159] ubi0: max/mean erase counter: 8/1, WL threshold: 4096, image sequence number: 935963569 [ 2.534278] ubi0: available PEBs: 0, total reserved PEBs: 1968, PEBs reserved for bad PEB handling: 40 [ 2.543655] ubi0: background thread "ubi_bgt0d" started, PID 44 [ 2.549951] hctosys: unable to open rtc device (rtc0) [ 2.555830] ALSA device list: [ 2.555836] No soundcards found. [ 2.574116] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 45 [ 2.612345] UBIFS (ubi0:0): recovery needed [ 2.719664] UBIFS (ubi0:0): recovery completed [ 2.724588] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs" [ 2.732022] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 2.742022] UBIFS (ubi0:0): FS size: 242905088 bytes (231 MiB, 1913 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs) [ 2.752811] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB) [ 2.758693] UBIFS (ubi0:0): media format: w4/r0 (latest is w5/r0), UUID C8F4E3B6-7FEB-486F-ABEC-EEF47A9446C1, small LPT model [ 2.770599] VFS: Mounted root (ubifs filesystem) on device 0:14. [ 2.777392] devtmpfs: mounted [ 2.781859] Freeing unused kernel memory: 1024K [ 2.824116] NOHZ: local_softirq_pending 40 [ 2.964124] NOHZ: local_softirq_pending 40 [ 3.030839] systemd[1]: System time before build time, advancing clock. [ 3.054119] NOHZ: local_softirq_pending 40 [ 3.128094] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4) [ 3.149857] systemd[1]: Detected architecture arm. Welcome to Arago 2018.08! [ 3.186766] systemd[1]: Set hostname to . [ 3.404120] NOHZ: local_softirq_pending 40 [ 3.484097] NOHZ: local_softirq_pending 40 [ 3.524128] NOHZ: local_softirq_pending 40 [ 3.883141] random: systemd: uninitialized urandom read (16 bytes read) [ 3.892023] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 3.924470] random: systemd: uninitialized urandom read (16 bytes read) [ 3.931632] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe. [ OK ] Listening on /dev/initctl Compatibility Named Pipe. [ 4.014422] random: systemd: uninitialized urandom read (16 bytes read) [ 4.021624] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 4.055303] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 4.096534] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ 4.134918] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 4.164786] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ OK ] Listening on udev Control Socket. [ OK ] Listening on udev Kernel Socket. [ OK ] Created slice User and Session Slice. [ OK ] Started Forward Password Requests to Wall Directory Watch. [ OK ] Reached target Paths. [ OK ] Listening on Process Core Dump Socket. [ OK ] Reached target Remote File Systems. [ OK ] Created slice System Slice. Starting Load Kernel Modules... [ OK ] Created slice system-getty.slice. [ 4.532253] cryptodev: loading out-of-tree module taints kernel. [ 4.540697] cryptodev: driver 1.9 loaded. [ OK ] Created slice system-serial\x2dgetty.slice. Mounting Temporary Directory (/tmp)... Starting Remount Root and Kernel File Systems... [ OK ] Reached target Slices. Mounting Kernel Debug File System... Starting Journal Service... Mounting POSIX Message Queue File System... [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted POSIX Message Queue File System. [ 4.804122] NOHZ: local_softirq_pending 40 [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Started Load Kernel Modules. [ OK ] Started Remount Root and Kernel File Systems. Starting udev Coldplug all Devices... Starting Create Static Device Nodes in /dev... Mounting Kernel Configuration File System... Starting Apply Kernel Variables... [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Journal Service. Starting Flush Journal to Persistent Storage... [ OK ] Started Apply Kernel Variables. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... Mounting /var/volatile... Starting udev Kernel Device Manager... [ 5.524132] NOHZ: local_softirq_pending 40 [ OK ] Mounted /var/volatile. [ OK ] Mounted /media/ram. [ 5.660068] systemd-journald[65]: Received request to flush runtime journal from PID 1 Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. [ OK ] Started udev Kernel Device Manager. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Load/Save Random Seed. Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Synchronized. [ 7.604791] input: gpio-decoder as /devices/platform/gpio-decoder/input/input0 [ OK ] Found device /dev/ttyS0. [ 7.795049] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 7.908281] omap_rtc 44e3e000.rtc: registered as rtc0 [ OK ] Started udev Coldplug all Devices. [ OK ] Reached target System Initialization. [ OK ] Started Daily Cleanup of Temporary Directories. Starting Network Service... [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Started Daily rotation of log files. [ OK ] Reached target Timers. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. Starting Print notice about GPLv3 packages... [ OK ] Started Kernel Logging Service. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Started Periodic Command Scheduler. Starting Login Service... Starting RPC Bind Service... [ 9.097567] random: crng init done [ 9.101021] random: 7 urandom warning(s) missed due to ratelimiting [ OK ] Started System Logging Service. Starting telnetd.service... [ OK ] Started Job spooling tools. [ OK ] Reached target Containers. [ OK ] Started D-Bus System Message Bus. [ 10.887065] omap-sham 53100000.sham: hw accel on OMAP rev 4.3 [ 11.044439] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2 [ 11.097317] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle [ 11.122451] remoteproc remoteproc0: wkup_m3 is available [ 11.156702] omap-aes 53500000.aes: will run requests pump with realtime priority [ 11.428025] remoteproc remoteproc0: powering up wkup_m3 [ 11.498654] PM: Cannot get wkup_m3_ipc handle [ 11.714878] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224628 [ 11.723286] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 11.729860] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192 [ OK ] Started RPC Bind Service. [ OK ] Started telnetd.service. [ OK ] Started Network Service. [ 12.741805] net eth1: initializing cpsw version 1.12 (0) [ 12.843297] libphy: PHY not found [ 12.914364] net eth1: phy "" not found on slave 1, err -19 [ 13.059607] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready [ 13.401611] net eth0: initializing cpsw version 1.12 (0) [ 13.547977] TI DP83867 4a101000.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL) [ OK ] Found device /dev/ttyS3. [ 13.683525] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ OK ] Started Login Service. [ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. [ OK ] Reached target Network. Starting Network Name Resolution... Starting Permit User Sessions... Starting thttpd.service... [ OK ] Started Permit User Sessions. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS0. [ OK ] Started Serial Getty on ttyS3. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... [ 15.766080] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx [ OK ] Started thttpd.service. [ 15.823299] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ OK ] Started Synchronize System and HW clocks. Starting rng-tools.service... [ OK ] Started Network Name Resolution. [ OK ] Reached target Host and Network Name Lookups. [ 16.162038] PM: bootloader does not support rtc-only! [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ OK ] Started rng-tools.service. Starting thermal-zone-init.service... [ OK ] Started thermal-zone-init.service. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: bash binutils cifs-utils cpio dosfstools elfutils gawk gzip libdw1 libelf1 libreadline7 m4 which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ OK ] Started Print notice about GPLv3 packages. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyS0 Arago 2018.08 am335x-evm ttyS0