U-Boot 2010.06-00272-g041f487 (Mar 10 2016 - 14:09:14) TI8148-GP rev 3.0 ARM clk: 600MHz DDR clk: 400MHz DRAM: 2 GiB MMC: OMAP SD/MMC: 0 Using default environment The 2nd stage U-Boot will now be auto-loaded Please do not interrupt the countdown till TI8148_EVM prompt if 2nd stage is already flashed Hit any key to stop autoboot: 0 reading u-boot.bin 185284 bytes read ## Starting application at 0x80800000 ... U-Boot 2010.06-00272-g041f487 (Mar 10 2016 - 14:07:47) TI8148-GP rev 3.0 ARM clk: 600MHz DDR clk: 400MHz I2C: ready DRAM: 2 GiB NAND: HW ECC BCH8 Selected 1024 MiB MMC: OMAP SD/MMC: 0 *** Warning - bad CRC, using default environment .:;rrr;;. ,5#@@@@#####@@@@@@#2, ,A@@@hi;;;r5;;;;r;rrSG@@@A, r@@#i;:;s222hG;rrsrrrrrr;ri#@@r :@@hr:r;SG3ssrr2r;rrsrsrsrsrr;rh@@: B@H;;rr;3Hs;rrr;sr;;rrsrsrsrsrsr;;H@B @@s:rrs;5#;;rrrr;r#@H:;;rrsrsrsrsrr:s@@ @@;;srs&X#9;r;r;;,2@@@rrr:;;rrsrsrsrr;;@@ @@;;rrsrrs@MB#@@@@@###@@@@@@#rsrsrsrsrr;;@@ G@r;rrsrsr;#X;SX25Ss#@@#M@#9H9rrsrsrsrsrs;r@G @9:srsrsrs;2@;:;;:.X@@@@@H::;rrsrsrsrsrsrr:3@ X@;rrsrsrsrr;XAi;;:&@@#@Bs:rrsrsrsrsrsrsrsrr;@X @#;rsrsrsrsrr;r2ir@@@###::rrsrsrsrsrsrsrsrsr:@@ @A:rrsrsrsrr;:2@29@@M@@@;:;rrrrsrsrsrsrsrsrs;H@ @&;rsrsrsrr;A@@@@@@###@@@s::;:;;rrsrsrsrsrsr;G@ @#:rrsrsrsr;G@5Hr25@@@#@@@#9XG9s:rrrrsrsrsrs:#@ M@;rsrsrsrs;r@&#;::S@@@@@@@M@@@@Grr:;rsrsrsr;@# :@s;rsrsrsrr:M#Msrr;;&#@@@@@@@@@@H@@5;rsrsr;s@, @@:rrsrsrsr;S@rrrsr;:;r3MH@@#@M5,S@@irrsrr:@@ @A:rrsrsrsrrrrrsrsrrr;::;@##@r:;rH@h;srr:H@ ;@9:rrsrsrsrrrsrsrsrsr;,S@Hi@i:;s;MX;rr:h@; r@B:rrrrsrsrsrsrsrr;;sA@#i,i@h;r;S5;r:H@r ,@@r;rrrsrsrsrsrr;2BM3r:;r:G@:rrr;;r@@, B@Mr;rrrrsrsrsr@@S;;;rrr:5M;rr;rM@H .@@@i;;rrrrsrs2i;rrrrr;r@M:;i@@@. .A@@#5r;;;r;;;rrr;r:r#AsM@@H. ;&@@@@MhXS5i5SX9B@@@@G; :ihM#@@@@@##hs, Net: not set. Reading from E-fuse Detected MACID:74:da:ea:42:a3:44 cpsw Hit any key to stop autoboot: 0 reading boot.scr 354 bytes read Running bootscript from MMC/SD to set the ENV... ## Executing script at 80900000 reading ti_logo.bmp ** Unable to read "ti_logo.bmp" from mmc 0:1 ** Unknown command 'bmp' - try 'help' reading uImage 2898972 bytes read ## Booting kernel from Legacy Image at 80009000 ... Image Name: Linux-2.6.37+ Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2898908 Bytes = 2.8 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 2.6.37+ (root@vefone2aileen) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #98 Mon Jul 4 14:09:56 HKT 2016 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f [ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: ti8148evm [ 0.000000] reserved size = 52428800 at 0x0 [ 0.000000] FB: Reserving 52428800 bytes SDRAM for VRAM [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] OMAP chip is TI8148 3.0 [ 0.000000] SRAM: Mapped pa 0x402f1000 to va 0xfe400000 size: 0xf000 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 160648 [ 0.000000] Kernel command line: console=ttyO0,115200n8 rootwait root=/dev/mmcblk0p2 rw mem=364M@0x80000000 mem=320M@0x9FC00000 vmalloc=500M notifyk.vpssm3_sva=0xBF900000 ip=off noinitrd [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 364MB 270MB = 634MB total [ 0.000000] Memory: 637124k/637124k available, 63292k reserved, 276480K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] DMA : 0xfee00000 - 0xffe00000 ( 16 MB) [ 0.000000] vmalloc : 0xd7000000 - 0xf8000000 ( 528 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd6c00000 ( 364 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .init : 0xc0008000 - 0xc003d000 ( 212 kB) [ 0.000000] .text : 0xc003d000 - 0xc057a000 (5364 kB) [ 0.000000] .data : 0xc057a000 - 0xc05c8960 ( 315 kB) [ 0.000000] SLUB: Genslabs=11, HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] NR_IRQS:407 [ 0.000000] omap_hwmod: gpio2: softreset failed (waited 10000 usec) [ 0.000000] omap_hwmod: gpio3: softreset failed (waited 10000 usec) [ 0.000000] omap_hwmod: gpio4: softreset failed (waited 10000 usec) [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] GPMC revision 6.0 [ 0.000000] Trying to install interrupt handler for IRQ400 [ 0.000000] Trying to install interrupt handler for IRQ401 [ 0.000000] Trying to install interrupt handler for IRQ402 [ 0.000000] Trying to install interrupt handler for IRQ403 [ 0.000000] Trying to install interrupt handler for IRQ404 [ 0.000000] Trying to install interrupt handler for IRQ405 [ 0.000000] Trying to install interrupt handler for IRQ406 [ 0.000000] Trying to install type control for IRQ407 [ 0.000000] Trying to set irq flags for IRQ407 [ 0.000000] OMAP clockevent source: GPTIMER1 at 20000000 Hz [ 0.000000] Console: colour dummy device 80x30 [ 0.000000] Calibrating delay loop... 599.65 BogoMIPS (lpj=2998272) [ 0.230000] pid_max: default: 32768 minimum: 301 [ 0.230000] Security Framework initialized [ 0.230000] Mount-cache hash table entries: 512 [ 0.230000] CPU: Testing write buffer coherency: ok [ 0.230000] devtmpfs: initialized [ 0.230000] omap_voltage_early_init: voltage driver support not added [ 0.230000] regulator: core version 0.5 [ 0.230000] regulator: dummy: [ 0.230000] NET: Registered protocol family 16 [ 0.230000] omap_voltage_domain_lookup: Voltage driver init not yet happened.Faulting! [ 0.230000] omap_voltage_add_dev: VDD specified does not exist! [ 0.230000] OMAP GPIO hardware version 0.1 [ 0.230000] OMAP GPIO hardware version 0.1 [ 0.230000] OMAP GPIO hardware version 0.1 [ 0.230000] OMAP GPIO hardware version 0.1 [ 0.230000] omap_mux_init: Add partition: #1: core, flags: 4 [ 0.230000] NOR: Can't request GPMC CS [ 0.250000] Debugfs: Only enabling/disabling deep sleep and wakeup timer is supported now [ 0.250000] registered ti81xx_vpss device [ 0.250000] registered ti81xx_vidout device [ 0.250000] registered ti81xx on-chip HDMI device [ 0.250000] registered ti81xx_fb device [ 0.250000] registered ti81xx_vin device [ 0.260000] ti81xx_pcie: Invoking PCI BIOS... [ 0.260000] ti81xx_pcie: Setting up Host Controller... [ 0.260000] ti81xx_pcie: Register base mapped @0xd7018000 [ 0.370000] ti81xx_pcie: Starting PCI scan... [ 0.370000] PCI: bus0: Fast back to back transfers enabled [ 0.370000] bio: create slab at 0 [ 0.380000] Timer6 will run at at 20000000 Hz [ 0.380000] vgaarb: loaded [ 0.380000] SCSI subsystem initialized [ 0.380000] usbcore: registered new interface driver usbfs [ 0.380000] usbcore: registered new interface driver hub [ 0.380000] usbcore: registered new device driver usb [ 0.380000] USBSS revision 4ea2080b [ 0.380000] registerd cppi-dma Intr @ IRQ 17 [ 0.380000] Cppi41 Init Done [ 0.380000] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz [ 0.380000] pcf857x: probe of 1-0021 failed with error -121 [ 0.380000] regulator: VRTC: 1800 mV [ 0.380000] regulator: VIO: 1500 mV [ 0.390000] regulator: VDD1: 600 <--> 1500 mV at 1200 mV [ 0.390000] regulator: VDD2: 600 <--> 1500 mV at 1200 mV [ 0.390000] regulator: VDDCTRL: 600 <--> 1400 mV at 1200 mV [ 0.390000] regulator: LDO1: 1100 <--> 3300 mV at 1800 mV [ 0.390000] regulator: LDO2: 1100 <--> 3300 mV at 1800 mV [ 0.390000] regulator: LDO3: 1100 <--> 3300 mV at 3300 mV [ 0.390000] regulator: LDO4: 1100 <--> 3300 mV at 1800 mV [ 0.400000] regulator: LDO5: 1100 <--> 3300 mV at 3300 mV [ 0.400000] regulator: LDO6: 1100 <--> 3300 mV at 3300 mV [ 0.400000] regulator: LDO7: 1100 <--> 3300 mV at 3300 mV [ 0.400000] regulator: LDO8: 1100 <--> 3300 mV at 1800 mV [ 0.400000] tps65910 1-002d: No interrupt support, no core IRQ [ 0.420000] omap_i2c omap_i2c.4: bus 4 rev4.0 at 100 kHz [ 0.420000] Advanced Linux Sound Architecture Driver Version 1.0.23. [ 0.420000] Switching to clocksource gp timer [ 0.430000] musb-hdrc: version 6.0, host, debug=0 [ 0.430000] musb-hdrc musb-hdrc.0: dma type: dma-cppi41 [ 0.430000] MUSB controller-0 revision 4ea20800 [ 0.430000] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 0.430000] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1 [ 0.430000] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.430000] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.430000] usb usb1: Product: MUSB HDRC host driver [ 0.430000] usb usb1: Manufacturer: Linux 2.6.37+ musb-hcd [ 0.430000] usb usb1: SerialNumber: musb-hdrc.0 [ 0.430000] hub 1-0:1.0: USB hub found [ 0.430000] hub 1-0:1.0: 1 port detected [ 0.430000] musb-hdrc musb-hdrc.0: USB Host mode controller at d701e000 using DMA, IRQ 18 [ 0.430000] musb-hdrc musb-hdrc.1: dma type: dma-cppi41 [ 0.430000] MUSB controller-1 revision 4ea20800 [ 0.430000] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.430000] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2 [ 0.430000] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.430000] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.430000] usb usb2: Product: MUSB HDRC host driver [ 0.430000] usb usb2: Manufacturer: Linux 2.6.37+ musb-hcd [ 0.430000] usb usb2: SerialNumber: musb-hdrc.1 [ 0.430000] hub 2-0:1.0: USB hub found [ 0.430000] hub 2-0:1.0: 1 port detected [ 0.430000] musb-hdrc musb-hdrc.1: USB Host mode controller at d702a800 using DMA, IRQ 19 [ 0.430000] NET: Registered protocol family 2 [ 0.430000] IP route cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.430000] TCP established hash table entries: 65536 (order: 7, 524288 bytes) [ 0.430000] TCP bind hash table entries: 65536 (order: 6, 262144 bytes) [ 0.440000] TCP: Hash tables configured (established 65536 bind 65536) [ 0.440000] TCP reno registered [ 0.440000] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.440000] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.440000] NET: Registered protocol family 1 [ 0.440000] RPC: Registered udp transport module. [ 0.440000] RPC: Registered tcp transport module. [ 0.440000] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.440000] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.440000] PMU: registered new PMU device of type 0 [ 0.440000] omap-iommu omap-iommu.0: ducati registered [ 0.440000] omap-iommu omap-iommu.1: sys registered [ 0.580000] highmem bounce pool size: 64 pages [ 0.590000] JFFS2 version 2.2. (NAND) ? 2001-2006 Red Hat, Inc. [ 0.590000] msgmni has been set to 704 [ 0.590000] io scheduler noop registered [ 0.590000] io scheduler deadline registered [ 0.590000] io scheduler cfq registered (default) [ 0.590000] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled [ 0.590000] omap_uart.0: ttyO0 at MMIO 0x48020000 (irq = 72) is a OMAP UART0 [ 1.450000] console [ttyO0] enabled [ 1.460000] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 1.470000] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 1.470000] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 1.480000] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 1.490000] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 1.500000] brd: module loaded [ 1.510000] loop: module loaded [ 1.520000] ahci ahci.0: forcing PORTS_IMPL to 0x1 [ 1.520000] ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode [ 1.530000] ahci ahci.0: flags: ncq sntf pm led clo only pmp pio slum part ccc apst [ 1.540000] scsi0 : ahci_platform [ 1.540000] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a150fff] port 0x100 irq 16 [ 1.550000] m25p80 spi1.0: w25q64 (8192 Kbytes) [ 1.560000] Creating 5 MTD partitions on "spi_flash": [ 1.560000] 0x000000000000-0x000000040000 : "U-Boot-min" [ 1.570000] 0x000000040000-0x0000000c0000 : "U-Boot" [ 1.570000] 0x0000000c0000-0x000000100000 : "U-Boot Env" [ 1.580000] 0x000000100000-0x000000500000 : "Kernel" [ 1.590000] 0x000000500000-0x000000800000 : "Reserved" [ 1.590000] omap2-nand driver initializing [ 1.600000] ONFI flash detected [ 1.600000] ONFI param page 0 valid [ 1.610000] NAND device: Manufacturer ID: 0x01, Chip ID: 0xd3 (AMD NAND 1GiB 3,3V 8-bit) [ 1.610000] Creating 5 MTD partitions on "omap2-nand.0": [ 1.620000] 0x000000000000-0x000000040000 : "U-Boot-min" [ 1.630000] 0x000000040000-0x0000000c0000 : "U-Boot" [ 1.630000] 0x0000000c0000-0x000000100000 : "U-Boot Env" [ 1.640000] 0x000000100000-0x000000500000 : "Kernel" [ 1.650000] 0x000000500000-0x000020000000 : "File System" [ 1.870000] usb 2-1: new high speed USB device using musb-hdrc and address 2 [ 1.930000] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.930000] davinci_mdio davinci_mdio.0: detected phy mask fffffffc [ 1.940000] davinci_mdio.0: probed [ 1.940000] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.950000] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown [ 1.960000] CAN device driver interface [ 1.960000] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.970000] d_can d_can.0: d_can device registered (irq=52, irq_obj=53) [ 1.980000] d_can d_can.1: d_can device registered (irq=55, irq_obj=56) [ 1.980000] usbcore: registered new interface driver cdc_ether [ 1.990000] usbcore: registered new interface driver dm9601 [ 2.000000] usbcore: registered new interface driver cdc_acm [ 2.000000] cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters [ 2.010000] Initializing USB Mass Storage driver... [ 2.020000] usbcore: registered new interface driver usb-storage [ 2.020000] USB Mass Storage support registered. [ 2.030000] mice: PS/2 mouse device common for all mice [ 2.030000] ata1: SATA link down (SStatus 0 SControl 300) [ 2.040000] ads7846 spi1.2: touchscreen, irq 182 [ 2.040000] input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.2/input/input0 [ 2.060000] usb 2-1: New USB device found, idVendor=0409, idProduct=005a [ 2.060000] usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0 [ 2.070000] hub 2-1:1.0: USB hub found [ 2.070000] tps65910-rtc tps65910-rtc: rtc core: registered tps65910-rtc as rtc0 [ 2.080000] i2c /dev entries driver [ 2.090000] Linux video capture interface: v2.00 [ 2.090000] usbcore: registered new interface driver uvcvideo [ 2.100000] USB Video Class driver (v1.0.0) [ 2.100000] Timer7 will run at at 20000000 Hz [ 2.110000] pwm-fan pwm-fan.1: PWM fan initialized [ 2.110000] hub 2-1:1.0: 4 ports detected [ 2.120000] tmp102 1-0049: initialized [ 2.130000] OMAP Watchdog Timer Rev 0x00: initial timeout 60 sec [ 2.130000] usbcore: registered new interface driver usbhid [ 2.140000] usbhid: USB HID core driver [ 2.140000] notify_init : notify drivercreated for remote proc id 2 at physical Address 0xbf900000 [ 2.150000] usbcore: registered new interface driver snd-usb-audio [ 2.160000] asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok [ 2.170000] ALSA device list: [ 2.170000] #0: TI81XX EVM [ 2.180000] nf_conntrack version 0.5.0 (9955 buckets, 39820 max) [ 2.180000] ip_tables: (C) 2000-2006 Netfilter Core Team [ 2.190000] TCP cubic registered [ 2.190000] NET: Registered protocol family 17 [ 2.200000] can: controller area network core (rev 20090105 abi 8) [ 2.210000] NET: Registered protocol family 29 [ 2.210000] can: raw protocol (rev 20090105) [ 2.210000] can: broadcast manager protocol (rev 20090105 t) [ 2.220000] Registering the dns_resolver key type [ 2.230000] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 2.240000] omap_voltage_late_init: Voltage driver support not added [ 2.240000] Power Management for TI81XX. [ 2.250000] Detected MACID=74:da:ea:42:a3:44 [ 2.260000] Detected MACID=74:da:ea:42:a3:45 [ 2.270000] tps65910-rtc tps65910-rtc: setting system clock to 2016-05-13 07:20:34 UTC (1463124034) [ 2.280000] Waiting for root device /dev/mmcblk0p2... [ 2.360000] mmc0: new high speed SDHC card at address aaaa [ 2.360000] mmcblk0: mmc0:aaaa SS08G 7.40 GiB [ 2.370000] mmcblk0: p1 p2 [ 2.390000] EXT3-fs: barriers not enabled [ 2.400000] kjournald starting. Commit interval 5 seconds [ 2.410000] EXT3-fs (mmcblk0p2): using internal journal [ 2.410000] EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode [ 2.420000] VFS: Mounted root (ext3 filesystem) on device 179:2. [ 2.430000] devtmpfs: mounted [ 2.430000] Freeing init memory: 212K INIT: version 2.86 booting Please wait: booting... Error opening /dev/fb0: No such file or directory Starting udev [ 2.930000] udevd (88): /proc/88/oom_adj is deprecated, please use /proc/88/oom_score_adj instead. Remounting root file system... Caching udev devnodes [ 7.720000] NET: Registered protocol family 10 ALSA: Restoring mixer settings... Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device ifconfig: SIOCGIFFLAGS: No such device eth0 No such device ifconfig: SIOCGIFFLAGS: No such device done. Setting up IP spoofing protection: rp_filter. INIT: Entering runlevel: 5 Loading HDVICP2 Firmware DM814X prcm_config_app version: 2.0.0.1 Doing PRCM settings... PRCM for IVHD0 is in Progress, Please wait..... BW Phy Addr : 0x48180600 Data : 0x00000001 AW Phy Addr : 0x48180600 Data : 0x00000002 Phy Addr : 0x48180c04 Data : 0x00000037 BW Phy Addr : 0x48180620 Data : 0x00070000 AW Phy Addr : 0x48180620 Data : 0x00070002 BW Phy Addr : 0x48180624 Data : 0x00030000 AW Phy Addr : 0x48180624 Data : 0x00010002 Phy Addr : 0x48180600 Data : 0x00000102 BW Phy Addr : 0x48180c10 Data : 0x00000007 AW Phy Addr : 0x48180c10 Data : 0x00000003 Phy Addr : 0x48180c14 Data : 0x00000004 BW Phy Addr : 0x58088000 Data : 0xeafffffe AW Phy Addr : 0x58088000 Data : 0xeafffffe BW Phy Addr : 0x58098000 Data : 0xeafffffe AW Phy Addr : 0x58098000 Data : 0xeafffffe BW Phy Addr : 0x48180c10 Data : 0x00000003 AW Phy Addr : 0x48180c10 Data : 0x00000000 Phy Addr : 0x48180c14 Data : 0x00000007 PRCM for IVHD0 is Done Successfully PRCM Initialization completed [ 10.040000] SysLink version : 2.20.02.20 [ 10.040000] SysLink module created on Date:Jul 1 2016 Time:11:49:19 FIRMWARE: I2cInit will be done by M3 FIRMWARE: Memory map bin file not passed Usage : firmware_loader [-mmap ] [-i2c <0|1>] ===Mandatory arguments=== 0: DSP, 1: Video-M3, 2: Vpss-M3 firmware binary file to start/stop the firmware ===Optional arguments=== -mmap input memory map bin file name -i2c 0: i2c init not done by M3, 1(default): i2c init done by M3 FIRMWARE: isI2cInitRequiredOnM3: 1 FIRMWARE: Default memory configuration is used Firmware Loader debugging not configured Default FL_DEBUG: warning Allowed FL_DEBUG levels: error, warning, info, debug, log MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1 FIRMWARE: 1 start Successful Loading HDVPSS Firmware FIRMWARE: I2cInit will be done by M3 FIRMWARE: Memory map bin file not passed Usage : firmware_loader [-mmap ] [-i2c <0|1>] ===Mandatory arguments=== 0: DSP, 1: Video-M3, 2: Vpss-M3 firmware binary file to start/stop the firmware ===Optional arguments=== -mmap input memory map bin file name -i2c 0: i2c init not done by M3, 1(default): i2c init done by M3 FIRMWARE: isI2cInitRequiredOnM3: 1 FIRMWARE: Default memory configuration is used Firmware Loader debugging not configured Default FL_DEBUG: warning Allowed FL_DEBUG levels: error, warning, info, debug, log MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.2.1 FIRMWARE: 2 start Successful [ 11.670000] VPSS_FVID2: M3 firmware version 0x1000145 is newer,driver may not work properly. Configuring fb0 to LCD [ 11.900000] HDMI W1 rev 4.0 [ 11.900000] HDMI CEC Spec version 1.2 [ 12.230000] I2C No Ack [ 12.230000] Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR Usage: insmod filename [args] FATAL: Module omaplfb not found. FATAL: Module bufferclass_ti not found. BusyBox v1.13.2 (2012-12-26 15:45:54 IST) multi-call binary Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR Create a special file (block, character, or pipe) Options: -m Create the special file using the specified mode (default a=rw) TYPEs include: b: Make a block device c or u: Make a character device p: Make a named pipe (MAJOR and MINOR are ignored) chmod: /dev/pvrsrvkm: No such file or directory /dev/mem opened. Memory mapped at address 0x4027b000. Read at address 0x48180F04 (0x4027bf04): 0x00000001 Write at address 0x48180F04 (0x4027bf04): 0x00000000, readback 0x00000000 /dev/mem opened. Memory mapped at address 0x40136000. Read at address 0x48180900 (0x40136900): 0x00000001 Write at address 0x48180900 (0x40136900): 0x00000002, readback 0x00000002 /dev/mem opened. Memory mapped at address 0x402ee000. Read at address 0x48180920 (0x402ee920): 0x00070000 Write at address 0x48180920 (0x402ee920): 0x00000002, readback 0x00000002 Starting Matrix GUI application. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org dm814x-evm ttyO0 Arago 2011.09 dm814x-evm ttyO0 dm814x-evm login: root root@dm814x-evm:~#