U-Boot SPL 2016.05-00019-g2127b02 (Jun 28 2019 - 20:52:22) DRA752-GP ES2.0 no pinctrl for hs200_1_8v no pinctrl for ddr_1_8v Card did not respond to voltage select! *** Warning - MMC init failed, using default environment Trying to boot from MMC1 reading dra7-ipu2-fw.lzop spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1 spl: error reading image dra7-ipu2-fw.lzop, err - -1 Error loading remotecore IPU2!,Continuing with boot ... reading dra7-dsp1-fw.lzop spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1 spl: error reading image dra7-dsp1-fw.lzop, err - -1 Error loading remotecore DSP1!,Continuing with boot ... reading dra7-dsp2-fw.lzop spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1 spl: error reading image dra7-dsp2-fw.lzop, err - -1 Error loading remotecore DSP2!,Continuing with boot ... reading dra7-ipu1-fw.lzop spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1 spl: error reading image dra7-ipu1-fw.lzop, err - -1 Error loading remotecore IPU1!,Continuing with boot ... spl: falcon_args_file not set in environment, falling back to default reading single-stage-boot.dtb spl_load_image_fat_os: error reading image single-stage-boot.dtb, err - -1 reading u-boot.img reading u-boot.img reading u-boot.img reading u-boot.img U-Boot 2016.05-00019-g2127b02 (Jun 28 2019 - 20:52:22 +0530) CPU : DRA752-GP ES2.0 Model: TI DRA742 Board: DRA74x Cascade EVM REV H.4 DRAM: 4 GiB MMC: i2c_write: error waiting for data ACK (status=0x116) pcf8575_i2c_write_le16 i2c write failed to addr 21 OMAP SD/MMC: 0, OMAP SD/MMC: 1 Card did not respond to voltage select! *** Warning - MMC init failed, using default environment Card did not respond to voltage select! ERROR: invalid mmc device at arch/arm/cpu/armv7/omap-common/utils.c:193/mmc_get_part_size() Warning: fastboot.userdata_size: unable to calc SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: Could not get PHY for ethernet@48484000: addr 2 Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 0 ## Error: "board_findfdt" not defined MMC: no card present MMC: no card present MMC: no card present Card did not respond to voltage select! MMC: no card present Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value Booting from eMMC ... Wrong Image Format for bootm command ERROR: can't get kernel image! =>