/*
 * Board functions for CRSCD AM437X based board
 *
 * Copyright (C) 2018 crscd Ltd - http://www.crscd.com/
 *
 * Author: xiaoyiping <xiaoyiping@crscd.com>
 *
 * SPDX-License-Identifier:	GPL-2.0+
 */

#include <common.h>
#include <i2c.h>
#include <asm/errno.h>
#include <spl.h>
#include <usb.h>
#include <asm/omap_sec_common.h>
#include <asm/arch/clock.h>
#include <asm/arch/sys_proto.h>
#include <asm/arch/mux.h>
#include <asm/arch/ddr_defs.h>
#include <asm/arch/gpio.h>
#include <asm/emif.h>
#include "../common/board_detect.h"
#include "board.h"
#include <power/pmic.h>
#include <power/tps65218.h>
#include <power/tps62362.h>
#include <miiphy.h>
#include <cpsw.h>
#include <linux/usb/gadget.h>
#include <dwc3-uboot.h>
#include <dwc3-omap-uboot.h>
#include <ti-usb-phy-uboot.h>

DECLARE_GLOBAL_DATA_PTR;

static struct ctrl_dev *cdev = (struct ctrl_dev *)CTRL_DEVICE_BASE; /*cpu的version信息基址*/

/*add@20180308 for crsc 同步myir spl不走本文件，注掉spl相关代码*/
#if 0
/*
 * Read header information from EEPROM into global structure.
 */
#ifdef CONFIG_TI_I2C_BOARD_DETECT
void do_board_detect(void)
{
	if (ti_i2c_eeprom_am_get(-1, CONFIG_SYS_I2C_EEPROM_ADDR))
		printf("ti_i2c_eeprom_init failed\n");
}
#endif

#ifndef CONFIG_SKIP_LOWLEVEL_INIT

#define NUM_OPPS	6

const struct dpll_params dpll_mpu[NUM_CRYSTAL_FREQ][NUM_OPPS] = {
	{	/* 19.2 MHz */
		{125, 3, 2, -1, -1, -1, -1},	/* OPP 50 */
		{-1, -1, -1, -1, -1, -1, -1},	/* OPP RESERVED	*/
		{125, 3, 1, -1, -1, -1, -1},	/* OPP 100 */
		{150, 3, 1, -1, -1, -1, -1},	/* OPP 120 */
		{125, 2, 1, -1, -1, -1, -1},	/* OPP TB */
		{625, 11, 1, -1, -1, -1, -1}	/* OPP NT */
	},
	{	/* 24 MHz */
		{300, 23, 1, -1, -1, -1, -1},	/* OPP 50 */
		{-1, -1, -1, -1, -1, -1, -1},	/* OPP RESERVED	*/
		{600, 23, 1, -1, -1, -1, -1},	/* OPP 100 */
		{720, 23, 1, -1, -1, -1, -1},	/* OPP 120 */
		{800, 23, 1, -1, -1, -1, -1},	/* OPP TB */
		{1000, 23, 1, -1, -1, -1, -1}	/* OPP NT */
	},
	{	/* 25 MHz */
		{300, 24, 1, -1, -1, -1, -1},	/* OPP 50 */
		{-1, -1, -1, -1, -1, -1, -1},	/* OPP RESERVED	*/
		{600, 24, 1, -1, -1, -1, -1},	/* OPP 100 */
		{720, 24, 1, -1, -1, -1, -1},	/* OPP 120 */
		{800, 24, 1, -1, -1, -1, -1},	/* OPP TB */
		{1000, 24, 1, -1, -1, -1, -1}	/* OPP NT */
	},
	{	/* 26 MHz */
		{300, 25, 1, -1, -1, -1, -1},	/* OPP 50 */
		{-1, -1, -1, -1, -1, -1, -1},	/* OPP RESERVED	*/
		{600, 25, 1, -1, -1, -1, -1},	/* OPP 100 */
		{720, 25, 1, -1, -1, -1, -1},	/* OPP 120 */
		{800, 25, 1, -1, -1, -1, -1},	/* OPP TB */
		{1000, 25, 1, -1, -1, -1, -1}	/* OPP NT */
	},
};

const struct dpll_params dpll_core[NUM_CRYSTAL_FREQ] = {
		{625, 11, -1, -1, 10, 8, 4},	/* 19.2 MHz */
		{1000, 23, -1, -1, 10, 8, 4},	/* 24 MHz */
		{1000, 24, -1, -1, 10, 8, 4},	/* 25 MHz */
		{1000, 25, -1, -1, 10, 8, 4}	/* 26 MHz */
};

const struct dpll_params dpll_per[NUM_CRYSTAL_FREQ] = {
		{400, 7, 5, -1, -1, -1, -1},	/* 19.2 MHz */
		{400, 9, 5, -1, -1, -1, -1},	/* 24 MHz */
		{384, 9, 5, -1, -1, -1, -1},	/* 25 MHz */
		{480, 12, 5, -1, -1, -1, -1}	/* 26 MHz */
};

const struct dpll_params epos_evm_dpll_ddr[NUM_CRYSTAL_FREQ] = {
		{665, 47, 1, -1, 4, -1, -1}, /*19.2*/
		{133, 11, 1, -1, 4, -1, -1}, /* 24 MHz */
		{266, 24, 1, -1, 4, -1, -1}, /* 25 MHz */
		{133, 12, 1, -1, 4, -1, -1}  /* 26 MHz */
};

const struct dpll_params gp_evm_dpll_ddr = {
		50, 2, 1, -1, 2, -1, -1};

static const struct dpll_params idk_dpll_ddr = {
	400, 23, 1, -1, 2, -1, -1
};

static const u32 ext_phy_ctrl_const_base_lpddr2[] = {
	0x00500050,
	0x00350035,
	0x00350035,
	0x00350035,
	0x00350035,
	0x00350035,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x00000000,
	0x40001000,
	0x08102040
};

const struct ctrl_ioregs ioregs_lpddr2 = {
	.cm0ioctl		= LPDDR2_ADDRCTRL_IOCTRL_VALUE,
	.cm1ioctl		= LPDDR2_ADDRCTRL_WD0_IOCTRL_VALUE,
	.cm2ioctl		= LPDDR2_ADDRCTRL_WD1_IOCTRL_VALUE,
	.dt0ioctl		= LPDDR2_DATA0_IOCTRL_VALUE,
	.dt1ioctl		= LPDDR2_DATA0_IOCTRL_VALUE,
	.dt2ioctrl		= LPDDR2_DATA0_IOCTRL_VALUE,
	.dt3ioctrl		= LPDDR2_DATA0_IOCTRL_VALUE,
	.emif_sdram_config_ext	= 0x1,
};

const struct emif_regs emif_regs_lpddr2 = {
	.sdram_config			= 0x808012BA,
	.ref_ctrl			= 0x0000040D,
	.sdram_tim1			= 0xEA86B411,
	.sdram_tim2			= 0x103A094A,
	.sdram_tim3			= 0x0F6BA37F,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x50074BE4,
	.temp_alert_config		= 0x0,
	.emif_rd_wr_lvl_rmp_win		= 0x0,
	.emif_rd_wr_lvl_rmp_ctl		= 0x0,
	.emif_rd_wr_lvl_ctl		= 0x0,
	.emif_ddr_phy_ctlr_1		= 0x0E284006,
	.emif_rd_wr_exec_thresh		= 0x80000405,
	.emif_ddr_ext_phy_ctrl_1	= 0x04010040,
	.emif_ddr_ext_phy_ctrl_2	= 0x00500050,
	.emif_ddr_ext_phy_ctrl_3	= 0x00500050,
	.emif_ddr_ext_phy_ctrl_4	= 0x00500050,
	.emif_ddr_ext_phy_ctrl_5	= 0x00500050,
	.emif_prio_class_serv_map	= 0x80000001,
	.emif_connect_id_serv_1_map	= 0x80000094,
	.emif_connect_id_serv_2_map	= 0x00000000,
	.emif_cos_config			= 0x000FFFFF
};

const struct ctrl_ioregs ioregs_ddr3 = {
	.cm0ioctl		= DDR3_ADDRCTRL_IOCTRL_VALUE,
	.cm1ioctl		= DDR3_ADDRCTRL_WD0_IOCTRL_VALUE,
	.cm2ioctl		= DDR3_ADDRCTRL_WD1_IOCTRL_VALUE,
	.dt0ioctl		= DDR3_DATA0_IOCTRL_VALUE,
	.dt1ioctl		= DDR3_DATA0_IOCTRL_VALUE,
	.dt2ioctrl		= DDR3_DATA0_IOCTRL_VALUE,
	.dt3ioctrl		= DDR3_DATA0_IOCTRL_VALUE,
	.emif_sdram_config_ext	= 0xc163,
};

const struct emif_regs ddr3_emif_regs_400Mhz = {
	.sdram_config			= 0x638413B2,
	.ref_ctrl			= 0x00000C30,
	.sdram_tim1			= 0xEAAAD4DB,
	.sdram_tim2			= 0x266B7FDA,
	.sdram_tim3			= 0x107F8678,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x50074BE4,
	.temp_alert_config		= 0x0,
	.emif_ddr_phy_ctlr_1		= 0x0E004008,
	.emif_ddr_ext_phy_ctrl_1	= 0x08020080,
	.emif_ddr_ext_phy_ctrl_2	= 0x00400040,
	.emif_ddr_ext_phy_ctrl_3	= 0x00400040,
	.emif_ddr_ext_phy_ctrl_4	= 0x00400040,
	.emif_ddr_ext_phy_ctrl_5	= 0x00400040,
	.emif_rd_wr_lvl_rmp_win		= 0x0,
	.emif_rd_wr_lvl_rmp_ctl		= 0x0,
	.emif_rd_wr_lvl_ctl		= 0x0,
	.emif_rd_wr_exec_thresh		= 0x80000405,
	.emif_prio_class_serv_map	= 0x80000001,
	.emif_connect_id_serv_1_map	= 0x80000094,
	.emif_connect_id_serv_2_map	= 0x00000000,
	.emif_cos_config		= 0x000FFFFF
};

/* EMIF DDR3 Configurations are different for beta AM43X GP EVMs */
const struct emif_regs ddr3_emif_regs_400Mhz_beta = {
	.sdram_config			= 0x638413B2,
	.ref_ctrl			= 0x00000C30,
	.sdram_tim1			= 0xEAAAD4DB,
	.sdram_tim2			= 0x266B7FDA,
	.sdram_tim3			= 0x107F8678,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x50074BE4,
	.temp_alert_config		= 0x0,
	.emif_ddr_phy_ctlr_1		= 0x0E004008,
	.emif_ddr_ext_phy_ctrl_1	= 0x08020080,
	.emif_ddr_ext_phy_ctrl_2	= 0x00000065,
	.emif_ddr_ext_phy_ctrl_3	= 0x00000091,
	.emif_ddr_ext_phy_ctrl_4	= 0x000000B5,
	.emif_ddr_ext_phy_ctrl_5	= 0x000000E5,
	.emif_rd_wr_exec_thresh		= 0x80000405,
	.emif_prio_class_serv_map	= 0x80000001,
	.emif_connect_id_serv_1_map	= 0x80000094,
	.emif_connect_id_serv_2_map	= 0x00000000,
	.emif_cos_config		= 0x000FFFFF
};

/* EMIF DDR3 Configurations are different for production AM43X GP EVMs */
const struct emif_regs ddr3_emif_regs_400Mhz_production = {
	.sdram_config			= 0x638413B2,
	.ref_ctrl			= 0x00000C30,
	.sdram_tim1			= 0xEAAAD4DB,
	.sdram_tim2			= 0x266B7FDA,
	.sdram_tim3			= 0x107F8678,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x50074BE4,
	.temp_alert_config		= 0x0,
	.emif_ddr_phy_ctlr_1		= 0x0E004008,
	.emif_ddr_ext_phy_ctrl_1	= 0x08020080,
	.emif_ddr_ext_phy_ctrl_2	= 0x00000066,
	.emif_ddr_ext_phy_ctrl_3	= 0x00000091,
	.emif_ddr_ext_phy_ctrl_4	= 0x000000B9,
	.emif_ddr_ext_phy_ctrl_5	= 0x000000E6,
	.emif_rd_wr_exec_thresh		= 0x80000405,
	.emif_prio_class_serv_map	= 0x80000001,
	.emif_connect_id_serv_1_map	= 0x80000094,
	.emif_connect_id_serv_2_map	= 0x00000000,
	.emif_cos_config		= 0x000FFFFF
};

static const struct emif_regs ddr3_sk_emif_regs_400Mhz = {
	.sdram_config			= 0x638413b2,
	.sdram_config2			= 0x00000000,
	.ref_ctrl			= 0x00000c30,
	.sdram_tim1			= 0xeaaad4db,
	.sdram_tim2			= 0x266b7fda,
	.sdram_tim3			= 0x107f8678,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x50074be4,
	.temp_alert_config		= 0x0,
	.emif_ddr_phy_ctlr_1		= 0x0e084008,
	.emif_ddr_ext_phy_ctrl_1	= 0x08020080,
	.emif_ddr_ext_phy_ctrl_2	= 0x89,
	.emif_ddr_ext_phy_ctrl_3	= 0x90,
	.emif_ddr_ext_phy_ctrl_4	= 0x8e,
	.emif_ddr_ext_phy_ctrl_5	= 0x8d,
	.emif_rd_wr_lvl_rmp_win		= 0x0,
	.emif_rd_wr_lvl_rmp_ctl		= 0x00000000,
	.emif_rd_wr_lvl_ctl		= 0x00000000,
	.emif_rd_wr_exec_thresh		= 0x80000000,
	.emif_prio_class_serv_map	= 0x80000001,
	.emif_connect_id_serv_1_map	= 0x80000094,
	.emif_connect_id_serv_2_map	= 0x00000000,
	.emif_cos_config		= 0x000FFFFF
};

static const struct emif_regs ddr3_idk_emif_regs_400Mhz = {
	.sdram_config			= 0x61a11b32,
	.sdram_config2			= 0x00000000,
	.ref_ctrl			= 0x00000c30,
	.sdram_tim1			= 0xeaaad4db,
	.sdram_tim2			= 0x266b7fda,
	.sdram_tim3			= 0x107f8678,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x50074be4,
	.temp_alert_config		= 0x00000000,
	.emif_ddr_phy_ctlr_1		= 0x00008009,
	.emif_ddr_ext_phy_ctrl_1	= 0x08020080,
	.emif_ddr_ext_phy_ctrl_2	= 0x00000040,
	.emif_ddr_ext_phy_ctrl_3	= 0x0000003e,
	.emif_ddr_ext_phy_ctrl_4	= 0x00000051,
	.emif_ddr_ext_phy_ctrl_5	= 0x00000051,
	.emif_rd_wr_lvl_rmp_win		= 0x00000000,
	.emif_rd_wr_lvl_rmp_ctl		= 0x00000000,
	.emif_rd_wr_lvl_ctl		= 0x00000000,
	.emif_rd_wr_exec_thresh		= 0x00000405,
	.emif_prio_class_serv_map	= 0x00000000,
	.emif_connect_id_serv_1_map	= 0x00000000,
	.emif_connect_id_serv_2_map	= 0x00000000,
	.emif_cos_config		= 0x00ffffff
};

void emif_get_ext_phy_ctrl_const_regs(const u32 **regs, u32 *size)
{
	if (board_is_eposevm()) {
		*regs = ext_phy_ctrl_const_base_lpddr2;
		*size = ARRAY_SIZE(ext_phy_ctrl_const_base_lpddr2);
	}

	return;
}

/*
 * get_sys_clk_index : returns the index of the sys_clk read from
 *			ctrl status register. This value is either
 *			read from efuse or sysboot pins.
 */
static u32 get_sys_clk_index(void)
{
	struct ctrl_stat *ctrl = (struct ctrl_stat *)CTRL_BASE;
	u32 ind = readl(&ctrl->statusreg), src;

	src = (ind & CTRL_CRYSTAL_FREQ_SRC_MASK) >> CTRL_CRYSTAL_FREQ_SRC_SHIFT;
	if (src == CTRL_CRYSTAL_FREQ_SRC_EFUSE) /* Value read from EFUSE */
		return ((ind & CTRL_CRYSTAL_FREQ_SELECTION_MASK) >>
			CTRL_CRYSTAL_FREQ_SELECTION_SHIFT);
	else /* Value read from SYS BOOT pins */
		return ((ind & CTRL_SYSBOOT_15_14_MASK) >>
			CTRL_SYSBOOT_15_14_SHIFT);
}

const struct dpll_params *get_dpll_ddr_params(void)
{
	int ind = get_sys_clk_index();

	if (board_is_eposevm())
		return &epos_evm_dpll_ddr[ind];
	else if (board_is_evm() || board_is_sk())
		return &gp_evm_dpll_ddr;
	else if (board_is_idk())
		return &idk_dpll_ddr;

	printf(" Board '%s' not supported\n", board_ti_get_name());
	return NULL;
}


/*
 * get_opp_offset:
 * Returns the index for safest OPP of the device to boot.
 * max_off:	Index of the MAX OPP in DEV ATTRIBUTE register.
 * min_off:	Index of the MIN OPP in DEV ATTRIBUTE register.
 * This data is read from dev_attribute register which is e-fused.
 * A'1' in bit indicates OPP disabled and not available, a '0' indicates
 * OPP available. Lowest OPP starts with min_off. So returning the
 * bit with rightmost '0'.
 */
static int get_opp_offset(int max_off, int min_off)
{
	struct ctrl_stat *ctrl = (struct ctrl_stat *)CTRL_BASE;
	int opp, offset, i;

	/* Bits 0:11 are defined to be the MPU_MAX_FREQ */
	opp = readl(&ctrl->dev_attr) & ~0xFFFFF000;

	for (i = max_off; i >= min_off; i--) {
		offset = opp & (1 << i);
		if (!offset)
			return i;
	}

	return min_off;
}

/*移到spl.c了，在am33xx调用，同步的cm_t43的spl代码*/
const struct dpll_params *get_dpll_mpu_params(void)
{
	int opp = get_opp_offset(DEV_ATTR_MAX_OFFSET, DEV_ATTR_MIN_OFFSET);
	u32 ind = get_sys_clk_index();

	return &dpll_mpu[ind][opp];
}

const struct dpll_params *get_dpll_core_params(void)
{
	int ind = get_sys_clk_index();

	return &dpll_core[ind];
}

const struct dpll_params *get_dpll_per_params(void)
{
	int ind = get_sys_clk_index();

	return &dpll_per[ind];
}

void scale_vcores_generic(u32 m)
{
	int mpu_vdd;

	if (i2c_probe(TPS65218_CHIP_PM))
		return;

	switch (m) {
	case 1000:
		mpu_vdd = TPS65218_DCDC_VOLT_SEL_1330MV;
		break;
	case 800:
		mpu_vdd = TPS65218_DCDC_VOLT_SEL_1260MV;
		break;
	case 720:
		mpu_vdd = TPS65218_DCDC_VOLT_SEL_1200MV;
		break;
	case 600:
		mpu_vdd = TPS65218_DCDC_VOLT_SEL_1100MV;
		break;
	case 300:
		mpu_vdd = TPS65218_DCDC_VOLT_SEL_0950MV;
		break;
	default:
		puts("Unknown MPU clock, not scaling\n");
		return;
	}

	/* Set DCDC1 (CORE) voltage to 1.1V */
	if (tps65218_voltage_update(TPS65218_DCDC1,
				    TPS65218_DCDC_VOLT_SEL_1100MV)) {
		printf("%s failure\n", __func__);
		return;
	}

	/* Set DCDC2 (MPU) voltage */
	if (tps65218_voltage_update(TPS65218_DCDC2, mpu_vdd)) {
		printf("%s failure\n", __func__);
		return;
	}
}

void scale_vcores_idk(u32 m)
{
	int mpu_vdd;

	if (i2c_probe(TPS62362_I2C_ADDR))
		return;

	switch (m) {
	case 1000:
		mpu_vdd = TPS62362_DCDC_VOLT_SEL_1330MV;
		break;
	case 800:
		mpu_vdd = TPS62362_DCDC_VOLT_SEL_1260MV;
		break;
	case 720:
		mpu_vdd = TPS62362_DCDC_VOLT_SEL_1200MV;
		break;
	case 600:
		mpu_vdd = TPS62362_DCDC_VOLT_SEL_1100MV;
		break;
	case 300:
		mpu_vdd = TPS62362_DCDC_VOLT_SEL_1330MV;
		break;
	default:
		puts("Unknown MPU clock, not scaling\n");
		return;
	}

	/* Set VDD_MPU voltage */
	if (tps62362_voltage_update(TPS62362_SET3, mpu_vdd)) {
		printf("%s failure\n", __func__);
		return;
	}
}

void gpi2c_init(void)
{
	/* When needed to be invoked prior to BSS initialization */
	static bool first_time = true;

	if (first_time) {
		enable_i2c0_pin_mux();
		i2c_init(CONFIG_SYS_OMAP24_I2C_SPEED,
			 CONFIG_SYS_OMAP24_I2C_SLAVE);
		first_time = false;
	}
}

/*移到spl.c了，在am33xx调用，同步的cm_t43的spl代码*/
void scale_vcores(void)
{
	const struct dpll_params *mpu_params;

	/* Ensure I2C is initialized for PMIC configuration */
	gpi2c_init();

	/* Get the frequency */
	mpu_params = get_dpll_mpu_params();

	if (board_is_idk())
		scale_vcores_idk(mpu_params->m);
	else
		scale_vcores_generic(mpu_params->m);
}

#endif
#endif

/*此文件不在xxx中编译 函数需要移到mux.c中*/
/*这2个接口封装后给armv7/am33xx下提供接口。*/
#if 0
void set_uart_mux_conf(void)
{
	enable_uart0_pin_mux();
}

void set_mux_conf_regs(void)
{
	enable_board_pin_mux();
}
#endif

#if 0
#if 0
static void enable_vtt_regulator(void)
{
	u32 temp;

	/* enable module */
	writel(GPIO_CTRL_ENABLEMODULE, AM33XX_GPIO5_BASE + OMAP_GPIO_CTRL);

	/* enable output for GPIO5_7 */
	writel(GPIO_SETDATAOUT(7),
	       AM33XX_GPIO5_BASE + OMAP_GPIO_SETDATAOUT);
	temp = readl(AM33XX_GPIO5_BASE + OMAP_GPIO_OE);
	temp = temp & ~(GPIO_OE_ENABLE(7));
	writel(temp, AM33XX_GPIO5_BASE + OMAP_GPIO_OE);
}

enum {
	RTC_BOARD_EPOS = 1,
	RTC_BOARD_EVM14,
	RTC_BOARD_EVM12,
	RTC_BOARD_GPEVM,
	RTC_BOARD_SK,
};

/*
 * In the rtc_only boot path we have the board type info in the rtc scratch pad
 * register hence we bypass the costly i2c reads to eeprom and directly program
 * the board name string
 */
void rtc_only_update_board_type(u32 btype)
{
	const char *name = "";
	const char *rev = "1.0";

	switch (btype) {
	case RTC_BOARD_EPOS:
		name = "AM43EPOS";
		break;
	case RTC_BOARD_EVM14:
		name = "AM43__GP";
		rev = "1.4";
		break;
	case RTC_BOARD_EVM12:
		name = "AM43__GP";
		rev = "1.2";
		break;
	case RTC_BOARD_GPEVM:
		name = "AM43__GP";
		break;
	case RTC_BOARD_SK:
		name = "AM43__SK";
		break;
	}
	ti_i2c_eeprom_am_set(name, rev);
}

u32 rtc_only_get_board_type(void)
{
	if (board_is_eposevm())
		return RTC_BOARD_EPOS;
	else if (board_is_evm_14_or_later())
		return RTC_BOARD_EVM14;
	else if (board_is_evm_12_or_later())
		return RTC_BOARD_EVM12;
	else if (board_is_gpevm())
		return RTC_BOARD_GPEVM;
	else if (board_is_sk())
		return RTC_BOARD_SK;

	return 0;
}

void sdram_init(void)
{
	/*
	 * EPOS EVM has 1GB LPDDR2 connected to EMIF.
	 * GP EMV has 1GB DDR3 connected to EMIF
	 * along with VTT regulator.
	 */
	if (board_is_eposevm()) {
		config_ddr(0, &ioregs_lpddr2, NULL, NULL, &emif_regs_lpddr2, 0);
	} else if (board_is_evm_14_or_later()) {
		enable_vtt_regulator();
		config_ddr(0, &ioregs_ddr3, NULL, NULL,
			   &ddr3_emif_regs_400Mhz_production, 0);
	} else if (board_is_evm_12_or_later()) {
		enable_vtt_regulator();
		config_ddr(0, &ioregs_ddr3, NULL, NULL,
			   &ddr3_emif_regs_400Mhz_beta, 0);
	} else if (board_is_evm()) {
		enable_vtt_regulator();
		config_ddr(0, &ioregs_ddr3, NULL, NULL,
			   &ddr3_emif_regs_400Mhz, 0);
	} else if (board_is_sk()) {
		config_ddr(400, &ioregs_ddr3, NULL, NULL,
			   &ddr3_sk_emif_regs_400Mhz, 0);
	} else if (board_is_idk()) {
		config_ddr(400, &ioregs_ddr3, NULL, NULL,
			   &ddr3_idk_emif_regs_400Mhz, 0);
	}
}
#endif
#endif

/* setup board specific PMIC */
int power_init_board(void)
{
	struct pmic *p;
	uchar tps_status = 0;

    puts("PMIC:  TPS65218 skip!\n");
    return 0;

/*add@20180308 for crsc 同步myir 使用65218电源芯片*/
#if 0
	if (board_is_idk()) {
		power_tps62362_init(I2C_PMIC);
		p = pmic_get("TPS62362");
		if (p && !pmic_probe(p))
			puts("PMIC:  TPS62362\n");
	} else 
#else
    if(board_is_crsc_c437x_idk())
#endif
	{
		power_tps65218_init(I2C_PMIC);
		p = pmic_get("TPS65218_PMIC");
		if (p && !pmic_probe(p))
		{
			puts("PMIC:  TPS65218\n");
			
			/*begin:add@20180308 for crsc 同步myir*/
			/* We don't care if fseal is locked, but we do need it set */
			tps65218_lock_fseal();
			tps65218_reg_read(TPS65218_STATUS, &tps_status);
			if (!(tps_status & TPS65218_FSEAL))
				printf("WARNING: RTC not backed by battery!\n");
		    /*end:add@20180308 for crsc 同步myir*/
		}
	}

	return 0;
}

int board_init(void)
{
	struct l3f_cfg_bwlimiter *bwlimiter = (struct l3f_cfg_bwlimiter *)L3F_CFG_BWLIMITER;
	u32 mreqprio_0, mreqprio_1, modena_init0_bw_fractional,
	    modena_init0_bw_integer, modena_init0_watermark_0;

	gd->bd->bi_boot_params = CONFIG_SYS_SDRAM_BASE + 0x100;
	gpmc_init();

	/* Clear all important bits for DSS errata that may need to be tweaked*/
	mreqprio_0 = readl(&cdev->mreqprio_0) & MREQPRIO_0_SAB_INIT1_MASK &
	                   MREQPRIO_0_SAB_INIT0_MASK;

	mreqprio_1 = readl(&cdev->mreqprio_1) & MREQPRIO_1_DSS_MASK;

	modena_init0_bw_fractional = readl(&bwlimiter->modena_init0_bw_fractional) &
	                                   BW_LIMITER_BW_FRAC_MASK;

	modena_init0_bw_integer = readl(&bwlimiter->modena_init0_bw_integer) &
	                                BW_LIMITER_BW_INT_MASK;

	modena_init0_watermark_0 = readl(&bwlimiter->modena_init0_watermark_0) &
	                                 BW_LIMITER_BW_WATERMARK_MASK;

	/* Setting MReq Priority of the DSS*/
	mreqprio_0 |= 0x77;

	/*
	 * Set L3 Fast Configuration Register
	 * Limiting bandwith for ARM core to 700 MBPS
	 */
	modena_init0_bw_fractional |= 0x10;
	modena_init0_bw_integer |= 0x3;

	writel(mreqprio_0, &cdev->mreqprio_0);
	writel(mreqprio_1, &cdev->mreqprio_1);

	writel(modena_init0_bw_fractional, &bwlimiter->modena_init0_bw_fractional);
	writel(modena_init0_bw_integer, &bwlimiter->modena_init0_bw_integer);
	writel(modena_init0_watermark_0, &bwlimiter->modena_init0_watermark_0);

	return 0;
}

#ifdef CONFIG_BOARD_LATE_INIT
int board_late_init(void)
{
#ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG
	set_board_info_env("crsc_c437x_idk");

	/*
	 * Default FIT boot on HS devices. Non FIT images are not allowed
	 * on HS devices.
	 */
	if (get_device_type() == HS_DEVICE)
		setenv("boot_fit", "1");
#endif
	return 0;
}
#endif

#ifdef CONFIG_USB_DWC3
static struct dwc3_device usb_otg_ss1 = {
	.maximum_speed = USB_SPEED_HIGH,
	.base = USB_OTG_SS1_BASE,
	.tx_fifo_resize = false,
	.index = 0,
};

static struct dwc3_omap_device usb_otg_ss1_glue = {
	.base = (void *)USB_OTG_SS1_GLUE_BASE,
	.utmi_mode = DWC3_OMAP_UTMI_MODE_SW,
	.index = 0,
};

static struct ti_usb_phy_device usb_phy1_device = {
	.usb2_phy_power = (void *)USB2_PHY1_POWER,
	.index = 0,
};

static struct dwc3_device usb_otg_ss2 = {
	.maximum_speed = USB_SPEED_HIGH,
	.base = USB_OTG_SS2_BASE,
	.tx_fifo_resize = false,
	.index = 1,
};

static struct dwc3_omap_device usb_otg_ss2_glue = {
	.base = (void *)USB_OTG_SS2_GLUE_BASE,
	.utmi_mode = DWC3_OMAP_UTMI_MODE_SW,
	.index = 1,
};

static struct ti_usb_phy_device usb_phy2_device = {
	.usb2_phy_power = (void *)USB2_PHY2_POWER,
	.index = 1,
};

int usb_gadget_handle_interrupts(int index)
{
	u32 status;

	status = dwc3_omap_uboot_interrupt_status(index);
	if (status)
		dwc3_uboot_handle_interrupt(index);

	return 0;
}
#endif /* CONFIG_USB_DWC3 */

#if defined(CONFIG_USB_DWC3) || defined(CONFIG_USB_XHCI_OMAP)
int board_usb_init(int index, enum usb_init_type init)
{
	enable_usb_clocks(index);
#ifdef CONFIG_USB_DWC3
	switch (index) {
	case 0:
		if (init == USB_INIT_DEVICE) {
			usb_otg_ss1.dr_mode = USB_DR_MODE_PERIPHERAL;
			usb_otg_ss1_glue.vbus_id_status = OMAP_DWC3_VBUS_VALID;
			dwc3_omap_uboot_init(&usb_otg_ss1_glue);
			ti_usb_phy_uboot_init(&usb_phy1_device);
			dwc3_uboot_init(&usb_otg_ss1);
		}
		break;
	case 1:
		if (init == USB_INIT_DEVICE) {
			usb_otg_ss2.dr_mode = USB_DR_MODE_PERIPHERAL;
			usb_otg_ss2_glue.vbus_id_status = OMAP_DWC3_VBUS_VALID;
			ti_usb_phy_uboot_init(&usb_phy2_device);
			dwc3_omap_uboot_init(&usb_otg_ss2_glue);
			dwc3_uboot_init(&usb_otg_ss2);
		}
		break;
	default:
		printf("Invalid Controller Index\n");
	}
#endif

	return 0;
}

int board_usb_cleanup(int index, enum usb_init_type init)
{
#ifdef CONFIG_USB_DWC3
	switch (index) {
	case 0:
	case 1:
		if (init == USB_INIT_DEVICE) {
			ti_usb_phy_uboot_exit(index);
			dwc3_uboot_exit(index);
			dwc3_omap_uboot_exit(index);
		}
		break;
	default:
		printf("Invalid Controller Index\n");
	}
#endif
	disable_usb_clocks(index);

	return 0;
}
#endif /* defined(CONFIG_USB_DWC3) || defined(CONFIG_USB_XHCI_OMAP) */

#ifndef CONFIG_DM_ETH  /*crsc当前定义了，则不编译以下部分*/
#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
	(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
static void cpsw_control(int enabled)
{
	/* Additional controls can be added here */
	return;
}

/*add@20180308 for crsc 同步myir增加多组初始值*/
static struct cpsw_slave_data cpsw_slaves[] = {
	{
		.slave_reg_ofs	= 0x208, /*CPSW_PORT 0x4A10_0100+108h: CPSW_PORT_P1_MAX_BLKS*/
		.sliver_reg_ofs	= 0xd80, /*CPSW_SL1 0x4A10_0D80: Ethernet Sliver for Port 1*/
		.phy_addr	= 0, 
	},
	{
		.slave_reg_ofs	= 0x208,
		.sliver_reg_ofs	= 0xd80,
		.phy_addr	= 1,
	},
	{
		.slave_reg_ofs	= 0x208,
		.sliver_reg_ofs	= 0xd80,
		.phy_addr	= 4,
	},
	{
		.slave_reg_ofs	= 0x308, /*CPSW_PORT 0x4A10_0100+208h: CPSW_PORT_P2_MAX_BLKS*/
		.sliver_reg_ofs	= 0xdc0, /*CPSW_SL2 0x4A10_0DC0: Ethernet Sliver for Port 2*/
		.phy_addr	= 0,
	},
	{
		.slave_reg_ofs	= 0x308,
		.sliver_reg_ofs = 0xdc0,
		.phy_addr	= 1,
	},
	{
		.slave_reg_ofs	= 0x308,
		.sliver_reg_ofs = 0xdc0,
		.phy_addr	= 4,
	},
};

static struct cpsw_platform_data cpsw_data = {
	.mdio_base		= CPSW_MDIO_BASE,  /*CPSW_MDIO 0x4A10_1000*/
	.cpsw_base		= CPSW_BASE,  /*0x4A10_0000*/
	.mdio_div		= 0xff,
	.channels		= 8,
	.cpdma_reg_ofs	= 0x800,
	.slaves			= 6, /*add@20180308 for crsc 同步myir由1改为6，扫描多个slave地址*/
	.slave_data		= cpsw_slaves,
	.ale_reg_ofs		= 0xd00,
	.ale_entries		= 1024,
	.host_port_reg_ofs	= 0x108,
	.hw_stats_reg_ofs	= 0x900,
	.bd_ram_ofs		    = 0x2000,
	.mac_control		= (1 << 5),
	.control		    = cpsw_control,
	.host_port_num		= 0,
	.version		    = CPSW_CTRL_VERSION_2,
};
#endif

/*
 * This function will:
 * Read the eFuse for MAC addresses, and set ethaddr/eth1addr/usbnet_devaddr
 * in the environment
 * Perform fixups to the PHY present on certain boards.  We only need this
 * function in:
 * - SPL with either CPSW or USB ethernet support
 * - Full U-Boot, with either CPSW or USB ethernet
 * Build in only these cases to avoid warnings about unused variables
 * when we build an SPL that has neither option but full U-Boot will.
 */
#if ((defined(CONFIG_SPL_ETH_SUPPORT) || \
	defined(CONFIG_SPL_USBETH_SUPPORT)) && \
	defined(CONFIG_SPL_BUILD)) || \
	((defined(CONFIG_DRIVER_TI_CPSW) || \
	  defined(CONFIG_USB_ETHER)) && !defined(CONFIG_SPL_BUILD))
int board_eth_init(bd_t *bis)
{
	int rv;
	uint8_t mac_addr[6];
	uint32_t mac_hi, mac_lo;

    /*crsc新增 cpu2需要初始化
    if (board_is_crsc_c437x_idk())
    {
        puts("crsc_c437x not support eth!\n");
        return 0;
    }*/

	/* try reading mac address from efuse 从cpu寄存器读出mac值*/
	mac_lo = readl(&cdev->macid0l);
	mac_hi = readl(&cdev->macid0h);
	mac_addr[0] = mac_hi & 0xFF;
	mac_addr[1] = (mac_hi & 0xFF00) >> 8;
	mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
	mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
	mac_addr[4] = mac_lo & 0xFF;
	mac_addr[5] = (mac_lo & 0xFF00) >> 8;

#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
	(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
	if (!getenv("ethaddr")) {
		puts("<ethaddr> not set. Validating first E-fuse MAC\n");
		if (is_valid_ethaddr(mac_addr))
			eth_setenv_enetaddr("ethaddr", mac_addr);
	}

#ifndef CONFIG_SPL_BUILD
	mac_lo = readl(&cdev->macid1l);
	mac_hi = readl(&cdev->macid1h);
	mac_addr[0] = mac_hi & 0xFF;
	mac_addr[1] = (mac_hi & 0xFF00) >> 8;
	mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
	mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
	mac_addr[4] = mac_lo & 0xFF;
	mac_addr[5] = (mac_lo & 0xFF00) >> 8;

	if (!getenv("eth1addr")) {
		if (is_valid_ethaddr(mac_addr))
			eth_setenv_enetaddr("eth1addr", mac_addr);
	}

#endif

/*add@20180308 for crsc 同步myir 注掉其他分支*/
#if 0
	if (board_is_eposevm()) {
		writel(RMII_MODE_ENABLE | RMII_CHIPCKL_ENABLE, &cdev->miisel);
		cpsw_slaves[0].phy_if = PHY_INTERFACE_MODE_RMII;
		cpsw_slaves[0].phy_addr = 16;
	} else if (board_is_sk()) {
		writel(RGMII_MODE_ENABLE, &cdev->miisel);
		cpsw_slaves[0].phy_if = PHY_INTERFACE_MODE_RGMII;
		cpsw_slaves[0].phy_addr = 4;
		cpsw_slaves[1].phy_addr = 5;
	} else if (board_is_idk()) 
#else
    if (board_is_crsc_c437x_idk())
#endif
	{
		//writel(RGMII_MODE_ENABLE, &cdev->miisel);
		/*RMII选择启用CPU的参考时钟*/
		writel(RMII_MODE_ENABLE | RMII_CHIPCKL_ENABLE, &cdev->miisel);
        cpsw_slaves[0].phy_if = PHY_INTERFACE_MODE_RMII;
        cpsw_slaves[1].phy_if = PHY_INTERFACE_MODE_RMII;
        cpsw_slaves[2].phy_if = PHY_INTERFACE_MODE_RMII;
		cpsw_slaves[3].phy_if = PHY_INTERFACE_MODE_RMII;
        cpsw_slaves[4].phy_if = PHY_INTERFACE_MODE_RMII;
        cpsw_slaves[5].phy_if = PHY_INTERFACE_MODE_RMII;
		/*cpsw_slaves[0].phy_addr = 4; 由0改为4但是注掉了*/
	} 
#if 0
	else {
		writel(RGMII_MODE_ENABLE, &cdev->miisel);
		cpsw_slaves[0].phy_if = PHY_INTERFACE_MODE_RGMII;
		cpsw_slaves[0].phy_addr = 0;
	}
#endif

	rv = cpsw_register(&cpsw_data);
	if (rv < 0) {
		printf("Error %d registering CPSW switch\n", rv);
		return rv;
	}
#endif
#if defined(CONFIG_USB_ETHER) && \
	(!defined(CONFIG_SPL_BUILD) || defined(CONFIG_SPL_USBETH_SUPPORT))
	if (is_valid_ethaddr(mac_addr))
		eth_setenv_enetaddr("usbnet_devaddr", mac_addr);

	rv = usb_eth_initialize(bis);
	if (rv < 0)
		printf("Error %d registering USB_ETHER\n", rv);
#endif

	return rv;
}
#endif
#endif

/*add@20180308 for crsc 此文件不在spl中编译，需要将此函数移到spl.c中*/
#if 0
#ifdef CONFIG_SPL_LOAD_FIT
int board_fit_config_name_match(const char *name)
{
/*add@20180308 for crsc*/
#if 0
	if (board_is_evm() && !strcmp(name, "am437x-gp-evm"))
		return 0;
	else if (board_is_sk() && !strcmp(name, "am437x-sk-evm"))
		return 0;
	else if (board_is_eposevm() && !strcmp(name, "am43x-epos-evm"))
		return 0;
	else if (board_is_idk() && !strcmp(name, "am437x-idk-evm"))
		return 0;
	else
		return -1;
#else
    if (board_is_crsc_c437x_idk() && !strcmp(name, "crsc_c437x"))
    {
        return 0;
    }
    else
    {
        return -1;
    }
#endif
}
#endif
#endif

#ifdef CONFIG_TI_SECURE_DEVICE
void board_fit_image_post_process(void **p_image, size_t *p_size)
{
	secure_boot_verify_image(p_image, p_size);
}
#endif