# dhcpd.conf # # Sample configuration file for ISC dhcpd # # Attention: If /etc/ltsp/dhcpd.conf exists, that will be used as # configuration file instead of this file. # # option definitions common to all supported networks... option domain-name "example.org"; # JM option domain-name-servers ns1.example.org, ns2.example.org; default-lease-time 600; max-lease-time 7200; # The ddns-updates-style parameter controls whether or not the server will # attempt to do a DNS update when a lease is confirmed. We default to the # behavior of the version 2 packages ('none', since DHCP v2 didn't # have support for DDNS.) ddns-update-style none; # If this DHCP server is the official DHCP server for the local # network, the authoritative directive should be uncommented. #authoritative; # Use this to send dhcp log messages to a different log file (you also # have to hack syslog.conf to complete the redirection). #log-facility local7; # No service will be given on this subnet, but declaring it helps the # DHCP server to understand the network topology. #subnet 10.152.187.0 netmask 255.255.255.0 { #} # This is a very basic subnet declaration. #subnet 10.254.239.0 netmask 255.255.255.224 { # range 10.254.239.10 10.254.239.20; # option routers rtr-239-0-1.example.org, rtr-239-0-2.example.org; #} # This declaration allows BOOTP clients to get dynamic addresses, # which we don't really recommend. #subnet 10.254.239.32 netmask 255.255.255.224 { # range dynamic-bootp 10.254.239.40 10.254.239.60; # option broadcast-address 10.254.239.31; # option routers rtr-239-32-1.example.org; #} # A slightly different configuration for an internal subnet. #subnet 10.5.5.0 netmask 255.255.255.224 { # range 10.5.5.26 10.5.5.30; # option domain-name-servers ns1.internal.example.org; # option domain-name "internal.example.org"; # option subnet-mask 255.255.255.224; # option routers 10.5.5.1; # option broadcast-address 10.5.5.31; # default-lease-time 600; # max-lease-time 7200; #} # Hosts which require special configuration options can be listed in # host statements. If no address is specified, the address will be # allocated dynamically (if possible), but the host-specific information # will still come from the host declaration. #host passacaglia { # hardware ethernet 0:0:c0:5d:bd:95; # filename "vmunix.passacaglia"; # server-name "toccata.example.com"; #} # Fixed IP addresses can also be specified for hosts. These addresses # should not also be listed as being available for dynamic assignment. # Hosts for which fixed IP addresses have been specified can boot using # BOOTP or DHCP. Hosts for which no fixed address is specified can only # be booted with DHCP, unless there is an address range on the subnet # to which a BOOTP client is connected which has the dynamic-bootp flag # set. #host fantasia { # hardware ethernet 08:00:07:26:c0:a5; # fixed-address fantasia.example.com; #} # You can declare a class of clients and then do address allocation # based on that. The example below shows a case where all clients # in a certain class get addresses on the 10.17.224/24 subnet, and all # other clients get addresses on the 10.0.29/24 subnet. #class "foo" { # match if substring (option vendor-class-identifier, 0, 4) = "SUNW"; #} #shared-network 224-29 { # subnet 10.17.224.0 netmask 255.255.255.0 { # option routers rtr-224.example.org; # } # subnet 10.0.29.0 netmask 255.255.255.0 { # option routers rtr-29.example.org; # } # pool { # allow members of "foo"; # range 10.17.224.10 10.17.224.250; # } # pool { # deny members of "foo"; # range 10.0.29.10 10.0.29.230; # } #} # Jim's TEST option subnet-mask 255.255.255.0; option broadcast-address 192.168.1.255; option routers 192.168.1.254; option domain-name-servers 192.168.1.1, 8.8.8.8; #subnet 192.168.1.0 netmask 255.255.255.0 { #range 192.168.1.201 192.168.1.220; #} subnet 192.168.1.0 netmask 255.255.255.0 { range dynamic-bootp 192.168.1.201 192.168.1.210; if substring (option vendor-class-identifier, 0, 16) = "TI K3 Bootp Boot" { filename "tiboot3.bin"; } elsif substring (option vendor-class-identifier, 0, 20) = "AM62X U-Boot R5 SPL" { filename "tispl.bin"; } elsif substring (option vendor-class-identifier, 0, 21) = "AM62X U-Boot A53 SPL" { filename "u-boot.img"; } range 192.168.1.211 192.168.1.220; default-lease-time 60000; max-lease-time 720000; next-server 192.168.1.1; }