CCCCCCCC U-Boot SPL 2011.09 (Apr 08 2012 - 18:29:14) Texas Instruments Revision detection unimplemented OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2011.09 (Apr 08 2012 - 18:25:03) I2C: ready DRAM: 256 MiB WARNING: Caches not enabled Found a daughter card connected NAND: HW ECC Hamming Code selected 256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Error: Bad compare! failed Error: Bad compare! failed Error: Bad compare! failed NAND read from offset 260000 failed -74 *** Warning - readenv() failed, using default environment Net: cpsw Hit any key to stop autoboot: 0 SD/MMC found on device 0 reading uEnv.txt ** Unable to read "uEnv.txt" from mmc 0:1 ** reading uImage 3232704 bytes read ## Booting kernel from Legacy Image at 80007fc0 ... Image Name: Linux-3.2.33-rt10 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 3232640 Bytes = 3.1 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK XIP Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.33-rt10 (phillips@vm-benson-ubu-12) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #2 PREEMPT RT Thu Nov 22 13:53:03 IST 2012 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none [ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes) [ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Memory: 256MB = 256MB total [ 0.000000] Memory: 253116k/253116k available, 9028k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB) [ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc05b8000 (5824 kB) [ 0.000000] .init : 0xc05b8000 - 0xc05f8000 ( 256 kB) [ 0.000000] .data : 0xc05f8000 - 0xc0665908 ( 439 kB) [ 0.000000] .bss : 0xc066592c - 0xc0693888 ( 184 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000244] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.058929] pid_max: default: 32768 minimum: 301 [ 0.059082] Security Framework initialized [ 0.059204] Mount-cache hash table entries: 512 [ 0.059661] CPU: Testing write buffer coherency: ok [ 0.080535] omap_hwmod: pruss: failed to hardreset [ 0.081909] print_constraints: dummy: [ 0.082366] NET: Registered protocol family 16 [ 0.085205] OMAP GPIO hardware version 0.1 [ 0.089294] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.092254] omap_i2c.1: alias fck already exists [ 0.093414] omap2_mcspi.1: alias fck already exists [ 0.093719] omap2_mcspi.2: alias fck already exists [ 0.094635] edma.0: alias fck already exists [ 0.094665] edma.0: alias fck already exists [ 0.094696] edma.0: alias fck already exists [ 0.136505] bio: create slab at 0 [ 0.140350] SCSI subsystem initialized [ 0.142608] usbcore: registered new interface driver usbfs [ 0.143035] usbcore: registered new interface driver hub [ 0.143310] usbcore: registered new device driver usb [ 0.159332] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.161743] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.164337] print_constraints: VRTC: [ 0.165893] print_constraints: VIO: at 1800 mV [ 0.168365] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.170989] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.172119] print_constraints: VDD3: 5000 mV [ 0.173645] print_constraints: VDIG1: at 1800 mV [ 0.175201] print_constraints: VDIG2: at 1800 mV [ 0.176727] print_constraints: VPLL: at 1800 mV [ 0.178283] print_constraints: VDAC: at 1800 mV [ 0.179870] print_constraints: VAUX1: at 1800 mV [ 0.181457] print_constraints: VAUX2: at 3300 mV [ 0.182983] print_constraints: VAUX33: at 3300 mV [ 0.184539] print_constraints: VMMC: at 3300 mV [ 0.185150] tps65910 1-002d: No interrupt support, no core IRQ [ 0.186859] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.188354] Switching to clocksource gp timer [ 0.210723] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.211364] NET: Registered protocol family 2 [ 0.211608] IP route cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.211975] TCP established hash table entries: 8192 (order: 4, 65536 bytes) [ 0.212158] TCP bind hash table entries: 8192 (order: 5, 196608 bytes) [ 0.212554] TCP: Hash tables configured (established 8192 bind 8192) [ 0.212554] TCP reno registered [ 0.212585] UDP hash table entries: 128 (order: 1, 8192 bytes) [ 0.212615] UDP-Lite hash table entries: 128 (order: 1, 8192 bytes) [ 0.212860] NET: Registered protocol family 1 [ 0.213256] RPC: Registered named UNIX socket transport module. [ 0.213256] RPC: Registered udp transport module. [ 0.213287] RPC: Registered tcp transport module. [ 0.213287] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.213562] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.217681] VFS: Disk quotas dquot_6.5.2 [ 0.217742] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.218933] msgmni has been set to 494 [ 0.222900] alg: No test for stdrng (krng) [ 0.223693] io scheduler noop registered [ 0.223693] io scheduler deadline registered [ 0.223785] io scheduler cfq registered (default) [ 0.225250] Could not set LED4 to fully on [ 0.227355] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.746551] console [ttyO0] enabled [ 0.747283] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.747833] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.748352] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.748962] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.749481] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.762420] brd: module loaded [ 0.769470] loop: module loaded [ 0.769714] i2c-core: driver [tsl2550] using legacy suspend method [ 0.769714] i2c-core: driver [tsl2550] using legacy resume method [ 0.769805] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.776641] Detected a daughter card on AM335x EVM.. [ 0.776672] Unknown CPLD version found [ 0.776702] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.784942] Board name: A33515BB [ 0.784942] Board version: 1.1 [ 0.784942] SKU: SKU#01 [ 0.785491] The board is general purpose EVM in profile 0 [ 0.786010] da8xx_lcdc.0: alias fck already exists [ 0.786621] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel [ 0.913513] Console: switching to colour frame buffer device 100x30 [ 0.930664] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 0.930694] Registering NAND on CS0 [ 0.931549] omap_i2c.2: alias fck already exists [ 0.948852] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 0.949768] tsl2550 2-0039: standard operating mode [ 0.950469] tsl2550 2-0039: support ver. 1.2 enabled [ 0.951232] davinci-mcasp.1: alias fck already exists [ 0.951782] omap_hsmmc.0: alias fck already exists [ 0.952148] omap_hsmmc.2: alias fck already exists [ 0.952514] Configure Bluetooth Enable pin... [ 0.954284] registered am33xx_sr device [ 0.954589] _regulator_get: 2-0018 supply Vdd not found, using dummy regulator [ 0.954681] _regulator_get: 2-0018 supply Vdd_IO not found, using dummy regulator [ 0.969299] lis3lv02d: 8 bits 3DLH sensor found [ 1.062927] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0 [ 1.065704] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.066528] omap2-nand driver initializing [ 1.066894] ONFI flash detected [ 1.067016] ONFI param page 0 valid [ 1.067047] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP) [ 1.067352] Creating 8 MTD partitions on "omap2-nand.0": [ 1.067382] 0x000000000000-0x000000020000 : "SPL" [ 1.069427] 0x000000020000-0x000000040000 : "SPL.backup1" [ 1.071166] 0x000000040000-0x000000060000 : "SPL.backup2" [ 1.072875] 0x000000060000-0x000000080000 : "SPL.backup3" [ 1.074462] 0x000000080000-0x000000260000 : "U-Boot" [ 1.076873] 0x000000260000-0x000000280000 : "U-Boot Env" [ 1.078521] 0x000000280000-0x000000780000 : "Kernel" [ 1.082641] 0x000000780000-0x000010000000 : "File System" [ 1.188659] OneNAND driver initializing [ 1.208953] CAN device driver interface [ 1.208953] CAN bus driver for Bosch D_CAN controller 1.0 [ 1.268829] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.268829] davinci_mdio davinci_mdio.0: detected phy mask fffffffe [ 1.279449] davinci_mdio.0: probed [ 1.279479] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown [ 1.279907] usbcore: registered new interface driver zd1201 [ 1.286651] usbcore: registered new interface driver cdc_ether [ 1.286865] usbcore: registered new interface driver cdc_eem [ 1.287078] usbcore: registered new interface driver dm9601 [ 1.287139] cdc_ncm: 04-Aug-2011 [ 1.287353] usbcore: registered new interface driver cdc_ncm [ 1.287353] Initializing USB Mass Storage driver... [ 1.289001] usbcore: registered new interface driver usb-storage [ 1.289001] USB Mass Storage support registered. [ 1.299255] mousedev: PS/2 mouse device common for all mice [ 1.300659] input: matrix-keypad as /devices/platform/matrix-keypad/input/input1 [ 1.310089] input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input2 [ 1.319824] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 1.329010] i2c /dev entries driver [ 1.329895] Linux video capture interface: v2.00 [ 1.330352] usbcore: registered new interface driver uvcvideo [ 1.330352] USB Video Class driver (1.1.1) [ 1.335388] lm75 2-0048: hwmon0: sensor 'tmp275' [ 1.348999] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 1.359375] cpuidle: using governor ladder [ 1.368194] cpuidle: using governor menu [ 1.382415] omap4_aes_mod_init: loading AM33X AES driver [ 1.382537] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02 [ 1.383331] omap4_aes_probe: probe() done [ 1.389007] omap4_sham_mod_init: loading AM33X SHA/MD5 driver [ 1.389312] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03 [ 1.461364] omap4_sham_probe: probe() done [ 1.489501] usbcore: registered new interface driver usbhid [ 1.489501] usbhid: USB HID core driver [ 1.490570] usbcore: registered new interface driver snd-usb-audio [ 1.504119] mmc0: new SDHC card at address e624 [ 1.509399] _regulator_get: 2-001b supply IOVDD not found, using dummy regulator [ 1.509460] _regulator_get: 2-001b supply DVDD not found, using dummy regulator [ 1.509552] _regulator_get: 2-001b supply AVDD not found, using dummy regulator [ 1.509613] _regulator_get: 2-001b supply DRVDD not found, using dummy regulator [ 1.513061] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok [ 1.514190] mmcblk0: mmc0:e624 SD08G 7.40 GiB [ 1.519683] mmcblk0: p1 p2 [ 1.529541] ALSA device list: [ 1.529571] #0: AM335X EVM [ 1.529571] nf_conntrack version 0.5.0 (3954 buckets, 15816 max) [ 1.530212] ip_tables: (C) 2000-2006 Netfilter Core Team [ 1.530334] TCP cubic registered [ 1.530364] NET: Registered protocol family 17 [ 1.530364] can: controller area network core (rev 20090105 abi 8) [ 1.530517] NET: Registered protocol family 29 [ 1.530517] can: raw protocol (rev 20090105) [ 1.530517] can: broadcast manager protocol (rev 20090105 t) [ 1.530578] Registering the dns_resolver key type [ 1.530670] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 1.530700] ThumbEE CPU extension supported. [ 1.530761] mux: Failed to setup hwmod io irq -22 [ 1.531829] Power Management for AM33XX family [ 1.703460] mmc1: card claims to support voltages below the defined range. These will be ignored. [ 1.713287] mmc1: queuing unknown CIS tuple 0x91 (3 bytes) [ 1.714294] mmc1: new SDIO card at address 0001 [ 1.748809] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 1.748992] Copied the M3 firmware to UMEM [ 1.749328] smartreflex smartreflex: am33xx_sr_probe: Zero NValue read from EFUSE [ 1.749359] smartreflex: probe of smartreflex failed with error -22 [ 1.749877] sr_init: platform driver register failed [ 1.757934] clock: disabling unused clocks to save power [ 1.780059] Detected MACID=d4:94:a1:90:c6:b5 [ 1.781677] cpsw: Detected MACID = d4:94:a1:90:c6:b6 [ 1.783752] input: gpio-keys as /devices/platform/gpio-keys/input/input3 [ 1.789978] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 2.683319] EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended [ 2.683502] kjournald starting. Commit interval 5 seconds [ 2.686279] EXT3-fs (mmcblk0p2): using internal journal [ 2.686309] EXT3-fs (mmcblk0p2): recovery complete [ 2.688903] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 2.688995] VFS: Mounted root (ext3 filesystem) on device 179:2. [ 2.689514] Freeing init memory: 256K INIT: version 2.86 booting Please wait: booting... Starting udev Remounting root file system... Caching udev devnodes ALSA: Restoring mixer settings... Configuring network interfaces... No state is present for card EVM Found hardware: "AM335X_EVM" "" "" "" "" Hardware is initialized using a generic method No state is present for card EVM eth0 no wireless extensions. udhcpc (v1.13.2) started Sending discover... Sending discover... Sending discover... No lease, forking to background done. Setting up IP spoofing protection: rp_filter. Wed Apr 11 08:27:00 UTC 2012 [ 3.426116] udevd (958): /proc/958/oom_adj is deprecated, please use /proc/958/oom_score_adj instead. [ 8.610809] alignment: ignoring faults is unsafe on this CPU. Defaulting to fixup mode. [ 10.526885] net eth0: CPSW phy found : id is : 0x4dd074 [ 13.520355] PHY: 0:00 - Link is Up - 100/Full INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Hardware abstraction layer hald Starting Dropbear SSH server: dropbear. Starting telnet daemon. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Starting PVR Usage: insmod filename [args] Could not find pvrsrvkm driver Starting Lighttpd Web Server: lighttpd. 2012-04-11 08:27:02: (log.c.166) server started / Starting Matrix GUI application. [ 23.680541] net eth0: CPSW phy found : id is : 0x4dd074 [ 25.681243] PHY: 0:00 - Link is Up - 100/Full *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2011.09 am335x-evm ttyO0