U-Boot 2021.01-g2dd2e1d366 (Sep 24 2022 - 18:36:08 +0000) SoC: AM62X SR1.0 GP Model: Texas Instruments AM625 SK EEPROM not available at 0x50, trying to read at 0x51 Board: AM62-SKEVM rev E2 DRAM: 2 GiB MMC: mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645 gpt_verify_headers: *** ERROR: Invalid GPT *** Verify GPT: error! Broken MMC partition scheme Running Fastboot... dwc3-generic-peripheral usb@31000000: failed to enable ep0out failed to start : -110 g_dnl_register: failed!, error: -110 Error: mmc 0:misc read failed (-1) Warning: BCB is corrupted or does not exist Loading Android boot partition... switch to partitions #0, OK mmc0(part 0) is current device misc partition not found A/B cmdline addition: androidboot.slot_suffix=_ Running without AVB... mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan [mode] mmc part - lists available partition on current mmc device mmc dev [dev] [part] [mode] - show or set current mmc device [partition] and set mode - the required speed mode is passed as the index from the following list [MMC_LEGACY, MMC_HS, SD_HS, MMC_HS_52, MMC_DDR_52, UHS_SDR12, UHS_SDR25, UHS_SDR50, UHS_DDR50, UHS_SDR104, MMC_HS_200, MMC_HS_400, MMC_HS_400_ES] mmc list - lists available devices mmc wp - power on write protect boot partitions mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize - Change sizes of boot and RPMB partitions of specified device mmc partconf dev [boot_ack boot_partition partition_access] - Show or change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr - set DSR register value Failed to boot Android... dwc3-generic-peripheral usb@31000000: failed to enable ep0out failed to start : -110 g_dnl_register: failed!, error: -110 => => fastboot 0 dwc3-generic-peripheral usb@31000000: failed to enable ep0out failed to start : -110 g_dnl_register: failed!, error: -110 exit not allowed from main input shell. => fastboot fastboot - run as a fastboot usb or udp device Usage: fastboot [-l addr] [-s size] usb | udp addr - address of buffer used during data transfers (0xC0000000) size - size of buffer used during data transfers (0x2F000000) => fastboot 1 No USB device found USB init failed: -19 => fastboot 2 No USB device found USB init failed: -19 => fastboot 0 dwc3-generic-peripheral usb@31000000: failed to enable ep0out failed to start : -110 g_dnl_register: failed!, error: -110 exit not allowed from main input shell. =>