#The camera is not connected root@am62axx-evm:/opt/edgeai-gst-apps# x=0; while [ $x -le 31 ]; do printf "Register 0x%02X = " $x ; phytool read eth0/0/$x $(( x++ )) ; done Register 0x00 = 0x1140 Register 0x01 = 0x7949 Register 0x02 = 0x2000 Register 0x03 = 0xa231 Register 0x04 = 0x05e1 Register 0x05 = 0000 Register 0x06 = 0x0066 Register 0x07 = 0x2001 Register 0x08 = 0000 Register 0x09 = 0x0200 Register 0x0A = 0000 Register 0x0B = 0000 Register 0x0C = 0000 Register 0x0D = 0x401f Register 0x0E = 0x0050 Register 0x0F = 0x3000 Register 0x10 = 0x5048 Register 0x11 = 0x0002 Register 0x12 = 0000 Register 0x13 = 0x1c46 Register 0x14 = 0x2bc7 Register 0x15 = 0x0127 Register 0x16 = 0000 Register 0x17 = 0x0040 Register 0x18 = 0x6150 Register 0x19 = 0x4444 Register 0x1A = 0x0002 Register 0x1B = 0000 Register 0x1C = 0000 Register 0x1D = 0000 Register 0x1E = 0x0202 Register 0x1F = 0000 #I connected the camera at this moment root@am62axx-evm:/opt/edgeai-gst-apps# [ 4325.112811] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off [ 4327.148577] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down root@am62axx-evm:/opt/edgeai-gst-apps# x=0; while [ $x -le 31 ]; do printf "Register 0x%02X = " $x ; phytool read eth0/0/$x $(( x++ )) ; done Register 0x00 = 0x1140 Register 0x01 = 0x796d Register 0x02 = 0x2000 Register 0x03 = 0xa231 Register 0x04 = 0x05e1 Register 0x05 = 0xc1e1 Register 0x06 = 0x006f Register 0x07 = 0x2001 Register 0x08 = 0x6801 Register 0x09 = 0x0200 Register 0x0A = 0000 Register 0x0B = 0000 Register 0x0C = 0000 Register 0x0D = 0x401f Register 0x0E = 0x0049 Register 0x0F = 0x3000 Register 0x10 = 0x5048 Register 0x11 = 0x7c02 Register 0x12 = 0000 Register 0x13 = 0x1c46 Register 0x14 = 0x2bc7 Register 0x15 = 0x012c Register 0x16 = 0000 Register 0x17 = 0x0040 Register 0x18 = 0x6150 Register 0x19 = 0x4444 Register 0x1A = 0x0002 Register 0x1B = 0000 Register 0x1C = 0000 Register 0x1D = 0000 Register 0x1E = 0x0202 Register 0x1F = 0000 [ 4531.947588] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off root@am62axx-evm:/opt/edgeai-gst-apps# x=0; while [ $x -le 31 ]; do printf "Register 0x%02X = " $x ; phytool read eth0/0/$x $(( x++ )) ; done Register 0x00 = 0x1140 Register 0x01 = 0x796d Register 0x02 = 0x2000 Register 0x03 = 0xa231 Register 0x04 = 0x05e1 Register 0x05 = 0xc1e1 Register 0x06 = 0x006f Register 0x07 = 0x2001 Register 0x08 = 0x6801 Register 0x09 = 0x0200 Register 0x0A = 0000 Register 0x0B = 0000 Register 0x0C = 0000 Register 0x0D = 0x401f Register 0x0E = 0x004d Register 0x0F = 0x3000 Register 0x10 = 0x5048 Register 0x11 = 0x6f02 Register 0x12 = 0000 Register 0x13 = 0x1c44 Register 0x14 = 0x2bc7 Register 0x15 = 0x012c Register 0x16 = 0000 Register 0x17 = 0x0040 Register 0x18 = 0x6150 Register 0x19 = 0x4444 Register 0x1A = 0x0002 Register 0x1B = 0000 Register 0x1C = 0000 Register 0x1D = 0000 Register 0x1E = 0x0202 Register 0x1F = 0000