U-Boot SPL 2021.01-g2ee8efd654 (Feb 24 2023 - 05:37:51 +0000) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') SPL initial stack usage: 13424 bytes Trying to boot from MMC1 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from MMC... OK init_env from device 9 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 05:33:19, Feb 24 2023 U-Boot SPL 2021.01-g2ee8efd654 (Feb 24 2023 - 05:36:12 +0000) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') Trying to boot from MMC1 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2021.01-g2ee8efd654 (Feb 24 2023 - 05:36:12 +0000) SoC: AM62X SR1.0 GP Model: Texas Instruments AM625 SK EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed 1 DRAM: 2 GiB MMC: mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 EEPROM not available at 0x50, trying to read at 0x51 Reading on-board EEPROM at 0x51 failed 1 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0(part 0) is current device SD/MMC found on device 0 Failed to load 'boot.scr' ** Unrecognized filesystem type ** 18862592 bytes read in 109 ms (165 MiB/s) 57533 bytes read in 4 ms (13.7 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.10.168-rt83-gc1a1291911 (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT_RT Fri Feb 24 05:50:07 UTC 2023 [ 0.000000] Machine model: Texas Instruments AM625 SK [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 3 MiB [ 0.000000] OF: reserved mem: initialized node ipc-memories@9c800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cb00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node m4f-dma-memory@9cb00000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009cc00000, size 14 MiB [ 0.000000] OF: reserved mem: initialized node m4f-memory@9cc00000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009da00000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9da00000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009db00000, size 12 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9db00000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009c7fffff] [ 0.000000] node 0: [mem 0x000000009c800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff] [ 0.000000] node 0: [mem 0x000000009e780000-0x000000009fffffff] [ 0.000000] node 0: [mem 0x00000000a0000000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] On node 0 totalpages: 524288 [ 0.000000] DMA zone: 8192 pages used for memmap [ 0.000000] DMA zone: 0 pages reserved [ 0.000000] DMA zone: 524288 pages, LIFO batch:63 [ 0.000000] cma: Reserved 512 MiB at 0x00000000dd000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 18 pages/cpu s35392 r8192 d30144 u73728 [ 0.000000] pcpu-alloc: s35392 r8192 d30144 u73728 alloc=18*4096 [ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516096 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=344e7b40-01 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1456212K/2097152K available (11008K kernel code, 1204K rwdata, 4272K rodata, 1792K init, 438K bss, 116652K reserved, 524288K cma-reserved) [ 0.000000] Unable to handle kernel paging request at virtual address ffff800112e61c50 [ 0.000000] Mem abort info: [ 0.000000] ESR = 0x96000005 [ 0.000000] EC = 0x25: DABT (current EL), IL = 32 bits [ 0.000000] SET = 0, FnV = 0 [ 0.000000] EA = 0, S1PTW = 0 [ 0.000000] Data abort info: [ 0.000000] ISV = 0, ISS = 0x00000005 [ 0.000000] CM = 0, WnR = 0 [ 0.000000] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000082f01000 [ 0.000000] [ffff800112e61c50] pgd=00000000fffff003, p4d=00000000fffff003, pud=0000000000000000 [ 0.000000] Internal error: Oops: 96000005 [#1] PREEMPT_RT SMP [ 0.000000] Modules linked in: [ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 5.10.168-rt83-gc1a1291911 #1 [ 0.000000] Hardware name: Texas Instruments AM625 SK (DT) [ 0.000000] pstate: 20000085 (nzCv daIf -PAN -UAO -TCO BTYPE=--) [ 0.000000] pc : +0x1c91f8/0x1270000 [ 0.000000] lr : +0x1cbc44/0x1270000 [ 0.000000] sp : ffff8000110d3cd0 [ 0.000000] x29: ffff8000110d3cd0 x28: ffff8000111e5200 [ 0.000000] x27: 0000000000000010 x26: 0000000000000000 [ 0.000000] x25: 0000000000000000 x24: ffff00007fb93c28 [ 0.000000] x23: 0000000000000000 x22: 0000000000000000 [ 0.000000] x21: 0000000000000000 x20: 00000000000000c0 [ 0.000000] x19: ffff00007fb93c38 x18: 0000000000000002 [ 0.000000] x17: 0000000000012000 x16: ffff8000111e6000 [ 0.000000] x15: 0000000000000000 x14: 0000000000000000 [ 0.000000] x13: 000000000000000a x12: ffff8000111e56d0 [ 0.000000] x11: ffff00007fb93c38 x10: 000000000000000c [ 0.000000] x9 : 0000000000000000 x8 : 0000000000000000 [ 0.000000] x7 : ffff800112e61c50 x6 : ffff8000111e56d0 [ 0.000000] x5 : ffff800010af1c78 x4 : ffff8000110d3de7 [ 0.000000] x3 : 0000000000000000 x2 : 0000000101c7c580 [ 0.000000] x1 : 000000000000000a x0 : 00000000101c7c58 [ 0.000000] Call trace: [ 0.000000] +0x1c91f8/0x1270000 [ 0.000000] +0x1ced90/0x1270000 [ 0.000000] +0x1ea0fc/0x1270000 [ 0.000000] +0x1eee0c/0x1270000 [ 0.000000] +0xf21cc0/0xf575bc [ 0.000000] +0xf265a4/0xf575bc [ 0.000000] +0xf10dd8/0xf575bc [ 0.000000] Code: 9b2a1445 d503201f 937c7c02 8b0200c7 (f86268c2) [ 0.000000] ---[ end trace 0000000000000001 ]--- [ 0.000000] Kernel panic - not syncing: [ 0.000000] Attempted to kill the idle task! [ 0.000000] ---[ end Kernel panic - not syncing: Attempted to kill the idle task! ]---