U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000) EEPROM not available at 0x50, trying to read at 0x51 Resetting on cold boot to workaround ErrataID:i2331 Please resend tiboot3.bin in case of UART/DFU boot resetting ... U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000) EEPROM not available at 0x50, trying to read at 0x51 SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') SPL initial stack usage: 13376 bytes Trying to boot from MMC2 mmc fail to send stop cmd Error reading cluster Authentication passed Authentication passed Authentication passed Authentication passed Loading Environment from MMC... MMC Device 0 not found *** Warning - No MMC card found, using default environment Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty NOTICE: BL31: Built : 00:42:57, Jan 13 2023 I/TC: I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') Trying to boot from MMC2 Authentication passed Authentication passed U-Boot 2023.04-g24098ea90d (Jul 06 2023 - 12:59:40 +0000) SoC: AM64X SR2.0 HS-FS Model: Texas Instruments AM642 SK Board: AM64B-SKEVM rev A DRAM: 2 GiB Core: 63 devices, 31 uclasses, devicetree: separate MMC: mmc@fa00000: 1 Loading Environment from MMC... MMC Device 0 not found *** Warning - No MMC card found, using default environment In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: ethernet@8000000port@1 Warning: ethernet@8000000port@2 MAC addresses don't match: Address in ROM is 34:08:e1:80:ae:13 Address in environment is 70:ff:76:1e:bc:49 , eth1: ethernet@8000000port@2 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 574 bytes read in 29 ms (18.6 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... mmc fail to send stop cmd ** fs_devread read error - block Failed to load '/boot/Image' ** No partition table - mmc 1 ** Couldn't find partition mmc 1:2 Can't set block device libfdt fdt_check_header(): FDT_ERR_BADMAGIC No FDT memory address configured. Please configure the FDT address via "fdt addr
" command. Aborting! ERROR: Did not find a cmdline Flattened Device Tree Could not find a valid device tree MMC Device 0 not found no mmc device at slot 0 switch to partitions #0, OK mmc1 is current device Scanning mmc 1:1... No EFI system partition No EFI system partition Failed to persist EFI variables BootOrder not defined EFI boot manager: Cannot load any image Found EFI removable media binary efi/boot/bootaa64.efi 733184 bytes read in 60 ms (11.7 MiB/s) Booting /efi\boot\bootaa64.efi Welcome to GRUB! error: no such device: ((hd0,msdos1)/efi/boot)/EFI/BOOT/grub.cfg. error: serial port `com0' isn't found. GNU GRUB version 2.06 lqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqk x*boot x x x x x x x x x x x x x x x x x x x x x x x x x x x x x mqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqqj Use the ? and ? keys to select which entry is highlighted. Press enter to boot the selected OS, `e' to edit the commands before booting or `c' for a command-line. The highlighted entry will be executed automatically in 0s. Booting `boot' mmc fail to send stop cmd error: failure reading sector 0x1100 from `hd0'. Press any key to continue...