[Start: Blackhawk XDS560v2-USB System Trace Emulator_0] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ /home/mcla/.ti/ti/0/0/BrdDat/testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'bh560v2u.out'. Loaded FPGA Image: /home/mcla/ti/ccsv6/ccs_base/common/uscif/./././././dtc_top.jbc The library build date was 'Feb 19 2015'. The library build time was '00:08:17'. The library package version is '5.1.641.0'. The library component version is '35.34.40.0'. The controller does not use a programmable FPGA. The controller has a version number of '6' (0x00000006). The controller has an insertion length of '0' (0x00000000). The cable+pod has a version number of '8' (0x00000008). The cable+pod has a capability number of '7423' (0x00001cff). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the Nano-TBC VHDL. The link is a 560-class second-generation-560 cable. The software is configured for Nano-TBC VHDL features. The controller will be software reset via its registers. The controller has a logic ONE on its EMU[0] input pin. The controller has a logic ONE on its EMU[1] input pin. The controller will use falling-edge timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '2' (0x0002). The utility logic has not previously detected a power-loss. The utility logic is not currently detecting a power-loss. Loaded FPGA Image: /home/mcla/ti/ccsv6/ccs_base/common/uscif/./././././dtc_top.jbc An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-230' (0xffffff1a). The title is 'SC_ERR_PATH_MEASURE'. The explanation is: The measured lengths of the JTAG IR and DR scan-paths are invalid. This indicates that an error exists in the link-delay or scan-path. [End: Blackhawk XDS560v2-USB System Trace Emulator_0]