U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:46:46 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') read_dqs_training:ERROR: Read DQS Gate training failed DRAM init failed: -22 resetting ... U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:46:46 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') read_dqs_training:ERROR: Read DQS Gate training failed DRAM init failed: -22 resetting ... U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:46:46 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') read_dqs_training:ERROR: Read DQS Gate training failed DRAM init failed: -22 resetting ... U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:46:46 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') rest_training: ERROR: Write Leveling adjustment failed DRAM init failed: -22 resetting ... U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:46:46 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') rest_training: ERROR: Write Leveling adjustment failed DRAM init failed: -22 resetting ... U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:46:46 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') rest_training: ERROR: Write Leveling adjustment failed DRAM init failed: -22 resetting ... U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:46:46 +0000) SYSFW ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') Trying to boot from MMC2 Starting ATF on ARM64 core... NOTICE: BL31: v2.1(release):ti2019.01-rc2 NOTICE: BL31: Built : 04:28:26, Jul 7 2019 I/TC: I/TC: OP-TEE version: 3.2.0-583-g251f7c6-dev #1 Sun Jul 7 04:40:43 UTC 2019 aarch64 I/TC: Initialized U-Boot SPL 2019.01-g8b90adfb16 (Jul 07 2019 - 05:09:26 +0000) detected AM6-IDKAPPEVM detected SER-PCIE2LEVM Trying to boot from MMC2 U-Boot 2019.01-g8b90adfb16 (Jul 07 2019 - 05:09:26 +0000) Model: Texas Instruments AM654 Base Board DRAM: 4 GiB MMC: sdhci@4f80000: 0, sdhci@04FA0000: 1 Loading Environment from MMC... *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial detected AM6-IDKAPPEVM detected SER-PCIE2LEVM Net: eth2: pruss0_eth Warning: cpsw_nuss@046000000 using MAC address from ROM , eth0: cpsw_nuss@046000000, eth1: pruss2_eth Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 ** Unable to read file boot.scr ** 1490 bytes read in 3 ms (484.4 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... 1 bytes read in 2 ms (0 Bytes/s) Already setup. 12632072 bytes read in 1062 ms (11.3 MiB/s) 71809 bytes read in 11 ms (6.2 MiB/s) 11402 bytes read in 3 ms (3.6 MiB/s) 2084 bytes read in 2 ms (1017.6 KiB/s) ## Flattened Device Tree blob at 82000000 Booting using the fdt blob at 0x82000000 Loading Device Tree to 00000000fddb7000, end 00000000fdecbfff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 4.19.38-g4dae378bbe (oe-user@oe-host) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 SMP PREEMPT Sun Jul 7 03:42:51 UTC 2019 [ 0.000000] Machine model: Texas Instruments AM654 Base Board [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] bootconsole [ns16550a0] enabled [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9b100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c100000, size 7 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@9c100000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 512 MiB at 0x00000000c0000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.1 [ 0.000000] random: get_random_bytes called from start_kernel+0x94/0x3e4 with crng_init=0 [ 0.000000] percpu: Embedded 2 pages/cpu s48536 r8192 d74344 u131072 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: enabling workaround for ARM erratum 845719 [ 0.000000] Speculative Store Bypass Disable mitigation not required [ 0.000000] CPU features: detected: Kernel page table isolation (KPTI) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64704 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),-@8m(ospi.rootfs) root=PARTUUID=5d2ac6ad-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes) [ 0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes) [ 0.000000] software IO TLB: mapped [mem 0xf9db0000-0xfddb0000] (64MB) [ 0.000000] Memory: 3529856K/4145152K available (8062K kernel code, 752K rwdata, 2880K rodata, 576K init, 614K bss, 91008K reserved, 524288K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4. [ 0.000000] Tasks RCU enabled. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: no VLPI support, no direct LPI support [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8c0800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GIC: using LPI property table @0x00000008c00c0000 [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] CPU0: using LPI pending table @0x00000008c00d0000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000005] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008698] Console: colour dummy device 80x25 [ 0.013293] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023981] pid_max: default: 32768 minimum: 301 [ 0.028806] Security Framework initialized [ 0.033067] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes) [ 0.039948] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes) [ 0.071385] ASID allocator initialised with 32768 entries [ 0.084953] rcu: Hierarchical SRCU implementation. [ 0.098034] Platform MSI: gic-its@18200000 domain created [ 0.103879] PCI/MSI: /interconnect@100000/interrupt-controller@1800000/gic-its@18200000 domain created [ 0.121447] smp: Bringing up secondary CPUs ... [ 0.158571] Detected VIPT I-cache on CPU1 [ 0.158610] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.158666] CPU1: using LPI pending table @0x00000008c0330000 [ 0.158713] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.220252] Detected VIPT I-cache on CPU2 [ 0.220294] GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000 [ 0.220358] CPU2: using LPI pending table @0x00000008c03c0000 [ 0.220406] CPU2: Booted secondary processor 0x0000000100 [0x410fd034] [ 0.252664] Detected VIPT I-cache on CPU3 [ 0.252694] GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000 [ 0.252750] CPU3: using LPI pending table @0x00000008c0450000 [ 0.252787] CPU3: Booted secondary processor 0x0000000101 [0x410fd034] [ 0.252927] smp: Brought up 1 node, 4 CPUs [ 0.328557] SMP: Total of 4 processors activated. [ 0.333380] CPU features: detected: GIC system register CPU interface [ 0.339991] CPU features: detected: 32-bit EL0 Support [ 0.367819] CPU: All CPU(s) started at EL2 [ 0.372039] alternatives: patching kernel code [ 0.378055] devtmpfs: initialized [ 0.393211] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.403215] futex hash table entries: 1024 (order: 0, 65536 bytes) [ 0.410953] pinctrl core: initialized pinctrl subsystem [ 0.416947] NET: Registered protocol family 16 [ 0.422731] vdso: 2 pages (1 code @ (____ptrval____), 1 data @ (____ptrval____)) [ 0.430321] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.443710] DMA: preallocated 256 KiB pool for atomic allocations [ 0.452543] davinci_gpio 42110000.wkup_gpio0: IRQ not populated, err = -517 [ 0.466827] davinci_gpio 600000.main_gpio0: IRQ not populated, err = -517 [ 0.474034] davinci_gpio 601000.main_gpio1: IRQ not populated, err = -517 [ 0.492117] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.498996] HugeTLB registered 512 MiB page size, pre-allocated 0 pages [ 0.507812] cryptd: max_cpu_qlen set to 1000 [ 0.514003] media: Linux media interface: v0.10 [ 0.518684] videodev: Linux video capture interface: v2.00 [ 0.524342] pps_core: LinuxPPS API ver. 1 registered [ 0.529425] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.538786] PTP clock support registered [ 0.542827] EDAC MC: Ver: 3.0.0 [ 0.547350] Advanced Linux Sound Architecture Driver Initialized. [ 0.554534] clocksource: Switched to clocksource arch_sys_counter [ 0.560991] VFS: Disk quotas dquot_6.6.0 [ 0.565101] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes) [ 0.579401] NET: Registered protocol family 2 [ 0.584559] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes) [ 0.592711] TCP established hash table entries: 32768 (order: 2, 262144 bytes) [ 0.600404] TCP bind hash table entries: 32768 (order: 3, 524288 bytes) [ 0.607757] TCP: Hash tables configured (established 32768 bind 32768) [ 0.614624] UDP hash table entries: 2048 (order: 0, 65536 bytes) [ 0.620889] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes) [ 0.627771] NET: Registered protocol family 1 [ 0.632838] RPC: Registered named UNIX socket transport module. [ 0.638917] RPC: Registered udp transport module. [ 0.643735] RPC: Registered tcp transport module. [ 0.648551] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.656304] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 0.669630] Initialise system trusted keyrings [ 0.674404] workingset: timestamp_bits=46 max_order=16 bucket_order=0 [ 0.686270] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.693084] NFS: Registering the id_resolver key type [ 0.698290] Key type id_resolver registered [ 0.702575] Key type id_legacy registered [ 0.706695] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.713722] 9p: Installing v9fs 9p2000 file system support [ 0.724163] Key type asymmetric registered [ 0.728376] Asymmetric key parser 'x509' registered [ 0.733436] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.741115] io scheduler noop registered [ 0.745140] io scheduler deadline registered [ 0.749669] io scheduler cfq registered (default) [ 0.754496] io scheduler mq-deadline registered [ 0.759152] io scheduler kyber registered [ 0.765018] pinctrl-single 4301c000.pinmux: 70 pins, size 280 [ 0.771600] pinctrl-single 11c000.pinmux: 185 pins, size 740 [ 0.777546] pinctrl-single 11c2e8.pinmux: 9 pins, size 36 [ 0.784280] pinctrl-single a40000.timesync_router: 512 pins, size 2048 [ 0.799736] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.822940] brd: module loaded [ 0.833392] loop: module loaded [ 0.838986] libphy: Fixed MDIO Bus: probed [ 0.843750] tun: Universal TUN/TAP device driver, 1.6 [ 0.849722] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k [ 0.857750] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.863865] sky2: driver version 1.30 [ 0.869092] VFIO - User Level meta-driver version: 0.3 [ 0.875296] i2c /dev entries driver [ 0.880324] sdhci: Secure Digital Host Controller Interface driver [ 0.886664] sdhci: Copyright(c) Pierre Ossman [ 0.891597] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.898763] ledtrig-cpu: registered to indicate activity on CPUs [ 0.905016] ti-sci interconnect@100000:interconnect@28380000:interconnect@42040000:dmsc: invalid resource [ 0.915869] optee: probing for conduit method from DT. I/TC: Dynamic shared memory is disabled [ 0.921163] optee: revision 3.4 (251f7c63) [ 0.925102] optee: initialized driver [ 0.934489] NET: Registered protocol family 17 [ 0.939127] 9pnet: Installing 9P2000 support [ 0.943568] Key type dns_resolver registered [ 0.948579] registered taskstats version 1 [ 0.952784] Loading compiled-in X.509 certificates [ 0.958756] davinci_gpio 42110000.wkup_gpio0: IRQ not populated, err = -517 [ 0.966332] davinci_gpio 600000.main_gpio0: IRQ not populated, err = -517 [ 0.973542] davinci_gpio 601000.main_gpio1: IRQ not populated, err = -517 [ 0.990720] ti-sci interconnect@100000:interconnect@28380000:interconnect@42040000:dmsc: invalid resource [ 1.000723] ti-sci interconnect@100000:interconnect@28380000:interconnect@42040000:dmsc: ABI: 2.6 (firmware rev 0x0013 '19.4.1-v2019.04a (Curious Crow)') [ 1.034061] random: fast init done [ 1.536881] davinci_gpio 42110000.wkup_gpio0: IRQ not populated, err = -517 [ 1.544432] davinci_gpio 600000.main_gpio0: IRQ not populated, err = -517 [ 1.551632] davinci_gpio 601000.main_gpio1: IRQ not populated, err = -517 [ 1.560032] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz [ 1.566505] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz [ 1.595957] omap_i2c 2000000.i2c: bus 2 rev0.12 at 400 kHz [ 1.602315] omap_i2c 2010000.i2c: bus 3 rev0.12 at 400 kHz [ 1.608638] omap_i2c 2020000.i2c: bus 4 rev0.12 at 400 kHz [ 1.614936] omap_i2c 2030000.i2c: bus 5 rev0.12 at 100 kHz [ 1.629264] keystone-pcie 5500000.pcie: Linked as a consumer to phy-900000.serdes.0 [ 1.637145] keystone-pcie 5500000.pcie: Linked as a consumer to phy-910000.serdes.1 [ 1.650432] keystone-pcie 5500000.pcie: host bridge /interconnect@100000/pcie@5500000 ranges: [ 1.659193] keystone-pcie 5500000.pcie: IO 0x10020000..0x1002ffff -> 0x00000000 [ 1.666959] keystone-pcie 5500000.pcie: MEM 0x10030000..0x17ffffff -> 0x10030000 [ 2.675033] keystone-pcie 5500000.pcie: Phy link never came up [ 2.681137] keystone-pcie 5500000.pcie: PCI host bridge to bus 0000:00 [ 2.687832] pci_bus 0000:00: root bus resource [bus 00-ff] [ 2.693453] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 2.699786] pci_bus 0000:00: root bus resource [mem 0x10030000-0x17ffffff] [ 2.715732] pci 0000:00:00.0: BAR 6: assigned [mem 0x10030000-0x1003ffff pref] [ 2.723141] pci 0000:00:00.0: PCI bridge to [bus 01-ff] [ 2.729574] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,160] sci-dev-id:195 [ 2.739573] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: enabled [ 2.746261] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66344100, num_proxies:64 [ 2.754122] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:818, gp-rings[304,464] sci-dev-id:187 [ 2.764201] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: enabled [ 2.770888] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66344100, num_proxies:64 [ 2.778688] omap8250 40a00000.serial: PM domain ti_sci_pd will not be powered off [ 2.786771] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 8, base_baud = 6000000) is a 8250 [ 2.796485] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 22, base_baud = 3000000) is a 8250 [ 2.805262] console [ttyS2] enabled [ 2.805262] console [ttyS2] enabled [ 2.812317] bootconsole [ns16550a0] disabled [ 2.812317] bootconsole [ns16550a0] disabled [ 2.821698] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 23, base_baud = 3000000) is a 8250 [ 2.830980] 2820000.serial: ttyS4 at MMIO 0x2820000 (irq = 24, base_baud = 3000000) is a 8250 [ 2.841989] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes) [ 2.848199] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 2.854816] Creating 7 MTD partitions on "47040000.spi.0": [ 2.860306] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 2.866652] 0x000000080000-0x000000280000 : "ospi.tispl" [ 2.872679] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 2.878746] 0x000000680000-0x0000006a0000 : "ospi.env" [ 2.884567] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 2.890940] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 2.896867] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 3.010892] cadence-qspi 47040000.spi: Cadence QSPI NOR probe failed -517 [ 3.026126] am65-cpsw-nuss 46000000.ethernet: rx-flow-id-base is not set -22 [ 3.033294] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA07100, cpsw version 0x6BA80100 Ports: 2 [ 3.044831] UDMA has not been proped [ 3.048424] am65-cpsw-nuss 46000000.ethernet: Failed to request tx dma channel -517 [ 3.058722] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a2109, freq:200000000, add_val:4 pps:0 [ 3.067470] thermal thermal_zone1: failed to read out thermal zone (-22) [ 3.074197] thermal thermal_zone2: failed to read out thermal zone (-22) [ 3.081632] OF: /interconnect@100000/interconnect@28380000/rti@40610000: arguments longer than property [ 3.091042] keystone-wdt 40610000.rti: heartbeat 60 sec [ 3.097194] mmc0: Unknown controller version (4). You may experience problems. [ 3.135534] mmc0: SDHCI controller on 4f80000.sdhci [4f80000.sdhci] using ADMA 64-bit [ 3.144141] mmc1: Unknown controller version (4). You may experience problems. [ 3.181274] mmc1: SDHCI controller on 4fa0000.sdhci [4fa0000.sdhci] using ADMA 64-bit [ 3.190485] mmc0: new HS200 MMC card at address 0001 [ 3.196594] mmcblk0: mmc0:0001 S0J56X 14.8 GiB [ 3.202149] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB [ 3.211962] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB [ 3.220833] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (243:0) [ 3.254636] mmc1: Problem switching card into high-speed mode! [ 3.262165] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc5900 [ 3.268878] mmc1: new SDHC card at address 0001 [ 3.273643] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc5900 [ 3.281344] mmcblk1: mmc1:0001 SD32G 29.0 GiB [ 3.286797] ti-udma 285c0000.udmap: Channels: 96 (tchan: 48, echan: 0, rchan: 48, rflow: 96) [ 3.295327] mmcblk1: p1 p2 [ 3.305180] ti-udma 31150000.udmap: Channels: 267 (tchan: 120, echan: 32, rchan: 150, rflow: 300) [ 3.330155] cadence-qspi 47040000.spi: mt35xu512aba (65536 Kbytes) [ 3.336373] 7 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 3.342987] Creating 7 MTD partitions on "47040000.spi.0": [ 3.348478] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 3.354831] 0x000000080000-0x000000280000 : "ospi.tispl" [ 3.360786] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 3.366812] 0x000000680000-0x0000006a0000 : "ospi.env" [ 3.372623] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 3.379031] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 3.384973] 0x000000800000-0x000004000000 : "ospi.rootfs" [ 3.398072] m25p80 spi7.0: n25q128a13 (16384 Kbytes) [ 3.404331] am65-cpsw-nuss 46000000.ethernet: rx-flow-id-base is not set -22 [ 3.411495] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA07100, cpsw version 0x6BA80100 Ports: 2 [ 3.431744] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 3.445159] pps pps0: new PPS source ptp1 [ 3.449416] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a2109, freq:200000000, add_val:4 pps:1 [ 3.458412] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 0.4 [ 3.465634] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 3.510551] am65-cpsw-nuss 46000000.ethernet: davinci mdio revision 9.7, bus freq 1000000 [ 3.518728] libphy: 46000000.ethernet: probed [ 3.526466] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 3.533482] hctosys: unable to open rtc device (rtc0) [ 3.635821] ALSA device list: [ 3.638807] No soundcards found. [ 3.824205] EXT4-fs (mmcblk1p2): 2 orphan inodes deleted [ 3.829570] EXT4-fs (mmcblk1p2): recovery complete [ 3.862472] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [ 3.870627] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 3.891838] devtmpfs: mounted [ 3.895116] Freeing unused kernel memory: 576K [ 3.899605] Run /sbin/init as init process [ 4.575035] systemd[1]: System time before build time, advancing clock. [ 4.765774] NET: Registered protocol family 10 [ 4.771371] Segment Routing with IPv6 [ 4.840300] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 4.862060] systemd[1]: Detected architecture arm64. Welcome to Arago 2019.05! [ 4.904061] systemd[1]: Set hostname to . [ 5.224733] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling. [ 5.241797] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.) [ 5.572522] random: systemd: uninitialized urandom read (16 bytes read) [ 5.579590] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 5.602704] random: systemd: uninitialized urandom read (16 bytes read) [ 5.612085] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 5.630677] random: systemd: uninitialized urandom read (16 bytes read) [ 5.637571] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 5.654649] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 5.670829] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password Requests to Wall Directory Watch. [ OK ] Listening on Journal Socket (/dev/log). [ OK ] Created slice system-serial\x2dgetty.slice. [ OK ] Listening on Journal Socket. Starting Create list of required stcce nodes for the current kernel... [ OK ] Started Hardware RNG Entropy Gatherer Daemon. Starting Remount Root and Kernel File Systems... Starting Load Kernel Modules... [ 5.802285] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null) Mounting Huge Pages File System... Mounting Kernel Debug File System... [ 5.827867] cryptodev: loading out-of-tree module taints kernel. [ OK ] Listening on udev Kernel Socket. [ 5.843172] cryptodev: driver 1.9 loaded. [ OK ] Created slice User and Session Slice. [ OK ] Reached target Slices. Starting Journal Service... [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ OK ] Reached target Paths. Mounting POSIX Message Queue File System... [ OK ] Reached target Swap. Mounting Temporary Directory (/tmp)... [ OK ] Listening on Process Core Dump Socket. [ OK ] Listening on udev Control Socket. Starting udev Coldplug all Devices... [ OK ] Started Journal Service. [ OK ] Started Create list of required stacvice nodes for the current kernel. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Load Kernel Modules. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Temporary Directory (/tmp). Mounting Kernel Configuration File System... Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev... Starting Flush Journal to Persistent Storage... [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Apply Kernel Variables. [ 6.291374] systemd-journald[165]: Received request to flush runtime journal from PID 1 [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... [ OK ] Reached target Containers. Mounting /media/ram... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. [ OK ] Mounted /media/ram. [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... Starting Load/Save Random Seed... [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started udev Kernel Device Manager. [ OK ] Started Update UTMP about System Boot/Shutdown. Starting Network Service... [ OK ] Started udev Coldplug all Devices. [ 6.893859] input: gpio-decoder as /devices/platform/gpio-decoder/input/input1 [ OK ] Started Network Service. Starting Network Name Resolution... [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Synchronized. [ OK ] Reached target System Initialization. [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Reboot and dump vmcore via kexec... [ OK ] Started Daily rotation of log files. [ OK ] Reached target Timers. [ OK ] Listening on dropbear.socket.[ 7.194781] omap_rng 4e10000.trng: Random Number Generator ver. 230b34c [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. Starting RPC Bind Service... [ OK ] Started D-Bus System Message Bus. [ 7.339638] CAN device driver interface Starting TI IPC Daemon... [ 7.344305] [drm] Initialized pvr 1.17.4948957 20110701 for 7000000.gpu on minor 0 Starting Login Service... [ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf. Starting Print notice about GPLv3 packages... [ OK ] Started irqbalance daemon. Starting rng-tools.service... [ 7.457515] m_can 40528000.mcan: m_can device registered (irq=17, version=32) [ 7.479128] m_can 40568000.mcan: m_can device registered (irq=19, version=32) [ OK ] Started Periodic Command Scheduler. [ OK ] Started Job spooling tools. [ OK ] Started Network Name Resolution. [ OK ] Found device /dev/ttyS2. [ 7.587840] k3_r5_rproc interconnect@100000:interconnect@28380000:r5fss@41000000: creating child devices for R5F cores [ OK ] [ 7.602752] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@9c000000 Started TI IPC Daemon. [ 7.612634] remoteproc remoteproc0: 41000000.r5f is available [ OK ] Reached target Host and Network Name Lookups. [ OK ] Reached target Network. Starting Simple Network Management Protocol (SNMP) Daemon.... Starting Lightning Fast Webserver With Light System Requirements... Starting Permit User Sessions... [ 8.141130] random: crng init done [ 8.144722] random: 7 urandom warning(s) missed due to ratelimiting [ 8.166484] TI DP83867 k3-cpsw-mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=k3-cpsw-mdio:00, irq=POLL) [ 8.178408] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 8.474572] davinci_mdio b032400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 8.482184] libphy: b032400.mdio: probed [ 8.486771] remoteproc remoteproc0: powering up 41000000.r5f [ 8.492544] remoteproc remoteproc0: Booting fw image am65x-mcu-r5f0_0-fw, size 4050720 [ 8.511728] platform 41000000.r5f: booting R5F core using boot addr = 0x0 [ 8.512383] davinci_mdio b032400.mdio: phy[0]: device b032400.mdio:00, driver TI DP83867 [ 8.519810] remoteproc remoteproc0: registered virtio0 (type 7) [ 8.527093] davinci_mdio b032400.mdio: phy[3]: device b032400.mdio:03, driver TI DP83867 [ 8.536265] remoteproc remoteproc0: remote processor 41000000.r5f is now up [ 8.590708] davinci_mdio b132400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 8.598823] libphy: b132400.mdio: probed [ 8.627140] davinci_mdio b132400.mdio: phy[0]: device b132400.mdio:00, driver TI DP83867 [ 8.638665] davinci_mdio b132400.mdio: phy[3]: device b132400.mdio:03, driver TI DP83867 [ 8.730897] davinci_mdio b232400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 8.741863] libphy: b232400.mdio: probed [ 8.772986] davinci_mdio b232400.mdio: phy[0]: device b232400.mdio:00, driver TI DP83867 [ 8.786079] davinci_mdio b232400.mdio: phy[3]: device b232400.mdio:03, driver TI DP83867 [ 8.825901] remoteproc remoteproc1: b034000.pru is available [ 8.838703] pru-rproc b034000.pru: PRU rproc node pru@b034000 probed successfully [ 8.856329] remoteproc remoteproc2: b004000.rtu is available [ 8.864371] pru-rproc b004000.rtu: PRU rproc node rtu@b004000 probed successfully [ 8.879450] remoteproc remoteproc3: b038000.pru is available [ 8.890371] pru-rproc b038000.pru: PRU rproc node pru@b038000 probed successfully [ 8.901594] remoteproc remoteproc4: b006000.rtu is available [ 8.914291] pru-rproc b006000.rtu: PRU rproc node rtu@b006000 probed successfully [ 8.934070] remoteproc remoteproc5: b134000.pru is available [ 8.942970] pru-rproc b134000.pru: PRU rproc node pru@b134000 probed successfully [ 8.953268] remoteproc remoteproc6: b104000.rtu is available [ 8.973331] pru-rproc b104000.rtu: PRU rproc node rtu@b104000 probed successfully [ 8.983702] remoteproc remoteproc7: b138000.pru is available [ 9.000344] pru-rproc b138000.pru: PRU rproc node pru@b138000 probed successfully [ 9.008837] remoteproc remoteproc8: b106000.rtu is available [ 9.015295] pru-rproc b106000.rtu: PRU rproc node rtu@b106000 probed successfully [ 9.024930] remoteproc remoteproc9: b234000.pru is available [ 9.030929] pru-rproc b234000.pru: PRU rproc node pru@b234000 probed successfully [ 9.039396] remoteproc remoteproc10: b204000.rtu is available [ 9.051191] pru-rproc b204000.rtu: PRU rproc node rtu@b204000 probed successfully [ 9.061085] remoteproc remoteproc11: b238000.pru is available [ 9.067236] pru-rproc b238000.pru: PRU rproc node pru@b238000 probed successfully [ 9.085033] remoteproc remoteproc12: b206000.rtu is available [ 9.091154] pru-rproc b206000.rtu: PRU rproc node rtu@b206000 probed successfully [ 9.187974] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down [ 9.290881] icssg-prueth pruss1_eth: TI PRU ethernet initialized: dual EMAC mode, dual_icssg 0 [ OK ] Started Reboot and dump vmcore via kexec. [ OK ] Started RPC Bind Service. [ OK ] Started rng-tools.service. [ OK ] Started Lightning Fast Webserver With Light System Requirements. [ OK ] Started Permit User Sessions. [ 9.440658] icssg-prueth pruss0_eth: TI PRU ethernet initialized: dual EMAC mode, dual_icssg 0 [ 9.538746] icssg-prueth pruss2_eth: TI PRU ethernet initialized: dual EMAC mode, dual_icssg 0 [ 9.550725] NET: Registered protocol family 15 [ 9.617299] dwc3 4010000.usb: Failed to get clk 'ref': -2 [ 9.629043] dwc3 4030000.usb: Failed to get clk 'ref': -2 [ 9.655092] OF: graph: no port node found in /interconnect@100000/phy@4110000 [ 9.782951] virtio_rpmsg_bus virtio0: rpmsg host is online [ 9.784004] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x3d [ 9.811483] Initializing XFRM netlink socket [ 10.059457] NET: Registered protocol family 45 [ 10.130093] icssg-prueth pruss0_eth eth3: flow id base = 150 [ 10.141069] icssg-prueth pruss0_eth eth3: mgm flow id base = 154 [ 10.153704] remoteproc remoteproc1: powering up b034000.pru [ 10.177218] usbcore: registered new interface driver usbfs [ 10.183136] usbcore: registered new interface driver hub [ 10.188723] usbcore: registered new device driver usb [ 10.216580] remoteproc remoteproc1: Booting fw image ti-pruss/am65x-pru0-prueth-fw.elf, size 14868 [ 10.226014] remoteproc remoteproc1: remote processor b034000.pru is now up [ 10.232989] remoteproc remoteproc2: powering up b004000.rtu [ 10.260443] remoteproc remoteproc2: Booting fw image ti-pruss/am65x-rtu0-prueth-fw.elf, size 15488 [ 10.269519] remoteproc remoteproc2: remote processor b004000.rtu is now up [ 10.277610] net eth3: started [ 10.281330] IPv6: ADDRCONF(NETDEV_UP): eth3: link is not ready [ 10.316672] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 10.323086] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1 [ 10.331456] xhci-hcd xhci-hcd.2.auto: hcc params 0x0298fe6d hci version 0x110 quirks 0x0000000000010010 [ 10.341420] xhci-hcd xhci-hcd.2.auto: irq 309, io mem 0x04010000 [ 10.347449] icssg-prueth pruss2_eth eth5: flow id base = 157 [ 10.353741] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19 [ 10.362081] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 10.369402] usb usb1: Product: xHCI Host Controller [ 10.374341] usb usb1: Manufacturer: Linux 4.19.38-g4dae378bbe xhci-hcd [ 10.380954] usb usb1: SerialNumber: xhci-hcd.2.auto [ 10.386681] hub 1-0:1.0: USB hub found [ 10.390644] hub 1-0:1.0: 1 port detected [ 10.395668] icssg-prueth pruss2_eth eth5: mgm flow id base = 161 [ 10.396335] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 10.404459] remoteproc remoteproc9: powering up b234000.pru [ 10.407753] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2 [ 10.413283] remoteproc remoteproc9: Booting fw image ti-pruss/am65x-pru0-prueth-fw.elf, size 14868 [ 10.421484] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed [ 10.429898] remoteproc remoteproc9: remote processor b234000.pru is now up [ 10.436812] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 10.443210] remoteproc remoteproc10: powering up b204000.rtu [ 10.451562] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19 [ 10.457119] remoteproc remoteproc10: Booting fw image ti-pruss/am65x-rtu0-prueth-fw.elf, size 15488 [ 10.465323] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 10.474440] remoteproc remoteproc10: remote processor b204000.rtu is now up [ 10.481604] usb usb2: Product: xHCI Host Controller [ 10.481617] usb usb2: Manufacturer: Linux 4.19.38-g4dae378bbe xhci-hcd [ 10.490040] net eth5: started [ 10.493535] usb usb2: SerialNumber: xhci-hcd.2.auto [ 10.495138] hub 2-0:1.0: USB hub found [ 10.500355] IPv6: ADDRCONF(NETDEV_UP): eth5: link is not ready [ 10.503153] hub 2-0:1.0: 1 port detected [ 10.513816] icssg-prueth pruss1_eth eth2: flow id base = 164 [ 10.534776] icssg-prueth pruss1_eth eth2: mgm flow id base = 168 [ 10.544271] remoteproc remoteproc7: powering up b138000.pru [ 10.571391] remoteproc remoteproc7: Booting fw image ti-pruss/am65x-pru1-prueth-fw.elf, size 14868 [ 10.580443] remoteproc remoteproc7: remote processor b138000.pru is now up [ 10.588988] remoteproc remoteproc8: powering up b106000.rtu [ OK ] Started Login Service. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached targ[ 10.616283] remoteproc remoteproc8: Booting fw image ti-pruss/am65x-rtu1-prueth-fw.elf, size 15488 et Login Prompts. [ 10.628978] remoteproc remoteproc8: remote processor b106000.rtu is now up Starting Synchronize System and HW clocks... [ 10.638687] net eth2: started Starting rc.pvr.service...[ 10.645621] IPv6: ADDRCONF(NETDEV_UP): eth2: link is not ready [ 10.663185] icssg-prueth pruss2_eth eth6: flow id base = 171 [ 10.673368] icssg-prueth pruss2_eth eth6: mgm flow id base = 175 [ 10.683206] remoteproc remoteproc11: powering up b238000.pru [ OK ] [ 10.689577] remoteproc remoteproc11: Booting fw image ti-pruss/am65x-pru1-prueth-fw.elf, size 14868 Started NFS status monitor for NFSv2/3 locking.. [ 10.700196] remoteproc remoteproc11: remote processor b238000.pru is now up [FAILED] Failed to start Synchronize System and HW c[ 10.712461] remoteproc remoteproc12: powering up b206000.rtu locks. [ 10.723354] remoteproc remoteproc12: Booting fw image ti-pruss/am65x-rtu1-prueth-fw.elf, size 15488 [ 10.737809] remoteproc remoteproc12: remote processor b206000.rtu is now up [ 10.746442] net eth6: started [ 10.749684] IPv6: ADDRCONF(NETDEV_UP): eth6: link is not ready [ 10.764224] icssg-prueth pruss1_eth eth1: flow id base = 178 [ 10.774394] icssg-prueth pruss1_eth eth1: mgm flow id base = 182 [ 10.784253] remoteproc remoteproc5: powering up b134000.pru [ 10.790597] remoteproc remoteproc5: Booting fw image ti-pruss/am65x-pru0-prueth-fw.elf, size 14868 [ 10.799654] remoteproc remoteproc5: remote processor b134000.pru is now up [ 10.806614] remoteproc remoteproc6: powering up b104000.rtu [ 10.812292] remoteproc remoteproc6: Booting fw image ti-pruss/am65x-rtu0-prueth-fw.elf, size 15488 [ 10.821449] remoteproc remoteproc6: remote processor b104000.rtu is now up [ 10.829479] net eth1: started [ 10.832696] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready [ 10.844169] icssg-prueth pruss0_eth eth4: flow id base = 185 [ 10.853940] icssg-prueth pruss0_eth eth4: mgm flow id base = 189 [ 10.864209] remoteproc remoteproc3: powering up b038000.pru [ 10.870358] remoteproc remoteproc3: Booting fw image ti-pruss/am65x-pru1-prueth-fw.elf, size 14868 [ 10.879434] remoteproc remoteproc3: remote processor b038000.pru is now up [ 10.886447] remoteproc remoteproc4: powering up b006000.rtu [ 10.892545] remoteproc remoteproc4: Booting fw image ti-pruss/am65x-rtu1-prueth-fw.elf, size 15488 [ 10.901582] remoteproc remoteproc4: remote processor b006000.rtu is now up [ 10.909788] net eth4: started [ 10.913010] IPv6: ADDRCONF(NETDEV_UP): eth4: link is not ready [ 11.044795] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ] [ OK ] Started rc.pvr.service. Starting weston.service... [ OK ] Started weston.service. Starting Matrix GUI... Starting telnetd.service... [ OK ] Started telnetd.service. Starting thttpd.service... [ OK ] Started Matrix GUI. [ OK ] Started thttpd.service. Starting thermal-zone-init.service... [ OK ] Created slice system-systemd\x2dfsck.slice. [ OK ] Started thermal-zone-init.service. [ OK ] Found device /dev/mmcblk1p1. Starting File System Check on /dev/mmcblk1p1... [ OK ] Started Simple Network Management Protocol (SNMP) Daemon.. [ OK ] Started File System Check on /dev/mmcblk1p1. Mounting /run/media/mmcblk1p1... [ OK ] Mounted /run/media/mmcblk1p1. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am65xx-evm ttyS2 Arago 2019.05 am65xx-evm ttyS2 am65xx-evm login: *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash bc binutils cifs-utils cpio cpp-symlinks cpp dosfstools elfutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext glmark2 gstreamer1.0-libav gzip hidapi libbfd libdw1 libelf1 libgdbm-compat4 libgdbm6 libgettextlib libgettextsrc libgmp10 libidn2-0 libmpc3 libmpfr6 libreadline7 libunistring2 m4 make nettle parted pdm-anomaly-detection which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** ***************************************************************