U-Boot SPL 2013.10-00001-gb1a1b45 (Dec 07 2016 - 16:27:49) [divelk-2.0.0] reading u-boot.img reading u-boot.img U-Boot 2013.10-00001-gb1a1b45 (Dec 07 2016 - 16:27:49) [divelk-2.0.0] AM335X-GP rev 2.1 600 MHz I2C: ready DRAM: 256 MiB Now running in RAM - U-Boot at: 8ff4f000 NAND: 256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB Net: cpsw, usb_ether autoboot in 1 seconds (stop with PASSWORD)... NAND read: device 0 offset 0x2a0000, size 0x492350 4793168 bytes read: OK NAND read: device 0 offset 0x280000, size 0xa000 40960 bytes read: OK ## Booting kernel from Legacy Image at 80007fc0 ... Image Name: Linux-3.12.10-divelk-2.0.0-xeno2 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 4792480 Bytes = 4.6 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK ## Flattened Device Tree blob at 80f80000 Booting using the fdt blob at 0x80f80000 XIP Kernel Image ... OK Loading Device Tree to 8fe01000, end 8fe0d96a ... OK Starting kernel ... [ 0.192785] DSS not supported on this SoC [ 0.805628] mtdoops: mtd device (mtddev=name/number) must be supplied [ 0.849004] musb-hdrc musb-hdrc.0.auto: Falied to request rx1. [ 0.855211] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517 [ 0.866935] musb-hdrc musb-hdrc.1.auto: Falied to request rx1. [ 0.873407] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517 [ 0.915296] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517 [ 0.936793] cpu cpu0: cpu0 regulator not ready, retry INIT: version 2.88 booting Starting udev ERROR: could not open directory /lib/modules/3.12.10-divelk-2.0.0-xeno2-00008-g68052cfc: No such file or directory WARNING: -e needs -E or -F ERROR: could not open directory /lib/modules/3.12.10-divelk-2.0.0-xeno2-00008-g68052cfc: No such file or directory FATAL: could not search modules: No such file or directory cat: can't open '/etc/modules-load.d/*.conf': No such file or directory Starting Bootlog daemon: bootlogd. Configuring network interfaces... Successfully initialized wpa_supplicant rfkill: Cannot open RFKILL control device Could not read interface wlan0 flags: No such device WEXT: Could not set interface 'wlan0' UP wlan0: Failed to initialize driver interface Cannot find device "wlan0" done. Sun Dec 27 14:53:00 UTC 2015 INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting syslogd/klogd: done *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** Starting Lighttpd Web Server: lighttpd. 2015-12-27 14:53:03: (log.c.194) server started Starting LLExec. Starting Signal Software*********** SIGNAL SRL BOOT ********* Loading USB gadget printer driver USB gadget printer driver loaded Programming FPGA fd =3 JTAG Sitara programmer (C) Signal s.r.l. (LC) Ver 1.00 Oct 12 2016 17:00:42 ZZZ l=130460 NOTE "CREATOR" = "QUARTUS PRIME JAM COMPOSER 16.0" NOTE "DATE" = "2018/07/24" NOTE "DEVICE" = "EP4CE6" NOTE "NEED_FREQUENCY_CONTROL" = "0" NOTE "FILE" = "tpl2055.sof" NOTE "TARGET" = "1" NOTE "IDCODE" = "020F10DD" NOTE "USERCODE" = "20000004" NOTE "CHECKSUM" = "00289A70" NOTE "SAVE_DATA" = "DEVICE_DATA" NOTE "SAVE_DATA_VARIABLES" = "V0, A12, A13, A25, A42, A93, A43, A92, A94, A95, A105, A109, A111" NOTE "STAPL_VERSION" = "JESD71" NOTE "JAM_VERSION" = "2.0" NOTE "ALG_VERSION" = "67" first_word = 0x4A414D01 1 status = 0 2 status = 0 Device #1 IDCODE is 020F10DD configuring SRAM device(s)... DONE Exit code = 0... Success Retry n.1 Duration=2.310863s FPGA programmed . Stopping Bootlog daemon: bootlogd. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org diva ttyO0 Arago 2013.12 diva ttyO0 diva login: