#platform PLATFORM=am335x-evm #defconfig DEFCONFIG=tisdk_am335x-evm_defconfig #Architecture ARCH=armv7-a #u-boot machine UBOOT_MACHINE=am335x_evm_config #Points to the root of the TI SDK export TI_SDK_PATH=/home/dattatray/ti-processor-sdk-linux-am335x-evm-04.01.00.06 #root of the target file system for installing applications DESTDIR=/home/dattatray/ti-processor-sdk-linux-am335x-evm-04.01.00.06/targetNFS #Points to the root of the Linux libraries and headers matching the #demo file system. export LINUX_DEVKIT_PATH=$(TI_SDK_PATH)/linux-devkit #Cross compiler prefix export CROSS_COMPILE=$(LINUX_DEVKIT_PATH)/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- #Default CC value to be used when cross compiling. This is so that the #GNU Make default of "cc" is not used to point to the host compiler export CC=$(CROSS_COMPILE)gcc #Location of environment-setup file export ENV_SETUP=$(LINUX_DEVKIT_PATH)/environment-setup #The directory that points to the SDK kernel source tree LINUXKERNEL_INSTALL_DIR=$(TI_SDK_PATH)/board-support/linux-4.9.41+gitAUTOINC+e3a80a1c5c-ge3a80a1c5c CFLAGS= -march=armv7-a -marm -mfpu=neon -mfloat-abi=hard #Strip modules when installing to conserve disk space INSTALL_MOD_STRIP=1 SDK_PATH_TARGET=$(TI_SDK_PATH)/linux-devkit/sysroots/armv7ahf-neon-linux-gnueabi/ # Set EXEC_DIR to install example binaries EXEC_DIR=/home/dattatray/ti-processor-sdk-linux-am335x-evm-04.01.00.06/targetNFS/home/root/am335x-evm MAKE_JOBS=8