/*
 * Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com
 *
 * Author: Felipe Balbi <balbi@ti.com>
 *
 * Based on board/ti/dra7xx/evm.c
 *
 * SPDX-License-Identifier:	GPL-2.0+
 */

#include <common.h>
#include <palmas.h>
#include <sata.h>
#include <usb.h>
#include <asm/omap_common.h>
#include <asm/omap_sec_common.h>
#include <asm/emif.h>
#include <asm/gpio.h>
#include <asm/arch/gpio.h>
#include <asm/arch/clock.h>
#include <asm/arch/dra7xx_iodelay.h>
#include <asm/arch/sys_proto.h>
#include <asm/arch/mmc_host_def.h>
#include <asm/arch/sata.h>
#include <asm/arch/gpio.h>
#include <asm/arch/omap.h>
#include <environment.h>
#include <usb.h>
#include <linux/usb/gadget.h>
#include <dwc3-uboot.h>
#include <dwc3-omap-uboot.h>
#include <ti-usb-phy-uboot.h>

#include "mux_data.h"
#include "hw_info.h"

#ifdef CONFIG_DRIVER_TI_CPSW
#include <cpsw.h>
#endif

/* The processor supports both DDR-1066 & DDR-1333 and the installed DRAM
 * supports even higher speeds.  This board file was originally developed from
 * one supporting a TI evaluation board and needed to be changed to match the
 * RV700 HW.  The original change was an ugly hack whose effect was to select
 * DDR-1066.  When this code was later reviewed and the unfortunate speed
 * choice was discovered, it was decided that it was too late in the project
 * to risk changing to the higher speed and so the first version will ship
 * with DDR-1066.
 *
 * Note that there's a spec in the data sheet that implies that DDR-1333 isn't
 * supported however this was chased down with TI and that spec was determined
 * to be a typo.  By the time this comment is next read, it's possible that the
 * data sheet will have been updated to correct that error.
 *
 * Bottom line: at some future point when there's sufficient test time
 * available, it is probably worth selecting DDR-1333 for a 25% speed boost.
 */
#define DRAM_SPEED 1066  /* 1.870 ns cyle time, CL = 7 */
//#define DRAM_SPEED 1333  /* 1.500 ns cyle time, CL = 9 */

DECLARE_GLOBAL_DATA_PTR;

/* GPIO 7_11 */
#define GPIO_DDR_VTT_EN 203

#define SYSINFO_BOARD_NAME_MAX_LEN	45

#define TPS65903X_PRIMARY_SECONDARY_PAD2	0xFB
#define TPS65903X_PAD2_POWERHOLD_MASK		0x20

/* MiiS@20200227 DarkHou add to fix some main board can't power on issue. TFS-Bug 11153 begin */
#define OCMC_RAM1_REBOOT_REASON_ADDR  0x4035FF00  /* Chip ram address to save boot reason */
#define REBOOT_BY_IO_CAL_ERROR        0x34562301  /* Reboot reason - I/O calibration failed */
#define NORMAL_POWER_ON               0x32346643  /* Normal power on */
/* MiiS@20200227 DarkHou add to fix some main board can't power on issue. TFS-Bug 11153 end */
/* define "board info string": must start with "Board: " and end w/ '\n' */
const struct omap_sysinfo sysinfo = {
	"Board: RV700\n"
};

static const struct dmm_lisa_map_regs rv700_am5718_lisa_regs = {
	.dmm_lisa_map_3 = 0x80700100,
	.is_ma_present  = 0x1
};

void emif_get_dmm_regs(const struct dmm_lisa_map_regs **dmm_lisa_regs)
{
	*dmm_lisa_regs = &rv700_am5718_lisa_regs;		
}

static const struct emif_regs beagle_x15_emif1_ddr3_532mhz_emif_regs = {
	.sdram_config_init		= 0x61851b32,
	.sdram_config			= 0x61851b32,
	.sdram_config2			= 0x08000000,
	.ref_ctrl			= 0x000040F1,
	.ref_ctrl_final			= 0x00001035,
	.sdram_tim1			= 0xcccf36ab,
	.sdram_tim2			= 0x308f7fda,
	.sdram_tim3			= 0x409f88a8,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x5007190b,
	.temp_alert_config		= 0x00000000,
	.emif_ddr_phy_ctlr_1_init 	= 0x0024400b,
	.emif_ddr_phy_ctlr_1		= 0x0e24400b,
	.emif_ddr_ext_phy_ctrl_1 	= 0x10040100,
	.emif_ddr_ext_phy_ctrl_2 	= 0x00910091,
	.emif_ddr_ext_phy_ctrl_3 	= 0x00950095,
	.emif_ddr_ext_phy_ctrl_4 	= 0x009b009b,
	.emif_ddr_ext_phy_ctrl_5 	= 0x009e009e,
	.emif_rd_wr_lvl_rmp_win		= 0x00000000,
	.emif_rd_wr_lvl_rmp_ctl		= 0x80000000,
	.emif_rd_wr_lvl_ctl		= 0x00000000,
	.emif_rd_wr_exec_thresh		= 0x00000305
};

/* Ext phy ctrl regs 1-35 */
static const u32 beagle_x15_emif1_ddr3_ext_phy_ctrl_const_regs[] = {
	0x10040100,
	0x00910091,
	0x00950095,
	0x009B009B,
	0x009E009E,
	0x00980098,
	0x00340034,
	0x00350035,
	0x00340034,
	0x00310031,
	0x00340034,
	0x007F007F,
	0x007F007F,
	0x007F007F,
	0x007F007F,
	0x007F007F,
	0x00480048,
	0x004A004A,
	0x00520052,
	0x00550055,
	0x00500050,
	0x00000000,
	0x00600020,
	0x40011080,
	0x08102040,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0
};

static const struct emif_regs beagle_x15_emif2_ddr3_532mhz_emif_regs = {
	.sdram_config_init		= 0x61851b32,
	.sdram_config			= 0x61851b32,
	.sdram_config2			= 0x08000000,
	.ref_ctrl			= 0x000040F1,
	.ref_ctrl_final			= 0x00001035,
	.sdram_tim1			= 0xcccf36b3,
	.sdram_tim2			= 0x308f7fda,
	.sdram_tim3			= 0x407f88a8,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x5007190b,
	.temp_alert_config		= 0x00000000,
	.emif_ddr_phy_ctlr_1_init 	= 0x0024400b,
	.emif_ddr_phy_ctlr_1		= 0x0e24400b,
	.emif_ddr_ext_phy_ctrl_1 	= 0x10040100,
	.emif_ddr_ext_phy_ctrl_2 	= 0x00910091,
	.emif_ddr_ext_phy_ctrl_3 	= 0x00950095,
	.emif_ddr_ext_phy_ctrl_4 	= 0x009b009b,
	.emif_ddr_ext_phy_ctrl_5 	= 0x009e009e,
	.emif_rd_wr_lvl_rmp_win		= 0x00000000,
	.emif_rd_wr_lvl_rmp_ctl		= 0x80000000,
	.emif_rd_wr_lvl_ctl		= 0x00000000,
	.emif_rd_wr_exec_thresh		= 0x00000305
};

static const u32 beagle_x15_emif2_ddr3_ext_phy_ctrl_const_regs[] = {
	0x10040100,
	0x00910091,
	0x00950095,
	0x009B009B,
	0x009E009E,
	0x00980098,
	0x00340034,
	0x00350035,
	0x00340034,
	0x00310031,
	0x00340034,
	0x007F007F,
	0x007F007F,
	0x007F007F,
	0x007F007F,
	0x007F007F,
	0x00480048,
	0x004A004A,
	0x00520052,
	0x00550055,
	0x00500050,
	0x00000000,
	0x00600020,
	0x40011080,
	0x08102040,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0,
	0x0
};

#if DRAM_SPEED == 1333
static const struct emif_regs am571x_emif1_ddr3_666mhz_emif_regs = {
	.sdram_config_init		= 0x61863332,
	.sdram_config			= 0x61863332,
	.sdram_config2			= 0x08000000,
	.ref_ctrl			= 0x0000514d,
	.ref_ctrl_final			= 0x0000144a,
	.sdram_tim1			= 0xd333887c,
	.sdram_tim2			= 0x40b37fe3,
	.sdram_tim3			= 0x409f8ada,
	.read_idle_ctrl			= 0x00050000,
	.zq_config			= 0x5007190b,
	.temp_alert_config		= 0x00000000,
	.emif_ddr_phy_ctlr_1_init	= 0x0024400f,
	.emif_ddr_phy_ctlr_1		= 0x0e24400f,
	.emif_ddr_ext_phy_ctrl_1	= 0x10040100,
	.emif_ddr_ext_phy_ctrl_2	= 0x00910091,
	.emif_ddr_ext_phy_ctrl_3	= 0x00950095,
	.emif_ddr_ext_phy_ctrl_4	= 0x009b009b,
	.emif_ddr_ext_phy_ctrl_5	= 0x009e009e,
	.emif_rd_wr_lvl_rmp_win		= 0x00000000,
	.emif_rd_wr_lvl_rmp_ctl		= 0x80000000,
	.emif_rd_wr_lvl_ctl		= 0x00000000,
	.emif_rd_wr_exec_thresh		= 0x00000305
};
#endif

void emif_get_reg_dump(u32 emif_nr, const struct emif_regs **regs)
{
	switch (emif_nr) {
	case 1:
#if DRAM_SPEED == 1066
		*regs = &beagle_x15_emif1_ddr3_532mhz_emif_regs;
#elif DRAM_SPEED == 1333
		*regs = &am571x_emif1_ddr3_666mhz_emif_regs;
#else
    #error DRAM_SPEED not defined
#endif
		break;
	case 2:
		*regs = &beagle_x15_emif2_ddr3_532mhz_emif_regs;
		break;
	}
}

void emif_get_ext_phy_ctrl_const_regs(u32 emif_nr, const u32 **regs, u32 *size)
{
	switch (emif_nr) {
	case 1:
		*regs = beagle_x15_emif1_ddr3_ext_phy_ctrl_const_regs;
		*size = ARRAY_SIZE(beagle_x15_emif1_ddr3_ext_phy_ctrl_const_regs);
		break;
	case 2:
		*regs = beagle_x15_emif2_ddr3_ext_phy_ctrl_const_regs;
		*size = ARRAY_SIZE(beagle_x15_emif2_ddr3_ext_phy_ctrl_const_regs);
		break;
	}
}

struct vcores_data rv700_volts = {
	.mpu.value[OPP_NOM]	= VDD_MPU_DRA7_NOM,
	.mpu.efuse.reg[OPP_NOM]	= STD_FUSE_OPP_VMIN_MPU_NOM,
	.mpu.efuse.reg_bits     = DRA752_EFUSE_REGBITS,
	.mpu.addr		= TPS659038_REG_ADDR_SMPS12,
	.mpu.pmic		= &tps659038,
	.mpu.abb_tx_done_mask	= OMAP_ABB_MPU_TXDONE_MASK,

	.eve.value[OPP_NOM]	= VDD_EVE_DRA7_NOM,
	.eve.value[OPP_OD]	= VDD_EVE_DRA7_OD,
	.eve.value[OPP_HIGH]	= VDD_EVE_DRA7_HIGH,
	.eve.efuse.reg[OPP_NOM]	= STD_FUSE_OPP_VMIN_DSPEVE_NOM,
	.eve.efuse.reg[OPP_OD]	= STD_FUSE_OPP_VMIN_DSPEVE_OD,
	.eve.efuse.reg[OPP_HIGH]	= STD_FUSE_OPP_VMIN_DSPEVE_HIGH,
	.eve.efuse.reg_bits	= DRA752_EFUSE_REGBITS,
	.eve.addr		= TPS659038_REG_ADDR_SMPS45,
	.eve.pmic		= &tps659038,
	.eve.abb_tx_done_mask	= OMAP_ABB_EVE_TXDONE_MASK,

	.gpu.value[OPP_NOM]	= VDD_GPU_DRA7_NOM,
	.gpu.value[OPP_OD]	= VDD_GPU_DRA7_OD,
	.gpu.value[OPP_HIGH]	= VDD_GPU_DRA7_HIGH,
	.gpu.efuse.reg[OPP_NOM]	= STD_FUSE_OPP_VMIN_GPU_NOM,
	.gpu.efuse.reg[OPP_OD]	= STD_FUSE_OPP_VMIN_GPU_OD,
	.gpu.efuse.reg[OPP_HIGH]	= STD_FUSE_OPP_VMIN_GPU_HIGH,
	.gpu.efuse.reg_bits	= DRA752_EFUSE_REGBITS,
	.gpu.addr		= TPS659038_REG_ADDR_SMPS45,
	.gpu.pmic		= &tps659038,
	.gpu.abb_tx_done_mask	= OMAP_ABB_GPU_TXDONE_MASK,

	.core.value[OPP_NOM]	= VDD_CORE_DRA7_NOM,
	.core.efuse.reg[OPP_NOM]	= STD_FUSE_OPP_VMIN_CORE_NOM,
	.core.efuse.reg_bits	= DRA752_EFUSE_REGBITS,
	.core.addr		= TPS659038_REG_ADDR_SMPS6,
	.core.pmic		= &tps659038,

	.iva.value[OPP_NOM]	= VDD_IVA_DRA7_NOM,
	.iva.value[OPP_OD]	= VDD_IVA_DRA7_OD,
	.iva.value[OPP_HIGH]	= VDD_IVA_DRA7_HIGH,
	.iva.efuse.reg[OPP_NOM]	= STD_FUSE_OPP_VMIN_IVA_NOM,
	.iva.efuse.reg[OPP_OD]	= STD_FUSE_OPP_VMIN_IVA_OD,
	.iva.efuse.reg[OPP_HIGH]	= STD_FUSE_OPP_VMIN_IVA_HIGH,
	.iva.efuse.reg_bits	= DRA752_EFUSE_REGBITS,
	.iva.addr		= TPS659038_REG_ADDR_SMPS45,
	.iva.pmic		= &tps659038,
	.iva.abb_tx_done_mask	= OMAP_ABB_IVA_TXDONE_MASK,
};

int get_voltrail_opp(int rail_offset)
{
	int opp;

	switch (rail_offset) {
	case VOLT_MPU:
		opp = DRA7_MPU_OPP;
		break;
	case VOLT_CORE:
		opp = DRA7_CORE_OPP;
		break;
	case VOLT_GPU:
		opp = DRA7_GPU_OPP;
		break;
	case VOLT_EVE:
		opp = DRA7_DSPEVE_OPP;
		break;
	case VOLT_IVA:
		opp = DRA7_IVA_OPP;
		break;
	default:
		opp = OPP_NOM;
	}

	return opp;
}

void vcores_init(void)
{
	*omap_vcores = &rv700_volts;
}

void hw_data_init(void)
{
	*prcm = &dra7xx_prcm;
#if DRAM_SPEED == 1066
	*dplls_data = &dra7xx_dplls;
#elif DRAM_SPEED == 1333
	*dplls_data = &dra72x_dplls;
#else
    #error DRAM_SPEED not defined
#endif
	*ctrl = &dra7xx_ctrl;
}

int board_init(void)
{
	gpmc_init();
	gd->bd->bi_boot_params = (CONFIG_SYS_SDRAM_BASE + 0x100);

	return 0;
}

int board_late_init(void)
{
	/*
	 * DEV_CTRL.DEV_ON = 1 please - else palmas switches off in 8 seconds
	 * This is the POWERHOLD-in-Low behavior.
	 */
	palmas_i2c_write_u8(TPS65903X_CHIP_P1, 0xA0, 0x1);

	/*
	 * Set the GPIO7 Pad to POWERHOLD. This has higher priority
	 * over DEV_CTRL.DEV_ON bit. This can be reset in case of
	 * PMIC Power off. So to be on the safer side set it back
	 * to POWERHOLD mode irrespective of the current state.
	 */
	u8 val;
	palmas_i2c_read_u8(TPS65903X_CHIP_P1, TPS65903X_PRIMARY_SECONDARY_PAD2,
			   &val);
	val = val | TPS65903X_PAD2_POWERHOLD_MASK;
	palmas_i2c_write_u8(TPS65903X_CHIP_P1, TPS65903X_PRIMARY_SECONDARY_PAD2,
			    val);

#if !defined(CONFIG_SPL_BUILD) && defined(CONFIG_DRIVER_TI_CPSW)
	board_ti_set_ethaddr(2);
#endif

	if (get_hw_version() > 0) {
		const struct pad_conf_entry *pconf_hw_1_0;
		int pconf_sz_hw_1_0;
	
		pconf_hw_1_0 = core_padconf_array_rv700_am5718_board_1_0;
		pconf_sz_hw_1_0 =
			ARRAY_SIZE(core_padconf_array_rv700_am5718_board_1_0);
		do_set_mux32((*ctrl)->control_padconf_core_base,
			     pconf_hw_1_0, pconf_sz_hw_1_0);
	}
	
	return 0;
}

void set_muxconf_regs(void)
{
	do_set_mux32((*ctrl)->control_padconf_core_base,
		     early_padconf, ARRAY_SIZE(early_padconf));
}

#ifdef CONFIG_IODELAY_RECALIBRATION
void recalibrate_iodelay(void)
{
	const struct pad_conf_entry *pconf;
	const struct iodelay_cfg_entry *iod;
	int pconf_sz, iod_sz;
	int ret;
	int *reboot_reason = (int *) OCMC_RAM1_REBOOT_REASON_ADDR;

	pconf = core_padconf_array_rv700_am5718_board_base;
	pconf_sz = ARRAY_SIZE(core_padconf_array_rv700_am5718_board_base);

	iod = iodelay_cfg_array_rv700_am5718_board_base;
	iod_sz = ARRAY_SIZE(iodelay_cfg_array_rv700_am5718_board_base);
	
	// Setup I/O isolation 
	ret = __recalibrate_iodelay_start();

        /* I/O Calibration failed */
	if (ret) {
                /* Set reboot reason as I/O calibration error at first time */
		if (*reboot_reason != REBOOT_BY_IO_CAL_ERROR) {
			*reboot_reason = REBOOT_BY_IO_CAL_ERROR;
		}
                /* Don't reboot again for second I/O calibration failed case */
		else
		{
			*reboot_reason = NORMAL_POWER_ON;
		}
	}
        /* I/O Calibration sucucess*/
	else
	{
                /* Set reboot reason as normal power on */
		*reboot_reason = NORMAL_POWER_ON;
	}

	/* Do the muxing here */
	do_set_mux32((*ctrl)->control_padconf_core_base, pconf, pconf_sz);

	/* Setup IOdelay configuration */
	ret = do_set_iodelay((*ctrl)->iodelay_config_base, iod, iod_sz);

	/* Closeup.. remove isolation */
	__recalibrate_iodelay_end(ret);
}
#endif

#if defined(CONFIG_GENERIC_MMC)
int board_mmc_init(bd_t *bis)
{
	omap_mmc_init(0, 0, 0, -1, -1);
	omap_mmc_init(1, 0, 0, -1, -1);
	return 0;
}
#endif

#if defined(CONFIG_IODELAY_RECALIBRATION) && \
	(defined(CONFIG_SPL_BUILD) || !defined(CONFIG_DM_MMC))

struct pinctrl_desc {
	const char *name;
	struct omap_hsmmc_pinctrl_state *pinctrl;
};

static struct pinctrl_desc pinctrl_descs_hsmmc1[] = {
	{"default", &hsmmc1_default},
	{"hs", &hsmmc1_default},
	{NULL}
};

static struct pinctrl_desc pinctrl_descs_hsmmc2_am571[] = {
	{"default", &hsmmc2_default_hs},
	{"hs", &hsmmc2_default_hs},
	{"ddr_1_8v", &hsmmc2_ddr_am571},
	{NULL}
};

struct omap_hsmmc_pinctrl_state *platform_fixup_get_pinctrl_by_mode
				  (struct hsmmc *base, const char *mode)
{
	struct pinctrl_desc *p = NULL;

	switch ((u32)&base->res1) {
	case OMAP_HSMMC1_BASE:
		p = pinctrl_descs_hsmmc1;
		break;
	case OMAP_HSMMC2_BASE:
		p = pinctrl_descs_hsmmc2_am571;
	default:
		break;
	}

	if (!p) {
		printf("%s no pinctrl defined for MMC@%p\n", __func__,
		       base);
		return NULL;
	}
	while (p->name) {
		if (strcmp(mode, p->name) == 0)
			return p->pinctrl;
		p++;
	}
	return NULL;
}
#endif

#ifdef CONFIG_OMAP_HSMMC
int platform_fixup_disable_uhs_mode(void)
{
	return omap_revision() == DRA752_ES1_1;
}
#endif

#if defined(CONFIG_SPL_BUILD) && defined(CONFIG_SPL_OS_BOOT)
int spl_start_uboot(void)
{
	/* break into full u-boot on 'c' */
	if (serial_tstc() && serial_getc() == 'c')
		return 1;

#ifdef CONFIG_SPL_ENV_SUPPORT
	env_init();
	env_relocate_spec();
	if (getenv_yesno("boot_os") != 1)
		return 1;
#endif

	return 0;
}
#endif

#ifdef CONFIG_USB_DWC3
static struct dwc3_device usb_otg_ss2 = {
	.maximum_speed = USB_SPEED_HIGH,
	.base = DRA7_USB_OTG_SS2_BASE,
	.tx_fifo_resize = false,
	.index = 1,
};

static struct dwc3_omap_device usb_otg_ss2_glue = {
	.base = (void *)DRA7_USB_OTG_SS2_GLUE_BASE,
	.utmi_mode = DWC3_OMAP_UTMI_MODE_SW,
	.index = 1,
};

static struct ti_usb_phy_device usb_phy2_device = {
	.usb2_phy_power = (void *)DRA7_USB2_PHY2_POWER,
	.index = 1,
};

int usb_gadget_handle_interrupts(int index)
{
	u32 status;

	status = dwc3_omap_uboot_interrupt_status(index);
	if (status)
		dwc3_uboot_handle_interrupt(index);

	return 0;
}
#endif /* CONFIG_USB_DWC3 */

#if defined(CONFIG_USB_DWC3) || defined(CONFIG_USB_XHCI_OMAP)
int board_usb_init(int index, enum usb_init_type init)
{
	enable_usb_clocks(index);
	switch (index) {
	case 0:
		if (init == USB_INIT_DEVICE) {
			printf("port %d can't be used as device\n", index);
			disable_usb_clocks(index);
			return -EINVAL;
		}
		break;
	case 1:
		if (init == USB_INIT_DEVICE) {
#ifdef CONFIG_USB_DWC3
			usb_otg_ss2.dr_mode = USB_DR_MODE_PERIPHERAL;
			usb_otg_ss2_glue.vbus_id_status = OMAP_DWC3_VBUS_VALID;
			ti_usb_phy_uboot_init(&usb_phy2_device);
			dwc3_omap_uboot_init(&usb_otg_ss2_glue);
			dwc3_uboot_init(&usb_otg_ss2);
#endif
		} else {
			printf("port %d can't be used as host\n", index);
			disable_usb_clocks(index);
			return -EINVAL;
		}

		break;
	default:
		printf("Invalid Controller Index\n");
	}

	return 0;
}

int board_usb_cleanup(int index, enum usb_init_type init)
{
#ifdef CONFIG_USB_DWC3
	switch (index) {
	case 0:
	case 1:
		if (init == USB_INIT_DEVICE) {
			ti_usb_phy_uboot_exit(index);
			dwc3_uboot_exit(index);
			dwc3_omap_uboot_exit(index);
		}
		break;
	default:
		printf("Invalid Controller Index\n");
	}
#endif
	disable_usb_clocks(index);
	return 0;
}
#endif /* defined(CONFIG_USB_DWC3) || defined(CONFIG_USB_XHCI_OMAP) */

#ifdef CONFIG_DRIVER_TI_CPSW

/* Delay value to add to calibrated value */
#define RGMII0_TXCTL_DLY_VAL		((0x3 << 5) + 0x8)
#define RGMII0_TXD0_DLY_VAL		((0x3 << 5) + 0x8)
#define RGMII0_TXD1_DLY_VAL		((0x3 << 5) + 0x2)
#define RGMII0_TXD2_DLY_VAL		((0x4 << 5) + 0x0)
#define RGMII0_TXD3_DLY_VAL		((0x4 << 5) + 0x0)
#define VIN2A_D13_DLY_VAL		((0x3 << 5) + 0x8)
#define VIN2A_D17_DLY_VAL		((0x3 << 5) + 0x8)
#define VIN2A_D16_DLY_VAL		((0x3 << 5) + 0x2)
#define VIN2A_D15_DLY_VAL		((0x4 << 5) + 0x0)
#define VIN2A_D14_DLY_VAL		((0x4 << 5) + 0x0)

static void cpsw_control(int enabled)
{
	/* VTP can be added here */
}

static struct cpsw_slave_data cpsw_slaves[] = {
	{
		.slave_reg_ofs	= 0x208,
		.sliver_reg_ofs	= 0xd80,
		.phy_addr	= 1,
	},
	{
		.slave_reg_ofs	= 0x308,
		.sliver_reg_ofs	= 0xdc0,
		.phy_addr	= 2,
	},
};

static struct cpsw_platform_data cpsw_data = {
	.mdio_base		= CPSW_MDIO_BASE,
	.cpsw_base		= CPSW_BASE,
	.mdio_div		= 0xff,
	.channels		= 8,
	.cpdma_reg_ofs		= 0x800,
	.slaves			= 1,
	.slave_data		= cpsw_slaves,
	.ale_reg_ofs		= 0xd00,
	.ale_entries		= 1024,
	.host_port_reg_ofs	= 0x108,
	.hw_stats_reg_ofs	= 0x900,
	.bd_ram_ofs		= 0x2000,
	.mac_control		= (1 << 5),
	.control		= cpsw_control,
	.host_port_num		= 0,
	.version		= CPSW_CTRL_VERSION_2,
};

static u64 mac_to_u64(u8 mac[6])
{
	int i;
	u64 addr = 0;

	for (i = 0; i < 6; i++) {
		addr <<= 8;
		addr |= mac[i];
	}

	return addr;
}

static void u64_to_mac(u64 addr, u8 mac[6])
{
	mac[5] = addr;
	mac[4] = addr >> 8;
	mac[3] = addr >> 16;
	mac[2] = addr >> 24;
	mac[1] = addr >> 32;
	mac[0] = addr >> 40;
}

int board_eth_init(bd_t *bis)
{
	int ret;
	uint8_t mac_addr[6];
	uint32_t mac_hi, mac_lo;
	uint32_t ctrl_val;
	int i;
	u64 mac1, mac2;
	u8 mac_addr1[6], mac_addr2[6];
	int num_macs;

	/* try reading mac address from efuse */
	mac_lo = readl((*ctrl)->control_core_mac_id_0_lo);
	mac_hi = readl((*ctrl)->control_core_mac_id_0_hi);
	mac_addr[0] = (mac_hi & 0xFF0000) >> 16;
	mac_addr[1] = (mac_hi & 0xFF00) >> 8;
	mac_addr[2] = mac_hi & 0xFF;
	mac_addr[3] = (mac_lo & 0xFF0000) >> 16;
	mac_addr[4] = (mac_lo & 0xFF00) >> 8;
	mac_addr[5] = mac_lo & 0xFF;

	if (!getenv("ethaddr")) {
		printf("<ethaddr> not set. Validating first E-fuse MAC\n");

		if (is_valid_ethaddr(mac_addr))
			eth_setenv_enetaddr("ethaddr", mac_addr);
	}

	mac_lo = readl((*ctrl)->control_core_mac_id_1_lo);
	mac_hi = readl((*ctrl)->control_core_mac_id_1_hi);
	mac_addr[0] = (mac_hi & 0xFF0000) >> 16;
	mac_addr[1] = (mac_hi & 0xFF00) >> 8;
	mac_addr[2] = mac_hi & 0xFF;
	mac_addr[3] = (mac_lo & 0xFF0000) >> 16;
	mac_addr[4] = (mac_lo & 0xFF00) >> 8;
	mac_addr[5] = mac_lo & 0xFF;

	if (!getenv("eth1addr")) {
		if (is_valid_ethaddr(mac_addr))
			eth_setenv_enetaddr("eth1addr", mac_addr);
	}

	ctrl_val = readl((*ctrl)->control_core_control_io1) & (~0x33);
	ctrl_val |= 0x22;
	writel(ctrl_val, (*ctrl)->control_core_control_io1);

	ret = cpsw_register(&cpsw_data);
	if (ret < 0)
		printf("Error %d registering CPSW switch\n", ret);

	/*
	 * Export any Ethernet MAC addresses from EEPROM.
	 * On AM57xx the 2 MAC addresses define the address range
	 */
	board_ti_get_eth_mac_addr(0, mac_addr1);
	board_ti_get_eth_mac_addr(1, mac_addr2);

	if (is_valid_ethaddr(mac_addr1) && is_valid_ethaddr(mac_addr2)) {
		mac1 = mac_to_u64(mac_addr1);
		mac2 = mac_to_u64(mac_addr2);

		/* must contain an address range */
		num_macs = mac2 - mac1 + 1;
		/* <= 50 to protect against user programming error */
		if (num_macs > 0 && num_macs <= 50) {
			for (i = 0; i < num_macs; i++) {
				u64_to_mac(mac1 + i, mac_addr);
				if (is_valid_ethaddr(mac_addr)) {
					eth_setenv_enetaddr_by_index("eth",
								     i + 2,
								     mac_addr);
				}
			}
		}
	}

	return ret;
}
#endif /* CONFIG_DRIVER_TI_CPSW */

#ifdef CONFIG_BOARD_EARLY_INIT_F
/* VTT regulator enable */
static inline void vtt_regulator_enable(void)
{
	if (omap_hw_init_context() == OMAP_INIT_CONTEXT_UBOOT_AFTER_SPL)
		return;

	gpio_request(GPIO_DDR_VTT_EN, "ddr_vtt_en");
	gpio_direction_output(GPIO_DDR_VTT_EN, 1);
}

int board_early_init_f(void)
{
	vtt_regulator_enable();
	return 0;
}
#endif

#if defined(CONFIG_OF_LIBFDT) && defined(CONFIG_OF_BOARD_SETUP)
int ft_board_setup(void *blob, bd_t *bd)
{
	ft_cpu_setup(blob, bd);

	return 0;
}
#endif

#ifdef CONFIG_TI_SECURE_DEVICE
void board_fit_image_post_process(void **p_image, size_t *p_size)
{
	secure_boot_verify_image(p_image, p_size);
}

void board_tee_image_process(ulong tee_image, size_t tee_size)
{
	secure_tee_install((u32)tee_image);
}

U_BOOT_FIT_LOADABLE_HANDLER(IH_TYPE_TEE, board_tee_image_process);
#endif