[ 1.968384] usbhid: USB HID core driver [ 1.973842] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xac [ 1.980270] nand: Micron MT29F4G08ABBDAHC [ 1.984314] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 [ 1.992393] Bad block table found at page 262080, version 0x01 [ 1.999205] Bad block table found at page 262016, version 0x01 [ 2.005567] 3 ofpart partitions found on MTD device 30000000.nand [ 2.011763] Creating 3 MTD partitions on "30000000.nand": [ 2.017227] 0x000000000000-0x000000100000 : "u-boot" [ 2.023816] 0x000000100000-0x000000180000 : "params" [ 2.030353] 0x000000180000-0x000020000000 : "ubifs" [ 2.037333] davinci_nand 30000000.nand: controller rev. 2.5 [ 2.043601] platform oprofile-perf.0: set dma_pfn_offset00780000 [ 2.050139] oprofile: using timer interrupt. [ 2.054506] Netfilter messages via NETLINK v0.30. [ 2.059295] nf_conntrack version 0.5.0 (7992 buckets, 31968 max) [ 2.066172] ctnetlink v0.93: registering with nfnetlink. [ 2.072174] ipip: IPv4 over IPv4 tunneling driver [ 2.077901] gre: GRE over IPv4 demultiplexor driver [ 2.083107] ip_tables: (C) 2000-2006 Netfilter Core Team [ 2.088632] ipt_CLUSTERIP: ClusterIP Version 0.8 loaded successfully [ 2.095084] arp_tables: (C) 2002 David S. Miller [ 2.099849] Initializing XFRM netlink socket [ 2.104188] NET: Registered protocol family 17 [ 2.108723] NET: Registered protocol family 15 [ 2.113215] 8021q: 802.1Q VLAN Support v1.8 [ 2.117603] Registering SWP/SWPB emulation handler [ 2.139044] 8021q: adding VLAN 0 to HW filter on device eth0 [ 2.156950] IP-Config: Complete: [ 2.160210] device=eth0, hwaddr=d4:f5:13:aa:d8:ba, ipaddr=172.17.1.57, mask=255.255.0.0, gw=172.17.0.3 [ 2.170054] host=172.17.1.57, domain=, nis-domain=(none) [ 2.175846] bootserver=172.17.1.146, rootserver=172.17.1.146, rootpath= [ 2.282033] VFS: Mounted root (nfs filesystem) on device 0:15. [ 2.288799] devtmpfs: mounted [ 2.292100] Freeing unused kernel memory: 316K (c06d5000 - c0724000) INIT: version 2.88 booting [ 3.458108] NET: Registered protocol family 41 Starting random number generator daemonread error read error . [ 3.786439] random: dd urandom read with 105 bits of entropy available Sat Jan 9 00:07:57 UTC 2016 INIT: Entering runlevel: 5 NOT configuring network interfaces: / is an NFS mount [ 4.738856] random: nonblocking pool is initialized udhcpc (v1.23.1) started Sending discover... Sending select for 172.17.2.177... Lease of 172.17.2.177 obtained, lease time 7200 /etc/udhcpc.d/50default: Adding DNS 172.17.0.1 /etc/udhcpc.d/50default: Adding DNS 8.8.8.8 /etc/udhcpc.d/50default: Adding DNS 8.8.4.4 /etc/udhcpc.d/50default: Adding DNS 202.251.202.3 Starting system message bus: dbus. Starting Dropbear SSH server: [ 7.091725] NET: Registered protocol family 10 dropbear. Starting mpmsrv daemon. platform: k2hk-evm Starting softhsm daemon. Starting telnet daemon. Starting tiipclad daemon GateMP is not supported for this device Opened log file: lad.txt numProcessors = 9 id = 0 baseId = 0 Spawned daemon: /usr/bin/lad_tci6638 . Starting rpcbind daemon...done. starting statd: done Starting thttpd. Starting Lighttpd Web Server: lighttpd. 2016-01-09 00:08:00: (/home/gtbldadm/processor-sdk-linux-fido-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-linux-gnueabi/lighttpd/1.4.35-r1/lighttpd-1.4.35/src/log.c.164) server started * starting FTP Server: vsftpd... done. #>>>>> LCD 12 IP Address: 172.17.1.57 Enabling thermal zones... /etc/rc5.d/S98thermal-zone-init: line 7: /sys/class/thermal/thermal_zone*/mode: No such file or directory *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf binutils-dev binutils bison-dev bison cpp-symlinks cpp g++-symlinks g++ gawk-dev gawk gcc-symlinks gcc gdb gdbc6x gdbserver libgmp10 libmpc3 libmpfr4 make If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org k2hk-evm /dev/ttyS0 Arago 2015.12 k2hk-evm /dev/ttyS0 k2hk-evm login: root root@k2hk-evm:~# cd / root@k2hk-evm:/# lsmod Module Size Used by ipv6 338366 30 rpmsg_proto 6823 0 virtio_rpmsg_bus 11766 1 rpmsg_proto remoteproc 25480 1 rpmsg_proto virtio 6460 2 remoteproc,virtio_rpmsg_bus virtio_ring 12987 2 remoteproc,virtio_rpmsg_bus root@k2hk-evm:/# root@k2hk-evm:/# root@k2hk-evm:/# mpmcl ping dsp0 ping succeeded root@k2hk-evm:/# mpmcl status dsp0 dsp0 is in idle state root@k2hk-evm:/# mpmcl load dsp0 m media/ mnt/ root@k2hk-evm:/# mpmcl load dsp0 mpmsrv_keystone2_example.out load failed (error: -104) root@k2hk-evm:/# mpmcl load dsp0 mpmsrv_keystone2_example.out load succeeded root@k2hk-evm:/# mpmcl run dsp0 run succeeded root@k2hk-evm:/# ls -l /sys/kernel/debug/remoteproc/ root@k2hk-evm:/# root@k2hk-evm:/# root@k2hk-evm:/# root@k2hk-evm:/#