/*
 * Copyright (C) 2012 - 2014 Texas Instruments Inc.
 *
 * K2HK EVM : Board initialization
 *
 * See file CREDITS for list of people who contributed to this
 * project.
 *
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA.
 */

#include <common.h>
#include <i2c.h>

#include <asm/arch/hardware.h>
#include <asm/arch/clock.h>
#include <asm/arch/clock_defs.h>
#include <asm/io.h>
#include <asm/arch/nand_defs.h>
#include <asm/arch/emac_defs.h>

DECLARE_GLOBAL_DATA_PTR;

unsigned int external_clk[ext_clk_count] = {
	[sys_clk]	=	122880000,
	[alt_core_clk]	=	125000000,
	[pa_clk]	=	122880000,
	[tetris_clk]	=	125000000,
	[ddr3a_clk]	=	100000000,
	[ddr3b_clk]	=	100000000,
	[mcm_clk]	=	312500000,
	[pcie_clk]	=	100000000,
	[sgmii_srio_clk] =	156250000,
	[xgmii_clk]	=	156250000,
	[usb_clk]	=	100000000,
	[rp1_clk]	=	123456789    /* TODO: cannot find
						what is that */
};

static struct async_emif_config async_emif_config[ASYNC_EMIF_NUM_CS] = {
	{			/* CS0 */
		.mode		= ASYNC_EMIF_MODE_NAND,
		.wr_setup	= 0xf,
		.wr_strobe	= 0x3f,
		.wr_hold	= 7,
		.rd_setup	= 0xf,
		.rd_strobe	= 0x3f,
		.rd_hold	= 7,
		.turn_around	= 3,
		.width		= ASYNC_EMIF_8,
	},

};

static struct pll_init_data core_pll_config[] = {
	{ CORE_PLL,	13,	1,	2 }, /* 799 */
	{ CORE_PLL,	122,	15,	1 }, /* 999 */
	{ CORE_PLL,	625,	32,	2 }, /* 1200 */
};

static struct pll_init_data tetris_pll_config[] = {
	{ TETRIS_PLL,	32,	5,	1 }, /* 800 */
	{ TETRIS_PLL,	40,	5,	1 }, /* 1000 */
	{ TETRIS_PLL,	48,	5,	1 }, /* 1200 */
	{ TETRIS_PLL,	54,	5,	1 }, /* 1350 */
	{ TETRIS_PLL,	56,	5,	1 }, /* 1400 */
};

static struct pll_init_data pa_pll_config =
	{ PASS_PLL,	16,	1,	2 }; /* 983 */


#ifdef CONFIG_SPL_BOARD_INIT
static struct pll_init_data spl_pll_config[] = {
	{ CORE_PLL,	13,	1,	2 }, /* 799 */
	{ TETRIS_PLL,	8,	1,	2 }, /* 500 */
};

void spl_init_keystone_plls(void)
{
	init_plls(ARRAY_SIZE(spl_pll_config), spl_pll_config);
}
#endif

int dram_init(void)
{
	init_ddr3();

	gd->ram_size = get_ram_size((long *)CONFIG_SYS_SDRAM_BASE,
				    CONFIG_MAX_RAM_BANK_SIZE);
	init_async_emif(ARRAY_SIZE(async_emif_config), async_emif_config);
	init_ddr3_ecc(K2HK_DDR3A_EMIF_CTRL_BASE);
	return 0;
}

#ifdef CONFIG_DRIVER_TI_KEYSTONE_NET
eth_priv_t eth_priv_cfg[] = {
#if 1
	{
		.int_name	= "K2HK_EMAC",
		.rx_flow	= CPSW_PORT_RX_FLOW(0),
		.phy_addr	= 0, /*Vyapi V1*/
//		.phy_addr	= 8, /*Vyapi V2*/
		.slave_port	= 1,
		.sgmii_link_type = SGMII_LINK_MAC_PHY,
	},
	{
		.int_name	= "K2HK_EMAC1",
		.rx_flow	= CPSW_PORT_RX_FLOW(1),
	//	.phy_addr	= 8,
		.phy_addr       = 1, //LWS
		.slave_port	= 2,
		.sgmii_link_type = SGMII_LINK_MAC_PHY,
	},
    {
		.int_name	= "K2HK_EMAC2",
		.rx_flow	= CPSW_PORT_RX_FLOW(2),
		.phy_addr	= 1,
//		.phy_addr       = 10, //added
		.slave_port	= 3,
		.sgmii_link_type = SGMII_LINK_MAC_PHY,
	},
#endif
  
	{
		.int_name	= "K2HK_EMAC3",
		.rx_flow	= CPSW_PORT_RX_FLOW(3),
		.phy_addr	= 0,
		.slave_port	= 4,
		.sgmii_link_type = SGMII_LINK_MAC_PHY,
	},
	{
		.int_name	= "K2HK_XMAC0",
		.rx_flow	= 0,
		.slave_port	= 1,
		.sgmii_link_type = XGMII_LINK_MAC_MAC_FORCED,
	},
	{
		.int_name	= "K2HK_XMAC1",
		.rx_flow	= 8,
		.slave_port	= 2,
		.sgmii_link_type = XGMII_LINK_MAC_MAC_FORCED,
	},
};

inline int get_num_eth_ports(void){
	int total_ports = sizeof(eth_priv_cfg) / sizeof(eth_priv_t);
//	printf("LWS 'get_num_eth' total_ports----->%d \n",total_ports);
	return sizeof(eth_priv_cfg) / sizeof(eth_priv_t);
}

eth_priv_t *get_eth_priv_ptr(int port_num)
{
	if (port_num < 0 || port_num >= get_num_eth_ports())
		return NULL;

	return &eth_priv_cfg[port_num];
}

int get_eth_env_param(char *env_name)
{
	char *env;
	int  res = -1;

	env = getenv(env_name);
	if (env)
		res = simple_strtol(env, NULL, 0);

	return res;
}

static int board_has_xge(void)
{
	int ret, current_bus, has_xge = 1, restore = 0;
	current_bus = i2c_get_bus_num();
//	printf("LWS i2c 'board_has_xge' current bus_num------->%d \n",current_bus);
	if (current_bus != RTM_BOC_XGE_RETIMER_I2C_BUS) {
		ret = i2c_set_bus_num(RTM_BOC_XGE_RETIMER_I2C_BUS);
		if (ret) {
			has_xge = 0;
			goto done;
		}
		restore = 1;
	}

	ret = i2c_probe(RTM_BOC_XGE_RETIMER1_I2C_ADDR);
	if (!ret)
		goto done;

	ret = i2c_probe(RTM_BOC_XGE_RETIMER2_I2C_ADDR);
	if (!ret)
		goto done;

	has_xge = 0;
done:
	/* restore previous bus num */
	if (restore)
		i2c_set_bus_num(current_bus);
//	printf("LWS 'board_has_xge'has_xge--->%d \n",has_xge);
	return has_xge;
}

int board_eth_init(bd_t *bis)
{
	int	j;
	int	res;
	char	link_type_name[32];
	int	has_xge = board_has_xge();
//	printf("LWS---> 'board_eth_init' has_xge---> %d \n",has_xge); //added
	for (j = 0; j < get_num_eth_ports(); j++) {
		if (IS_XGE(&eth_priv_cfg[j]) && !has_xge)
			continue;

		sprintf(link_type_name, "sgmii%d_link_type", j);
//		printf("LWS link_type name %s \n",link_type_name);//added
		res = get_eth_env_param(link_type_name);
//		printf("LWS res=%d \n",res);//added
		if (res >= 0)
			eth_priv_cfg[j].sgmii_link_type = res;
		if (j<=1){
			keystone2_emac_initialize(&eth_priv_cfg[j]);
	       		keystone2_eth_open_close(eth_priv_cfg[j].dev);
//			printf("LWS $$$$$$$$$$$$$$$$ open close %d\n",j);
	}

//	keystone2_eth_open_close(eth_priv_cfg[0].dev);
//	keystone2_eth_open_close(eth_priv_cfg[1].dev);
//	keystone2_eth_open_close(eth_priv_cfg[2].dev); 
}
	return 0;
}
#endif

#if defined(CONFIG_BOARD_EARLY_INIT_F)
int board_early_init_f(void)
{
	int speed;

	speed = get_max_dev_speed();

	if (speed != SPD800 && speed != SPD_RSV)
		init_pll(&core_pll_config[speed]);
	else
		init_pll(&core_pll_config[SPD800]);

	init_pll(&pa_pll_config);

	speed = get_max_arm_speed();

	if (speed != SPD800 && speed != SPD_RSV)
		init_pll(&tetris_pll_config[speed]);
	else
		init_pll(&tetris_pll_config[SPD800]);

	return 0;
}
#endif

int board_init(void)
{

	gd->bd->bi_arch_number = -1;
	gd->bd->bi_boot_params = LINUX_BOOT_PARAM_ADDR;

	return 0;
}