-------------------EP2000--------------------------- --------------Version : 203300---------------------- -------------R5F_MCU_1_0_CORE----------------------- -------DRV : CAN_TRCV-WdG-IPC-ADC-SPI--------------- -------APP : SOH-TEMP MON-VOLT MON-POWER_MAGR------- -------MOD : IMU_SMI130-POWER_MANGER---------------- ---------------------------------------------------- APTIV VIP-R5F: EP2000 - Tasks initialized !!! CAN TRCV Pin Init:- Read value 118 - 6 -36 Read value 118 - 7 -73 Read value 118 - 2 -255 Read value at 118 - 3 - 255 Read value 119 - 6 -36 Read value 119 - 7 -201 Read value 119 - 2 -255 Read value at 119 - 3 -255 Read value 116 - 6 -36 Read value 116 - 7 -73 Read value 116 - 2 -255 Read value at 116 - 3 - 255 Read value U11 - 7 -247 Read value at U11 - 3 - 247 CAN Profile App:Variant - Pre Compile being used !!! CAN Profile App: GCP-CAN is Initializing !!! WatchDog_Task_Intialize- STARTS !!! WDG MCAL Version Info --------------------- Vendor ID : 44 Module ID : 102 SW Major Version : 0 SW Minor Version : 1 SW Patch Version : 0 Starting WDG test !!! Variant - Pre Compile being used !!! WDG timeout is configured for 20000 millisecs WDG ESM Interrupt will be generated after 20000 * 5 i.e 100000 millisecs APTIV VIP-R5F:SPI Init !!! Temperature_Mon_Initialize APT Profile App: Controller started proCAN Profile App: Controller started properlyy:0 Temp sensor boardcfg Failed -6 IPC_Test_:File Before Resource Table LoadedCAN Profile App:Will Transmit 5 Messages, 5 times: 0 vtm_sensor_init IPC_Test_:File After Resource Table LoadedCAN Profile App:NOTE : CAN Write is successs : ctlr_cnt=0, loopCnt = 0 IPC_Test_:File IPC VirtIO Init DoneCAN Profile App:Dem error was reported, eventId = 65517, eventStatus = 1,ctlr_cnt=0,loopCnt= 0 IPC_Test_:File RPMsg Init DoneCAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 1 IPC_Test_:File Remote_Proc returned mcu1_0!!! IPN Profile App:NOTE : CAN Write is failing : cCAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 2 IPC_Test_:File rpmsg_vdevMonitorFxn mcu1_0!!! CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 3 IPC_Test_:FileInside Vdev Monitor Function IPN Profile App:NOTE : CAN Write is failingCAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 1 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 2 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 1 CAN R5F MCU_1_0 Alive Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 2 CAN Profile App:Det error was reported CAN Profile App:With Module ID as 102 CAN Profile App:With Module ID as 0 CAN Profile App:With Module ID as 5 CAN Profile App:With Module ID as 16 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 1 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 2 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 1 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 2 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=0,loopCnt = 4 CAN Profile App: Controller started properlyy:1 CAN Profile App:Will Transmit 5 Messages, 5 times: 1 CAN Profile App:NOTE : CAN Write is successs : ctlr_cnt=1, loopCnt = 0 CAN Profile App:Dem error was reported, eventId = 65517, eventStatus = 1,ctlr_cnt=1,loopCnt= 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 1 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 2 CAN Profile App:NOTE :R5F MCU_1_0 Alive CAN Write is failing : ctlr_cnt=1,loopCnt = 3 CAN Profile App:Det error was reported CAN Profile App:With Module ID as 102 CAN Profile App:With Module ID as 0 CAN Profile App:With Module ID as 5 CAN Profile App:With Module ID as 16 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 1 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 2 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 1 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 2 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 1 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 2 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 4 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 0 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 1 CAN Profile App:NOTE : CAN WriteR5F MCU_1_0 Alive is failing : ctlr_cnt=1,loopCnt = 2 CAN Profile App:Det error was reported CAN Profile App:With Module ID as 102 CAN Profile App:With Module ID as 0 CAN Profile App:With Module ID as 5 CAN Profile App:With Module ID as 16 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 3 CAN Profile App:NOTE : CAN Write is failing : ctlr_cnt=1,loopCnt = 4 CAN Profile App: 8192 bytes used for stack R5F MCU_1_0 Alive R5F MCU_1_0 Alive R5F MCU_1_0 Alive Average Temperature 35044 R5F MCU_1_0 Alive R5F MCU_1_0 Alive R5F MCU_1_0 Alive ²Í­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©!+²è +-¬É!«² ?v2¨µê²?­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©²?­T¿ì0(±)+ «©)ü£´ù3ý?ÿ¦ú¬ù²ù­ÿ´ù ü/þ%ø©þ þ¥ø¤þ­ûê)ü£´ù3ý?ÿ¦ú¬ù2þ­þ§6ù%ÿ­ÿ®ú´ÿ2þ8ÿ:ø2ü­ù³þ¡þ¥!ÿ®ÿ5ÿ£ù¨ú þµü£ù³þ ûíê¢ø4ý%þ9ø­ÿ.ø¬ú®ù!+²è +-¬É!«² ?