U-Boot SPL 2021.01-00001-geb4ef47698 (Jul 21 2023 - 17:27:35 -0500) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') SPL initial stack usage: 13424 bytes Trying to boot from DFU ################################################DOWNLOAD ... OK Ctrl+C to exit ... Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from MMC... MMC Device 0 not found *** Warning - No MMC card found, using default environment init_env from device 10 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb NOTICE: BL31: Built : 17:27:41, Jul 21 2023 I/TC: I/TC: OP-TEE version: 3.20.0-rc1 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Fri Jul 21 22:27:50 UTC 2023 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html I/TC: Primary CPU initializing I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2021.01-00001-geb4ef47698 (Jul 21 2023 - 17:27:55 -0500) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') Trying to boot from DFU ####DOWNLOAD ... OK Ctrl+C to exit ... U-Boot 2021.01-00001-geb4ef47698 (Jul 21 2023 - 17:27:55 -0500) SoC: AM62X SR1.0 GP Model: Texas Instruments AM625 SK EEPROM not available at 0x50, trying to read at 0x51 Board: AM62-SKEVM rev E3 DRAM: 2 GiB MMC: mmc@fa10000: 0, mmc@fa00000: 1, mmc@fa20000: 2 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => => setenv dfu_alt_info ${dfu_alt_info_emmc} => dfu 0 mmc 0 ##DOWNLOAD ... OK Ctrl+C to exit ... ###DOWNLOAD ... OK Ctrl+C to exit ... ####DOWNLOAD ... OK Ctrl+C to exit ... => mmc partconf 0 1 1 1 => mmc bootbus 0 2 0 0 => U-Boot SPL 2021.01-00001-gaca79e62eb (Jul 21 2023 - 17:27:24 -0500) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') SPL initial stack usage: 13424 bytes Trying to boot from MMC1 spl_load_fit_image: Skip load 'tee': image size is 0! Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from MMC... OK init_env from device 9 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb NOTICE: BL31: Built : 17:27:41, Jul 21 2023 ð U-Boot SPL 2021.01-00001-gaca79e62eb (Jul 21 2023 - 17:27:24 -0500) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') SPL initial stack usage: 13424 bytes Trying to boot from MMC1 spl_load_fit_image: Skip load 'tee': image size is 0! Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from MMC... OK init_env from device 9 not supported! Starting ATF on ARM64 core... NOTICE: BL31: v2.8(release):v2.8-226-g2fcd408bb NOTICE: BL31: Built : 17:27:41, Jul 21 2023