U-Boot SPL 2023.04 (Jul 14 2026 - 18:22:47 -0500) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)') i2c_write: error waiting for data ACK (status=0x116) read error from device: 41c86438 register: x! Trying to boot from SPI Authentication passed Authentication passed Authentication passed Returning so no mux is selected. We dont have this on Hydra Loading Environment from nowhere... OK Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release): NOTICE: BL31: Built : 18:22:21, Jul 14 2026 U-Boot SPL 2023.04 (Jul 14 2026 - 18:22:25 -0500) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.4--v09.02.04 (Kool Koala)') Trying to boot from SPI k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,32] sci-dev-id:235 k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled jedec_spi_nor flash@0: non-uniform erase sector maps are not supported yet. Authentication passed Authentication passed Returning so no mux is selected. We dont have this on Hydra U-Boot 2023.04 (Jul 14 2026 - 18:22:25 -0500) SoC: J7200 SR2.0 HS-FS Model: Texas Instruments K3 J7200 SoC Board: J7200X-PM1-SOM rev E7 DRAM: 1 GiB cdns3_bind: unsupported dr_mode Core: 93 devices, 32 uclasses, devicetree: separate Flash: 0 Bytes MMC: mmc@4f80000 - probe failed: -22 mmc@4fb0000: 1 Loading Environment from SPIFlash... k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[96,32] sci-dev-id:235 k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled jedec_spi_nor flash@0: non-uniform erase sector maps are not supported yet. SF: Detected s28hs512t with page size 256 Bytes, erase size 256 KiB, total 64 MiB *** Warning - bad CRC, using default environment In: serial@40a00000 Out: serial@40a00000 Err: serial@40a00000 am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 Net: CSD: in dp83867_config CSD: in dp83867_of_init CSD: Phy CFG4 reg is 0x10b1 eth0: ethernet@46000000port@1 Starting POST POST Now executing Memory alternating 1/0... Passed POST Now executing Memory marching 1s address... Passed POST Now executing Memory alternating 0/1... Passed POST Now executing Memory marching 1s... Passed POST Now executing Memory marching 0 Address... Passed POST Now executing BIST startup tests... Passed POST Now executing Memory marching 0s... Passed POST Now executing MCU VMON POK... Passed POST Now executing POR VMON POK... Passed POST Now executing ADC Glitch detected low... Passed POST Now executing ADC Glitch detected hi... Passed POST Now executing PMIC Buck 1/2 tests... Passed POST Now executing PMIC BUCK 3/4 tests... Passed POST Now executing PMIC Buck 5 tests... Passed POST Now executing PMIC LDO 1/2 tests... Passed POST Now executing PMIC LDO 3/4 tests... Passed POST Now executing HART EEPROM Test... POST Error: HART EEPROM Test, HART EEPROM not programmed POST Now executing Temperature Sensors testing... Passed POST execution complete! Hit any key to stop autoboot: 2  1  0 am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 2 CSD: leaving am65_cpsw_macsl_reset i = 0x64 ethernet@46000000port@1 Waiting for PHY auto negotiation to complete. done am65_cpsw_nuss_port ethernet@46000000port@1: CSD: mac_control is 0xa1, port->mac_control is 0x0, phy->link is 0x1 link up on port 1, speed 1000, full duplex BOOTP broadcast 1 BOOTP broadcast 2 BOOTP broadcast 3 DHCP client bound to address 10.0.1.223 (1002 ms) Using ethernet@46000000port@1 device TFTP from server 10.0.1.1; our IP address is 10.0.1.223 Filename 'ice2/ice2-vip'. Load address: 0x81000000 Loading: *################################################## 7.2 MiB 12 MiB/s done Bytes transferred = 7553848 (734338 hex) CSD: leaving am65_cpsw_macsl_wait_for_idle i = 0xffffffff and idle bits 0xf0000000 CSD: image_get_magic is 0x27051956 ## Booting kernel from Legacy Image at 81000000 ... CSD: image_get_magic is 0x27051956 Image Name: vxworks Image Type: AArch64 VxWorks Kernel Image (uncompressed) Data Size: 7553784 Bytes = 7.2 MiB Load Address: 80100000 Entry Point: 80100000 Verifying Checksum ... OK CSD: image_get_magic is 0x27051956 CSD: image_get_magic is 0x27051956 CSD: image_get_magic is 0x27051956 Working FDT set to 0 Loading Kernel Image !!! WARNING !!! Using legacy DTB ## Starting vxWorks at 0x80100000, device tree at 0x00000000 ... protecting primary core interrupt stack protecting root task stacks protecting idle tasks initialize VxBus install bus types: vxbMiiBus(MII bus type) vxbPciBus(PCI bus type) vxbFdtBus(Flattened Device Tree bus type) vxbNexusBus(Nexus bus type) vxbIeee1588Bus(IEEE1588 bus type) probe and attach devices Tprotecting non-primary core interrupt stacks arget Name: scp User: target _________ _________ \........\ /......../ \........\ /......../ \........\ /......../ \........\ /......../ \........\ \......./ \........\ \...../ VxWorks SMP 64-bit \........\ \.../ \........\ \./ Release version: 25.03 \........\ - Build date: Jul 9 2026 18:36:23 \........\ \......./ Copyright Wind River Systems, Inc. \...../ - 1984-2026 \.../ /.\ \./ /...\ - ------- Board: GEHC MR ICE2 J7200 - Cortex-A72 (ARMV8A) CPU Count: 2 OS Memory Size: 679MB ED&R Policy Mode: Deployed Debug Agent: Not started Stop Mode Agent: Not started Adding 15820 symbols for standalone.