U-Boot SPL 2017.01-00319-g9e3097f-dirty (Sep 15 2017 - 14:25:12) Trying to boot from NAND U-Boot 2017.01-00319-g9e3097f-dirty (Sep 15 2017 - 14:25:12 +0100) I2C: ready DRAM: 128 MiB WARNING: Caches not enabled NAND: 512 MiB MMC: davinci: 0 *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial Invalid MAC address read. Net: DaVinci-EMAC Warning: DaVinci-EMAC (eth0) using random MAC address - ce:62:ce:d7:c6:5a Hit any key to stop autoboot: 3  2  1  0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt ** Unable to read file uEnv.txt ** switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 2378000 bytes read in 2731 ms (849.6 KiB/s) 11945 bytes read in 61 ms (190.4 KiB/s) ## Flattened Device Tree blob at c0600000 Booting using the fdt blob at 0xc0600000 Loading Device Tree to c7e23000, end c7e28ea8 ... OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Booting Linux on physical CPU 0x0 Linux version 4.9.28-geed43d1050 (root@ubuntu) (gcc version 6.2.1 20161016 (Linaro GCC 6.2-2016.11) ) #37 PREEMPT Wed Feb 21 09:47:20 GMT 2018 CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=0005317f CPU: VIVT data cache, VIVT instruction cache OF: fdt:Machine model: DA850/AM1808/OMAP-L138 LCDK Reserved memory: created CMA memory pool at 0xc3000000, size 32 MiB OF: reserved mem: initialized node dsp_cma@c3000000, compatible id shared-dma-pool cma: Reserved 16 MiB at 0xc6c00000 Memory policy: Data cache writethrough DaVinci da850/omap-l138/am18x variant 0x1 Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32480 Kernel command line: console=ttyS2,115200n8 root=PARTUUID=725f1c6a-02 rw rootfstype=ext4 rootwait PID hash table entries: 512 (order: -1, 2048 bytes) Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) Memory: 73732K/131072K available (4554K kernel code, 309K rwdata, 1452K rodata, 228K init, 162K bss, 8188K reserved, 49152K cma-reserved) Virtual kernel memory layout: vector : 0xffff0000 - 0xffff1000 ( 4 kB) fixmap : 0xffc00000 - 0xfff00000 (3072 kB) vmalloc : 0xc8800000 - 0xff800000 ( 880 MB) lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) modules : 0xbf000000 - 0xc0000000 ( 16 MB) .text : 0xc0008000 - 0xc047aea0 (4556 kB) .init : 0xc05e7000 - 0xc0620000 ( 228 kB) .data : 0xc0620000 - 0xc066d628 ( 310 kB) .bss : 0xc066d628 - 0xc0696170 ( 163 kB) SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 Preemptible hierarchical RCU implementation. Build-time adjustment of leaf fanout to 32. NR_IRQS:245 clocksource: timer0_1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns Console: colour dummy device 80x30 Calibrating delay loop... 227.32 BogoMIPS (lpj=1136640) pid_max: default: 32768 minimum: 301 Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) CPU: Testing write buffer coherency: ok Setting up static identity map for 0xc0008400 - 0xc0008458 devtmpfs: initialized VFP support v0.3: not present clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns futex hash table entries: 256 (order: -1, 3072 bytes) pinctrl core: initialized pinctrl subsystem NET: Registered protocol family 16 DMA: preallocated 256 KiB pool for atomic coherent allocations cpuidle: using governor ladder cpuidle: using governor menu mux: initialized RTC_ALARM mux: Setting register RTC_ALARM mux: PINMUX0 (0x00000000) = 0x44080000 -> 0x24080000 No ATAGs? edma 1c00000.edma: memcpy is disabled edma 1c00000.edma: TI EDMA DMA engine driver edma 1e30000.edma: memcpy is disabled edma 1e30000.edma: TI EDMA DMA engine driver i2c_davinci i2c_davinci.1: could not find pctldev for node /soc@1c00000/pinmux@14120/pinmux_i2c0_pins, deferring probe pps_core: LinuxPPS API ver. 1 registered pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti PTP clock support registered clocksource: Switched to clocksource timer0_1 NET: Registered protocol family 2 TCP established hash table entries: 1024 (order: 0, 4096 bytes) TCP bind hash table entries: 1024 (order: 0, 4096 bytes) TCP: Hash tables configured (established 1024 bind 1024) UDP hash table entries: 256 (order: 0, 4096 bytes) UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) NET: Registered protocol family 1 RPC: Registered named UNIX socket transport module. RPC: Registered udp transport module. RPC: Registered tcp transport module. RPC: Registered tcp NFSv4.1 backchannel transport module. workingset: timestamp_bits=14 max_order=15 bucket_order=1 Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248) io scheduler noop registered (default) pinctrl-single 1c14120.pinmux: please update dts to use #pinctrl-cells = <2> pinctrl-single 1c14120.pinmux: 160 pins at pa fec14120 size 80 Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled console [ttyS2] disabled serial8250.2: ttyS2 at MMIO 0x1d0d000 (irq = 61, base_baud = 8250000) is a TI DA8xx/66AK2x console [ttyS2] enabled brd: module loaded libphy: Fixed MDIO Bus: probed davinci_mdio davinci_mdio.0: davinci mdio revision 1.5 davinci_mdio davinci_mdio.0: detected phy mask fffffffd libphy: davinci_mdio.0: probed davinci_mdio davinci_mdio.0: phy[1]: device davinci_mdio.0:01, driver NatSemi DP83640 i2c /dev entries driver davinci_mmc da830-mmc.0: Got CD GPIO davinci_mmc da830-mmc.0: Using DMA, 4-bit mode NET: Registered protocol family 10 sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver NET: Registered protocol family 17 console [netcon0] enabled netconsole: network logging started davinci_emac davinci_emac.1: incompatible machine/device type for reading mac address davinci_emac davinci_emac.1: using random MAC addr: 62:be:90:db:39:e5 mmc0: host does not support reading read-only switch, assuming write-enable input: gpio-keys as /devices/platform/gpio-keys/input/input0 mmc0: new high speed SDHC card at address 0002 mmcblk0: mmc0:0002 N/A 7.50 GiB mmcblk0: p1 p2 hctosys: unable to open rtc device (rtc0) random: fast init done EXT4-fs (mmcblk0p2): recovery complete EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) VFS: Mounted root (ext4 filesystem) on device 179:2. devtmpfs: mounted Freeing unused kernel memory: 228K (c05e7000 - c0620000) This architecture does not have kernel memory protection. systemd[1]: System time before build time, advancing clock. systemd[1]: systemd 230 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN) systemd[1]: Detected architecture arm. Welcome to Arago 2017.05! systemd[1]: Set hostname to . systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password Requests to Console Directory Watch. systemd[1]: Listening on /dev/initctl Compatibility Named Pipe. [ OK ] Listening on /dev/initctl Compatibility Named Pipe. systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password Requests to Wall Directory Watch. systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ OK ] Listening on Syslog Socket. [ OK ] Created slice System Slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-getty.slice. [ OK ] Reached target Slices. [ OK ] Listening on udev Control Socket. [ OK ] Reached target Swap. [ OK ] Listening on Journal Socket. Starting Create list of required st... nodes for the current kernel... Starting Load Kernel Modules... Starting Remount Root and Kernel File Systems... cryptodev: loading out-of-tree module taints kernel. cryptodev: driver 1.8 loaded. Starting Setup Virtual Console... Starting Journal Service... EXT4-fs (mmcblk0p2): re-mounted. Opts: (null) Mounting POSIX Message Queue File System... Mounting Temporary Directory... [ OK ] Reached target Paths. [ OK ] Listening on udev Kernel Socket. Mounting Debug File System... [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Debug File System. [ OK ] Mounted Temporary Directory. [ OK ] Started Create list of required sta...ce nodes for the current kernel. [ OK ] Started Load Kernel Modules. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Setup Virtual Console. [ OK ] Started Journal Service. Starting udev Coldplug all Devices... Starting Flush Journal to Persistent Storage... Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev... [ OK ] Started Apply Kernel Variables. systemd-journald[64]: Received request to flush runtime journal from PID 1 [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Create Static Device Nodes in /dev. Starting udev Kernel Device Manager... [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... Mounting /var/volatile... [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started udev Kernel Device Manager. [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Synchronized. Starting Synchronize System and HW clocks... [FAILED] Failed to start Synchronize System and HW clocks. See 'systemctl status sync-clocks.service' for details. davinci-rproc davinci-rproc.0: assigned reserved memory node dsp_cma@c3000000 remoteproc remoteproc0: dsp is available remoteproc remoteproc0: powering up dsp remoteproc remoteproc0: Booting fw image rproc-dsp-fw, size 4077796 remoteproc remoteproc0: registered virtio0 (type 7) remoteproc remoteproc0: remote processor dsp is now up [ OK ] Started udev Coldplug all Devices. [ OK ] Reached target System Initialization. [ OK ] Listening on D-Bus System Message Bus Socket. davinci-wdt davinci-wdt: heartbeat 60 sec [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Listening on dropbear.socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Kernel Logging Service. Linux video capture interface: v2.00 Starting Login Service... OF: /sound/simple-audio-card,cpu: could not get #sound-dai-cells for /soc@1c00000/mcasp@100000 0-0018 supply IOVDD not found, using dummy regulator 0-0018 supply DVDD not found, using dummy regulator 0-0018 supply AVDD not found, using dummy regulator 0-0018 supply DRVDD not found, using dummy regulator asoc-simple-card sound: parse error -22 Starting Ethernet Bridge Filtering Tables... asoc-simple-card: probe of sound failed with error -22 [ OK ] Started System Logger Daemon. tvp514x 0-005d: Write: retry ... 0 tvp514x 0-005d: Write: retry ... 1 tvp514x 0-005d: Write: retry ... 2 tvp514x 0-005d: Write: retry ... 3 tvp514x 0-005d: Write: retry ... 4 tvp514x 0-005d: Write: retry ... 5 [ OK ] Started D-Bus System Message Bus. tvp514x 0-005d: tvp514x 0-005d decoder driver registered !! vpif_capture vpif_capture: registered sub device tvp514x-0 tvp514x 0-005d: Write: retry ... 0 tvp514x 0-005d: Write: retry ... 1 tvp514x 0-005d: Write: retry ... 2 tvp514x 0-005d: Write: retry ... 3 tvp514x 0-005d: Write: retry ... 4 tvp514x 0-005d: Write: retry ... 5 Starting Network Service... [ OK ] Started System Logging Service. Starting telnetd.service... Starting Print notice about GPLv3 packages... Starting tiipclad-daemon.service... [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Started Ethernet Bridge Filtering Tables. [ OK ] Found device /dev/ttyS2. [ OK ] Started telnetd.service. [ OK ] Started Network Service. davinci_mdio davinci_mdio.0: resetting idled controller NatSemi DP83640 davinci_mdio.0:01: attached PHY driver [NatSemi DP83640] (mii_bus:phy_addr=davinci_mdio.0:01, irq=-1) IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ OK ] Started tiipclad-daemon.service. [ OK ] Reached target Network. Starting Simple Network Management Protocol (SNMP) Daemon.... [ OK ] Started Vsftpd ftp daemon. Starting Permit User Sessions... Starting Lightning Fast Webserver With Light System Requirements... [ OK ] Started strondavinci_emac davinci_emac.1 eth0: Link is Up - 100Mbps/Full - flow control rx/tx gSwan IPsec IKEvIPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready 1/IKEv2 daemon using ipsec.conf. Starting Network Name Resolution... Starting thttpd.service... [ OK ] Started Permit User Sessions. [ OK ] Started Lightning Fast Webserver With Light System Requirements. FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. [ OK ] Started Network Name Resolution. [ OK ] Started thttpd.service. [ OK ] Started Login Service. Starting rng-tools.service... [ OK ] Started Serial Getty on ttyS2. [ OK ] Started Getty on tty1. [ OK ] Reached target Login Prompts. random: crng init done _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org omapl138-lcdk ttyS2 Arago 2017.05 omapl138-lcdk ttyS2 virtio_rpmsg_bus virtio0: rpmsg host is online omapl138-lcdk login: nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xcc nand: Micron MT29F4G16ABADAH4 nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64 Bad block table not found for chip 0 Bad block table not found for chip 0 Scanning device for bad blocks Bad block table written to 0x00001ffe0000, version 0x01 Bad block table written to 0x00001ffc0000, version 0x01 3 ofpart partitions found on MTD device davinci-nand.0 Creating 3 MTD partitions on "davinci-nand.0": 0x000000000000-0x000000020000 : "u-boot env" 0x000000020000-0x0000000a0000 : "u-boot" 0x0000000a0000-0x000020000000 : "free space" davinci_nand davinci-nand.0: controller rev. 2.5 *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf binutils cpp-symlinks cpp dosfstools g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gstreamer1.0-libav hidapi libgmp10 libidn11 libmpc3 libmpfr4 libreadline6 m4 make nettle If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** ***************************************************************