U-Boot SPL 2018.01-00569-gf9c38b91a2-dirty (Jun 19 2019 - 14:18:29) Trying to boot from MMC1 SPL: Please implement spl_start_uboot() for your board SPL: Direct Linux boot not active! U-Boot 2018.01-00569-gf9c38b91a2-dirty (Jun 19 2019 - 14:18:23 +0300) CPU : AM437X-GP rev 1.2 Model: TI AM437x GP EVM DRAM: 512 MiB sdadadsadCan't find PMIC:TPS65218_PMIC NAND: 512 MiB MMC: OMAP SD/MMC: 0 *** Warning - bad CRC, using default environment Net: not set. Validating first E-fuse MAC cpsw, usb_ether Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 ** Unable to read file boot.scr ** 717 bytes read in 3 ms (233.4 KiB/s) Loaded env from uEnv.txt Importing environment from mmc0 ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 3887616 bytes read in 230 ms (16.1 MiB/s) 52821 bytes read in 24 ms (2.1 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff0000, end 8ffffe54 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.79-gbde58ab01e (oe-user@oe-host) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #1 PREEMPT Thu Dec 20 04:03:12 UTC 2018 [ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM437x GP EVM [ 0.000000] Memory policy: Data cache writeback [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 48 MiB at 0x9d000000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM437x ES1.2 (sgx neon) [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920 [ 0.000000] Kernel command line: console=ttyO0,115200n8 video=HDMI-A-1:800x600 root=PARTUUID=f9fdd9ec-02 rw rootfstype=ext4 rootwait [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 456852K/524288K available (8192K kernel code, 329K rwdata, 2560K rodata, 1024K init, 268K bss, 18284K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB) [ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB) [ 0.000000] .data : 0xc0d00000 - 0xc0d52448 ( 330 kB) [ 0.000000] .bss : 0xc0d52448 - 0xc0d9569c ( 269 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Tasks RCU enabled. [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] L2C: platform modifies aux control register: 0x0e030000 -> 0x3e430000 [ 0.000000] L2C: DT/platform modifies aux control register: 0x0e030000 -> 0x3e430000 [ 0.000000] L2C-310 enabling early BRESP for Cortex-A9 [ 0.000000] OMAP L2C310: ROM does not support power control setting [ 0.000000] L2C-310 dynamic clock gating disabled, standby mode disabled [ 0.000000] L2C-310 cache controller enabled, 16 ways, 256 kB [ 0.000000] L2C-310: CACHE_ID 0x410000c9, AUX_CTRL 0x4e430000 [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000011] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000028] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000037] OMAP clocksource: timer1 at 24000000 Hz [ 0.000429] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns [ 0.000439] OMAP clocksource: 32k_counter at 32768 Hz [ 0.000848] Console: colour dummy device 80x30 [ 0.000876] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000882] This ensures that you still see kernel messages. Please [ 0.000886] update your kernel commandline. [ 0.000907] Calibrating delay loop... 1993.93 BogoMIPS (lpj=9969664) [ 0.060152] pid_max: default: 32768 minimum: 301 [ 0.060316] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.060332] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.061026] CPU: Testing write buffer coherency: ok [ 0.061086] CPU0: Spectre v2: using BPIALL workaround [ 0.061776] Setting up static identity map for 0x80100000 - 0x80100060 [ 0.061920] Hierarchical SRCU implementation. [ 0.062241] EFI services will not be available. [ 0.063095] devtmpfs: initialized [ 0.071861] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0 [ 0.072283] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4 [ 0.072553] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.072573] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.076001] pinctrl core: initialized pinctrl subsystem [ 0.076669] DMI not present or invalid. [ 0.077042] NET: Registered protocol family 16 [ 0.078704] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.150048] cpuidle: using governor ladder [ 0.150085] cpuidle: using governor menu [ 0.155401] omap_gpio 44e07000.gpio: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/gpio0_pins, deferring probe [ 0.156204] OMAP GPIO hardware version 0.1 [ 0.158142] omap_gpio 48322000.gpio: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/display_mux_pins, deferring probe [ 0.161854] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/nand_flash_x8, deferring probe [ 0.165770] No ATAGs? [ 0.165795] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers. [ 0.165808] hw-breakpoint: maximum watchpoint size is 4 bytes. [ 0.177690] edma 49000000.edma: TI EDMA DMA engine driver [ 0.181886] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/i2c0_pins, deferring probe [ 0.181948] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp@44000000/l4_wkup@44c00000/scm@210000/pinmux@800/i2c1_pins, deferring probe [ 0.182081] media: Linux media interface: v0.10 [ 0.182117] Linux video capture interface: v2.00 [ 0.182216] pps_core: LinuxPPS API ver. 1 registered [ 0.182222] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.182251] PTP clock support registered [ 0.182283] EDAC MC: Ver: 3.0.0 [ 0.182689] dmi: Firmware registration failed. [ 0.183031] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.183409] Advanced Linux Sound Architecture Driver Initialized. [ 0.184449] clocksource: Switched to clocksource timer1 [ 0.191728] NET: Registered protocol family 2 [ 0.192336] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.192376] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.192417] TCP: Hash tables configured (established 4096 bind 4096) [ 0.192534] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.192550] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.192703] NET: Registered protocol family 1 [ 0.193110] RPC: Registered named UNIX socket transport module. [ 0.193121] RPC: Registered udp transport module. [ 0.193127] RPC: Registered tcp transport module. [ 0.193132] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.195161] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 0.198521] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.199266] NFS: Registering the id_resolver key type [ 0.199303] Key type id_resolver registered [ 0.199310] Key type id_legacy registered [ 0.199355] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.201367] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245) [ 0.201385] io scheduler noop registered [ 0.201392] io scheduler deadline registered [ 0.201579] io scheduler cfq registered (default) [ 0.201587] io scheduler mq-deadline registered [ 0.201594] io scheduler kyber registered [ 0.203640] pinctrl-single 44e10800.pinmux: 199 pins at pa f9e10800 size 796 [ 0.206795] pwm-backlight backlight: backlight supply power not found, using dummy regulator [ 0.248382] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled [ 0.250623] omap8250 44e09000.serial: No clock speed specified: using default: 48000000 [ 0.251292] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250 [ 0.979802] console [ttyS0] enabled [ 0.983784] omap8250 481a6000.serial: No clock speed specified: using default: 48000000 [ 0.992515] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 31, base_baud = 3000000) is a 8250 [ 1.003191] omap_rng 48310000.rng: Random Number Generator ver. 20 [ 1.010621] omapdss_dss 4832a000.dss: 4832a000.dss supply vdda_video not found, using dummy regulator [ 1.020085] DSS: OMAP DSS rev 2.0 [ 1.024246] omapdss_dss 4832a000.dss: bound 4832a400.dispc (ops dispc_component_ops) [ 1.033425] panel-dpi display: display supply vcc not found, using dummy regulator [ 1.053045] brd: module loaded [ 1.064370] loop: module loaded [ 1.070019] libphy: Fixed MDIO Bus: probed [ 1.144513] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.152215] davinci_mdio 4a101000.mdio: detected phy mask fffffffe [ 1.159576] libphy: 4a101000.mdio: probed [ 1.163617] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Micrel KSZ9031 Gigabit PHY [ 1.174253] cpsw 4a100000.ethernet: Detected MACID = 60:64:05:6b:e0:3c [ 1.181004] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.187475] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.192768] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 1.201236] i2c /dev entries driver [ 1.205295] IR NEC protocol handler initialized [ 1.209848] IR RC5(x/sz) protocol handler initialized [ 1.214957] IR RC6 protocol handler initialized [ 1.219504] IR JVC protocol handler initialized [ 1.224049] IR Sony protocol handler initialized [ 1.228693] IR SANYO protocol handler initialized [ 1.233414] IR Sharp protocol handler initialized [ 1.238146] IR MCE Keyboard/mouse protocol handler initialized [ 1.244000] IR XMP protocol handler initialized [ 1.250098] cpuidle: enable-method property 'ti,am4372' found operations [ 1.257290] sdhci: Secure Digital Host Controller Interface driver [ 1.263497] sdhci: Copyright(c) Pierre Ossman [ 1.324750] sdhci-pltfm: SDHCI platform and OF driver helper [ 1.334422] ledtrig-cpu: registered to indicate activity on CPUs [ 1.344696] NET: Registered protocol family 10 [ 1.351284] Segment Routing with IPv6 [ 1.355124] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.361679] NET: Registered protocol family 17 [ 1.366527] Key type dns_resolver registered [ 1.371003] omap_voltage_late_init: Voltage driver support not added [ 1.383478] omapdrm omapdrm.0: DMM not available, disable DMM support [ 1.390453] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 1.397174] [drm] No driver support for vblank timestamp query. [ 1.465712] Console: switching to colour frame buffer device 100x30 [ 1.488847] omapdrm omapdrm.0: fb0: omapdrm frame buffer device [ 1.495513] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0 [ 1.503238] GPIO line 119 (SelEMMCorNAND) hogged as output/low [ 1.509946] GPIO line 136 (SelLCDorHDMI) hogged as output/high [ 1.516559] omap-gpmc 50000000.gpmc: GPMC revision 6.0 [ 1.521730] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000 [ 1.529500] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xdc [ 1.535947] nand: Micron MT29F4G08ABAEAWP [ 1.539975] nand: 512 MiB, SLC, erase size: 256 KiB, page size: 4096, OOB size: 224 [ 1.547782] using OMAP_ECC_BCH16_CODE_HW ECC scheme [ 1.552803] 10 ofpart partitions found on MTD device omap2-nand.0 [ 1.558946] Creating 10 MTD partitions on "omap2-nand.0": [ 1.564398] 0x000000000000-0x000000040000 : "NAND.SPL" [ 1.570483] 0x000000040000-0x000000080000 : "NAND.SPL.backup1" [ 1.577208] 0x000000080000-0x0000000c0000 : "NAND.SPL.backup2" [ 1.583854] 0x0000000c0000-0x000000100000 : "NAND.SPL.backup3" [ 1.590530] 0x000000100000-0x000000180000 : "NAND.u-boot-spl-os" [ 1.597385] 0x000000180000-0x000000280000 : "NAND.u-boot" [ 1.603582] 0x000000280000-0x0000002c0000 : "NAND.u-boot-env" [ 1.610128] 0x0000002c0000-0x000000300000 : "NAND.u-boot-env.backup1" [ 1.617439] 0x000000300000-0x000000a00000 : "NAND.kernel" [ 1.624568] 0x000000a00000-0x000020000000 : "NAND.file-system" [ 1.724656] tps65218 0-0024: Failed to set masks in 0x3: -121 [ 1.730606] tps65218: probe of 0-0024 failed with error -121 [ 1.736741] omap_i2c 44e0b000.i2c: bus 0 rev0.12 at 100 kHz [ 1.743981] omap_i2c 4802a000.i2c: bus 1 rev0.12 at 100 kHz [ 1.750747] omap_hsmmc 48060000.mmc: Got CD GPIO [ 1.815819] hctosys: unable to open rtc device (rtc0) [ 1.821548] vmmcwl_fixed: disabling [ 1.825208] ALSA device list: [ 1.828256] No soundcards found. [ 1.835577] Waiting for root device PARTUUID=f9fdd9ec-02... [ 1.881522] mmc1: host does not support reading read-only switch, assuming write-enable [ 1.891469] mmc1: new high speed SDXC card at address 1234 [ 1.897524] mmcblk1: mmc1:1234 SA64G 58.0 GiB [ 1.903453] mmcblk1: p1 p2 [ 1.958622] EXT4-fs (mmcblk1p2): recovery complete [ 3.055697] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [ 3.063914] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 3.073220] devtmpfs: mounted [ 3.078046] Freeing unused kernel memory: 1024K [ 3.084482] random: fast init done [ 3.427960] systemd[1]: System time before build time, advancing clock. [ 3.487736] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN default-hierarchy=hybrid) [ 3.509354] systemd[1]: Detected architecture arm. Welcome to Arago 2018.10! [ 3.562621] systemd[1]: Set hostname to . [ 4.175576] random: systemd: uninitialized urandom read (16 bytes read) [ 4.182719] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 4.214875] random: systemd: uninitialized urandom read (16 bytes read) [ 4.221932] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ 4.264723] random: systemd: uninitialized urandom read (16 bytes read) [ 4.271695] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe. [ OK ] Listening on /dev/initctl Compatibility Named Pipe. [ 4.316938] systemd[1]: Created slice System Slice. [ OK ] Created slice System Slice. [ 4.345275] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 4.375180] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 4.423002] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ OK ] Created slice system-getty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. Starting Create list of required st…ce nodes for the current kernel... [ OK ] Listening on Journal Socket (/dev/log). Starting Remount Root and Kernel File Systems... [ OK ] Reached target Remote File Systems. [ 4.631424] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null) [ OK ] Reached target Swap. Mounting Temporary Directory (/tmp)... [ OK ] Listening on udev Kernel Socket. [ OK ] Started Forward Password Requests to Wall Directory Watch. [ OK ] Reached target Paths. Mounting POSIX Message Queue File System... [ OK ] Created slice User and Session Slice. [ OK ] Reached target Slices. Starting Load Kernel Modules... [ OK ] Listening on Syslog Socket. [ 4.938344] cmemk: loading out-of-tree module taints kernel. [ 4.947193] CMEMK module: reference Linux version 4.14.79 [ 4.953474] no physical memory specified [ 4.957629] cmemk initialized [ 4.976074] cryptodev: driver 1.9 loaded. Starting Journal Service... Mounting Kernel Debug File System... [ 5.019937] usbcore: registered new interface driver usbfs [ 5.056674] usbcore: registered new interface driver hub [ 5.056819] usbcore: registered new device driver usb [ 5.080316] usbcore: registered new interface driver usbserial [ OK ] Mounted POSIX Message Queue File System. [ 5.107914] usbcore: registered new interface driver ftdi_sio [ 5.113761] usbserial: USB Serial support registered for FTDI USB Serial Device [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Mounted Kernel Debug File System. [ OK ] Started Create list of required sta…vice nodes for the current kernel. [ OK ] Started Remount Root and Kernel File Systems. [ OK ] Started Load Kernel Modules. [ OK ] Started Journal Service. Mounting Kernel Configuration File System... Starting Apply Kernel Variables... Starting Rebuild Hardware Database... Starting Flush Journal to Persistent Storage... Starting Create System Users... [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Apply Kernel Variables. [ OK ] Started Create System Users. [ 5.639497] systemd-journald[69]: Received request to flush runtime journal from PID 1 Starting Create Static Device Nodes in /dev... [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /var/volatile... Mounting /media/ram... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. [ OK ] Mounted /media/ram. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Rebuild Dynamic Linker Cache... Starting Create Volatile Files and Directories... Starting Rebuild Journal Catalog... [ OK ] Started udev Kernel Device Manager. [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Rebuild Journal Catalog. [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Synchronized. [ OK ] Started Rebuild Dynamic Linker Cache. [ OK ] Started Rebuild Hardware Database. Starting Update is Completed... Starting udev Coldplug all Devices... [ OK ] Started Update is Completed. [ 12.360730] Unable to handle kernel paging request at virtual address 0000decc [ 12.398565] pgd = dba40000 [ 12.401302] [0000decc] *pgd=00000000 [ 12.416731] Internal error: Oops: 5 [#1] PREEMPT ARM [ 12.421731] Modules linked in: sch_fq_codel uio_module_drv(O) uio ftdi_sio usbserial usbcore usb_common cryptodev(O) cmemk(O) [ 12.433116] CPU: 0 PID: 110 Comm: systemd-udevd Tainted: G O 4.14.79-gbde58ab01e #1 [ 12.441938] Hardware name: Generic AM43 (Flattened Device Tree) [ 12.447881] task: dba49200 task.stack: db9bc000 [ 12.452448] PC is at link_path_walk+0x38/0x4ec [ 12.456911] LR is at path_openat+0x88/0x1124 [ 12.461197] pc : [] lr : [] psr: 20070013 [ 12.467487] sp : db9bddb8 ip : db9bde18 fp : db9bde14 [ 12.472729] r10: 00000005 r9 : dbfdea80 r8 : c0107ea4 [ 12.477973] r7 : 00000001 r6 : 0000dea8 r5 : dbf1e011 r4 : 0000dea8 [ 12.484524] r3 : 00000073 r2 : c0ab13e8 r1 : 0000dea8 r0 : dbf1e010 [ 12.491079] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none [ 12.498242] Control: 10c53c7d Table: 9ba40059 DAC: 00000051 [ 12.504009] Process systemd-udevd (pid: 110, stack limit = 0xdb9bc208) [ 12.510562] Stack: (0xdb9bddb8 to 0xdb9be000) [ 12.514935] dda0: c0213978 c02139e4 [ 12.523148] ddc0: c0d1c2b4 dbf77e80 c0d7f680 00000001 c0107ea4 db9bc000 db9bdea8 dbf1e010 [ 12.531361] dde0: db9bde14 db9bddf0 c022f3fc 0000dea8 dbf1e010 db9bdf5c 00000001 c0107ea4 [ 12.539572] de00: dbfdea80 00000005 db9bdea4 db9bde18 c0233488 c02319f0 dbf1e015 c0248ad8 [ 12.547785] de20: 00000000 dc0e6110 dc102bd0 00000000 dbf1e010 c0ab13e8 00000000 ffffe000 [ 12.555996] de40: 00000000 db9bde48 00000041 dbfdea80 dbf1e000 dbf1e010 db9bde94 00000000 [ 12.564208] de60: c0292948 c02425d0 00000000 00000000 dc100440 db9bc000 db9bdeb4 00000007 [ 12.572420] de80: db9bdea8 db9bdf5c 00000001 c0107ea4 db9bc000 00000005 db9bdf4c db9bdea8 [ 12.580631] dea0: c02353f8 c023340c db8db910 dc0e6110 000041ed 00000055 00000000 00000000 [ 12.588842] dec0: db8db910 dc0e6110 dc0fa2e8 00001051 00000002 00000250 00000001 00000000 [ 12.597055] dee0: 00000000 db9bdee8 c0d032ec 00000007 dc439180 dc439194 00000000 00000400 [ 12.605267] df00: db9bdf3c db9bdf10 c0245e84 c02454b0 000a0000 000a0000 dbf1e000 00000000 [ 12.613480] df20: fffff000 00000002 ffffff9c 00000005 00000007 ffffff9c dbf1e000 fffff000 [ 12.621692] df40: db9bdf94 db9bdf50 c02228e8 c0235398 0000000f 00000000 00000000 00020000 [ 12.629903] df60: 00000000 00000004 00000100 00000001 004c3a20 00000000 00000008 00000005 [ 12.638116] df80: c0107ea4 db9bc000 db9bdfa4 db9bdf98 c0222988 c022278c 00000000 db9bdfa8 [ 12.646328] dfa0: c0107ca0 c0222974 004c3a20 00000000 be8aaaa8 000a0000 000001b6 000001b6 [ 12.654540] dfc0: 004c3a20 00000000 00000008 00000005 00000000 00000000 be8aaae8 be8aaaf0 [ 12.662753] dfe0: 00000000 be8aa96c b6d59281 b6d94188 40070030 be8aaaa8 00000000 00000000 [ 12.670959] Backtrace: [ 12.673422] [] (link_path_walk) from [] (path_openat+0x88/0x1124) [ 12.681288] r10:00000005 r9:dbfdea80 r8:c0107ea4 r7:00000001 r6:db9bdf5c r5:dbf1e010 [ 12.689146] r4:0000dea8 [ 12.691692] [] (path_openat) from [] (do_filp_open+0x6c/0xd0) [ 12.699207] r10:00000005 r9:db9bc000 r8:c0107ea4 r7:00000001 r6:db9bdf5c r5:db9bdea8 [ 12.707065] r4:00000007 [ 12.709620] [] (do_filp_open) from [] (do_sys_open+0x168/0x1e8) [ 12.717307] r7:fffff000 r6:dbf1e000 r5:ffffff9c r4:00000007 [ 12.722992] [] (do_sys_open) from [] (SyS_open+0x20/0x24) [ 12.730157] r9:db9bc000 r8:c0107ea4 r7:00000005 r6:00000008 r5:00000000 r4:004c3a20 [ 12.737946] [] (SyS_open) from [] (ret_fast_syscall+0x0/0x54) [ 12.745462] Code: e353002f 0afffffc e3530000 0a0000da (e5963024) [ OK ] Created slice system-systemd\x2dcoredump.slice. [ OK ] Started Process Core Dump (PID 111/UID 0). [ 13.261549] remoteproc remoteproc0: wkup_m3 is available [ 13.390365] remoteproc remoteproc0: powering up wkup_m3 [ OK ] Found device /dev/ttyS0. [ 13.456329] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 13.491119] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224628 [ 13.539958] omap_rtc 44e3e000.rtc: char device (253:0) [ 13.540097] omap_rtc 44e3e000.rtc: registered as rtc0 [ 13.577761] ov2659 0-0030: GPIO lookup for consumer pwrdn [ 13.577767] ov2659 0-0030: using device tree for GPIO lookup [ 13.577785] of_get_named_gpiod_flags: can't parse 'pwrdn-gpios' property of node '/ocp@44000000/i2c@44e0b000/ov2659@30[0]' [ 13.577792] of_get_named_gpiod_flags: can't parse 'pwrdn-gpio' property of node '/ocp@44000000/i2c@44e0b000/ov2659@30[0]' [ 13.577796] ov2659 0-0030: using lookup tables for GPIO lookup [ 13.577802] ov2659 0-0030: lookup for GPIO pwrdn failed [ 13.608141] ov2659 0-0030: Sensor detection failed (3030, 0) [ 13.608583] ov2659 1-0030: GPIO lookup for consumer pwrdn [ 13.608589] ov2659 1-0030: using device tree for GPIO lookup [ 13.608607] of_get_named_gpiod_flags: can't parse 'pwrdn-gpios' property of node '/ocp@44000000/i2c@4802a000/ov2659@30[0]' [ 13.608614] of_get_named_gpiod_flags: can't parse 'pwrdn-gpio' property of node '/ocp@44000000/i2c@4802a000/ov2659@30[0]' [ 13.608618] ov2659 1-0030: using lookup tables for GPIO lookup [ 13.608624] ov2659 1-0030: lookup for GPIO pwrdn failed [ 13.637544] ov2659 1-0030: Sensor detection failed (3030, 0) [ 13.641114] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 13.641315] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 13.654641] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 13.706382] pixcir_ts 1-005c: GPIO lookup for consumer attb [ 13.706388] pixcir_ts 1-005c: using device tree for GPIO lookup [ 13.706409] of_get_named_gpiod_flags: can't parse 'attb-gpios' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' [ 13.706498] of_get_named_gpiod_flags: parsed 'attb-gpio' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' - status (0) [ 13.706567] pixcir_ts 1-005c: GPIO lookup for consumer reset [ 13.706571] pixcir_ts 1-005c: using device tree for GPIO lookup [ 13.706581] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' [ 13.706588] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' [ 13.706592] pixcir_ts 1-005c: using lookup tables for GPIO lookup [ 13.706597] pixcir_ts 1-005c: lookup for GPIO reset failed [ 13.706603] pixcir_ts 1-005c: GPIO lookup for consumer wake [ 13.706606] pixcir_ts 1-005c: using device tree for GPIO lookup [ 13.706612] of_get_named_gpiod_flags: can't parse 'wake-gpios' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' [ 13.706618] of_get_named_gpiod_flags: can't parse 'wake-gpio' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' [ 13.706621] pixcir_ts 1-005c: using lookup tables for GPIO lookup [ 13.706625] pixcir_ts 1-005c: lookup for GPIO wake failed [ 13.706630] pixcir_ts 1-005c: GPIO lookup for consumer enable [ 13.706634] pixcir_ts 1-005c: using device tree for GPIO lookup [ 13.706640] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' [ 13.706645] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/ocp@44000000/i2c@4802a000/pixcir_ts@5c[0]' [ 13.706649] pixcir_ts 1-005c: using lookup tables for GPIO lookup [ 13.706653] pixcir_ts 1-005c: lookup for GPIO enable failed [ 13.709615] pixcir_ts 1-005c: pixcir_set_power_mode: can't read reg 0x33 : -121 [ 13.709621] pixcir_ts 1-005c: Failed to set IDLE mode [ 13.710022] pixcir_ts: probe of 1-005c failed with error -121 [ 13.786044] CAN device driver interface [ 13.809844] c_can_platform 481cc000.can: c_can_platform device registered (regs=fa1cc000, irq=60) [ 13.810741] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 13.810903] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 13.811051] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 13.815848] c_can_platform 481d0000.can: c_can_platform device registered (regs=fa1d0000, irq=61) [ 13.816761] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 13.816934] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 13.817086] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 13.921977] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 13.922143] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 13.922290] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 13.940637] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 13.940806] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 13.940953] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.058207] ---[ end trace dec43064f7bc4877 ]--- [ 14.065585] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.065750] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.066219] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.086073] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.086239] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.086388] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.396378] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.396530] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.396675] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.453000] omap-sham 53100000.sham: hw accel on OMAP rev 0.0 [ 14.545081] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.545252] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.547795] omap-aes 53501000.aes: OMAP AES hw accel rev: 0.1 [ 14.549523] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.550599] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.550759] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.550894] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.578001] omap-aes 53501000.aes: will run requests pump with realtime priority [ 14.605491] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.605671] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.605978] omap-des 53701000.des: OMAP DES hw accel rev: 0.33 [ 14.606256] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.616658] omap-des 53701000.des: will run requests pump with realtime priority [ 14.630619] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.630790] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.631801] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 14.632464] [drm] Initialized pvr 1.14.3699939 20110701 for 56000000.sgx on minor 1 [ 14.634971] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 14.635171] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 14.635310] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 16.216508] PM: Cannot get wkup_m3_ipc handle [ 16.234997] of_get_named_gpiod_flags: parsed 'row-gpios' property of node '/matrix_keypad0[0]' - status (0) [ 16.235022] of_get_named_gpiod_flags: parsed 'row-gpios' property of node '/matrix_keypad0[1]' - status (0) [ 16.235045] of_get_named_gpiod_flags: parsed 'row-gpios' property of node '/matrix_keypad0[2]' - status (0) [ 16.235058] of_get_named_gpiod_flags: parsed 'col-gpios' property of node '/matrix_keypad0[0]' - status (0) [ 16.235074] of_get_named_gpiod_flags: parsed 'col-gpios' property of node '/matrix_keypad0[1]' - status (0) [ 16.235614] input: matrix_keypad0 as /devices/platform/matrix_keypad0/input/input1 [ 16.248741] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 16.248914] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 16.265228] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 16.265740] PM: Cannot get wkup_m3_ipc handle [ 16.373632] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck. [ 18.856445] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 18.856659] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 18.856809] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 18.857154] PM: Cannot get wkup_m3_ipc handle [ 20.091006] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.091169] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.091318] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.091663] PM: Cannot get wkup_m3_ipc handle [ 20.101077] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.101236] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.103931] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.104710] PM: Cannot get wkup_m3_ipc handle [ 20.181129] pruss 54400000.pruss: creating PRU cores and other child platform devices [ 20.184654] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.184840] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.184989] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.185330] PM: Cannot get wkup_m3_ipc handle [ 20.225031] pruss 54440000.pruss: creating PRU cores and other child platform devices [ 20.228492] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.228652] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.228796] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.229132] PM: Cannot get wkup_m3_ipc handle [ 20.354060] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 20.354100] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 20.369103] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f06d hci version 0x100 quirks 0x02010010 [ 20.369158] xhci-hcd xhci-hcd.0.auto: irq 104, io mem 0x48390000 [ 20.374255] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 20.374263] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 20.374269] usb usb1: Product: xHCI Host Controller [ 20.374273] usb usb1: Manufacturer: Linux 4.14.79-gbde58ab01e xhci-hcd [ 20.374277] usb usb1: SerialNumber: xhci-hcd.0.auto [ 20.375173] hub 1-0:1.0: USB hub found [ 20.375222] hub 1-0:1.0: 1 port detected [ 20.376279] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.376467] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.376617] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.376962] PM: Cannot get wkup_m3_ipc handle [ 20.378529] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.378690] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.379005] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 20.379024] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 20.379043] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed [ 20.380940] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.392522] PM: Cannot get wkup_m3_ipc handle [ 20.410865] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 20.410983] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003 [ 20.410990] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 20.410995] usb usb2: Product: xHCI Host Controller [ 20.410999] usb usb2: Manufacturer: Linux 4.14.79-gbde58ab01e xhci-hcd [ 20.411004] usb usb2: SerialNumber: xhci-hcd.0.auto [ 20.411755] hub 2-0:1.0: USB hub found [ 20.411808] hub 2-0:1.0: 1 port detected [ 20.412393] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 20.412420] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3 [ 20.415612] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.415791] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.433005] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.438893] PM: Cannot get wkup_m3_ipc handle [ 20.448272] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.457059] remoteproc remoteproc1: 54434000.pru is available [ 20.457123] pru-rproc 54434000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@0/pru@34000 probed successfully [ 20.457583] remoteproc remoteproc2: 54438000.pru is available [ 20.457644] pru-rproc 54438000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@0/pru@38000 probed successfully [ 20.458057] remoteproc remoteproc3: 54474000.pru is available [ 20.458115] pru-rproc 54474000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@40000/pru@74000 probed successfully [ 20.458463] remoteproc remoteproc4: 54478000.pru is available [ 20.458497] pru-rproc 54478000.pru: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@40000/pru@78000 probed successfully [ 20.464922] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.469155] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.469743] PM: Cannot get wkup_m3_ipc handle [ 20.471201] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.471354] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.477891] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ 20.481134] xhci-hcd xhci-hcd.1.auto: hcc params 0x0238f06d hci version 0x100 quirks 0x02010010 [ 20.481194] xhci-hcd xhci-hcd.1.auto: irq 105, io mem 0x483d0000 [ 20.481392] usb usb3: New USB device found, idVendor=1d6b, idProduct=0002 [ 20.481398] usb usb3: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 20.481403] usb usb3: Product: xHCI Host Controller [ 20.481408] usb usb3: Manufacturer: Linux 4.14.79-gbde58ab01e xhci-hcd [ 20.481412] usb usb3: SerialNumber: xhci-hcd.1.auto [ 20.482174] hub 3-0:1.0: USB hub found [ 20.482223] hub 3-0:1.0: 1 port detected [ 20.482604] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller [ 20.482624] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4 [ 20.482640] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed [ 20.482715] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM. [ 20.482814] usb usb4: New USB device found, idVendor=1d6b, idProduct=0003 [ 20.482821] usb usb4: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 20.482826] usb usb4: Product: xHCI Host Controller [ 20.482830] usb usb4: Manufacturer: Linux 4.14.79-gbde58ab01e xhci-hcd [ 20.482834] usb usb4: SerialNumber: xhci-hcd.1.auto [ 20.483409] hub 4-0:1.0: USB hub found [ 20.483447] hub 4-0:1.0: 1 port detected [ 20.489714] PM: Cannot get wkup_m3_ipc handle [ 20.491216] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp@44000000/i2c@4802a000/tlv320aic3106@1b[0]' [ 20.491374] tlv320aic3x-codec 1-001b: Failed to get supply 'DVDD': -517 [ 20.534176] tlv320aic3x-codec 1-001b: Failed to request supplies: -517 [ OK ] Started udev Coldplug all Devices. [ 21.574105] remoteproc remoteproc0: remote processor wkup_m3 is now up [ 21.580757] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192 [ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. [ OK ] Created slice system-systemd\x2dbacklight.slice. Starting Load/Save Screen Backlight…ightness of backlight:backlight... [ OK ] Started Load/Save Screen Backlight Brightness of backlight:backlight. [ OK ] Reached target System Initialization. [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Started Daily rotation of log files. Starting Network Service... [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on dropbear.socket. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Reached target Containers. Starting Print notice about GPLv3 packages... [ OK ] Started System Logging Service. [ OK ] Started Kernel Logging Service. Starting RPC Bind Service... [ OK ] Started D-Bus System Message Bus. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Started Job spooling tools. Starting uim-sysfs.service... [ 24.015531] random: crng init done [ 24.035402] random: 7 urandom warning(s) missed due to ratelimiting Starting Login Service... [ OK ] Started Periodic Command Scheduler. [ 24.153999] net eth0: initializing cpsw version 1.15 (0) Starting Avahi mDNS/DNS-SD Stack... [ OK ] Started Network Service. [ OK ] Started RPC Bind Service. [ OK ] Reached target Network. Starting Simple Network Management Protocol (SNMP) Daemon.... [ 24.339711] Micrel KSZ9031 Gigabit PHY 4a101000.mdio:00: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL) [ OK ] Started Redis In-Memory Data Store. Starting Enable and configure wl18xx bluetooth stack... [ 24.501684] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready Starting Lightning Fast Webserver With Light System Requirements... Starting Permit User Sessions... Starting Network Name Resolution... Starting Wait for Network to be Configured... [ OK ] Started Lightning Fast Webserver With Light System Requirements. [ OK ] Started Permit User Sessions. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Started Login Service. [ OK ] Started Serial Getty on ttyS0. [ OK ] Started Getty on tty1. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... [ OK ] Started Synchronize System and HW clocks. [ OK ] Started Network Name Resolution. [ OK ] Reached target Host and Network Name Lookups. [ OK ] Started NFS status monitor for NFSv2/3 locking.. [ OK ] Started Simple Network Management Protocol (SNMP) Daemon.. [ OK ] Started Enable and configure wl18xx bluetooth stack. [ OK ] Started uim-sysfs.service. Starting rc.pvr.service... [ 27.350956] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ] [ OK ] Started rc.pvr.service. Starting weston.service... [ OK ] Started weston.service. Starting Matrix GUI... Starting telnetd.service... [ OK ] Started Matrix GUI. [ OK ] Started telnetd.service. Starting thttpd.service... [ OK ] Started thttpd.service. Starting rng-tools.service... [ OK ] Started rng-tools.service. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash-dev bash binutils cifs-utils cpio cpp-symlinks cpp dosfstools elfutils findutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext glmark2 gstreamer1.0-libav gzip hidapi libdw1 libelf1 libgdbm-compat4 libgdbm-dev libgdbm4 libgettextlib libgettextsrc libgmp10 libidn11 libmavconn libmpc3 libmpfr4 libreadline-dev libreadline7 libunistring2 m4-dev m4 make mavlink mavros-extras mavros-msgs mavros nettle python3-pycairo socketcan-interface which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am437x-evm ttyS0 Arago 2018.10 am437x-evm ttyS0 am437x-evm login: [ 34.248139] alloc_contig_range: [9d051, 9d052) PFNs busy [ 34.257487] alloc_contig_range: [9d051, 9d052) PFNs busy