U-Boot SPL 2021.01-g15769936a5 (Dec 21 2021 - 03:26:17 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla') SPL initial stack usage: 1416 bytes Trying to boot from MMC2 Starting ATF on ARM64 core... NOTICE: BL31: v2.5(release):08.01.00.006-dirty NOTICE: BL31: Built : 02:55:10, Dec 21 2021 U-Boot SPL 2021.01-g15769936a5 (Dec 21 2021 - 02:56:45 +0000) SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla') Detected: Silicon SR2.0 i2c_omap i2c@42120000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19 Detected: AM6-IDKAPPEVM rev A Detected: SER-PCIE2LEVM rev A Trying to boot from MMC2 U-Boot 2021.01-g15769936a5 (Dec 21 2021 - 02:56:45 +0000) SoC: AM65X SR2.0 Model: Texas Instruments AM654 Base Board Board: AM6-COMPROCEVM rev A DRAM: 4 GiB MMC: sdhci@4f80000: 0, sdhci@4fa0000: 1 Loading Environment from MMC... OK In: serial Out: serial Err: serial Detected: Silicon SR2.0 Detected: AM6-IDKAPPEVM rev A Detected: SER-PCIE2LEVM rev A Net: am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00102 cpsw_ver: 0x6BA80102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000 eth0: ethernet@46000000, eth1: icssg2-eth Hit any key to stop autoboot: 2  1  0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 Failed to load 'boot.scr' 1011 bytes read in 4 ms (246.1 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... Using board_name = am65x 18158080 bytes read in 755 ms (22.9 MiB/s) 64207 bytes read in 7 ms (8.7 MiB/s) 11268 bytes read in 5 ms (2.1 MiB/s) 2333 bytes read in 5 ms (455.1 KiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 000000008feed000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.10.65-rt53-g541ec9a699 (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT_RT Tue Dec 21 02:58:35 UTC 2021 [ 0.000000] Machine model: Texas Instruments AM654 Base Board [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff] [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a20fffff] [ 0.000000] node 0: [mem 0x00000000a2100000-0x00000000ffffffff] [ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff] [ 0.000000] On node 0 totalpages: 1048576 [ 0.000000] DMA zone: 8192 pages used for memmap [ 0.000000] DMA zone: 0 pages reserved [ 0.000000] DMA zone: 524288 pages, LIFO batch:63 [ 0.000000] Normal zone: 8192 pages used for memmap [ 0.000000] Normal zone: 524288 pages, LIFO batch:63 [ 0.000000] cma: Reserved 24 MiB at 0x00000000fe800000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 18 pages/cpu s34752 r8192 d30784 u73728 [ 0.000000] pcpu-alloc: s34752 r8192 d30784 u73728 alloc=18*4096 [ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),57216k@8m(ospi.rootfs),128k(ospi.phypattern) root=PARTUUID=9b678ee1-02 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] software IO TLB: mapped [mem 0x00000000fa800000-0x00000000fe800000] (64MB) [ 0.000000] Memory: 3946780K/4194304K available (10624K kernel code, 1156K rwdata, 4108K rodata, 1728K init, 438K bss, 222948K reserved, 24576K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4. [ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms. [ 0.000000] rcu: RCU_SOFTIRQ processing moved to rcuc kthreads. [ 0.000000] No expedited grace period (rcu_normal_after_boot). [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 960 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000880040000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000 [ 0.000000] random: get_random_bytes called from start_kernel+0x320/0x4c8 with crng_init=0 [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000001] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008694] Console: colour dummy device 80x25 [ 0.013316] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.024037] pid_max: default: 32768 minimum: 301 [ 0.028901] LSM: Security Framework initializing [ 0.033720] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.041336] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear) [ 0.051556] rcu: Hierarchical SRCU implementation. [ 0.057083] Platform MSI: msi-controller@1820000 domain created [ 0.063486] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.072932] EFI services will not be available. [ 0.077943] smp: Bringing up secondary CPUs ... [ 0.083802] Detected VIPT I-cache on CPU1 [ 0.087947] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 0.095011] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000 [ 0.102475] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.110632] Detected VIPT I-cache on CPU2 [ 0.114800] GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000 [ 0.122046] GICv3: CPU2: using allocated LPI pending table @0x0000000880070000 [ 0.129518] CPU2: Booted secondary processor 0x0000000100 [0x410fd034] [ 0.137605] Detected VIPT I-cache on CPU3 [ 0.141746] GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000 [ 0.148986] GICv3: CPU3: using allocated LPI pending table @0x0000000880080000 [ 0.156429] CPU3: Booted secondary processor 0x0000000101 [0x410fd034] [ 0.163304] smp: Brought up 1 node, 4 CPUs [ 0.167549] SMP: Total of 4 processors activated. [ 0.172397] CPU features: detected: 32-bit EL0 Support [ 0.177690] CPU features: detected: CRC32 instructions [ 0.197997] CPU: All CPU(s) started at EL2 [ 0.202244] alternatives: patching kernel code [ 0.208349] devtmpfs: initialized [ 0.226494] KASLR disabled due to lack of seed [ 0.231335] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.241358] futex hash table entries: 1024 (order: 5, 131072 bytes, linear) [ 0.249874] pinctrl core: initialized pinctrl subsystem [ 0.255921] DMI not present or invalid. [ 0.260503] NET: Registered protocol family 16 [ 0.267436] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations [ 0.274915] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.283276] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.292185] thermal_sys: Registered thermal governor 'step_wise' [ 0.292997] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.306274] ASID allocator initialised with 65536 entries [ 0.363648] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.370595] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.377515] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.384413] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 0.393066] cryptd: max_cpu_qlen set to 1000 [ 0.402486] k3-chipinfo 43000014.chipid: Family:AM65X rev:SR2.0 JTAGID[0x1bb5a02f] Detected [ 0.411932] vcc3v3_io: supplied by evm_12v0 [ 0.417814] iommu: Default domain type: Translated [ 0.423373] SCSI subsystem initialized [ 0.428059] mc: Linux media interface: v0.10 [ 0.432517] videodev: Linux video capture interface: v2.00 [ 0.438258] pps_core: LinuxPPS API ver. 1 registered [ 0.443374] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.452767] PTP clock support registered [ 0.456832] EDAC MC: Ver: 3.0.0 [ 0.461605] FPGA manager framework [ 0.465242] Advanced Linux Sound Architecture Driver Initialized. [ 0.472793] clocksource: Switched to clocksource arch_sys_counter [ 0.479320] VFS: Disk quotas dquot_6.6.0 [ 0.483454] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.499482] NET: Registered protocol family 2 [ 0.504361] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear) [ 0.514640] tcp_listen_portaddr_hash hash table entries: 2048 (order: 5, 131072 bytes, linear) [ 0.523751] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.532318] TCP bind hash table entries: 32768 (order: 8, 1835008 bytes, linear) [ 0.542353] TCP: Hash tables configured (established 32768 bind 32768) [ 0.549388] UDP hash table entries: 2048 (order: 6, 262144 bytes, linear) [ 0.556772] UDP-Lite hash table entries: 2048 (order: 6, 262144 bytes, linear) [ 0.564913] NET: Registered protocol family 1 [ 0.570398] RPC: Registered named UNIX socket transport module. [ 0.576601] RPC: Registered udp transport module. [ 0.581437] RPC: Registered tcp transport module. [ 0.586267] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.592888] PCI: CLS 0 bytes, default 64 [ 0.598191] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.613063] Initialise system trusted keyrings [ 0.617920] workingset: timestamp_bits=46 max_order=20 bucket_order=0 [ 0.631938] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.638759] NFS: Registering the id_resolver key type [ 0.644030] Key type id_resolver registered [ 0.648344] Key type id_legacy registered [ 0.652587] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.659490] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.667370] 9p: Installing v9fs 9p2000 file system support [ 0.727092] Key type asymmetric registered [ 0.731354] Asymmetric key parser 'x509' registered [ 0.736432] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243) [ 0.744065] io scheduler mq-deadline registered [ 0.748738] io scheduler kyber registered [ 0.756269] pinctrl-single 4301c000.pinctrl: 70 pins, size 280 [ 0.763093] pinctrl-single 11c000.pinctrl: 185 pins, size 740 [ 0.769215] pinctrl-single 11c2e8.pinctrl: 9 pins, size 36 [ 0.783032] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.789440] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.801261] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.830808] brd: module loaded [ 0.845756] loop: module loaded [ 0.850142] megasas: 07.714.04.00-rc1 [ 0.858494] libphy: Fixed MDIO Bus: probed [ 0.864605] tun: Universal TUN/TAP device driver, 1.6 [ 0.870775] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 0.877251] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.883425] sky2: driver version 1.30 [ 0.888849] VFIO - User Level meta-driver version: 0.3 [ 0.895398] i2c /dev entries driver [ 0.900897] sdhci: Secure Digital Host Controller Interface driver [ 0.907268] sdhci: Copyright(c) Pierre Ossman [ 0.912537] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.920224] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource [ 0.927932] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.936328] optee: probing for conduit method. [ 0.940937] optee: revision 3.12 (3d47a131) [ 0.941546] optee: initialized driver [ 0.952633] NET: Registered protocol family 17 [ 0.957469] 9pnet: Installing 9P2000 support [ 0.961967] Key type dns_resolver registered [ 0.966825] printk: bootconsole [ns16550a0]: printing thread started [ 0.966908] Loading compiled-in X.509 certificates [ 0.980244] k3-ringacc 2b800000.ringacc: Failed to get MSI domain [ 0.980585] k3-ringacc 3c000000.ringacc: Failed to get MSI domain [ 0.988192] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource [ 0.988711] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla') [ 1.062262] random: fast init done [ 1.083809] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz [ 1.085304] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz [ 1.087663] pca953x 2-0021: supply vcc not found, using dummy regulator [ 1.087853] pca953x 2-0021: using no AI [ 1.109630] omap_i2c 2000000.i2c: bus 2 rev0.12 at 400 kHz [ 1.110868] omap_i2c 2010000.i2c: bus 3 rev0.12 at 400 kHz [ 1.112049] omap_i2c 2020000.i2c: bus 4 rev0.12 at 400 kHz [ 1.113163] omap_i2c 2030000.i2c: bus 5 rev0.12 at 100 kHz [ 1.114586] ti-sci-intr bus@100000:bus@28380000:bus@42040000:interrupt-controller2: Interrupt Router 156 domain created [ 1.114860] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 100 domain created [ 1.115113] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 182 domain created [ 1.115555] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 179 created [ 1.130724] keystone-pcie 5500000.pcie: host bridge /bus@100000/pcie@5500000 ranges: [ 1.130766] OF: /bus@100000/pcie@5500000: Missing device_type [ 1.130802] keystone-pcie 5500000.pcie: IO 0x0010020000..0x001002ffff -> 0x0000000000 [ 1.130834] keystone-pcie 5500000.pcie: MEM 0x0010030000..0x0017ffffff -> 0x0010030000 [ 2.131569] keystone-pcie 5500000.pcie: Phy link never came up [ 2.131775] keystone-pcie 5500000.pcie: PCI host bridge to bus 0000:00 [ 2.131787] pci_bus 0000:00: root bus resource [bus 00-ff] [ 2.131799] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] [ 2.131808] pci_bus 0000:00: root bus resource [mem 0x10030000-0x17ffffff] [ 2.157855] printk: console [ttyS2]: printing thread started [ 2.131889] pci 0000:00:00.0: [104c:b00c] type 01 class 0x060400 [ 2.157885] printk: console [ttyS2] enabled [ 2.157891] printk: bootconsole [ns16550a0] disabled [ 2.176816] printk: bootconsole [ns16550a0]: printing thread stopped [ 2.178154] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 30, base_baud = 3000000) is a 8250 [ 2.179215] 2820000.serial: ttyS4 at MMIO 0x2820000 (irq = 31, base_baud = 3000000) is a 8250 [ 2.236836] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 2.236866] libphy: 46000f00.mdio: probed [ 2.239410] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 2.239542] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000 [ 2.242733] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 2.246860] mmc0: CQHCI version 5.10 [ 2.261833] pca953x 0-0039: supply vcc not found, using dummy regulator [ 2.262043] pca953x 0-0039: using no AI [ 2.286753] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100 [ 2.287350] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100 [ 2.289543] ti-udma 285c0000.dma-controller: Channels: 28 (tchan: 14, rchan: 14, gp-rflow: 16) [ 2.291570] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit [ 2.297828] ti-udma 31150000.dma-controller: Channels: 119 (tchan: 53, rchan: 66, gp-rflow: 64) [ 2.312490] spi-nor spi7.0: mt35xu512aba (65536 Kbytes) [ 2.312545] 8 cmdlinepart partitions found on MTD device 47040000.spi.0 [ 2.312552] Creating 8 MTD partitions on "47040000.spi.0": [ 2.312561] 0x000000000000-0x000000080000 : "ospi.tiboot3" [ 2.314482] 0x000000080000-0x000000280000 : "ospi.tispl" [ 2.316055] 0x000000280000-0x000000680000 : "ospi.u-boot" [ 2.317640] 0x000000680000-0x0000006a0000 : "ospi.env" [ 2.319247] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup" [ 2.320873] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw" [ 2.322442] 0x000000800000-0x000003fe0000 : "ospi.rootfs" [ 2.323977] 0x000003fe0000-0x000004000000 : "ospi.phypattern" [ 2.337217] spi-nor spi9.0: n25q128a13 (16384 Kbytes) [ 2.378140] mmc0: Command Queue Engine enabled [ 2.378167] mmc0: new HS200 MMC card at address 0001 [ 2.379036] mmcblk0: mmc0:0001 S0J56X 14.8 GiB [ 2.379283] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB [ 2.379559] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB [ 2.379884] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (237:0) [ 2.380866] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 2.380904] libphy: 46000f00.mdio: probed [ 2.383748] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867 [ 2.383918] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000 [ 2.385856] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48 [ 2.386859] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4 [ 2.386872] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64 [ 2.388038] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0 [ 2.391776] vdd_mmc1_sd: supplied by vcc3v3_io [ 2.393820] debugfs: Directory 'pd:121' with parent 'pm_genpd' already present! [ 2.393891] debugfs: Directory 'pd:120' with parent 'pm_genpd' already present! [ 2.397470] mmc1: CQHCI version 5.10 [ 2.398136] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 2.421142] ALSA device list: [ 2.421154] No soundcards found. [ 3.311628] mmc1: SDHCI controller on 4fa0000.mmc [4fa0000.mmc] using ADMA 64-bit [ 3.312233] Waiting for root device PARTUUID=9b678ee1-02... [ 3.370417] mmc1: new ultra high speed SDR104 SDHC card at address aaaa [ 3.371253] mmcblk1: mmc1:aaaa SA08G 7.40 GiB [ 3.373221] mmcblk1: p1 p2 [ 3.663141] EXT4-fs (mmcblk1p2): recovery complete [ 3.664004] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null) [ 3.664108] VFS: Mounted root (ext4 filesystem) on device 179:98. [ 3.664946] devtmpfs: mounted [ 3.666343] Freeing unused kernel memory: 1728K [ 3.666514] Run /sbin/init as init process [ 3.793430] systemd[1]: System time before build time, advancing clock. [ 3.855934] NET: Registered protocol family 10 [ 3.861374] Segment Routing with IPv6 Welcome to Arago 2021.09! [ 3.881416] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 3.882077] systemd[1]: Detected architecture arm64. [ 3.922496] systemd[1]: Set hostname to . [ OK ] Created slice system-getty.slice. [ 4.330224] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly. [ 4.457197] random: systemd: uninitialized urandom read (16 bytes read) [ 4.457612] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling. [ 4.457669] systemd[1]: (This warning is only shown for the first unit using IP firewalling.) [ 4.462810] systemd[1]: Created slice system-getty.slice. [ 4.496587] random: systemd: uninitialized urandom read (16 bytes read) [ 4.498990] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ OK ] Created slice User and Session Slice. [ 4.556987] random: systemd: uninitialized urandom read (16 bytes read) [ 4.559026] systemd[1]: Created slice User and Session Slice. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 4.589708] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 4.613169] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Reached target Paths. [ 4.636740] systemd[1]: Reached target Paths. [ OK ] Reached target Remote File Systems. [ 4.653375] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Slices. [ 4.674540] systemd[1]: Reached target Slices. [ OK ] Reached target Swap. [ 4.689428] systemd[1]: Reached target Swap. [ OK ] Listening on RPCbind Server Activation Socket. [ 4.708205] systemd[1]: Listening on RPCbind Server Activation Socket. [ 4.725053] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ OK ] Listening on Process Core Dump Socket. [ 4.760421] systemd[1]: Listening on Process Core Dump Socket. [ 4.777365] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ OK ] Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket. [ 4.816029] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. [ 4.817090] systemd[1]: Listening on Journal Socket (/dev/log). [ 4.833954] systemd[1]: Listening on Journal Socket. [ 4.849851] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ OK ] Listening on udev Control Socket. [ 4.889582] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Kernel Socket. [ 4.905354] systemd[1]: Listening on udev Kernel Socket. Mounting Huge Pages File System... [ 4.927675] systemd[1]: Mounting Huge Pages File System... Mounting POSIX Message Queue File System..[ 4.951452] systemd[1]: Mounting POSIX Message Queue File System... . Mounting Kernel Debug File System... [ 4.979523] systemd[1]: Mounting Kernel Debug File System... Mounting Temporary Directory (/tmp)... [ 4.998515] systemd[1]: Mounting Temporary Directory (/tmp)... Starting Create list of st…odes for the current kernel... [ 5.019922] systemd[1]: Starting Create list of static device nodes for the current kernel... Starting Start psplash boot splash screen.[ 5.051547] systemd[1]: Starting Start psplash boot splash screen... .. Starting RPC Bind... [ 5.081383] systemd[1]: Starting RPC Bind... [ 5.093471] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 5.102127] systemd[1]: Starting Journal Service... Starting Journal Service... Starting Load Kernel Modules... [ 5.131563] systemd[1]: Starting Load Kernel Modules... Starting Remount Root and Kernel File Systems... [ 5.153413] systemd[1]: Starting Remount Root and Kernel File Systems... [ 5.155965] cryptodev: loading out-of-tree module taints kernel. [ 5.158785] cryptodev: driver 1.10 loaded. [ 5.177847] systemd[1]: Starting udev Coldplug all Devices... Starting udev Coldplug all Devices... [ OK ] Started RPC Bind. [ 5.202500] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null) [ 5.219799] systemd[1]: Started RPC Bind. [ OK ] Mounted Huge Pages File System. [ 5.236248] systemd[1]: Mounted Huge Pages File System. [ OK ] Started Journal Service. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory (/tmp). [ 5.259138] systemd[1]: Started Journal Service. [ OK ] Started Create list of sta… nodes for the current kernel. [FAILED] Failed to start Start psplash boot splash screen. See 'systemctl status psplash-start.service' for details. [DEPEND] Dependency failed for Star…progress communication helper. [ OK ] Started Load Kernel Modules. [ OK ] Started Remount Root and Kernel File Systems. Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage... Starting Apply Kernel Variables... Starting Create Static Device Nodes in /dev... [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Apply Kernel Variables. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /media/ram. [ OK ] Mounted /var/volatile. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started Create Volatile Files and Directories. [ 5.515476] systemd-journald[217]: Received client request to flush runtime journal. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started udev Kernel Device Manager. [ OK ] Started Update UTMP about System Boot/Shutdown. [ 8.265153] [drm] Initialized pvr 1.17.4948957 20110701 for 7000000.gpu on minor 0 [ OK ] Started udev Coldplug all Devices. [ 8.492949] random: crng init done [ 8.492965] random: 7 urandom warning(s) missed due to ratelimiting [ 8.505031] CAN device driver interface [ 8.516359] cal 6f03000.cal: Neither port is configured, no point in staying up [ 8.873982] m_can_platform 40528000.mcan: m_can device registered (irq=23, version=32) [ 8.926755] am65-cpsw-nuss 46000000.ethernet ets0: renamed from eth0 Starting udev Wait for Complete Device Initialization... [ OK ] Started Network Time Synchronization. [ 9.186734] platform 41000000.r5f: configured R5F for remoteproc mode [ 9.187852] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000 [ 9.224377] remoteproc remoteproc0: 41000000.r5f is available [ 9.233235] remoteproc remoteproc0: powering up 41000000.r5f [ 9.233263] remoteproc remoteproc0: Booting fw image am65x-mcu-r5f0_0-fw, size 81676 [ 9.271476] m_can_platform 40568000.mcan: m_can device registered (irq=25, version=32) [ 9.275580] remoteproc0#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000 [ 9.357539] virtio_rpmsg_bus virtio0: rpmsg host is online [ 9.377829] remoteproc0#vdev0buffer: registered virtio0 (type 7) [ 9.377855] remoteproc remoteproc0: remote processor 41000000.r5f is now up [ 9.490650] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd [ OK ] Started Load/Save Random Seed. [ 9.526630] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. [ 9.721306] davinci_mdio b032400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 9.721343] libphy: b032400.mdio: probed [ 9.813412] davinci_mdio b032400.mdio: phy[0]: device b032400.mdio:00, driver TI DP83867 [ 9.813442] davinci_mdio b032400.mdio: phy[3]: device b032400.mdio:03, driver TI DP83867 [ 9.953082] davinci_mdio b132400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 9.953120] libphy: b132400.mdio: probed [ 10.056179] davinci_mdio b132400.mdio: phy[0]: device b132400.mdio:00, driver TI DP83867 [ 10.056204] davinci_mdio b132400.mdio: phy[3]: device b132400.mdio:03, driver TI DP83867 [ 10.136980] davinci_mdio b232400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 10.137018] libphy: b232400.mdio: probed [ 10.263748] davinci_mdio b232400.mdio: phy[0]: device b232400.mdio:00, driver TI DP83867 [ 10.263776] davinci_mdio b232400.mdio: phy[3]: device b232400.mdio:03, driver TI DP83867 [ 10.930423] remoteproc remoteproc1: b034000.pru is available [ 10.931670] remoteproc remoteproc2: b004000.rtu is available [ 10.932444] remoteproc remoteproc3: b00a000.txpru is available [ 10.933109] remoteproc remoteproc4: b038000.pru is available [ 10.933730] remoteproc remoteproc5: b006000.rtu is available [ 10.935636] remoteproc remoteproc6: b00c000.txpru is available [ 10.936566] remoteproc remoteproc7: b134000.pru is available [ 10.941428] remoteproc remoteproc8: b104000.rtu is available [ 10.953208] remoteproc remoteproc9: b10a000.txpru is available [ 10.953845] remoteproc remoteproc10: b138000.pru is available [ 10.961257] remoteproc remoteproc11: b106000.rtu is available [ 10.962640] remoteproc remoteproc12: b10c000.txpru is available [ 10.963465] remoteproc remoteproc13: b234000.pru is available [ 10.970078] remoteproc remoteproc14: b204000.rtu is available [ 10.971157] remoteproc remoteproc15: b20a000.txpru is available [ 10.973279] remoteproc remoteproc16: b238000.pru is available [ 10.991658] remoteproc remoteproc17: b206000.rtu is available [ 10.992530] remoteproc remoteproc18: b20c000.txpru is available [ OK ] Created slice system-systemd\x2dfsck.slice. [ OK ] Found device /dev/mmcblk1p1. [ 12.355728] OF: graph: no port node found in /bus@100000/phy@4110000 Starting File System Check on /dev/mmcblk1p1... [ 12.592972] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c [ OK ] Created slice system-weston.slice. [ 13.217903] icssg-prueth icssg1-eth: TI PRU ethernet driver initialized: dual EMAC mode [ 13.327945] usbcore: registered new interface driver usbfs [ 13.341305] usbcore: registered new interface driver hub [ 13.344666] usbcore: registered new device driver usb Starting Start psplash boot splash screen... [ 13.476479] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 13.477495] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1 [ 13.477659] xhci-hcd xhci-hcd.2.auto: hcc params 0x0298fe6d hci version 0x110 quirks 0x0000000000010010 [ 13.478118] xhci-hcd xhci-hcd.2.auto: irq 594, io mem 0x04010000 [ 13.478763] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 [ 13.478780] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 13.478790] usb usb1: Product: xHCI Host Controller [ 13.478797] usb usb1: Manufacturer: Linux 5.10.65-rt53-g541ec9a699 xhci-hcd [ 13.478805] usb usb1: SerialNumber: xhci-hcd.2.auto [ 13.569153] hub 1-0:1.0: USB hub found [ 13.569241] hub 1-0:1.0: 1 port detected [ 13.578015] icssg-prueth icssg0-eth: TI PRU ethernet driver initialized: dual EMAC mode [ 13.590441] icssg-prueth icssg1-eth ets2_top_unused: renamed from eth1 [ 13.613422] icssg-prueth icssg1-eth ets2: renamed from eth0 [ 13.677733] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller [ 13.677777] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2 [ 13.677862] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed [ 13.678032] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 13.678218] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10 [ 13.678232] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 13.678244] usb usb2: Product: xHCI Host Controller [ 13.678251] usb usb2: Manufacturer: Linux 5.10.65-rt53-g541ec9a699 xhci-hcd [ 13.678259] usb usb2: SerialNumber: xhci-hcd.2.auto [ OK ] Started File System Check on /dev/mmcblk1p1. [ 13.794636] hub 2-0:1.0: USB hub found [ 13.794737] hub 2-0:1.0: 1 port detected [ 13.957726] icssg-prueth icssg2-eth: TI PRU ethernet driver initialized: dual EMAC mode [ 13.966973] icssg-prueth icssg0-eth ets1: renamed from eth2 [FAILED] Failed to start Start psplash boot splash screen. [ 14.007853] icssg-prueth icssg0-eth ets1_top_unused: renamed from eth3 See 'systemctl status psplash-start.service' for details. [DEPEND] Dependency failed for Star…progress communication helper. [ 14.036895] icssg-prueth icssg2-eth ets3: renamed from eth0 [ 14.092750] icssg-prueth icssg2-eth ets3_top_unused: renamed from eth1 [ OK ] Reached target Hardware activated USB gadget. Mounting /run/media/mmcblk1p1... [ OK ] Mounted /run/media/mmcblk1p1. [ OK ] Started udev Wait for Complete Device Initialization. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Reached target System Initialization. [ OK ] Started Daily rotation of log files. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API. [ OK ] Listening on dropbear.socket. Starting Reboot and dump vmcore via kexec... [ OK ] Listening on Docker Socket for the API. [ OK ] Started Reboot and dump vmcore via kexec. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. [ OK ] Started Periodic Command Scheduler. [ OK ] Started D-Bus System Message Bus. Starting Print notice about GPLv3 packages... Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ OK ] Started irqbalance daemon. Starting Telephony service... Starting rc.pvr.service... Starting Login Service... [ OK ] Started IPv6 Packet Filtering Framework. [ OK ] Started IPv4 Packet Filtering Framework. [ OK ] Reached target Network (Pre). Starting Network Service... [ OK ] Started Telephony service. [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. [ OK ] Started rc.pvr.service. [ 15.012205] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ] [ 15.049313] Bluetooth: Core ver 2.22 [ 15.049518] NET: Registered protocol family 31 Starting weston.service... [ 15.049526] Bluetooth: HCI device and connection manager initialized [ 15.049559] Bluetooth: HCI socket layer initialized [ 15.049573] Bluetooth: L2CAP socket layer initialized [ 15.049610] Bluetooth: SCO socket layer initialized [ OK ] Started weston.service. Starting telnetd.service... [ OK ] Started telnetd.service. [ OK ] Started Network Service. Starting Wait for Network to be Configured... Starting Network Name Resolution... [ OK ] Started Login Service. [ OK ] Started Network Name Resolution. [ OK ] Reached target Network. [ OK ] Reached target Host and Network Name Lookups. Starting Avahi mDNS/DNS-SD Stack... Starting Enable and configure wl18xx bluetooth stack... [ OK ] Started NFS status monitor for NFSv2/3 locking.. Starting Simple Network Ma…ent Protocol (SNMP) Daemon.... Starting Permit User Sessions... [ OK ] Started Permit User Sessions. [ OK ] Started Getty on tty1. [ OK ] Started Getty on tty4. [ OK ] Started Serial Getty on ttyS1. [ OK ] Started Serial Getty on ttyS2. [ OK ] Reached target Login Prompts. Starting Synchronize System and HW clocks... Starting Weston Wayland Compositor... [ OK ] Started Enable and configure wl18xx bluetooth stack. [FAILED] Failed to start Synchronize System and HW clocks. See 'systemctl status sync-clocks.service' for details. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Created slice User Slice of UID 0. Starting User Runtime Directory /run/user/0... [ OK ] Started User Runtime Directory /run/user/0. Starting User Manager for UID 0... [ OK ] Started User Manager for UID 0. [ OK ] Started Session c1 of user root. [ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon.. [FAILED] Failed to start Weston Wayland Compositor. See 'systemctl status weston@root.service' for details. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash-dev bash bc binutils cifs-utils coreutils-stdbuf coreutils cpio cpp-symlinks cpp dosfstools elfutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext glmark2 gstreamer1.0-libav-dev gstreamer1.0-libav gzip less libasm1 libbfd libdw1 libelf1 libgdbm-compat4 libgdbm-dev libgdbm6 libgettextlib libgettextsrc libgmp-dev libgmp10 libgmpxx4 libidn2-0 libidn2-dev libmpc3 libmpfr6 libreadline-dev libreadline8 libunistring-dev libunistring2 m4-dev m4 make nettle-dev nettle parted pdm-anomaly-detection python3-rfc3987 python3-strict-rfc3339 tar which zeromq If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ OK ] Started Print notice about GPLv3 packages. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am65xx-evm ttyS2 Arago 2021.09 am65xx-evm ttyS2 am65xx-evm login: þ