From linux-usb Tue Dec 08 16:31:50 2015 From: Bin Liu Date: Tue, 08 Dec 2015 16:31:50 +0000 To: linux-usb Subject: [[PATCH v3]] usb: phy: phy-am335x: bypass first VBUS sensing for host-only mode Message-Id: <1449592310-28995-1-git-send-email-b-liu () ti ! com> X-MARC-Message: https://marc.info/?l=linux-usb&m=144959233413958 To prevent VBUS contention, the am335x MUSB phy senses VBUS first before transitioning to host mode. However, for host-only mode, VBUS could be directly tied to 5V power rail which could prevent MUSB transitions to host mode. This change receives dr_mode of the controller then bypass the first VBUS sensing for host-only mode, so that MUSB can work in host mode event if VBUS is tied to 5V. Signed-off-by: Bin Liu --- v3: correct module dependency in Kconfig drivers/usb/phy/Kconfig | 1 + drivers/usb/phy/phy-am335x-control.c | 14 +++++++++++--- drivers/usb/phy/phy-am335x-control.h | 8 +++++--- drivers/usb/phy/phy-am335x.c | 15 ++++++++++----- 4 files changed, 27 insertions(+), 11 deletions(-) diff --git a/drivers/usb/phy/Kconfig b/drivers/usb/phy/Kconfig index 155694c..c690474 100644 --- a/drivers/usb/phy/Kconfig +++ b/drivers/usb/phy/Kconfig @@ -66,6 +66,7 @@ config AM335X_PHY_USB select USB_PHY select AM335X_CONTROL_USB select NOP_USB_XCEIV + select USB_COMMON help This driver provides PHY support for that phy which part for the AM335x SoC. diff --git a/drivers/usb/phy/phy-am335x-control.c b/drivers/usb/phy/phy-am335x-control.c index 23fca51..42a1afe 100644 --- a/drivers/usb/phy/phy-am335x-control.c +++ b/drivers/usb/phy/phy-am335x-control.c @@ -4,6 +4,7 @@ #include #include #include +#include #include "phy-am335x-control.h" struct am335x_control_usb { @@ -58,7 +59,8 @@ static void am335x_phy_wkup(struct phy_control *phy_ctrl, u32 id, bool on) spin_unlock(&usb_ctrl->lock); } -static void am335x_phy_power(struct phy_control *phy_ctrl, u32 id, bool on) +static void am335x_phy_power(struct phy_control *phy_ctrl, u32 id, + enum usb_dr_mode dr_mode, bool on) { struct am335x_control_usb *usb_ctrl; u32 val; @@ -80,8 +82,14 @@ static void am335x_phy_power(struct phy_control *phy_ctrl, u32 id, bool on) val = readl(usb_ctrl->phy_reg + reg); if (on) { - val &= ~(USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN); - val |= USBPHY_OTGVDET_EN | USBPHY_OTGSESSEND_EN; + if (dr_mode == USB_DR_MODE_HOST) { + val &= ~(USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN | + USBPHY_OTGVDET_EN); + val |= USBPHY_OTGSESSEND_EN; + } else { + val &= ~(USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN); + val |= USBPHY_OTGVDET_EN | USBPHY_OTGSESSEND_EN; + } } else { val |= USBPHY_CM_PWRDN | USBPHY_OTG_PWRDN; } diff --git a/drivers/usb/phy/phy-am335x-control.h b/drivers/usb/phy/phy-am335x-control.h index b96594d..e86b316 100644 --- a/drivers/usb/phy/phy-am335x-control.h +++ b/drivers/usb/phy/phy-am335x-control.h @@ -2,13 +2,15 @@ #define _AM335x_PHY_CONTROL_H_ struct phy_control { - void (*phy_power)(struct phy_control *phy_ctrl, u32 id, bool on); + void (*phy_power)(struct phy_control *phy_ctrl, u32 id, + enum usb_dr_mode dr_mode, bool on); void (*phy_wkup)(struct phy_control *phy_ctrl, u32 id, bool on); }; -static inline void phy_ctrl_power(struct phy_control *phy_ctrl, u32 id, bool on) +static inline void phy_ctrl_power(struct phy_control *phy_ctrl, u32 id, + enum usb_dr_mode dr_mode, bool on) { - phy_ctrl->phy_power(phy_ctrl, id, on); + phy_ctrl->phy_power(phy_ctrl, id, dr_mode, on); } static inline void phy_ctrl_wkup(struct phy_control *phy_ctrl, u32 id, bool on) diff --git a/drivers/usb/phy/phy-am335x.c b/drivers/usb/phy/phy-am335x.c index 8b6139d..39b424f 100644 --- a/drivers/usb/phy/phy-am335x.c +++ b/drivers/usb/phy/phy-am335x.c @@ -8,6 +8,7 @@ #include #include #include +#include #include "phy-am335x-control.h" #include "phy-generic.h" @@ -16,13 +17,14 @@ struct am335x_phy { struct usb_phy_generic usb_phy_gen; struct phy_control *phy_ctrl; int id; + enum usb_dr_mode dr_mode; }; static int am335x_init(struct usb_phy *phy) { struct am335x_phy *am_phy = dev_get_drvdata(phy->dev); - phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, true); + phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, true); return 0; } @@ -30,7 +32,7 @@ static void am335x_shutdown(struct usb_phy *phy) { struct am335x_phy *am_phy = dev_get_drvdata(phy->dev); - phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, false); + phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, false); } static int am335x_phy_probe(struct platform_device *pdev) @@ -46,12 +48,15 @@ static int am335x_phy_probe(struct platform_device *pdev) am_phy->phy_ctrl = am335x_get_phy_control(dev); if (!am_phy->phy_ctrl) return -EPROBE_DEFER; + am_phy->id = of_alias_get_id(pdev->dev.of_node, "phy"); if (am_phy->id < 0) { dev_err(&pdev->dev, "Missing PHY id: %d\n", am_phy->id); return am_phy->id; } + am_phy->dr_mode = of_usb_get_dr_mode_by_phy(pdev->dev.of_node); + ret = usb_phy_gen_create_phy(dev, &am_phy->usb_phy_gen, NULL); if (ret) return ret; @@ -75,7 +80,7 @@ static int am335x_phy_probe(struct platform_device *pdev) */ device_set_wakeup_enable(dev, false); - phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, false); + phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, false); return 0; } @@ -105,7 +110,7 @@ static int am335x_phy_suspend(struct device *dev) if (device_may_wakeup(dev)) phy_ctrl_wkup(am_phy->phy_ctrl, am_phy->id, true); - phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, false); + phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, false); return 0; } @@ -115,7 +120,7 @@ static int am335x_phy_resume(struct device *dev) struct platform_device *pdev = to_platform_device(dev); struct am335x_phy *am_phy = platform_get_drvdata(pdev); - phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, true); + phy_ctrl_power(am_phy->phy_ctrl, am_phy->id, am_phy->dr_mode, true); if (device_may_wakeup(dev)) phy_ctrl_wkup(am_phy->phy_ctrl, am_phy->id, false); -- 1.9.1 -- To unsubscribe from this list: send the line "unsubscribe linux-usb" in the body of a message to majordomo@vger.kernel.orgUntitled Document More majordomo info at http://vger.kernel.org/majordomo-info.html