U-Boot 2013.01.01-svn29730 (Mar 20 2017 - 17:08:42) I2C: ready DRAM: 128 MiB NAND: 256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Using default environment set_default_env::8105 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Peripheral mode controller at 47401000 using PIO, IRQ 0 musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn) musb-hdrc: MHDRC RTL version 2.0 musb-hdrc: setup fifo_mode 4 musb-hdrc: 28/31 max ep, 16384/16384 memory USB Host mode controller at 47401800 using PIO, IRQ 0 Net: not set. Validating first E-fuse MAC cpsw Hit any key to stop autoboot mmc_send_cmd : timeout: No status update Card did not respond to voltage select! (Re)start USB... USB0: lowlevel init failed USB error: all controllers failed lowlevel init Download Linux from USB to Nandflash... ** Bad device usb 0 ** ** Bad device usb 0 ** ** Bad device usb 0 ** ** Bad device usb 0 ** ** Bad device usb 0 ** Booting from nand ... NAND read: device 0 offset 0x3080000, size 0x300000 3145728 bytes read: OK ## Booting kernel from Legacy Image at 80200000 ... Image Name: Linux-3.2.0+ Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2667232 Bytes = 2.5 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK Loading Kernel Image ... OK OK Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0+ (ding@ding-desktop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #26 Thu Jan 7 12:05:10 ULAT 2016 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Ignoring tag cmdline (using the default kernel command line) [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs ro ubi.mtd=7,2048 rootfstype=ubifs rootwait=1t ip=none [ 0.000000] PID hash table entries: 512 (order: -1, 2048 bytes) [ 0.000000] Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) [ 0.000000] Memory: 128MB = 128MB total [ 0.000000] Memory: 123784k/123784k available, 7288k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xc8800000 - 0xff000000 ( 872 MB) [ 0.000000] lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc04d7084 (4925 kB) [ 0.000000] .init : 0xc04d8000 - 0xc0518000 ( 256 kB) [ 0.000000] .data : 0xc0518000 - 0xc05b3e68 ( 624 kB) [ 0.000000] .bss : 0xc05b3e8c - 0xc05fabb0 ( 284 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 25000000 Hz [ 0.000000] omap_dm_timer_switch_src: Switching to HW default clocksource(sys_clkin_ck) for timer1, this may impact timekeeping in low power state [ 0.000000] OMAP clocksource: GPTIMER1 at 25000000 Hz [ 0.000000] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 171798ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000215] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.057102] pid_max: default: 32768 minimum: 301 [ 0.057281] Mount-cache hash table entries: 512 [ 0.057671] CPU: Testing write buffer coherency: ok [ 0.057749] ftrace: allocating 13708 entries in 41 pages [ 0.107871] omap_hwmod: gfx: failed to hardreset [ 0.124017] omap_hwmod: pruss: failed to hardreset [ 0.125151] print_constraints: dummy: [ 0.125590] NET: Registered protocol family 16 [ 0.127799] OMAP GPIO hardware version 0.1 [ 0.130226] am335x_evm_init()++ [ 0.130446] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.132625] am335x_evm_i2c_init()++ [ 0.132864] omap_i2c.1: alias fck already exists [ 0.133060] am335x_evm_i2c_init()-- [ 0.133189] da8xx_panel_power_ctrl()++ [ 0.133227] back light switch = 1 [ 0.133249] da8xx_panel_power_ctrl()-- [ 0.133557] am335x_evm_init()-- [ 0.133846] omap2_mcspi.1: alias fck already exists [ 0.134060] omap2_mcspi.2: alias fck already exists [ 0.134312] edma.0: alias fck already exists [ 0.134333] edma.0: alias fck already exists [ 0.134352] edma.0: alias fck already exists [ 0.150288] bio: create slab at 0 [ 0.152436] SCSI subsystem initialized [ 0.154168] usbcore: registered new interface driver usbfs [ 0.154481] usbcore: registered new interface driver hub [ 0.154685] usbcore: registered new device driver usb [ 0.167171] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.169205] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.171894] print_constraints: VRTC: [ 0.173533] print_constraints: VIO: at 1500 mV [ 0.176197] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.178868] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.180015] print_constraints: VDD3: 5000 mV [ 0.181619] print_constraints: VDIG1: at 1800 mV [ 0.183242] print_constraints: VDIG2: at 1800 mV [ 0.184854] print_constraints: VPLL: at 1800 mV [ 0.186467] print_constraints: VDAC: at 1800 mV [ 0.188087] print_constraints: VAUX1: at 1800 mV [ 0.189702] print_constraints: VAUX2: at 3300 mV [ 0.191331] print_constraints: VAUX33: at 3300 mV [ 0.192948] print_constraints: VMMC: at 3300 mV [ 0.193428] tps65910 1-002d: No interrupt support, no core IRQ [ 0.194510] Switching to clocksource gp timer [ 0.214824] NET: Registered protocol family 2 [ 0.215031] IP route cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.215336] TCP established hash table entries: 4096 (order: 3, 32768 bytes) [ 0.215423] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.215477] TCP: Hash tables configured (established 4096 bind 4096) [ 0.215490] TCP reno registered [ 0.215503] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.215527] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.215700] NET: Registered protocol family 1 [ 0.215982] RPC: Registered named UNIX socket transport module. [ 0.215995] RPC: Registered udp transport module. [ 0.216004] RPC: Registered tcp transport module. [ 0.216014] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.216775] cpuidle-am33xx cpuidle-am33xx.0: failed to register driver [ 0.224079] Installing knfsd (copyright (C) 1996 okir@monad.swb.de). [ 0.224412] msgmni has been set to 241 [ 0.225103] io scheduler noop registered [ 0.225119] io scheduler deadline registered [ 0.225200] io scheduler cfq registered (default) [ 0.226234] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.770005] console [ttyO0] enabled [ 0.774190] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.781984] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.789728] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.797463] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.805194] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.821922] brd: module loaded [ 0.829955] loop: module loaded [ 0.833328] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.894553] No daughter card found [ 0.898155] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.905427] am335x_evm_setup()++ [ 0.964553] AM335X: EVM Config read fail: -110 [ 0.969185] No board detected, using GPBoard 1.1A as default [ 0.975306] The board is general purpose EVM in profile 0 [ 0.980935] Found invalid GP EVM revision, falling back to Rev1.1A [ 0.987392] -------siglent_fpga_init++ [ 0.991417] -------siglent_fpga_init-- [ 0.996130] da8xx_lcdc.0: alias fck already exists [ 1.001644] evm_nand_init()++ [ 1.005365] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 1.010369] Registering NAND on CS0 [ 1.014651] evm_nand_init()-- [ 1.017832] omap_i2c.2: alias fck already exists [ 1.034619] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 1.042826] haptics_init()++ [ 1.046884] haptics_init()-- [ 1.049893] out_triger_gpio_init()++ [ 1.053658] out_triger_gpio_init()-- [ 1.057888] am335x_evm_setup()-- [ 1.062731] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.069986] omap2-nand driver initializing [ 1.074618] ONFI flash detected [ 1.078028] ONFI param page 0 valid [ 1.081676] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP) [ 1.090267] Creating 12 MTD partitions on "omap2-nand.0": [ 1.095932] 0x000000000000-0x000000020000 : "SPL" [ 1.102217] 0x000000020000-0x000000040000 : "SPL.backup1" [ 1.109127] 0x000000040000-0x000000060000 : "SPL.backup2" [ 1.116022] 0x000000060000-0x000000080000 : "SPL.backup3" [ 1.122856] 0x000000080000-0x000000260000 : "U-Boot" [ 1.130067] 0x000000260000-0x000000280000 : "U-Boot Env" [ 1.136883] 0x000000280000-0x000000580000 : "Manufacturedata" [ 1.145369] 0x000000580000-0x000003080000 : "rootfs" [ 1.169601] 0x000003080000-0x000003680000 : "kerneldata" [ 1.178782] 0x000003680000-0x000006880000 : "firmdata0" [ 1.206188] 0x000006880000-0x000009a80000 : "firmdata1" [ 1.233576] 0x000009a80000-0x000010000000 : "datafs" [ 1.282266] OneNAND driver initializing [ 1.287013] UBI: attaching mtd7 to ubi0 [ 1.291028] UBI: physical eraseblock size: 131072 bytes (128 KiB) [ 1.297592] UBI: logical eraseblock size: 126976 bytes [ 1.303220] UBI: smallest flash I/O unit: 2048 [ 1.308131] UBI: sub-page size: 512 [ 1.312942] UBI: VID header offset: 2048 (aligned 2048) [ 1.319212] UBI: data offset: 4096 [ 1.734139] UBI: max. sequence number: 4 [ 1.752489] UBI warning: print_rsvd_warning: cannot reserve enough PEBs for bad PEB handling, reserved 9, need 15 [ 1.764161] UBI: attached mtd7 to ubi0 [ 1.768111] UBI: MTD device name: "rootfs" [ 1.773376] UBI: MTD device size: 43 MiB [ 1.778470] UBI: number of good PEBs: 344 [ 1.783281] UBI: number of bad PEBs: 0 [ 1.787919] UBI: number of corrupted PEBs: 0 [ 1.792549] UBI: max. allowed volumes: 128 [ 1.797369] UBI: wear-leveling threshold: 4096 [ 1.802270] UBI: number of internal volumes: 1 [ 1.806908] UBI: number of user volumes: 1 [ 1.811538] UBI: available PEBs: 0 [ 1.816178] UBI: total number of reserved PEBs: 344 [ 1.821260] UBI: number of PEBs reserved for bad PEB handling: 9 [ 1.827530] UBI: max/mean erase counter: 2/0 [ 1.831978] UBI: image sequence number: 631718590 [ 1.837097] UBI: background thread "ubi_bgt0d" started, PID 482 [ 1.994189] da8xx_lcdc da8xx_lcdc.0: GLCD: Found HANSTAR_HSD070IDW1_A panel [ 2.009673] Console: switching to colour frame buffer device 60x34 [ 2.021530] sdg800:Logo image from nandflash, color_addr=[0xc88cb034], color_len=[0x7f800]! [ 2.084583] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 2.091044] davinci_mdio davinci_mdio.0: detected phy mask bfffffff [ 2.097827] bus->id = 0, addr= 30 [ 2.101485] 11-- [ 2.103613] davinci_mdio.0: probed [ 2.107199] davinci_mdio davinci_mdio.0: phy[30]: device 0:1e, driver unknown [ 2.114982] usbcore: registered new interface driver cdc_ether [ 2.121225] usbcore: registered new interface driver dm9601 [ 2.127100] cdc_ncm: 04-Aug-2011 [ 2.130633] usbcore: registered new interface driver cdc_ncm [ 2.136555] Initializing USB Mass Storage driver... [ 2.141829] usbcore: registered new interface driver usb-storage [ 2.148109] USB Mass Storage support registered. [ 2.153352] mousedev: PS/2 mouse device common for all mice [ 2.159639] i2c /dev entries driver [ 2.164709] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 2.171719] TCP cubic registered [ 2.175128] NET: Registered protocol family 17 [ 2.179913] NET: Registered protocol family 33 [ 2.184589] Registering the dns_resolver key type [ 2.189551] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 2.197572] ThumbEE CPU extension supported. [ 2.202087] mux: Failed to setup hwmod io irq -22 [ 2.207620] Power Management for AM33XX family [ 2.212317] clock: disabling unused clocks to save power [ 2.219513] Detected MACID=f8:36:9b:fe:49:39 [ 2.371302] UBIFS error (pid 1): ubifs_recover_master_node: failed to recover master node [ 2.380474] List of all partitions: [ 2.384162] 1f00 128 mtdblock0 (driver?) [ 2.389482] 1f01 128 mtdblock1 (driver?) [ 2.394767] 1f02 128 mtdblock2 (driver?) [ 2.400046] 1f03 128 mtdblock3 (driver?) [ 2.405345] 1f04 1920 mtdblock4 (driver?) [ 2.410618] 1f05 128 mtdblock5 (driver?) [ 2.415905] 1f06 3072 mtdblock6 (driver?) [ 2.421183] 1f07 44032 mtdblock7 (driver?) [ 2.426467] 1f08 6144 mtdblock8 (driver?) [ 2.431740] 1f09 51200 mtdblock9 (driver?) [ 2.437027] 1f0a 51200 mtdblock10 (driver?) [ 2.442390] 1f0b 103936 mtdblock11 (driver?) [ 2.447759] No filesystem could mount root, tried: ubifs [ 2.453399] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) [ 2.462088] [] (unwind_backtrace+0x0/0x144) from [] (dump_stack+0x20/0x24) [ 2.471098] [] (dump_stack+0x20/0x24) from [] (panic+0x74/0x1a8) [ 2.479213] [] (panic+0x74/0x1a8) from [] (mount_block_root+0x29c/0x2b8) [ 2.488035] [] (mount_block_root+0x29c/0x2b8) from [] (prepare_namespace+0xac/0x1d4) [ 2.497942] [] (prepare_namespace+0xac/0x1d4) from [] (kernel_init+0x124/0x130) [ 2.507403] [] (kernel_init+0x124/0x130) from [] (kernel_thread_exit+0x0/0x8)