U-Boot SPL 2011.09 (Aug 24 2013 - 14:02:12) Texas Instruments Revision detection unimplemented gpio_request()++ gpio_request()-- gpio_direction_output()++ gpio_direction_output()-- config ddr_pll_config()++ ddr_pll_config()++ ddr_pll_config()-- is_ddr3 = 1 config ddr_pll_config()-- spl_board_init()++ U-Boot 2011.09 (Mar 22 2014 - 19:55:59) I2C: ready DRAM: 128 MiB WARNING: Caches not enabled board_init()++ No daughter card present board_id = 1, header.version = 87f3ae04 profile = 1, daughter_board_connected = 0 board_init()-include gpmc- NAND: HW ECC Hamming Code selected test-nand_get_flash_type()++ uboot reset nand uboot reset nand NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Toshiba ) NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron NAND 256MiB 3,3V 8-bit) NAND bus width 8 instead 8 bit chip->badblockpos = 0x0 test-nand_get_flash_type()--256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 create_bbt()++ create_bbt()-- *** Warning - bad CRC, using default environment Lcd_Init()++ SetUpLCD()++ SetUpLCD()-- HW ECC BCH8 Selected HW ECC BCH8 Selected Logo from nanndflash: base=0x81000000; end=0x8107f81f; end-base=0x7f81f; rwsize=0x7f820; r=0x0 RasterDMAFBConfig()++ RasterDMAFBConfig()-- RasterDMAFBConfig()++ RasterDMAFBConfig()-- Lcd_Init()-- Net: u-boot set rmii mode cpsw Hit any key to stop autoboot: 0 Card did not respond to voltage select! Booting from nand ... HW ECC BCH8 Selected NAND read: device 0 offset 0x3080000, size 0x300000 3145728 bytes read: OK ## Booting kernel from Legacy Image at 80007fc0 ... Image Name: Linux-3.2.0+ Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2706112 Bytes = 2.6 MiB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK XIP Kernel Image ... OK OK kernel loaded at 0x80008000, end = 0x8029cac0 Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0+ (ding@ding-desktop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #338 Wed Jul 9 14:17:15 ULAT 2014 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 32512 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=8,2048 noinitrd rootfstype=ubifs rootwait=1 ip=none [ 0.000000] PID hash table entries: 512 (order: -1, 2048 bytes) [ 0.000000] Dentry cache hash table entries: 16384 (order: 4, 65536 bytes) [ 0.000000] Inode-cache hash table entries: 8192 (order: 3, 32768 bytes) [ 0.000000] Memory: 128MB = 128MB total [ 0.000000] Memory: 123696k/123696k available, 7376k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xc8800000 - 0xff000000 ( 872 MB) [ 0.000000] lowmem : 0xc0000000 - 0xc8000000 ( 128 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc04e9bc4 (4999 kB) [ 0.000000] .init : 0xc04ea000 - 0xc052b000 ( 260 kB) [ 0.000000] .data : 0xc052c000 - 0xc05c94c8 ( 630 kB) [ 0.000000] .bss : 0xc05c94ec - 0xc0610230 ( 284 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 25000000 Hz [ 0.000000] omap_dm_timer_switch_src: Switching to HW default clocksource(sys_clkin_ck) for timer1, this may impact timekeeping in low power state [ 0.000000] OMAP clocksource: GPTIMER1 at 25000000 Hz [ 0.000000] sched_clock: 32 bits at 25MHz, resolution 40ns, wraps every 171798ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000206] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144) [ 0.057096] pid_max: default: 32768 minimum: 301 [ 0.057275] Mount-cache hash table entries: 512 [ 0.057669] CPU: Testing write buffer coherency: ok [ 0.057747] ftrace: allocating 13840 entries in 41 pages [ 0.108161] omap_hwmod: gfx: failed to hardreset [ 0.124214] omap_hwmod: pruss: failed to hardreset [ 0.125369] print_constraints: dummy: [ 0.125821] NET: Registered protocol family 16 [ 0.128053] OMAP GPIO hardware version 0.1 [ 0.130490] am335x_evm_init()++ [ 0.130715] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.132836] am335x_evm_i2c_init()++ [ 0.133082] omap_i2c.1: alias fck already exists [ 0.133280] am335x_evm_i2c_init()-- [ 0.133407] da8xx_panel_power_ctrl()++ [ 0.133446] back light switch = 1 [ 0.133468] da8xx_panel_power_ctrl()-- [ 0.133788] am335x_evm_init()-- [ 0.134100] omap2_mcspi.1: alias fck already exists [ 0.134328] omap2_mcspi.2: alias fck already exists [ 0.134583] edma.0: alias fck already exists [ 0.134604] edma.0: alias fck already exists [ 0.134623] edma.0: alias fck already exists [ 0.150805] bio: create slab at 0 [ 0.152978] SCSI subsystem initialized [ 0.154750] usbcore: registered new interface driver usbfs [ 0.155064] usbcore: registered new interface driver hub [ 0.155266] usbcore: registered new device driver usb [ 0.155413] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.155674] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.167164] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.169194] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.171908] print_constraints: VRTC: [ 0.173579] print_constraints: VIO: at 1500 mV [ 0.176242] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal [ 0.178908] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.180059] print_constraints: VDD3: 5000 mV [ 0.181676] print_constraints: VDIG1: at 1800 mV [ 0.183293] print_constraints: VDIG2: at 1800 mV [ 0.184918] print_constraints: VPLL: at 1800 mV [ 0.186533] print_constraints: VDAC: at 1800 mV [ 0.188173] print_constraints: VAUX1: at 1800 mV [ 0.189795] print_constraints: VAUX2: at 3300 mV [ 0.191414] print_constraints: VAUX33: at 3300 mV [ 0.193042] print_constraints: VMMC: at 3300 mV [ 0.193512] tps65910 1-002d: No interrupt support, no core IRQ [ 0.194620] Switching to clocksource gp timer [ 0.214989] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.215173] musb-hdrc musb-hdrc.0: dma type: pio [ 0.216049] musb-hdrc musb-hdrc.0: USB OTG mode controller at c881c000 using PIO, IRQ 18 [ 0.216218] musb-hdrc musb-hdrc.1: dma type: pio [ 0.216632] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.216702] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.216833] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.216849] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.216863] usb usb1: Product: MUSB HDRC host driver [ 0.216875] usb usb1: Manufacturer: Linux 3.2.0+ musb-hcd [ 0.216886] usb usb1: SerialNumber: musb-hdrc.1 [ 0.217652] hub 1-0:1.0: USB hub found [ 0.217682] hub 1-0:1.0: 1 port detected [ 0.218185] musb-hdrc musb-hdrc.1: USB Host mode controller at c881e800 using PIO, IRQ 19 [ 0.218628] NET: Registered protocol family 2 [ 0.218821] IP route cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.219109] TCP established hash table entries: 4096 (order: 3, 32768 bytes) [ 0.219198] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.219253] TCP: Hash tables configured (established 4096 bind 4096) [ 0.219266] TCP reno registered [ 0.219282] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.219307] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.219478] NET: Registered protocol family 1 [ 0.219746] RPC: Registered named UNIX socket transport module. [ 0.219759] RPC: Registered udp transport module. [ 0.219768] RPC: Registered tcp transport module. [ 0.219777] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.220509] cpuidle-am33xx cpuidle-am33xx.0: failed to register driver [ 0.227915] Installing knfsd (copyright (C) 1996 okir@monad.swb.de). [ 0.228259] msgmni has been set to 241 [ 0.228861] io scheduler noop registered [ 0.228875] io scheduler deadline registered [ 0.228954] io scheduler cfq registered (default) [ 0.230017] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.866066] console [ttyO0] enabled [ 0.870336] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.878150] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.885933] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.893647] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 0.901383] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 0.918198] brd: module loaded [ 0.926273] loop: module loaded [ 0.929638] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 0.994662] No daughter card found [ 0.998259] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.005531] am335x_evm_setup()++ [ 1.064763] AM335X: EVM Config read fail: -110 [ 1.069397] No board detected, using GPBoard 1.1A as default [ 1.075534] The board is general purpose EVM in profile 0 [ 1.081164] Found invalid GP EVM revision, falling back to Rev1.1A [ 1.088500] da8xx_lcdc.0: alias fck already exists [ 1.094413] evm_nand_init()++ [ 1.098101] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 1.103105] Registering NAND on CS0 [ 1.107319] evm_nand_init()-- [ 1.110497] omap_i2c.2: alias fck already exists [ 1.134730] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 1.142978] haptics_init()++ [ 1.147042] haptics_init()-- [ 1.150047] out_triger_gpio_init()++ [ 1.153811] out_triger_gpio_init()-- [ 1.158035] am335x_evm_setup()-- [ 1.162879] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.170023] omap2-nand driver initializing [ 1.174617] ONFI flash detected [ 1.178059] ONFI param page 0 valid [ 1.181704] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP) [ 1.190281] Creating 9 MTD partitions on "omap2-nand.0": [ 1.195858] 0x000000000000-0x000000020000 : "SPL" [ 1.202171] 0x000000020000-0x000000040000 : "SPL.backup1" [ 1.209093] 0x000000040000-0x000000060000 : "SPL.backup2" [ 1.215995] 0x000000060000-0x000000080000 : "SPL.backup3" [ 1.222875] 0x000000080000-0x000000260000 : "U-Boot" [ 1.230102] 0x000000260000-0x000000280000 : "U-Boot Env" [ 1.236864] 0x000000280000-0x000003080000 : "Manufacture data" [ 1.263197] 0x000003080000-0x000003680000 : "kernel data" [ 1.272490] 0x000003680000-0x000010000000 : "File system" [ 1.363152] OneNAND driver initializing [ 1.367914] UBI: attaching mtd8 to ubi0 [ 1.371928] UBI: physical eraseblock size: 131072 bytes (128 KiB) [ 1.378495] UBI: logical eraseblock size: 126976 bytes [ 1.384123] UBI: smallest flash I/O unit: 2048 [ 1.389036] UBI: sub-page size: 512 [ 1.393848] UBI: VID header offset: 2048 (aligned 2048) [ 1.400117] UBI: data offset: 4096 [ 3.318811] UBI: max. sequence number: 2140 [ 3.338677] UBI warning: print_rsvd_warning: cannot reserve enough PEBs for bad PEB handling, reserved 15, need 16 [ 3.350868] UBI: attached mtd8 to ubi0 [ 3.354826] UBI: MTD device name: "File system" [ 3.360544] UBI: MTD device size: 201 MiB [ 3.365729] UBI: number of good PEBs: 1605 [ 3.370629] UBI: number of bad PEBs: 7 [ 3.375268] UBI: number of corrupted PEBs: 0 [ 3.379896] UBI: max. allowed volumes: 128 [ 3.384715] UBI: wear-leveling threshold: 4096 [ 3.389616] UBI: number of internal volumes: 1 [ 3.394244] UBI: number of user volumes: 1 [ 3.398880] UBI: available PEBs: 0 [ 3.403509] UBI: total number of reserved PEBs: 1605 [ 3.408691] UBI: number of PEBs reserved for bad PEB handling: 15 [ 3.415050] UBI: max/mean erase counter: 5/2 [ 3.419498] UBI: image sequence number: 1955965245 [ 3.424711] UBI: background thread "ubi_bgt0d" started, PID 481 [ 3.582010] da8xx_lcdc da8xx_lcdc.0: GLCD: Found HANSTAR_HSD070IDW1_A panel [ 3.597534] Console: switching to colour frame buffer device 60x34 [ 3.609374] sdg800:Logo image from nandflash, color_addr=[0xc88cb034], color_len=[0x7f800]! [ 3.664704] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 3.671170] davinci_mdio davinci_mdio.0: detected phy mask bfffffff [ 3.677940] bus->id = 0, addr= 30 [ 3.681593] 11-- [ 3.683716] davinci_mdio.0: probed [ 3.687308] davinci_mdio davinci_mdio.0: phy[30]: device 0:1e, driver unknown [ 3.695100] usbcore: registered new interface driver cdc_ether [ 3.701336] usbcore: registered new interface driver dm9601 [ 3.707213] cdc_ncm: 04-Aug-2011 [ 3.710749] usbcore: registered new interface driver cdc_ncm [ 3.716669] Initializing USB Mass Storage driver... [ 3.721999] usbcore: registered new interface driver usb-storage [ 3.728281] USB Mass Storage support registered. [ 3.733536] mousedev: PS/2 mouse device common for all mice [ 3.739853] i2c /dev entries driver [ 3.744933] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 3.751965] TCP cubic registered [ 3.755370] NET: Registered protocol family 17 [ 3.760155] NET: Registered protocol family 33 [ 3.764825] Registering the dns_resolver key type [ 3.769789] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 3.777801] ThumbEE CPU extension supported. [ 3.782317] mux: Failed to setup hwmod io irq -22 [ 3.787842] Power Management for AM33XX family [ 3.792533] clock: disabling unused clocks to save power [ 3.799740] Detected MACID=88:33:14:ff:ca:8e [ 3.878974] UBIFS: recovery needed [ 4.184328] UBI: scrubbed PEB 573 (LEB 0:206), data moved to PEB 632 [ 4.428231] UBI: scrubbed PEB 576 (LEB 0:314), data moved to PEB 890 [ 4.571908] UBIFS error (pid 1): ubifs_check_node: bad CRC: calculated 0xd16d2326, read 0xfad91fad [ 4.581308] UBIFS error (pid 1): ubifs_check_node: bad node at LEB 309:76248 [ 4.588681] UBIFS error (pid 1): ubifs_scanned_corruption: corruption at LEB 309:76248 [ 4.603567] UBIFS error (pid 1): ubifs_scan: LEB 309 scanning failed [ 4.631739] VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0) [ 4.639144] Please append a correct "root=" boot option; here are the available partitions: [ 4.647915] 1f00 128 mtdblock0 (driver?) [ 4.653191] 1f01 128 mtdblock1 (driver?) [ 4.658480] 1f02 128 mtdblock2 (driver?) [ 4.663757] 1f03 128 mtdblock3 (driver?) [ 4.669042] 1f04 1920 mtdblock4 (driver?) [ 4.674314] 1f05 128 mtdblock5 (driver?) [ 4.679601] 1f06 47104 mtdblock6 (driver?) [ 4.684888] 1f07 6144 mtdblock7 (driver?) [ 4.690162] 1f08 206336 mtdblock8 (driver?) [ 4.695444] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) [ 4.704120] [] (unwind_backtrace+0x0/0x144) from [] (dump_stack+0x20/0x24) [ 4.713129] [] (dump_stack+0x20/0x24) from [] (panic+0x74/0x1a8) [ 4.721237] [] (panic+0x74/0x1a8) from [] (mount_block_root+0x214/0x2b8) [ 4.730061] [] (mount_block_root+0x214/0x2b8) from [] (prepare_namespace+0xac/0x1d4) [ 4.739971] [] (prepare_namespace+0xac/0x1d4) from [] (kernel_init+0x124/0x130) [ 4.749436] [] (kernel_init+0x124/0x130) from [] (kernel_thread_exit+0x0/0x8)