U-Boot SPL 2016.05-00319-ga0faac0-dirty (Jun 22 2017 - 12:43:55) Trying to boot from NAND The Expected Linux image was not found. Please check your NAND configuration. Trying to start u-boot now... U-Boot 2016.05-00319-ga0faac0-dirty (Jun 22 2017 - 12:43:55 +0530) CPU : AM335X-GP rev 2.1 Model: TI AM335x EVM Watchdog enabled I2C: ready DRAM: 512 MiB NAND: 256 MiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 MMC: no card present ** Bad device mmc 0 ** Using default environment not set. Validating first E-fuse MAC Net: eth0: ethernet@4a100000 Warning: usb_ether MAC addresses don't match: Address in SROM is de:ad:be:ef:00:01 Address in environment is 68:9e:19:81:98:50 , eth1: usb_ether Press SPACE to abort autoboot in 2 seconds Booting from nand ... NAND read: device 0 offset 0x80000, size 0x40000 262144 bytes read: OK NAND read: device 0 offset 0x200000, size 0x800000 8388608 bytes read: OK Kernel image @ 0x82000000 [ 0x000000 - 0x351160 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff2000, end 8ffff4e9 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Initializing cgroup subsys cpuacct [ 0.000000] Linux version 4.4.41-gf9f6f0db2d (root@EMMYS0683) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 PREEMPT Thu Jun 29 13:02:13 IST 2017 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine model: TI AM335x EVM [ 0.000000] cma: Reserved 48 MiB at 0x9d000000 [ 0.000000] Memory policy: Data cache writeback [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1 [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 459972K/524288K available (6611K kernel code, 317K rwdata, 2344K rodata, 264K init, 265K bss, 15164K reserved, 49152K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc08c704c (8957 kB) [ 0.000000] .init : 0xc08c8000 - 0xc090a000 ( 264 kB) [ 0.000000] .data : 0xc090a000 - 0xc09595b0 ( 318 kB) [ 0.000000] .bss : 0xc09595b0 - 0xc099bcd8 ( 266 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Build-time adjustment of leaf fanout to 32. [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000019] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000046] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000058] OMAP clocksource: timer1 at 24000000 Hz [ 0.000290] clocksource_probe: no matching clocksources found [ 0.000503] Console: colour dummy device 80x30 [ 0.000534] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0' [ 0.000543] This ensures that you still see kernel messages. Please [ 0.000550] update your kernel commandline. [ 0.000571] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032) [ 0.058728] pid_max: default: 32768 minimum: 301 [ 0.058901] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.058915] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.059765] Initializing cgroup subsys io [ 0.059800] Initializing cgroup subsys memory [ 0.059845] Initializing cgroup subsys devices [ 0.059863] Initializing cgroup subsys freezer [ 0.059882] Initializing cgroup subsys perf_event [ 0.059897] Initializing cgroup subsys pids [ 0.059933] CPU: Testing write buffer coherency: ok [ 0.060392] Setting up static identity map for 0x80008200 - 0x80008260 [ 0.063136] devtmpfs: initialized [ 0.080411] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.099916] omap_hwmod: debugss: _wait_target_disable failed [ 0.156945] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.161675] pinctrl core: initialized pinctrl subsystem [ 0.163270] NET: Registered protocol family 16 [ 0.166006] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.188793] cpuidle: using governor ladder [ 0.218781] cpuidle: using governor menu [ 0.224619] OMAP GPIO hardware version 0.1 [ 0.235417] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_s0, deferring probe [ 0.239252] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.279783] edma 49000000.edma: TI EDMA DMA engine driver [ 0.285426] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe [ 0.285624] media: Linux media interface: v0.10 [ 0.285706] Linux video capture interface: v2.00 [ 0.285781] pps_core: LinuxPPS API ver. 1 registered [ 0.285792] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti [ 0.285829] PTP clock support registered [ 0.285903] EDAC MC: Ver: 3.0.0 [ 0.287364] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400 [ 0.287796] Advanced Linux Sound Architecture Driver Initialized. [ 0.289375] clocksource: Switched to clocksource timer1 [ 0.303660] NET: Registered protocol family 2 [ 0.304622] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.304696] TCP bind hash table entries: 4096 (order: 2, 16384 bytes) [ 0.304757] TCP: Hash tables configured (established 4096 bind 4096) [ 0.304843] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.304870] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.305066] NET: Registered protocol family 1 [ 0.305534] RPC: Registered named UNIX socket transport module. [ 0.305556] RPC: Registered udp transport module. [ 0.305564] RPC: Registered tcp transport module. [ 0.305572] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.306702] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.309257] futex hash table entries: 256 (order: -1, 3072 bytes) [ 0.320174] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.321208] NFS: Registering the id_resolver key type [ 0.321289] Key type id_resolver registered [ 0.321300] Key type id_legacy registered [ 0.321391] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.325806] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247) [ 0.325842] io scheduler noop registered [ 0.325860] io scheduler deadline registered [ 0.326071] io scheduler cfq registered (default) [ 0.327889] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.332032] backlight supply power not found, using dummy regulator [ 0.413829] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled [ 0.418897] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250 [ 1.034386] console [ttyS0] enabled [ 1.039482] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250 [ 1.049857] [drm] Initialized drm 1.1.0 20060810 [ 1.055922] panel panel: found backlight [ 1.061710] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 1.068367] [drm] No driver support for vblank timestamp query. [ 1.106513] Console: switching to colour frame buffer device 100x30 [ 1.121000] tilcdc 4830e000.lcdc: fb0: frame buffer device [ 1.149606] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0 [ 1.164433] loop: module loaded [ 1.171100] spidev spi1.0: buggy DT: spidev listed directly in DT [ 1.177233] ------------[ cut here ]------------ [ 1.182059] WARNING: CPU: 0 PID: 1 at drivers/spi/spidev.c:719 spidev_probe+0x1cc/0x1dc() [ 1.190300] Modules linked in: [ 1.193390] CPU: 0 PID: 1 Comm: swapper Not tainted 4.4.41-gf9f6f0db2d #1 [ 1.200262] Hardware name: Generic AM33XX (Flattened Device Tree) [ 1.206384] Backtrace: [ 1.208875] [] (dump_backtrace) from [] (show_stack+0x18/0x1c) [ 1.216528] r7:c0440594 r6:000002cf r5:00000009 r4:00000000 [ 1.222279] [] (show_stack) from [] (dump_stack+0x24/0x28) [ 1.229603] [] (dump_stack) from [] (warn_slowpath_common+0x88/0xb4) [ 1.237742] [] (warn_slowpath_common) from [] (warn_slowpath_null+0x24/0x2c) [ 1.246610] r8:00000000 r7:c0945da0 r6:c0945d90 r5:dc430000 r4:dc430000 [ 1.253416] [] (warn_slowpath_null) from [] (spidev_probe+0x1cc/0x1dc) [ 1.261774] [] (spidev_probe) from [] (spi_drv_probe+0x84/0xb0) [ 1.269545] r8:00000000 r7:c0945da0 r6:c0945d90 r5:00000000 r4:dc430000 [ 1.276361] [] (spi_drv_probe) from [] (driver_probe_device+0x204/0x2f8) [ 1.284857] r7:c0945da0 r6:00000000 r5:dc430000 r4:c0991408 [ 1.290596] [] (driver_probe_device) from [] (__device_attach_driver+0x8c/0xb4) [ 1.299729] r9:00000000 r8:c09913e4 r7:00000001 r6:dc430000 r5:dc057c48 r4:c0945da0 [ 1.307569] [] (__device_attach_driver) from [] (bus_for_each_drv+0x68/0x9c) [ 1.316438] r7:00000001 r6:c03e3764 r5:dc057c48 r4:00000000 [ 1.322184] [] (bus_for_each_drv) from [] (__device_attach+0xb8/0x11c) [ 1.330528] r6:dc430034 r5:dc430000 r4:dc430000 [ 1.335196] [] (__device_attach) from [] (device_initial_probe+0x14/0x18) [ 1.343801] r7:00000000 r6:c0945840 r5:dc430000 r4:dc430008 [ 1.349543] [] (device_initial_probe) from [] (bus_probe_device+0x8c/0x94) [ 1.358228] [] (bus_probe_device) from [] (device_add+0x3f4/0x57c) [ 1.366199] r7:00000000 r6:dc430000 r5:dc3a9c00 r4:dc430008 [ 1.371943] [] (device_add) from [] (spi_add_device+0xa4/0x160) [ 1.379677] r10:dc3a9d72 r9:dc112610 r8:dcb57208 r7:dc112610 r6:dc3a9c00 r5:00000000 [ 1.387580] r4:dc430000 [ 1.390186] [] (spi_add_device) from [] (of_register_spi_device+0x22c/0x2f4) [ 1.399010] r7:dc3a9c00 r6:dcb57550 r5:dc430000 r4:00000000 [ 1.404754] [] (of_register_spi_device) from [] (spi_register_master+0x29c/0x484) [ 1.414057] r7:c085c6f8 r6:00000000 r5:dcb57550 r4:dc3a9c00 [ 1.419803] [] (spi_register_master) from [] (devm_spi_register_master+0x40/0x78) [ 1.429088] r10:dc3a9d72 r9:c085cc60 r8:dc3a9c00 r7:dc112610 r6:dc3a9c00 r5:dc372d90 [ 1.437011] r4:00000000 [ 1.439616] [] (devm_spi_register_master) from [] (omap2_mcspi_probe+0x2d4/0x364) [ 1.448875] r7:dc112610 r6:dc3a9c00 r5:dc3a9eb0 r4:00000000 [ 1.454648] [] (omap2_mcspi_probe) from [] (platform_drv_probe+0x54/0xb8) [ 1.463230] r10:00000000 r9:c08c8600 r8:00000000 r7:fffffdfb r6:c0945df4 r5:dc112610 [ 1.471205] r4:c0991408 [ 1.473763] [] (platform_drv_probe) from [] (driver_probe_device+0x204/0x2f8) [ 1.482694] r7:c0945df4 r6:00000000 r5:dc112610 r4:c0991408 [ 1.488445] [] (driver_probe_device) from [] (__driver_attach+0x94/0x98) [ 1.496938] r9:c08c8600 r8:000000a9 r7:00000000 r6:dc112644 r5:c0945df4 r4:dc112610 [ 1.504812] [] (__driver_attach) from [] (bus_for_each_dev+0x70/0xa4) [ 1.513044] r7:00000000 r6:c03e36cc r5:c0945df4 r4:00000000 [ 1.518795] [] (bus_for_each_dev) from [] (driver_attach+0x24/0x28) [ 1.526854] r6:c093fb20 r5:dc376980 r4:c0945df4 [ 1.531538] [] (driver_attach) from [] (bus_add_driver+0x1a8/0x220) [ 1.539630] [] (bus_add_driver) from [] (driver_register+0x80/0x100) [ 1.547757] r7:dc372980 r6:c090ed20 r5:c08eb9a4 r4:c0945df4 [ 1.553527] [] (driver_register) from [] (__platform_driver_register+0x48/0x50) [ 1.562632] r5:c08eb9a4 r4:c093fb20 [ 1.566248] [] (__platform_driver_register) from [] (omap2_mcspi_driver_init+0x1c/0x20) [ 1.576075] r5:c08eb9a4 r4:c090ed20 [ 1.579709] [] (omap2_mcspi_driver_init) from [] (do_one_initcall+0x98/0x1e4) [ 1.588670] [] (do_one_initcall) from [] (kernel_init_freeable+0x138/0x1cc) [ 1.597428] r10:00000007 r9:c08c8600 r8:000000a9 r7:c08fc830 r6:c0908f7c r5:c09595c0 [ 1.605378] r4:c09595c0 [ 1.607941] [] (kernel_init_freeable) from [] (kernel_init+0x18/0xf4) [ 1.616201] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c06767b4 [ 1.624124] r4:c09595c0 [ 1.626682] [] (kernel_init) from [] (ret_from_fork+0x14/0x3c) [ 1.634332] r5:c06767b4 r4:00000000 [ 1.637972] ---[ end trace ff4fcac48061668a ]--- [ 1.644546] libphy: Fixed MDIO Bus: probed [ 1.651516] mousedev: PS/2 mouse device common for all mice [ 1.657925] i2c /dev entries driver [ 1.662944] cpuidle: enable-method property 'ti,am3352' found operations [ 1.699684] pinctrl-single 44e10800.pinmux: pin 44e1099c.0 already requested by 481a0000.spi; cannot claim for 47810000.mmc [ 1.710966] pinctrl-single 44e10800.pinmux: pin-103 (47810000.mmc) status -22 [ 1.718185] pinctrl-single 44e10800.pinmux: could not request pin 103 (44e1099c.0) from group pinmux_wlan_pins on device pinctrl-single [ 1.730574] omap_hsmmc 47810000.mmc: Error applying setting, reverse things back [ 1.858374] ledtrig-cpu: registered to indicate activity on CPUs [ 1.881168] NET: Registered protocol family 10 [ 1.890010] sit: IPv6 over IPv4 tunneling driver [ 1.895670] NET: Registered protocol family 17 [ 1.909810] Key type dns_resolver registered [ 1.914415] omap_voltage_late_init: Voltage driver support not added [ 1.942270] omap-gpmc 50000000.gpmc: GPMC revision 6.0 [ 1.947463] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000 [ 1.971053] nand: device found, Manufacturer ID: 0x98, Chip ID: 0xda [ 1.977440] nand: Toshiba NAND 256MiB 3,3V 8-bit [ 1.986698] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 128 [ 2.002866] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme [ 2.008324] 10 ofpart partitions found on MTD device 8000000.nand [ 2.029384] Creating 10 MTD partitions on "8000000.nand": [ 2.034835] 0x000000000000-0x000000020000 : "NAND.SPL" [ 2.051055] 0x000000020000-0x000000040000 : "NAND.SPL.backup1" [ 2.068929] 0x000000040000-0x000000060000 : "NAND.SPL.backup2" [ 2.080866] 0x000000060000-0x000000080000 : "NAND.SPL.backup3" [ 2.100872] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os" [ 2.116778] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot" [ 2.124081] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env" [ 2.140879] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1" [ 2.160507] 0x000000200000-0x000000a00000 : "NAND.kernel" [ 2.180467] 0x000000a00000-0x000010000000 : "NAND.file-system" [ 2.399621] tps65910 0-002d: No interrupt support, no core IRQ [ 2.442209] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 2.456504] vmmc: supplied by vbat [ 2.509748] vdd_mpu: supplied by vbat [ 2.514859] ubi0: attaching mtd9 [ 3.872256] mmc1: MAN_BKOPS_EN bit is not set [ 3.891154] mmc1: new high speed MMC card at address 0001 [ 3.909784] mmcblk0: mmc1:0001 004G60 3.69 GiB [ 3.914674] mmcblk0boot0: mmc1:0001 004G60 partition 1 2.00 MiB [ 3.925822] mmcblk0boot1: mmc1:0001 004G60 partition 2 2.00 MiB [ 4.188580] ubi0: scanning is finished [ 4.202673] ubi0: attached mtd9 (name "NAND.file-system", size 246 MiB) [ 4.209339] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes [ 4.216377] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512 [ 4.223137] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096 [ 4.230147] ubi0: good PEBs: 1965, bad PEBs: 3, corrupted PEBs: 0 [ 4.236297] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128 [ 4.243573] ubi0: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 71294218 [ 4.252617] ubi0: available PEBs: 0, total reserved PEBs: 1965, PEBs reserved for bad PEB handling: 37 [ 4.261996] ubi0: background thread "ubi_bgt0d" started, PID 66 [ 4.269101] input: volume_keys@0 as /devices/platform/volume_keys@0/input/input0 [ 4.277337] hctosys: unable to open rtc device (rtc0) [ 4.286962] lis3_reg: disabling [ 4.290252] wlan-en-regulator: disabling [ 4.294642] ALSA device list: [ 4.297706] No soundcards found. [ 4.309506] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 67 [ 4.340782] UBIFS (ubi0:0): recovery needed [ 4.409476] UBIFS (ubi0:0): recovery completed [ 4.414146] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs" [ 4.421619] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 4.431690] UBIFS (ubi0:0): FS size: 242905088 bytes (231 MiB, 1913 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs) [ 4.442490] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB) [ 4.448360] UBIFS (ubi0:0): media format: w4/r0 (latest is w4/r0), UUID E729169E-45DF-4695-84C1-89D864A4AF44, small LPT model [ 4.461311] VFS: Mounted root (ubifs filesystem) on device 0:15. [ 4.468885] devtmpfs: mounted [ 4.472443] Freeing unused kernel memory: 264K (c08c8000 - c090a000) [ 4.478874] This architecture does not have kernel memory protection. [ 4.689602] systemd[1]: System time before build time, advancing clock. [ 4.746844] random: systemd: uninitialized urandom read (16 bytes read, 28 bits of entropy available) [ 4.779696] random: systemd: uninitialized urandom read (16 bytes read, 29 bits of entropy available) [ 4.803089] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN) [ 4.822961] systemd[1]: Detected architecture arm. Welcome to Arago 2016.10! [ 4.852182] systemd[1]: Set hostname to . [ 5.051521] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 29 bits of entropy available) [ 5.084561] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 29 bits of entropy available) [ 5.146025] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available) [ 5.207310] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available) [ 5.217378] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available) [ 5.228087] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available) [ 5.296276] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available) [ 5.332278] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available) [ 5.617595] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 5.651373] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 5.680153] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 5.709870] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 5.740135] systemd[1]: Listening on Syslog Socket. [ OK ] Listening on Syslog Socket. [ 5.770172] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 5.827845] systemd[1]: Created slice System Slice. [ OK ] Created slice System Slice. [ 5.856652] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 5.896989] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 5.956517] systemd[1]: Mounting Temporary Directory... Mounting Temporary Directory... [ 6.007869] systemd[1]: Starting Setup Virtual Console... Starting Setup Virtual Console... [ 6.082787] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 6.110432] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password Requests to Console Directory Watch. [ 6.144977] systemd[1]: Mounting Debug File System... Mounting Debug File System... [ 6.180422] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe. [ OK ] Listening on /dev/initctl Compatibility Named Pipe. [ 6.220960] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 6.255258] systemd[1]: Starting Journal Service... Starting Journal Service... [ 6.295691] systemd[1]: Starting Create Static Device Nodes in /dev... Starting Create Static Device Nodes in /dev... [ 6.360467] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password Requests to Wall Directory Watch. [ 6.389997] systemd[1]: Reached target Paths. [ OK ] Reached target Paths. [ 6.415136] systemd[1]: Starting Apply Kernel Variables... Starting Apply Kernel Variables... [ 6.449964] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 6.495386] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 6.591763] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 6.620096] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 6.727395] systemd[1]: Mounted Debug File System. [ OK ] Mounted Debug File System. [ 6.760256] systemd[1]: Mounted POSIX Message Queue File System. [ OK ] Mounted POSIX Message Queue File System. [ 6.780204] systemd[1]: Mounted Temporary Directory. [ OK ] Mounted Temporary Directory. [ 6.813677] systemd[1]: Started Setup Virtual Console. [ OK ] Started Setup Virtual Console. [ 6.852946] systemd[1]: Started Create Static Device Nodes in /dev. [ OK ] Started Create Static Device Nodes in /dev. [ 6.892399] systemd[1]: Started Apply Kernel Variables. [ OK ] Started Apply Kernel Variables. [ 6.912520] systemd[1]: Started Remount Root and Kernel File Systems. [ OK ] Started Remount Root and Kernel File Systems. [ 6.940953] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. Starting Flush Journal to Persistent Storage... Starting udev Coldplug all Devices... [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /var/volatile. [ OK ] Mounted /media/ram. [ OK ] Started udev Kernel Device Manager. [ 9.352377] systemd-journald[97]: Received request to flush runtime journal from PID 1 [ OK ] Started Flush Journal to Persistent Storage. Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started Load/Save Random Seed. [ OK ] Started Create Volatile Files and Directories. [ OK ] Found device /dev/ttyS0. [ OK ] Created slice system-systemd\x2dbacklight.slice. Starting Load/Save Screen Backlight...htness of backlight:backlight... Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started udev Coldplug all Devices. [ OK ] Started Load/Save Screen Backlight Brightness of backlight:backlight. [ OK ] Started Network Time Synchronization. [ 14.658291] EXT4-fs (mmcblk0): mounting ext3 file system using the ext4 subsystem [ 14.783525] EXT4-fs (mmcblk0): recovery complete [ 14.788215] EXT4-fs (mmcblk0): mounted filesystem with ordered data mode. Opts: (null) [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Found device /dev/ttyS3. [ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch. [ OK ] Reached target System Time Synchronized. Starting Synchronize System and HW clocks... [FAILED] Failed to start Synchronize System and HW clocks. See 'systemctl status sync-clocks.service' for details. [ OK ] Reached target System Initialization. [ OK ] Listening on RPCbind Server Activation Socket. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on D-Bus System Message Bus Socket. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started D-Bus System Message Bus. Starting Network Service... Starting telnetd.service... [ OK ] Started System Logging Service. Starting Login Service... Starting Print notice about GPLv3 packages... Starting Permit User Sessions... [ OK ] Started Kernel Logging Service. [ OK ] Started telnetd.service. [ OK ] Started Permit User Sessions. [ OK ] Started Network Service. [ OK ] Reached target Network. Starting Network Name Resolution... [ OK ] Started Serial Getty on ttyS0. [ OK ] Started Getty on tty1. [ OK ] Started Serial Getty on ttyS3. Starting thttpd.service... [ OK ] Started Login Service. [ OK ] Started thttpd.service. [ OK ] Started Network Name Resolution. Starting rng-tools.service... [ OK ] Started rng-tools.service. [ 22.482071] random: nonblocking pool is initialized Starting thermal-zone-init.service... [ OK ] Started thermal-zone-init.service. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: binutils dosfstools m4 If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove Where is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ OK ] Started Print notice about GPLv3 packages. _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___|