// SPDX-License-Identifier: GPL-2.0+ /* * Copyright (C) 2011 OMICRON electronics GmbH * * based on drivers/mtd/nand/raw/nand_spl_load.c * * Copyright (C) 2011 * Heiko Schocher, DENX Software Engineering, hs@denx.de. */ #include #include #include #include #include #include #include DECLARE_GLOBAL_DATA_PTR; #ifdef CONFIG_SPL_OS_BOOT /* * Load the kernel, check for a valid header we can parse, and if found load * the kernel and then device tree. */ static int spi_load_image_os(struct spl_image_info *spl_image, struct spi_flash *flash, struct image_header *header) { int err; /* Read for a header, parse or error out. */ spi_flash_read(flash, CONFIG_SYS_SPI_KERNEL_OFFS, sizeof(*header), (void *)header); if (image_get_magic(header) != IH_MAGIC) return -1; err = spl_parse_image_header(spl_image, header); if (err) return err; spi_flash_read(flash, CONFIG_SYS_SPI_KERNEL_OFFS, spl_image->size, (void *)spl_image->load_addr); /* Read device tree. */ spi_flash_read(flash, CONFIG_SYS_SPI_ARGS_OFFS, CONFIG_SYS_SPI_ARGS_SIZE, (void *)CONFIG_SYS_SPL_ARGS_ADDR); return 0; } #endif static ulong spl_spi_fit_read(struct spl_load_info *load, ulong sector, ulong count, void *buf) { struct spi_flash *flash = load->dev; ulong ret; ret = spi_flash_read(flash, sector, count, buf); if (!ret) return count; else return 0; } unsigned int __weak spl_spi_get_uboot_offs(struct spi_flash *flash) { return CONFIG_SYS_SPI_U_BOOT_OFFS; } u32 __weak spl_spi_boot_bus(void) { return CONFIG_SF_DEFAULT_BUS; } u32 __weak spl_spi_boot_cs(void) { return CONFIG_SF_DEFAULT_CS; } /* * The main entry for SPI booting. It's necessary that SDRAM is already * configured and available since this code loads the main U-Boot image * from SPI into SDRAM and starts it from there. */ static int spl_spi_load_image(struct spl_image_info *spl_image, struct spl_boot_device *bootdev) { int err = 0; unsigned int payload_offs; struct spi_flash *flash; struct image_header *header; unsigned int sf_bus = spl_spi_boot_bus(); unsigned int sf_cs = spl_spi_boot_cs(); /* * Load U-Boot image from SPI flash into RAM * In DM mode: defaults speed and mode will be * taken from DT when available */ flash = spi_flash_probe(sf_bus, sf_cs, CONFIG_SF_DEFAULT_SPEED, CONFIG_SF_DEFAULT_MODE); if (!flash) { puts("SPI probe failed.\n"); return -ENODEV; } payload_offs = spl_spi_get_uboot_offs(flash); header = spl_get_load_buffer(-sizeof(*header), sizeof(*header)); #if CONFIG_IS_ENABLED(OF_CONTROL) && !CONFIG_IS_ENABLED(OF_PLATDATA) payload_offs = fdtdec_get_config_int(gd->fdt_blob, "u-boot,spl-payload-offset", payload_offs); #endif printf("[%s: %d] ******** payload_offs = %u\n", __func__, __LINE__, payload_offs); #ifdef CONFIG_SPL_OS_BOOT if (spl_start_uboot() || spi_load_image_os(spl_image, flash, header)) #endif { /* Load u-boot, mkimage header is 64 bytes. */ err = spi_flash_read(flash, payload_offs, sizeof(*header), (void *)header); printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); if (err) { printf("%s: Failed to read from SPI flash (err=%d)\n", __func__, err); return err; } printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); if (IS_ENABLED(CONFIG_SPL_LOAD_FIT_FULL) && image_get_magic(header) == FDT_MAGIC) { err = spi_flash_read(flash, payload_offs, roundup(fdt_totalsize(header), 4), (void *)CONFIG_SYS_LOAD_ADDR); printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); if (err) return err; printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); err = spl_parse_image_header(spl_image, (struct image_header *)CONFIG_SYS_LOAD_ADDR); } else if (IS_ENABLED(CONFIG_SPL_LOAD_FIT) && image_get_magic(header) == FDT_MAGIC) { struct spl_load_info load; printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); printf("Found FIT\n"); load.dev = flash; load.priv = NULL; load.filename = NULL; load.bl_len = 1; load.read = spl_spi_fit_read; err = spl_load_simple_fit(spl_image, &load, payload_offs, header); } else if (IS_ENABLED(CONFIG_SPL_LOAD_IMX_CONTAINER)) { struct spl_load_info load; printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); load.dev = flash; load.priv = NULL; load.filename = NULL; load.bl_len = 1; load.read = spl_spi_fit_read; err = spl_load_imx_container(spl_image, &load, payload_offs); } else { printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); err = spl_parse_image_header(spl_image, header); printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); if (err) return err; printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); err = spi_flash_read(flash, payload_offs, spl_image->size, (void *)spl_image->load_addr); } printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); if (IS_ENABLED(CONFIG_SPI_FLASH_SOFT_RESET)) { printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); err = spi_nor_remove(flash); if (err) return err; printf("[%s: %d] ******** err = %u\n", __func__, __LINE__, err); } } return err; } /* Use priorty 1 so that boards can override this */ SPL_LOAD_IMAGE_METHOD("SPI", 1, BOOT_DEVICE_SPI, spl_spi_load_image);