[C66xx_0] ******************************** *********** CONSUMER *********** ******************************** WARNING: Please ensure that the CONSUMER is executing before running the PRODUCER!! Debug: Waiting for module reset... Debug: Waiting for module local reset... Debug: Waiting for SRIO ports to be operational... Debug: SRIO port 0 is NOT operational. Debug: Lanes status shows lanes formed as one 4x port Debug: AppConfig Tx Queue: 0x2a0 Flow Id: 0 Debug: SRIO Driver Instance 0x@00849120 has been created Debug: Running test in polled mode. Debug: SRIO Driver handle 0x849120. [C66xx_1] ******************************** *********** PRODUCER *********** ******************************** WARNING: Please ensure that the CONSUMER is executing before running the PRODUCER!! Debug: Waiting for module reset... Debug: Waiting for module local reset... Debug: Waiting for SRIO ports to be operational... Debug: SRIO port 0 is operational. Debug: Lanes status shows lanes formed as one 4x port Debug: AppConfig Tx Queue: 0x2a0 Flow Id: 0 Debug: SRIO Driver Instance 0x@00849030 has been created Debug: Running test in polled mode. Debug: SRIO Driver handle 0x849030. Latency: (Type-11, 1.250GBaud, 4X, tab delimited) Core Lanes Speed Conn MsgType PktSize NumPkts MnLCycs AgLCycs MxLCycs 1 4 1.250 B-E-B Type-11 16 100 772 16564490 1656368589 1 4 1.250 B-E-B Type-11 32 100 850 850 872 1 4 1.250 B-E-B Type-11 64 100 849 850 872 1 4 1.250 B-E-B Type-11 128 100 933 933 957 1 4 1.250 B-E-B Type-11 256 100 1096 1098 1119 1 4 1.250 B-E-B Type-11 512 100 1180 1180 1202 1 4 1.250 B-E-B Type-11 1024 100 1510 1510 1532 [C66xx_0] Throughput: (RX side, Type-11, 1.250GBaud, 4X, tab delimited) [C66xx_1] Throughput: (TX side, Type-11, 1.250GBaud, 4X, tab delimited) [C66xx_0] Core Lanes Speed Conn MsgType OHBytes PktSize Pacing Thruput PktsSec. NumPkts PktLoss AgPCycs AgLCycs AgICycs AgOCycs Seconds 0 4 1.250 B-E-B Type-11 24 16 0 28.26 220750.55 1200000 No 4530 590 3826 114 5.44 0 4 1.250 B-E-B Type-11 24 16 0 26.29 205423.17 1200000 No 4868 590 4164 114 5.84 0 4 1.250 B-E-B Type-11 24 16 0 25.56 199720.39 1000000 No 5007 590 4303 114 5.01 0 4 1.250 B-E-B Type-11 24 16 0 25.56 199720.39 1000000 No 5007 590 4303 114 5.01 0 4 1.250 B-E-B Type-11 24 16 0 25.56 199720.39 1000000 No 5007 590 4303 114 5.01 Error: RX_1210 Unable to get descriptor for sending the control message Error: RX_1338 Unable to get descriptor for sending the control message RX_1338 Error: CTRL_READY control failed to be sent. Error: RX_1152 Unable to get descriptor for sending the control message [C66xx_1] Error: Transmit is unable to send packets. Packet count: 1189265 Debug: SRIO status: 0x41800080. Debug: RX CPPI Security Violation Debug: Unsolicited Response Debug: Packet Response Time-out Debug: Message error response Debug: Port response timeout: 0xff0fff Debug: SRIO is an Agent or Slave device. Debug: SRIO processing element can issue requests. Debug: SRIO device has not been previously discovered. Debug: Various Register Display: 32211100 17395173 |||||||| 22211000 84062840 -------- PCR: 0x02900004:0x00000005 PER_SET_CNTL: 0x02900014:0x01053800 PER_SET_CNTL1: 0x02900018:0x00000000 ERR_RST_EVNT_ICSR: 0x029001e0:0x00000000 LSUx_Reg6: 0x02900d18:0x00000010 LSU_STAT_REG0: 0x02900de8:0x00000000 SP_RT_CTL: 0x0290b124:0xff0fff00 SP_GEN_CTL: 0x0290b13c:0x40000000 Port n Control 2 CSR: 0x0290b154:0x02aa0000 SPn_ERR_STAT: 0x0290b158:0x00020002 SPn_CTL: 0x0290b15c:0xd0600001 SPx_ERR_DET: 0x0290c040:0x00000001 SPx_ERR_RATE: 0x0290c068:0x80000000 LANEn_STAT0: 0x0290e010:0x00007008 LANEn_STAT1: 0x0290e014:0x00000000 PLM Port(n)Implement: 0x0291b080:0x00000000 PLM_SP(n)_Status: 0x0291b090:0x00000000 EM_PW_PORT_STAT: 0x0291b928:0x00000000 [C66xx_0] ******************************** *********** CONSUMER *********** ******************************** WARNING: Please ensure that the CONSUMER is executing before running the PRODUCER!! Debug: Waiting for module reset... Debug: Waiting for module local reset... Debug: Waiting for SRIO ports to be operational... Debug: SRIO port 0 is NOT operational. Debug: SRIO port 1 is NOT operational. Debug: SRIO port 2 is NOT operational. Debug: SRIO port 3 is NOT operational. Debug: Lanes status shows lanes formed as four 1x ports Debug: AppConfig Tx Queue: 0x2a0 Flow Id: 0 Debug: SRIO Driver Instance 0x@00849120 has been created Debug: Running test in polled mode. Debug: SRIO Driver handle 0x849120. [C66xx_1] ******************************** *********** PRODUCER *********** ******************************** WARNING: Please ensure that the CONSUMER is executing before running the PRODUCER!! Debug: Waiting for module reset... Debug: Waiting for module local reset... Debug: Waiting for SRIO ports to be operational... Debug: SRIO port 0 is operational. Debug: SRIO port 1 is operational. Debug: SRIO port 2 is operational. Debug: SRIO port 3 is operational. Debug: Lanes status shows lanes formed as four 1x ports Debug: AppConfig Tx Queue: 0x2a0 Flow Id: 0 Debug: SRIO Driver Instance 0x@00849030 has been created Debug: Running test in polled mode. Debug: SRIO Driver handle 0x849030. Latency: (DIO_NW, 5.000GBaud, 1X, tab delimited) Core Lanes Speed Conn MsgType PktSize NumPkts MnLCycs AgLCycs MxLCycs 1 1 5.000 B-E-B DIO_NW 4 100 290 290 324 1 1 5.000 B-E-B DIO_NW 8 100 290 290 305 1 1 5.000 B-E-B DIO_NW 16 100 295 295 310 1 1 5.000 B-E-B DIO_NW 32 100 308 308 323 1 1 5.000 B-E-B DIO_NW 64 100 326 326 341 1 1 5.000 B-E-B DIO_NW 128 100 362 362 382 1 1 5.000 B-E-B DIO_NW 256 100 434 434 436 1 1 5.000 B-E-B DIO_NW 512 100 542 542 562 1 1 5.000 B-E-B DIO_NW 1024 100 758 771 778 [C66xx_0] Throughput: (RX side, DIO_NW, 5.000GBaud, 1X, tab delimited) [C66xx_1] Throughput: (TX side, DIO_NW, 5.000GBaud, 1X, tab delimited) [C66xx_0] Core Lanes Speed Conn MsgType OHBytes PktSize Pacing Thruput PktsSec. NumPkts PktLoss AgPCycs AgLCycs AgICycs AgOCycs Seconds 0 1 5.000 B-E-B DIO_NW 16 4 0 8.40 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] Core Lanes Speed Conn MsgType OHBytes PktSize Pacing Thruput PktsSec. NumPkts PktLoss AgPCycs AgLCycs AgICycs AgOCycs Seconds 1 1 5.000 B-E-B DIO_NW 16 4 0 83.99 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 8 0 16.80 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 8 0 167.98 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 16 0 33.60 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 16 0 335.96 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 32 0 67.21 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 32 0 671.92 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 64 0 134.42 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 64 0 1343.83 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 128 0 268.84 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 128 0 2687.66 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 256 0 537.67 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 256 0 5375.33 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 512 0 1075.35 262536.09 1400000 No 3809 21 3788 0 5.33 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 512 0 10750.66 2624672.00 12600000 No 381 325 41 15 4.80 [C66xx_0] 0 1 5.000 B-E-B DIO_NW 16 1024 0 1587.90 193836.02 1000000 No 5159 21 5138 0 5.16 [C66xx_1] 1 1 5.000 B-E-B DIO_NW 16 1024 102 15875.97 1937984.50 9200000 No 516 324 177 15 4.75 Latency: (DIO_NR, 5.000GBaud, 1X, tab delimited) Core Lanes Speed Conn MsgType PktSize NumPkts MnLCycs AgLCycs MxLCycs 1 1 5.000 B-E-B DIO_NR 4 100 509 509 532 1 1 5.000 B-E-B DIO_NR 8 100 509 509 532 1 1 5.000 B-E-B DIO_NR 16 100 509 509 532 1 1 5.000 B-E-B DIO_NR 32 100 508 509 545 1 1 5.000 B-E-B DIO_NR 64 100 508 512 555 1 1 5.000 B-E-B DIO_NR 128 100 508 550 587 1 1 5.000 B-E-B DIO_NR 256 100 508 614 656 1 1 5.000 B-E-B DIO_NR 512 100 508 719 763