root@arm:/home/ubuntu# cat /usr/bin/startx #!/bin/sh # # This is just a sample implementation of a slightly less primitive # interface than xinit. It looks for user .xinitrc and .xserverrc # files, then system xinitrc and xserverrc files, else lets xinit choose # its default. The system xinitrc should probably do things like check # for .Xresources files and merge them in, start up a window manager, # and pop a clock and several xterms. # # Site administrators are STRONGLY urged to write nicer versions. # unset DBUS_SESSION_BUS_ADDRESS unset SESSION_MANAGER userclientrc=$HOME/.xinitrc sysclientrc=/etc/X11/xinit/xinitrc userserverrc=$HOME/.xserverrc sysserverrc=/etc/X11/xinit/xserverrc defaultclient=/usr/bin/xterm defaultserver=/usr/bin/X defaultclientargs="" defaultserverargs="" defaultdisplay=":0" clientargs="" serverargs="" vtarg="" enable_xauth=1 # Automatically determine an unused $DISPLAY d=0 while true ; do [ -e "/tmp/.X$d-lock" -o -S "/tmp/.X11-unix/X$d" ] || break d=$(($d + 1)) done defaultdisplay=":$d" unset d whoseargs="client" while [ x"$1" != x ]; do case "$1" in # '' required to prevent cpp from treating "/*" as a C comment. /''*|\./''*) if [ "$whoseargs" = "client" ]; then if [ x"$client" = x ] && [ x"$clientargs" = x ]; then client="$1" else clientargs="$clientargs $1" fi else if [ x"$server" = x ] && [ x"$serverargs" = x ]; then server="$1" else serverargs="$serverargs $1" fi fi ;; --) whoseargs="server" ;; *) if [ "$whoseargs" = "client" ]; then clientargs="$clientargs $1" else # display must be the FIRST server argument if [ x"$serverargs" = x ] && \ expr "$1" : ':[0-9][0-9]*$' > /dev/null 2>&1; then display="$1" else serverargs="$serverargs $1" fi fi ;; esac shift done # process client arguments if [ x"$client" = x ]; then client=$defaultclient # For compatibility reasons, only use startxrc if there were no client command line arguments if [ x"$clientargs" = x ]; then if [ -f "$userclientrc" ]; then client=$userclientrc elif [ -f "$sysclientrc" ]; then client=$sysclientrc fi fi fi # if no client arguments, use defaults if [ x"$clientargs" = x ]; then clientargs=$defaultclientargs fi # process server arguments if [ x"$server" = x ]; then server=$defaultserver # When starting the defaultserver start X on the current tty to avoid # the startx session being seen as inactive: # "https://bugzilla.redhat.com/show_bug.cgi?id=806491" tty=$(tty) if expr match "$tty" '^/dev/tty[0-9]\+$' > /dev/null; then tty_num=$(echo "$tty" | grep -oE '[0-9]+$') vtarg="vt$tty_num -keeptty" fi # For compatibility reasons, only use xserverrc if there were no server command line arguments if [ x"$serverargs" = x -a x"$display" = x ]; then if [ -f "$userserverrc" ]; then server=$userserverrc elif [ -f "$sysserverrc" ]; then server=$sysserverrc fi fi fi # if no server arguments, use defaults if [ x"$serverargs" = x ]; then serverargs=$defaultserverargs fi # if no vt is specified add vtarg (which may be empty) have_vtarg="no" for i in $serverargs; do if expr match "$i" '^vt[0-9]\+$' > /dev/null; then have_vtarg="yes" fi done if [ "$have_vtarg" = "no" ]; then serverargs="$serverargs $vtarg" fi # if no display, use default if [ x"$display" = x ]; then display=$defaultdisplay fi if [ x"$enable_xauth" = x1 ] ; then if [ x"$XAUTHORITY" = x ]; then XAUTHORITY=$HOME/.Xauthority export XAUTHORITY fi removelist= # set up default Xauth info for this machine # check for GNU hostname if hostname --version > /dev/null 2>&1; then if [ -z "`hostname --version 2>&1 | grep GNU`" ]; then hostname=`hostname -f` fi fi if [ -z "$hostname" ]; then hostname=`hostname` fi authdisplay=${display:-:0} mcookie=`/usr/bin/mcookie` if test x"$mcookie" = x; then echo "Couldn't create cookie" exit 1 fi dummy=0 # create a file with auth information for the server. ':0' is a dummy. xserverauthfile=`mktemp --tmpdir serverauth.XXXXXXXXXX` trap "rm -f '$xserverauthfile'" HUP INT QUIT ILL TRAP KILL BUS TERM xauth -q -f "$xserverauthfile" << EOF add :$dummy . $mcookie EOF serverargs=${serverargs}" -auth "${xserverauthfile} # now add the same credentials to the client authority file # if '$displayname' already exists do not overwrite it as another # server man need it. Add them to the '$xserverauthfile' instead. for displayname in $authdisplay $hostname$authdisplay; do authcookie=`xauth list "$displayname" \ | sed -n "s/.*$displayname[[:space:]*].*[[:space:]*]//p"` 2>/dev/null; if [ "z${authcookie}" = "z" ] ; then xauth -q << EOF add $displayname . $mcookie EOF removelist="$displayname $removelist" else dummy=$(($dummy+1)); xauth -q -f "$xserverauthfile" << EOF add :$dummy . $authcookie EOF fi done fi xinit "$client" $clientargs -- "$server" $display $serverargs retval=$? if [ x"$enable_xauth" = x1 ] ; then if [ x"$removelist" != x ]; then xauth remove $removelist fi if [ x"$xserverauthfile" != x ]; then rm -f "$xserverauthfile" fi fi if command -v deallocvt > /dev/null 2>&1; then deallocvt fi exit $retval